CC23xx or CC27xx SDK 8.40 to CC23xx or CC27xx SDK 9.10¶
This section will describe how to port a project from CC23xx or CC27xx SDK 8.40 to a CC23xx or CC27xx SDK 9.10 project.
Note
Vulnerability reports and mitigations can be found on Report potential product security vulnerabilities.
Porting Bluetooth LE Projects¶
The recommended method for porting an existing project from CC23xx or CC27xx SDK 8.40
to CC23xx or CC27xx SDK 9.10 is to modify the project using only the Code Composer Studio interface.
The following steps will detail the changes needed when porting an out of the box
example from the SDK such as basic_ble:
Import the project into Code Composer Studio.
2. In order to modify the SDK version, corresponding SysConfig version, as well as the compiler version,
right-click on the imported project folder inside the Project Explorer and select Properties.
3. In General, select Compiler and choose the correct version. Refer to the Dependencies section
in the SDK release notes
![]()
Figure 221. Code Composer Studio - Change Compiler Version.¶
4. Go to Dependencies and double-click on SimpleLink Low Power F3 SDK and choose the correct version.
Then double-click on SysConfig and do the same. Refer to the Dependencies Section in the SDK release notes
for the correct versions.
![]()
Figure 222. Code Composer Studio - Change SDK and SysConfig Version.¶
Go to
Arm Compilerand selectInclude Options. In there, remove the following include paths:All paths that include
ble5stack_flashsource/ti/bleapp/profiles/health_thermometer
source/ti/bleapp/services/health_thermometer
Go to
Advanced Optionsand selectCommand files. In there, remove the two file paths and add:${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/ble/stack_util/config/build_components.opt
${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/ble/stack_util/config/factory_config.opt
7. Exit the Properties menu. Right-click the SysConfig file in the project and select “Open With”, then
select “Text Editor”. Then, inside the SysConfig file, change all instances of ble5stack to ble.
8. Due to a change in the naming conventions, the following changes are needed for each instance of the following paths:
Change from |
Change to |
|---|---|
source/ti/ble5stack_flash |
source/ti/ble |
source/ti/ble5stack_flash/lib_projects |
source/ti/ble/lib |
source/ti/bleapp/services |
source/ti/ble/services |
source/ti/bleapp/profiles |
source/ti/ble/profiles |
source/ti/bleapp |
source/ti/ble/app_util |
tools/ble5stack |
tools/ble |
source/ti/ble/app_util/util/sw_update |
source/ti/ble/app_util/sw_update |
source/ti/bleapp/ble_app_util |
source/ti/ble/app_util/framework |
source/ti/bleapp/ble_app_util/inc |
source/ti/ble/app_util/framework |
source/ti/bleapp/menu_module |
source/ti/ble/app_util/menu |
source/ti/ble5stack/.meta |
source/ti/ble/.meta |
source/ti/ble5stack_flash |
source/t/ble/host |
source/ti/ble5stack_flash/npi |
source/ti/ble/app_util/npi |
source/ti/ble5stack_flash/npi/unified |
source/ti/ble/app_util/unpi |
source/ti/ble5stack_flash/health_toolkit |
source/ti/ble/stack_util |
source/ti/ble5stack_flash/osal |
source/ti/ble/stack_util/osal |
source/ti/ble5stack_flash/icall |
source/ti/ble/stack_util/icall |
source/ti/ble5stack_flash/rom |
source/ti/ble/stack_util/lib_opt |
source/ti/ble5stack_flash/config |
source/ti/ble/stack_util/config |
Go to
common=>Startupand click onocal_icall_ble.cand edit the following:Since the previous include paths were taken out in the properties section of the project, the following include paths will need to be changed:
Table 38. Include path changes in osal_icall_ble.c¶ Change from
Change to
#include “osal_snv.h”
#include “ti/ble/stack_util/osal/osal_snv.h”
#include “osal.h”
#include “ti/ble/stack_util/osal/osal.h”
#include <icall.h>
#include “ti/ble/stack_util/icall/app/icall.h”
#include “hal_types.h” and #include “hal_mcu.h”
#include “ti/ble/stack_util/comdef.h”
#include “osal_tasks.h”
#include “ti/ble/stack_util/osal/osal_tasks.h”
#include “ll.h”
#include “ti/ble/controller/ll/ll.h”
#include “osal_cbtimer.h”
#include “ti/ble/stack_util/osal/osal_cbtimer.h”
#include “l2cap.h”
#include “ti/ble/host/l2cap/l2cap.h”
#include “gap.h”
#include “ti/ble/host/gap/gap.h”
#include “gapbondmgr_internal.h”
#include “ti/ble/host/gapbondmgr/gapbondmgr_internal.h”
#include “gatt.h”
#include “ti/ble/host/gatt/gatt.h”
#include “hci_tl.h”
#include “ti/ble/controller/hci/hci_tl.h”
#include “gattservapp.h”
#include “ti/ble/host/gatt/gattservapp.h”
#include “gapbondmgr.h”
#include “ti/ble/host/gapbondmgr/gapbondmgr.h”
#include “ble_user_config.h”
#include “ti/ble/app_util/config/ble_user_config.h”
#include “ble_dispatch.h”
#include “ti/ble/stack_util/icall/stack/ble_dispatch_lite.h”
Inside pTaskEventHandlerFn:
#ifdef ICALL_LITE ble_dispatch_liteProcess, // task 9 #else bleDispatch_ProcessEvent // task 9 #endif /* ICALL_LITE */ Would become:: ble_dispatch_liteProcess
Inside osalInitTasks:
#ifdef ICALL_LITE ble_dispatch_liteInit(taskID++); #else /* ICall BLE Dispatcher Task */ bleDispatch_Init( taskID ); #endif /* ICALL_LITE */
Would become:
ble_dispatch_liteInit(taskID++);
Inside osalInitTasks, remove:
#ifndef ICALL_LITE /* Enroll the obtained dispatcher entity and OSAL task ID of HCI Ext App * to OSAL so that OSAL can route the dispatcher message into * the appropriate OSAL task. */ osal_enroll_dispatchid(taskID, entity); #endif /* ICALL_LITE */
Inside stack_main:
#ifdef ICALL_JT setBleUserConfig( (icall_userCfg_t *)arg ); #else /* !(ICALL_JT) */ setBleUserConfig( (bleUserCfg_t *)arg ); #endif /* ICALL_JT *
Would become:
setBleUserConfig( (icall_userCfg_t *)arg );
Inside stack_main:
#if defined(ICALL_LITE) && (!defined(STACK_LIBRARY)) { icall_liteTranslationInit((uint32_t*)bleAPItable); } #endif /* ICALL_LITE */ #ifdef ICALL_LITE { osal_set_icall_hook(icall_liteMsgParser); } #endif /* ICALL_LITE */
Would become:
osal_set_icall_hook(icall_liteMsgParser);
Go to main_freertos and edit the following:
Remove the following includes: #include <ti/common/cc26xx/uartlog/UartLog.h> and #include “ble_stack_api.h”
Change the following includes:
Table 39. Include path changes in main_freertos.c¶ Change from
Change to
#include <icall.h>
#include “ti/ble/stack_util/icall/app/icall.h”
#include “hal_assert.h”
#include “ti/ble/stack_util/health_toolkit/assert.h”
#include “bcomdef.h”
#include “ti/ble/stack_util/bcomdef.h”
#include “ble_user_config.h”
#include “ti/ble/app_util/config/ble_user_config.h”
Turn all log_error0 instances into HAL_ASSERT_SPINLOCK.
Delete the following files from the project:
ble_stack_api.c inside of iCallBLE folder
ble_stack_api.h inside of iCallBLE folder
icall_api_lite.c inside of iCallBLE folder
ble_user_config_stack.c inside of Startup folder
Import basic_ble from the CC23xx or CC27xx SDK 9.10 SDK, copy the “lib_opt” folder and paste it in the example you are attempting to migrate.
Some files inside the project will still be unresolved, due to the location change. To fix this:
Copy the path of the file. Each file’s correct path is included in the table below
Right-click on the unresolved file
Select “Edit Linked File”
Replace the current path with the one copied from the table below
Table 40. Linked File Paths¶ File
Path
bleapputil_api.h
${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/ble/app_util/framework/bleapputil_api.h
bleaputil_init.c
${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/ble/app_util/framework/src/bleapputil_init.c
bleapputil_process.c
${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/ble/app_util/framework/src/bleapputil_process.c
bleapputil_stack_callbacks.c
${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/ble/app_util/framework/src/bleapputil_stack_callbacks.c
bleapputil_task.c
${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/ble/app_util/framework/src/bleapputil_task.c
icall_addrs.h
${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/ble/stack_util/icall/app/icall_addrs.h
icall_cc23x0.c
${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/ble/stack_util/icall/app/src/icall_cc23x0.c
icall_platform.h
${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/ble/stack_util/icall/app/icall_platform.h
icall_POSIX.c
${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/ble/stack_util/icall/app/src/icall_POSIX.c
icall_user_config.c
${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/ble/stack_util/icall/app/src/icall_user_config.c
icall_user_config.h
${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/ble/stack_util/icall/app/icall_user_config.h
icall.h
${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/ble/stack_util/icall/app/icall.h
ble_user_config.c
${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/ble/app_util/config/src/ble_user_config.c
ble_user_config.h
${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/ble/app_util/config/ble_user_config.h
icall_ble_apimsg.h
${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/ble/stack_util/icall/app/icall_ble_apimsg.h
menu_module.c
${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/ble/app_util/menu/src/menu_module.c
menu_module.h
${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/ble/app_util/menu/menu_module.h
simple_gatt_profile.c
${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/ble/app_util/menu/src/menu_module.c
simple_gatt_profile.h
${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/ble/profiles/simple_gatt/simple_gatt_profile.h
dev_info_service.c
${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/ble/services/dev_info/src/dev_info_service.c
dev_info_service.h
${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/ble/services/dev_info/dev_info_service.h
rom_init.c
${COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR}/source/ti/ble/stack_util/lib_opt/rom_init.c
Note
These edits pertain to the basic_ble project. Other projects may require similar edits to other files as well!
Legacy Porting¶
Warning
The following section covers a legacy porting method. Current SDK porting does not require this process and should instead see Porting Bluetooth LE Projects.
For this guide, a peripheral project from CC23xx or CC27xx SDK 8.40 will be ported over to CC23xx or CC27xx SDK 9.10. The recommended approach is to start with the Basic BLE project on CC23xx or CC27xx SDK 9.10 and modify the base configuration to match the peripheral configuration used in the CC23xx or CC27xx SDK 8.40 project. Afterwards, the custom application code should be transferred to the new project.
Import a CC23xx or CC27xx SDK 9.10 Basic BLE project.
Change the default Basic BLE project configuration options in the BLE Module present in SysConfig to match the configuration used in the CC23xx or CC27xx SDK 8.40 project.
Transfer all custom application logic from the CC23xx or CC27xx SDK 8.40 into the CC23xx or CC27xx SDK 9.10 Basic BLE project.
Move any profiles and services that the application is using to the CC23xx or CC27xx SDK 9.10 project.
Transfer the SysConfig settings either visually through the GUI or open both the old and the new project
.syscfgfiles and copy-paste the desired settings.If necessary, update the project to use the newer TI drivers that are supplied with the SimpleLink Low Power F3 SDK. Additional details are provided in A Few Noteworthy Changes from CC23xx or CC27xx SDK 8.40 to CC23xx or CC27xx SDK 9.10.
Refer to the Core SDK release notes for additional information and the FreeRTOS examples included with SimpleLink Low Power F3 SDK. The Core SDK release notes may be found in
{SDK_INSTALL_DIR}/docs/simplelink_mcu_sdk/release_notes_coresdk_lpf3_x_xx_xx_xx.htmlFor additional information on how CC23xx or CC27xx SDK 9.10 uses FreeRTOS see FreeRTOS (RTOS Kernel) Overview.
For any utilized TI Drivers, review TI Drivers API Reference.
A Few Noteworthy Changes from CC23xx or CC27xx SDK 8.40 to CC23xx or CC27xx SDK 9.10¶
You can follow the guide above without addressing these updates; they are listed for your information only. All fine grained details might not be mentioned. However, please keep in mind that the file name changes need to be addressed regardless of the project being migrated.
Also, due to the crypto drivers being removed from the drivers library and moved into a seperate secure drivers library, the lib folder will need to be added (source/ti/drivers/secure/lib). Please refer to the specific example you need to port and do a compare between the old and new project files.
Please refer to the BLE5-Stack Release Notes for all the details.