Device Version and Compatibility Testing¶
This procedure is to be used for verifying a part for software compatibility
and version identification. The procedure can be used both externally by
reading through SWD or by on-board software by reading memory mapped
locations. The physical addressing of the data location depends on which of
these methods are chosen but yields the same data. When DEVICEID
is read use
SYS0:DEVICEID
when running on-board software or CFGAP:DEVICEID
over SWD.
When PARTID
is read, use SYS0:PARTID
when running on-board software or
CFGAP:PARTID
over SWD.
All fields shall be parsed as unsigned binary coded integers.
To use SWD please refer to the CC23xx or CC27xx techincal reference manual.
Reading SYS0
Register CCS¶
Code Composer Studio provides an interface to read registers from CC23xx or CC27xx.
Start a debug session with the CC23xx or CC27xx.
Click on
View
→Registers
.
Reading SYS0
Register HWREG()
Macro¶
HWREG()
may be used to read internal registers using their base
addresses. Base addresses for various registers may be found in the CC23xx or CC27xx
technical reference manual. If using this macro, please be aware of any
limitations to the address accessed i.e. if it supports word and/or byte access.
1// Read example
2my32BitVar = HWREG(base_addr + offset) ;
3
4// Write example
5HWREG(base_addr + offset) = my32BitVar ;
The base address for the SYS0
register is 0x40004000
. The offset for
DEVICEID
is 0x3FC
and PARTID
is 0x7F8
. Please see the CC23xx or CC27xx
technical reference manual for more information.
Process¶
First, establish that the device is a CC23xx or CC27xx family device by reading the manufacturer identifier. If running on-board software, this is assumed to be given. If this does not match, this document does not apply to the device.
Read DEVICEID.DEVICE
, DEVICEID.MANUFACTURER
and DEVICEID.ALWAYSONE
and verify this value is identical to the expected value. Ignore
DEVICEID.VERSION
as this value can change without changing compatibility.
If it does not match, stop.
If DEVICEID
matches then check PARTID
as follows:
- Check that
PARTID.PART
is exactly the expected value. If this is different the part is a different device in the same family and code must be checked and potentially re-verified.
- Check that
- Check that
PARTID.VARIANT
is exactly as expected. If this is different this is a memory or package variant of the same device and code must be checked for compatibility with this variant.
- Check that
- Check that
PARTID.MAJORREV
is exactly as expected. If this value is less than expected the device is older and may have reduced functionality. If it is higher it may have changes that break existing software compatibility and errata information should be checked and software should be re-verified for the new revision.
- Check that
- Check that
PARTID.MINORREV
is greater than or equal to the expected value. No action is needed as any changes on the device is assured from the manufacturer to be compatible. If it is less than the expected value there may be added workarounds or features missing that may cause compatibility issues so errata notes and version update notes should be checked and software should be re-verified.
- Check that