40 #ifndef ti_drivers_I2CSupport__include 41 #define ti_drivers_I2CSupport__include int_fast16_t I2CSupport_primeTransfer(I2C_Handle handle, I2C_Transaction *transaction)
Function to initialize transfers.
void I2CSupport_controllerFinish(I2C_HWAttrs const *hwAttrs)
Function to send a finish command to the controller module.
void I2CSupport_powerSetConstraint(void)
Function to set power constraint.
I2C driver's custom configuration structure.
Definition: I2C.h:714
Defines a transaction to be used with I2C_transfer() or I2C_transferTimeout()
Definition: I2C.h:416
void I2CSupport_powerRelConstraint(void)
Function to release power constraint.
Inter-Integrated Circuit (I2C) Controller Driver.