ECDSA.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2017-2024, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
443 #ifndef ti_drivers_ECDSA__include
444 #define ti_drivers_ECDSA__include
445 
446 #include <stdbool.h>
447 #include <stddef.h>
448 #include <stdint.h>
449 
452 
453 #ifdef __cplusplus
454 extern "C" {
455 #endif
456 
469 #define ECDSA_STATUS_RESERVED (-32)
470 
477 #define ECDSA_STATUS_SUCCESS (0)
478 
485 #define ECDSA_STATUS_ERROR (-1)
486 
496 #define ECDSA_STATUS_RESOURCE_UNAVAILABLE (-2)
497 
504 #define ECDSA_STATUS_R_LARGER_THAN_ORDER (-3)
505 
512 #define ECDSA_STATUS_S_LARGER_THAN_ORDER (-4)
513 
520 #define ECDSA_STATUS_PUBLIC_KEY_NOT_ON_CURVE (-5)
521 
529 #define ECDSA_STATUS_PUBLIC_KEY_LARGER_THAN_PRIME (-6)
530 
536 #define ECDSA_STATUS_POINT_AT_INFINITY (-7)
537 
541 #define ECDSA_STATUS_CANCELED (-8)
542 
551 #define ECDSA_STATUS_INVALID_KEY_SIZE (-10)
552 
559 #define ECDSA_STATUS_KEYSTORE_ERROR (-11)
560 
561 #if (DeviceFamily_PARENT == DeviceFamily_PARENT_CC27XX)
562 
566  #define ECDSA_STATUS_NO_VALID_CURVE_TYPE_PROVIDED (-12)
567 
571  #define ECDSA_STATUS_INVALID_KEY_ENCODING (-13)
572 
576  #define ECDSA_STATUS_HARDWARE_ERROR (-14)
577 
578 #endif
579 
591 typedef struct
592 {
594  void *object;
595 
597  void const *hwAttrs;
598 } ECDSA_Config;
599 
604 
627 typedef enum
628 {
644 
645 #if (DeviceFamily_PARENT == DeviceFamily_PARENT_CC27XX)
646 
649 typedef enum
650 {
659 
663 typedef enum
664 {
672 
676 typedef enum
677 {
683 #endif
684 
688 typedef struct
689 {
690 #if (DeviceFamily_PARENT == DeviceFamily_PARENT_CC27XX)
692 #endif
697  const uint8_t *hash;
701  uint8_t *r;
707  uint8_t *s;
713 
717 typedef struct
718 {
719 #if (DeviceFamily_PARENT == DeviceFamily_PARENT_CC27XX)
721 #else
722  const ECCParams_CurveParams *curve;
723 #endif
727  const uint8_t *hash;
731  const uint8_t *r;
737  const uint8_t *s;
744 
748 typedef union
749 {
753 
757 typedef enum
758 {
762 
782 typedef void (*ECDSA_CallbackFxn)(ECDSA_Handle handle,
783  int_fast16_t returnStatus,
784  ECDSA_Operation operation,
785  ECDSA_OperationType operationType);
786 
795 typedef struct
796 {
801  uint32_t timeout;
804  void *custom;
807 } ECDSA_Params;
808 
814 extern const ECDSA_Params ECDSA_defaultParams;
815 
824 void ECDSA_init(void);
825 
835 void ECDSA_close(ECDSA_Handle handle);
836 
854 ECDSA_Handle ECDSA_open(uint_least8_t index, const ECDSA_Params *params);
855 
869 
879 
889 
918 int_fast16_t ECDSA_sign(ECDSA_Handle handle, ECDSA_OperationSign *operation);
919 
947 int_fast16_t ECDSA_verify(ECDSA_Handle handle, ECDSA_OperationVerify *operation);
948 
962 int_fast16_t ECDSA_cancelOperation(ECDSA_Handle handle);
963 
988 ECDSA_Handle ECDSA_construct(ECDSA_Config *config, const ECDSA_Params *params);
989 
990 #ifdef __cplusplus
991 }
992 #endif
993 
994 #endif /* ti_drivers_ECDSA__include */
Definition: ECDSA.h:652
ECDSA_CurveType
Enum for the curve types supported by the driver.
Definition: ECDSA.h:649
ECDSA_ReturnBehavior
The way in which ECDSA function calls return after performing an encryption + authentication or decry...
Definition: ECDSA.h:627
Definition: ECDSA.h:655
ADC_Params params
Definition: Driver_Init.h:11
uint8_t * s
Definition: ECDSA.h:707
The CryptoKey type is an opaque representation of a cryptographic key.
const CryptoKey * myPrivateKey
Definition: ECDSA.h:694
ECDSA_CurveType curveType
Definition: ECDSA.h:720
Definition: ECDSA.h:760
const uint8_t * hash
Definition: ECDSA.h:697
Definition: ECDSA.h:654
void ECDSA_OperationSign_init(ECDSA_OperationSign *operation)
Function to initialize an ECDSA_OperationSign struct to its defaults.
Definition: ECDSA.h:653
void const * hwAttrs
Definition: ECDSA.h:597
const CryptoKey * theirPublicKey
Definition: ECDSA.h:724
void(* ECDSA_CallbackFxn)(ECDSA_Handle handle, int_fast16_t returnStatus, ECDSA_Operation operation, ECDSA_OperationType operationType)
The definition of a callback function used by the ECDSA driver when used in ECDSA_RETURN_BEHAVIOR_CAL...
Definition: ECDSA.h:782
Definition: ECDSA.h:668
Definition: ECDSA.h:651
ECDSA_ReturnBehavior returnBehavior
Definition: ECDSA.h:797
const uint8_t * s
Definition: ECDSA.h:737
Definition: ECDSA.h:656
Definition: ECDSA.h:680
CryptoKey datastructure.
Definition: CryptoKey.h:208
ECDSA_DigestLength
Enum for the hash digest lengths in bits supported by the driver.
Definition: ECDSA.h:676
ECDSA Global configuration.
Definition: ECDSA.h:591
Definition: ECDSA.h:670
void ECDSA_close(ECDSA_Handle handle)
Function to close an ECDSA peripheral specified by the ECDSA handle.
void ECDSA_init(void)
This function initializes the ECDSA module.
Struct containing the parameters required for signing a message.
Definition: ECDSA.h:688
const ECDSA_Params ECDSA_defaultParams
Default ECDSA_Params structure.
Definition: ECDSA.h:666
Definition: ECDSA.h:679
ECDSA Parameters.
Definition: ECDSA.h:795
ECDSA_CurveLength
Enum for signature sizes in bits supported by the driver.
Definition: ECDSA.h:663
const ECCParams_CurveParams * curve
Definition: ECDSA.h:693
ECDSA_OperationType
Enum for the operation types supported by the driver.
Definition: ECDSA.h:757
Definition: ECDSA.h:669
void ECDSA_Params_init(ECDSA_Params *params)
Function to initialize the ECDSA_Params struct to its defaults.
const uint8_t * r
Definition: ECDSA.h:731
Union containing pointers to all supported operation structs.
Definition: ECDSA.h:748
Definition: ECDSA.h:665
Definition: ECDSA.h:639
int_fast16_t ECDSA_sign(ECDSA_Handle handle, ECDSA_OperationSign *operation)
Signs a hashed message.
void * custom
Definition: ECDSA.h:804
ECDSA_Config * ECDSA_Handle
A handle that is returned from an ECDSA_open() call.
Definition: ECDSA.h:603
uint8_t * r
Definition: ECDSA.h:701
int_fast16_t ECDSA_verify(ECDSA_Handle handle, ECDSA_OperationVerify *operation)
Verifies a received signature matches a hash and public key.
Struct containing the parameters required for verifying a message.
Definition: ECDSA.h:717
void * object
Definition: ECDSA.h:594
Definition: ECDSA.h:657
ECDSA_CallbackFxn callbackFxn
Definition: ECDSA.h:800
Definition: ECDSA.h:678
ECDSA_OperationVerify * verify
Definition: ECDSA.h:751
Definition: ECDSA.h:635
ECDSA_CurveType curveType
Definition: ECDSA.h:691
A structure containing the parameters of an elliptic curve.
Definition: ECCParams.h:143
Definition: ECDSA.h:629
const uint8_t * hash
Definition: ECDSA.h:727
ECDSA_Handle ECDSA_open(uint_least8_t index, const ECDSA_Params *params)
This function opens a given ECDSA peripheral.
Definition: ECDSA.h:681
Definition: ECDSA.h:759
ECDSA_OperationSign * sign
Definition: ECDSA.h:750
uint32_t timeout
Definition: ECDSA.h:801
Definition: ECDSA.h:667
ECDSA_Handle ECDSA_construct(ECDSA_Config *config, const ECDSA_Params *params)
Constructs a new ECDSA object.
void ECDSA_OperationVerify_init(ECDSA_OperationVerify *operation)
Function to initialize an ECDSA_OperationSign struct to its defaults.
int_fast16_t ECDSA_cancelOperation(ECDSA_Handle handle)
Cancels an ongoing ECDSA operation.
© Copyright 1995-2024, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale