39 #ifndef ti_drivers_cryptoutils_sharedresources_CryptoResourceLPF3__include 40 #define ti_drivers_cryptoutils_sharedresources_CryptoResourceLPF3__include HwiP structure.
Definition: HwiP.h:78
void CryptoResourceLPF3_constructRTOSObjects(void)
bool CryptoResourceLPF3_acquireLock(uint32_t timeout)
Semaphore module for the RTOS Porting Interface.
volatile bool CryptoResourceLPF3_pollingFlag
SemaphoreP_Struct CryptoResourceLPF3_accessSemaphore
void CryptoResourceLPF3_destructRTOSObjects(void)
void CryptoResourceLPF3_releaseLock(void)
Hardware Interrupt module for the RTOS Porting Interface.
SemaphoreP_Struct CryptoResourceLPF3_operationSemaphore
SemaphoreP structure.
Definition: SemaphoreP.h:84
HwiP_Struct CryptoResourceLPF3_hwi