273 #ifndef ti_drivers_AESCTRDRBG__include 274 #define ti_drivers_AESCTRDRBG__include 300 #define AESCTRDRBG_STATUS_RESERVED AES_STATUS_RESERVED 308 #define AESCTRDRBG_STATUS_SUCCESS AES_STATUS_SUCCESS 316 #define AESCTRDRBG_STATUS_ERROR AES_STATUS_ERROR 326 #define AESCTRDRBG_STATUS_RESOURCE_UNAVAILABLE AES_STATUS_RESOURCE_UNAVAILABLE 334 #define AESCTRDRBG_STATUS_RESEED_REQUIRED (AES_STATUS_DRIVER_SPECIFIC_ERROR - 0) 340 #define AESCTRDRBG_STATUS_UNINSTANTIATED (AES_STATUS_DRIVER_SPECIFIC_ERROR - 1) 349 #define AESCTRDRBG_STATUS_UNALIGNED_IO_NOT_SUPPORTED (AES_STATUS_DRIVER_SPECIFIC_ERROR - 2) 357 #define AESCTRDRBG_STATUS_KEYSTORE_ERROR (AES_STATUS_KEYSTORE_GENERIC_ERROR) 362 #define AESCTRDRBG_AES_BLOCK_SIZE_BYTES 16 631 const void *additionalData,
632 size_t additionalDataLength);
ADC_Params params
Definition: Driver_Init.h:11
The CryptoKey type is an opaque representation of a cryptographic key.
AESCTRDRBG_AES_KEY_LENGTH
Length in bytes of the internal AES key used by an instance.
Definition: AESCTRDRBG.h:367
#define AESCTRDRBG_AES_BLOCK_SIZE_BYTES
The AES block size in bytes.
Definition: AESCTRDRBG.h:362
void AESCTRDRBG_close(AESCTRDRBG_Handle handle)
Function to close an AESCTRDRBG instance specified by the AESCTRDRBG_Handle.
Definition: AESCTRDRBG.h:413
Definition: AESCTRDRBG.h:408
const AESCTRDRBG_Params AESCTRDRBG_defaultParams
Default AESCTRDRBG_Params structure.
AES Global configuration.
Definition: AESCommon.h:154
void AESCTRDRBG_init(void)
This function initializes the AESCTRDRBG driver.
CryptoKey datastructure.
Definition: CryptoKey.h:208
AESCTRDRBG_SEED_LENGTH
Length in bytes of seed used to instantiate or reseed instance.
Definition: AESCTRDRBG.h:376
Definition: AESCTRDRBG.h:379
int_fast16_t AESCTRDRBG_generateKey(AESCTRDRBG_Handle handle, CryptoKey *randomKey)
Populates the provided CryptoKey object's plaintext key-material with random bytes.
Definition: AESCTRDRBG.h:378
AESCTRDRBG_Handle AESCTRDRBG_construct(AESCTRDRBG_Config *config, const AESCTRDRBG_Params *params)
Constructs a new AESCTRDRBG object.
AESCTRDRBG Parameters.
Definition: AESCTRDRBG.h:442
AESCTRDRBG_ReturnBehavior
The way in which AESCTRDRBG function calls return after generating the requested entropy.
Definition: AESCTRDRBG.h:402
Definition: AESCTRDRBG.h:369
const void * seed
Definition: AESCTRDRBG.h:451
int_fast16_t AESCTRDRBG_getRandomBytes(AESCTRDRBG_Handle handle, void *randomBytes, size_t randomBytesSize)
Generates the requested number of random bytes and outputs to the given array.
void * custom
Definition: AESCTRDRBG.h:471
uint32_t reseedInterval
Definition: AESCTRDRBG.h:447
AESCommon_Config AESCTRDRBG_Config
AESCTRDRBG Global configuration.
Definition: AESCTRDRBG.h:427
AESCTRDRBG_Config * AESCTRDRBG_Handle
A handle that is returned from an AESCTRDRBG_open() call.
Definition: AESCTRDRBG.h:432
AESCTRDRBG_AES_KEY_LENGTH keyLength
Definition: AESCTRDRBG.h:444
int_fast16_t AESCTRDRBG_reseed(AESCTRDRBG_Handle handle, const void *seed, const void *additionalData, size_t additionalDataLength)
Reseed an AESCTRDRBG instance.
AESCTRDRBG_Handle AESCTRDRBG_open(uint_least8_t index, const AESCTRDRBG_Params *params)
This function opens a given AESCTRDRBG instance.
AES common module header for all devices.
int_fast16_t AESCTRDRBG_getBytes(AESCTRDRBG_Handle handle, CryptoKey *randomBytes)
Generates the requested number of random bytes.
AESCTRDRBG_ReturnBehavior returnBehavior
Definition: AESCTRDRBG.h:464
void AESCTRDRBG_Params_init(AESCTRDRBG_Params *params)
Function to initialize the AESCTRDRBG_Params struct to its defaults.
size_t personalizationDataLength
Definition: AESCTRDRBG.h:460
Definition: AESCTRDRBG.h:370
const void * personalizationData
Definition: AESCTRDRBG.h:456