Flash Layout for Off-Chip OAD¶
This section will describe the method for placing images in internal and external flash when using off-chip OAD.
Internal flash refers to the flash memory inside the CC23xx and external flash refers to an external SPI flash memory connected to the CC23xx via SPI.
See requirements below for off-chip OAD.
Requirements and Constraints for Off-chip OAD¶
In order to perform an Off-chip OAD the target system must have:
An off-chip flash storage as large as the application size + one external flash page to store the external flash image header. (default example will use 1MB of external flash)
A serial connection (SPI) is used to communicate with the off-chip flash component.
Free GPIO pins to interface to the external memory (i.e. 4 wires for SPI)
- The following software limitations exist on the external flash:
Only the secondary slot is stored on the external flash.
The OAD images’ headers shall be stored in the first 1 MBytes of the external flash addressable space.
The total size of the stored images should not exceed 4 GBytes.
Note
Off-chip OAD using the BLE5-Stack has only be tested using a 1 MBytes external flash. The out-of-the-box software do not allow larger external flash size.
Internal Flash Memory Layout¶
The internal flash of the device contains the active user application and MCUboot. Off-chip OAD maximizes the available flash space to the user application because of its ability to store the incoming image in external flash during the download process.
Note
When using security, the BIM may use a second page depending on the page size of the device. Consult the BIM’s linker file for more information.
![../_images/ditaa-0fe585d78dbb21bdb49696374885c61add8cee34.png](../_images/ditaa-0fe585d78dbb21bdb49696374885c61add8cee34.png)
The user application pictured above is responsible for the following:
Implementing the protocol stack specific implementation of the OAD transport
Finding a suitable location in external flash for the image and storing its image header in the table.
External Flash Memory Layout¶
The off-chip flash memory on the CC23xx LaunchPad contains the secondary slot of the user applications.
The memory map layout of the external flash is defined in flash_map_backend.h
.
The size of the image in external flash can be determined
once the image header vector is sent over the air.
The application will round up as necessary according to the equation below:
The memory partition of the application for Off-chip OAD is depicted in below.
![../_images/ditaa-099a40a5b8f27872949ef5436e5a010fbf557426.png](../_images/ditaa-099a40a5b8f27872949ef5436e5a010fbf557426.png)
Enabling External Flash support on CC2340R5 4x4 board¶
The following modifications are necessary to enable an external flash enabled configuration on the CC2340R5 device using a 4x4 board. The exact pin assignments will depend on your custom board. The following pin values were used as a reference.
Within the {SDK_INSTALL_DIR}/source/ti/common/flash/no_rtos/extFlash/bsp.h
,
locate the following code:
#define BSP_IOID_FLASH_CS 6 #define BSP_SPI_MOSI 13 #define BSP_SPI_MISO 12 #define BSP_SPI_CLK_FLASH 18
The above code should be changed to the following:
#define BSP_IOID_FLASH_CS 11 #define BSP_SPI_MOSI 13 #define BSP_SPI_MISO 21 #define BSP_SPI_CLK_FLASH 24
Within the {SDK_INSTALL_DIR}/source/ti/common/flash/no_rtos/extFlash/bsp_spi_lpf3.c
,
locate the following code:
#define MISO_PINMUX GPIO_MUX_PORTCFG_PFUNC_1 #define MOSI_PINMUX GPIO_MUX_PORTCFG_PFUNC_2 #define CLK_PINMUX GPIO_MUX_PORTCFG_PFUNC_4
The above code should be changed to the following:
#define MISO_PINMUX GPIO_MUX_PORTCFG_PFUNC_4 #define MOSI_PINMUX GPIO_MUX_PORTCFG_PFUNC_2 #define CLK_PINMUX GPIO_MUX_PORTCFG_PFUNC_1
On the 4x4 board, the 2-4 P2 and 5-3 P6 jumpers should be placed to enable external flash SPI access.