![]() |
![]() |
TI BLE5-Stack API Documentation
3.03.01.00
|
Micro BLE GAP API.
This file contains the interface to the Micro GAP Layer.
Go to the source code of this file.
Data Structures | |
struct | ugapBcastCBs_t |
Set of Broadcaster callbacks - must be setup by the application. More... | |
Macros | |
#define | UGAP_BCAST_STATE_ADVERTISING 3 |
Advertising. | |
#define | UGAP_BCAST_STATE_IDLE 2 |
Advertising or Waiting stopped. | |
#define | UGAP_BCAST_STATE_INITIALIZED 1 |
Initialized. Waiting for start request. | |
#define | UGAP_BCAST_STATE_INVALID 0 |
Invalid state. Not even initialized. | |
#define | UGAP_BCAST_STATE_SUSPENDED 5 |
Advertising or Waiting is suspended. | |
#define | UGAP_BCAST_STATE_WAITING 4 |
Advertising paused during duty off period. | |
#define | UGAP_DUTY_TIME_UNIT 100L |
Duty Control Time Unit. More... | |
#define | UGB_EVT_ADV_POSTPROCESS 3 |
Adv has just been done. Do post processing if necessary. | |
#define | UGB_EVT_ADV_PREPARE 2 |
About to issue the next adv. Prepare adv payload. | |
#define | UGB_EVT_STATE_CHANGE 1 |
Broadcaster's state has changed. | |
Typedefs | |
typedef void(* | ugapBcastAdvDoneCb_t) (bStatus_t status) |
Callback of when an Advertising Event has just been done. More... | |
typedef void(* | ugapBcastAdvPrepareCb_t) (void) |
Callback of when the next Advertising Event is about to start. More... | |
typedef uint8 | ugapBcastState_t |
Broadcaster state. | |
typedef void(* | ugapBcastStateChangeCb_t) (ugapBcastState_t state) |
Callback of when the Broadcaster's state changes. More... | |
Functions | |
bStatus_t | ugap_bcastInit (ugapBcastCBs_t *pCBs) |
Initialize Micro Broadcaster. More... | |
bStatus_t | ugap_bcastSetDuty (uint16 dutyOnTime, uint16 dutyOffTime) |
Set Broadcaster Duty On/Off time. More... | |
bStatus_t | ugap_bcastStart (uint16 numAdvEvent) |
Start Broadcaster. Proceed the state from either Initialized or IDLE to Advertising. More... | |
bStatus_t | ugap_bcastStop (void) |
Stop Broadcaster. Proceed the state from either Advertising or Waiting to IDLE. More... | |