38 void hal_init_fsm(
void (*setupFsmCb)(
void),
void (*schedFsmCb)(
void),
39 void (*commandFsmCb)(
void));
void hal_trigger_scheduler_fsm(void)
Definition: hal_cc23x0.c:176
void hal_enable_hard_stop_time_irq(void)
Definition: hal_cc23x0.c:227
void hal_disable_command_radio_interrupt(uint32_t mask)
Definition: hal_cc23x0.c:361
void hal_disable_all_command_radio_interrupts(void)
Definition: hal_cc23x0.c:367
void hal_arm_cmd_done_cap(void)
void hal_arm_cmd_start_cap(void)
uint32_t hal_get_hfxt_ratio_default(void)
Definition: hal_cc23x0.c:468
void hal_disable_all_dispatch_radio_interrupts(void)
Definition: hal_cc23x0.c:373
void hal_enable_setup_time_irq(void)
Definition: hal_cc23x0.c:193
void hal_setup_cmd_start_cap(void)
void hal_setup_start_time(uint32_t startTime)
Definition: hal_cc23x0.c:211
void hal_power_open(void(*f)(RCL_PowerEvent))
Definition: hal_cc23x0.c:432
uint32_t hal_get_sync_found_cap(void)
void hal_init_dispatch_radio_interrupts(uint32_t mask)
Definition: hal_cc23x0.c:344
void hal_power_close(void)
Definition: hal_cc23x0.c:443
RCL_PowerEvent
Definition: hal.h:77
void hal_setup_setup_time(uint32_t setupTime)
Definition: hal_cc23x0.c:198
uint32_t hal_get_current_time(void)
Definition: hal_cc23x0.c:182
void hal_init_fsm(void(*setupFsmCb)(void), void(*schedFsmCb)(void), void(*commandFsmCb)(void))
Definition: hal_cc23x0.c:131
uint32_t hal_get_cmd_done_cap(void)
void hal_clear_rcl_clock_enable(uint16_t mask)
Definition: hal_cc23x0.c:386
void hal_setup_cmd_done_cap(void)
void hal_cancel_start_time(void)
Definition: hal_cc23x0.c:267
void hal_enable_graceful_stop_time_irq(void)
Definition: hal_cc23x0.c:244
uint32_t hal_get_dispatch_ifg_reg(void)
Definition: hal_cc23x0.c:117
void hal_disable_hard_stop_time_irq(void)
Definition: hal_cc23x0.c:232
int16_t hal_get_temperature(void)
void hal_enable_command_radio_interrupt(uint32_t mask)
Definition: hal_cc23x0.c:350
void hal_set_rcl_clock_enable(uint16_t mask)
Definition: hal_cc23x0.c:379
void hal_trigger_command_fsm(void)
Definition: hal_cc23x0.c:164
void hal_cancel_setup_time(void)
Definition: hal_cc23x0.c:262
void hal_power_release_constraint(void)
Definition: hal_cc23x0.c:423
uint32_t hal_get_hfxt_ratio(void)
Definition: hal_cc23x0.c:463
void hal_enable_clk_buffer(void)
Definition: hal_cc23x0.c:285
uint32_t hal_get_command_ifg_reg(void)
Definition: hal_cc23x0.c:104
void hal_trigger_dispatch_fsm(void)
Definition: hal_cc23x0.c:170
void hal_power_set_constraint(void)
Definition: hal_cc23x0.c:414
void hal_setup_graceful_stop_time(uint32_t stopTime)
Definition: hal_cc23x0.c:237
HalTimerEvent hal_check_clear_timer_compare(void)
Definition: hal_cc23x0.c:304
void hal_temperature_init(void)
Definition: hal_cc23x0.c:452
void hal_setup_hard_stop_time(uint32_t stopTime)
Definition: hal_cc23x0.c:219
void hal_cancel_hard_stop_time(void)
Definition: hal_cc23x0.c:272
void hal_clear_command_radio_interrupt(uint32_t mask)
Definition: hal_cc23x0.c:356
void hal_arm_sync_found_cap(void)
HalTimerEvent
Definition: hal.h:69
void hal_setup_sync_found_cap(void)
Definition: hal_cc23x0.c:293
void hal_cancel_graceful_stop_time(void)
Definition: hal_cc23x0.c:277
uint32_t hal_get_cmd_start_cap(void)