41 #if defined(DeviceFamily_CC23X0R5) || defined(DeviceFamily_CC23X0R2) || defined(DeviceFamily_CC27XX) || defined(DeviceFamily_CC23X0R22) || defined(DeviceFamily_CC2340R53) 42 # include <ti/devices/DeviceFamily.h> 43 # include DeviceFamily_constructPath(inc/hw_types.h) 44 # include DeviceFamily_constructPath(inc/hw_lrfdpbe.h) 48 #ifdef DeviceFamily_CC1308 49 # define BUFFER_SPLIT_SUPPORT 50 # include "LRFCC1308.h" 57 #define LRF_TxPower_Use_Min ((LRF_TxPowerTable_Index){.rawValue = -128}) 62 #define LRF_TxPower_Use_Max ((LRF_TxPowerTable_Index){.rawValue = 125}) 67 #define LRF_TxPower_Use_Raw ((LRF_TxPowerTable_Index){.rawValue = 126}) 73 #define LRF_TxPower_None ((LRF_TxPowerTable_Index){.rawValue = 127}) 79 #define LRF_SETTINGS_BUFFER_UNLIMITED 0x3FFF 85 #define LRF_RSSI_INVALID (127) 88 typedef enum LRF_RadioState_e {
97 typedef enum LRF_SetupResult_e {
116 uint32_t lengthMinus1 : 12;
118 uint32_t startAddress : 16;
131 uint32_t length : 14;
132 uint32_t invertedFeatureMask : 1;
133 uint32_t compoundSegment : 1;
134 uint32_t featureMask : 16;
170 #ifdef BUFFER_SPLIT_SUPPORT 174 uint32_t segmentLength;
179 uint32_t regionLength;
180 uint32_t regionStart;
184 #define LRF_PhyFeatures_Default 0 187 #define __ERROR_Address_is_in_an_invalid_range_for_LRF_setup 0x00040000 189 #define _ADDRESS_REGION_BIT(_address) \ 190 ((((((uintptr_t)(_address)) >= (LRF_BASE_ADDR)) && \ 191 ((uintptr_t)(_address)) < ((LRF_BASE_ADDR) + 0x10000)) ? 0 : \ 192 ((((uintptr_t)(_address)) >= (PBE_RAM_BASE_ADDR)) && \ 193 (((uintptr_t)(_address)) < ((PBE_RAM_BASE_ADDR) + 0x10000)) ? \ 195 (((((uintptr_t)(_address)) >= 0) && \ 196 (((uintptr_t)(_address)) < 0x10000)) ? \ 198 (__ERROR_Address_is_in_an_invalid_range_for_LRF_setup)))) << 14) 200 #define LRF_SETTINGS_CLEAR(_startAddress, _numWords) \ 201 ((((_numWords) - 1) & 0x0FFF) | \ 202 _ADDRESS_REGION_BIT(_startAddress) | \ 203 ((((uintptr_t)(_startAddress)) & 0xFFFF) << 16)) 205 #define LRF_SETTINGS_16BIT_BLOCK(_startAddress, _numWords) \ 206 ((((_numWords) - 1) & 0x0FFF) | \ 207 _ADDRESS_REGION_BIT(_startAddress) | (1 << 12) | \ 208 ((((uintptr_t)(_startAddress)) & 0xFFFF) << 16)) 210 #define LRF_SETTINGS_16BIT_DUAL_ENTRY(_value0, _value1) \ 211 (((_value0) & 0xFFFF) | (((_value1) & 0xFFFF) << 16)) 213 #define LRF_SETTINGS_32BIT_BLOCK(_startAddress, _numWords) \ 214 ((((_numWords) - 1) & 0x0FFF) | \ 215 _ADDRESS_REGION_BIT(_startAddress) | (2 << 12) | \ 216 ((((uintptr_t)(_startAddress)) & 0xFFFF) << 16)) 218 #define LRF_SETTINGS_16BIT_SPARSE_BLOCK(_startAddress, _numWords) \ 219 ((((_numWords) - 1) & 0x0FFF) | \ 220 _ADDRESS_REGION_BIT(_startAddress) | (3 << 12)) \ 222 #define LRF_SETTINGS_16BIT_SPARSE_ENTRY(_address, _value) \ 223 (((((uintptr_t)(_address)) & 0xFFFF) << 16) | ((_value) & 0xFFFF)) 225 #define LRF_SETTINGS_16BIT_MASKED_BLOCK(_startAddress, _numWords) \ 226 ((((_numWords) - 1) & 0x0FFF) | (11 << 12) | \ 227 ((((uintptr_t)(_startAddress)) & 0xFFFF) << 16)) 229 #define LRF_SETTINGS_16BIT_MASKED_ENTRY(_mask, _value) \ 230 ((((_mask) & 0xFFFF) << 16) | ((_value) & 0xFFFF)) 238 #ifdef BUFFER_SPLIT_SUPPORT 239 state->totalLength = 0;
247 uint16_t phyFeatures);
250 int32_t bufferAvailWords);
int8_t LRF_readRssi(void)
Definition: LRFCC23X0.c:1413
void LRF_rclEnableRadioClocks(void)
Definition: LRFCC23X0.c:1389
void LRF_setClockEnable(uint16_t mask, uint8_t entryNumber)
static void LRF_resetSettingsState(LRF_ApplySettingsState *state)
Definition: LRF.h:236
LRF_SetupResult LRF_loadImage(const LRF_TOPsmImage *image, uint32_t destinationAddress)
Definition: LRF.c:46
LRF_RadioState
Definition: LRF.h:88
LRF_SetupResult
Setup operation result.
Definition: LRF.h:97
void LRF_sendHardStop(void)
LRF_SetupResult LRF_setupRadio(const LRF_Config *lrfConfig, uint16_t phyFeatures, LRF_RadioState lrfState)
Definition: LRFCC23X0.c:93
Single entry of the tx power table. Maps power in dBm to specific register settings.
Definition: LRFCC23X0.h:186
void LRF_sendGracefulStop(void)
void LRF_discardRxFifoWords(uint32_t wordLength)
Definition: LRFCC23X0.c:820
uint32_t value32
Definition: LRF.h:120
uint32_t image[]
Definition: LRF.h:111
Tx power table, containing all characterized dBm to register settings mappings.
Definition: LRFCC23X0.h:205
void LRF_writeTxFifoWords(const uint32_t *data32, uint32_t wordLength)
Definition: LRFCC23X0.c:861
LRF_SetupResult LRF_applySettings(LRF_ConfigWord *config, LRF_ApplySettingsState *state, int32_t bufferAvailWords)
Definition: LRF.c:122
void LRF_clearClockEnable(uint16_t mask, uint8_t entryNumber)
Index of the tx power table.
Definition: LRFCC23X0.h:173
Radio configuration structure.
Definition: LRFCC23X0.h:518
uint32_t LRF_enableSynthRefsys(void)
Definition: LRFCC23X0.c:1359
uint32_t LRF_prepareRxFifo(void)
Definition: LRFCC23X0.c:704
uint8_t * LRF_getTxFifoWrAddr(int32_t offset)
Definition: LRFCC23X0.c:759
static void LRF_clearHwInterrupt(uint32_t mask)
Definition: LRF.h:306
LRF_ApplySettingsBase
Definition: LRF.h:160
uint32_t imageLen
Definition: LRF.h:110
bool LRF_imagesNeedUpdate(const LRF_Config *lrfConfig)
Definition: LRFCC23X0.c:190
void hal_enable_command_radio_interrupt(uint32_t mask)
Definition: hal_cc23x0.c:350
uint32_t swParamList[]
Definition: LRFCC23X0.c:75
static void LRF_disableHwInterrupt(uint32_t mask)
Definition: LRF.h:301
void hal_clear_command_radio_interrupt(uint32_t mask)
Definition: hal_cc23x0.c:356
void LRF_setRxFifoEffSz(uint32_t maxSz)
Definition: LRFCC23X0.c:886
void hal_disable_command_radio_interrupt(uint32_t mask)
Definition: hal_cc23x0.c:361
void LRF_disable(void)
Definition: LRFCC23X0.c:671
void LRF_rclDisableRadioClocks(void)
Definition: LRFCC23X0.c:1401
void LRF_programFrequency(uint32_t frequency, bool tx)
Definition: LRFCC23X0.c:1270
static void LRF_enableHwInterrupt(uint32_t mask)
Definition: LRF.h:296
void LRF_disableSynthRefsys(void)
Definition: LRFCC23X0.c:1384
LRF_TxPowerTable_Entry LRF_TxPowerTable_findValue(const LRF_TxPowerTable *table, LRF_TxPowerTable_Index powerLevel)
Search for settings corresponding to the highest tx power lower than specified value in the tx power ...
Definition: LRF.c:725
const size_t swParamListSz
Definition: LRFCC23X0.c:76
uint16_t phyFeatures
Definition: LRF.h:167
void LRF_initSettingsState(LRF_ApplySettingsState *state, LRF_ApplySettingsBase includeBase, uint16_t phyFeatures)
Definition: LRF.c:113
uint32_t LRF_prepareTxFifo(void)
Definition: LRFCC23X0.c:723
void LRF_waitForTopsmReady(void)
Definition: LRFCC23X0.c:695
void LRF_enable(void)
Definition: LRFCC23X0.c:649
uint32_t numEntries
Definition: LRF.h:139
void LRF_setRawTxPower(uint32_t value, uint32_t temperatureCoefficient)
Definition: LRFCC23X0.c:1418
uint32_t LRF_peekTxFifo(int32_t offset)
Definition: LRFCC23X0.c:748
LRF_ApplySettingsBase includeBase
Definition: LRF.h:168
void LRF_readRxFifoWords(uint32_t *data32, uint32_t wordLength)
Definition: LRFCC23X0.c:834
LRF_RegionOperation
Definition: LRF.h:143
LRF_TxPowerTable_Entry LRF_getRawTxPower(void)
Definition: LRFCC23X0.c:1425
void LRF_skipTxFifoWords(uint32_t wordLength)
Definition: LRFCC23X0.c:809
uint32_t LRF_peekRxFifo(int32_t offset)
Definition: LRFCC23X0.c:736