84 #ifndef ti_drivers_power_PowerCC27XX_ 85 #define ti_drivers_power_PowerCC27XX_ 91 #include <ti/devices/DeviceFamily.h> 92 #include DeviceFamily_constructPath(inc/hw_pmctl.h) 93 #include DeviceFamily_constructPath(inc/hw_clkctl.h) 94 #include DeviceFamily_constructPath(inc/hw_lrfddbell.h) 95 #include DeviceFamily_constructPath(inc/hw_memmap.h) 96 #include DeviceFamily_constructPath(inc/hw_types.h) 97 #include DeviceFamily_constructPath(driverlib/pmctl.h) 104 #define PowerCC27XX_RESUMETIMESTANDBY 400 107 #define PowerCC27XX_TOTALTIMESTANDBY 1000 110 #define PowerCC27XX_WAKEDELAYSTANDBY 500 119 #define PowerCC27XX_PERIPH_GROUP_M 0xFF00 120 #define PowerCC27XX_PERIPH_GROUP_CLKCTL0 0x0000 121 #define PowerCC27XX_PERIPH_GROUP_CLKCTL1 0x0100 122 #define PowerCC27XX_PERIPH_GROUP_LRFD 0x0200 123 #define PowerCC27XX_PERIPH_BIT_INDEX_M 0x00FF 128 typedef uint16_t PowerLPF3_Resource;
134 #define PowerLPF3_PERIPH_GPIO (PowerCC27XX_PERIPH_GROUP_CLKCTL0 | CLKCTL_DESCEX0_GPIO_S) 137 #define PowerLPF3_PERIPH_UART0 (PowerCC27XX_PERIPH_GROUP_CLKCTL0 | CLKCTL_DESCEX0_UART0_S) 140 #define PowerLPF3_PERIPH_UART1 (PowerCC27XX_PERIPH_GROUP_CLKCTL0 | CLKCTL_DESCEX0_UART1_S) 143 #define PowerLPF3_PERIPH_I2C0 (PowerCC27XX_PERIPH_GROUP_CLKCTL0 | CLKCTL_DESCEX0_I2C0_S) 146 #define PowerLPF3_PERIPH_SPI0 (PowerCC27XX_PERIPH_GROUP_CLKCTL0 | CLKCTL_DESCEX0_SPI0_S) 149 #define PowerLPF3_PERIPH_SPI1 (PowerCC27XX_PERIPH_GROUP_CLKCTL0 | CLKCTL_DESCEX0_SPI1_S) 152 #define PowerLPF3_PERIPH_ADC0 (PowerCC27XX_PERIPH_GROUP_CLKCTL0 | CLKCTL_DESCEX0_ADC0_S) 155 #define PowerLPF3_PERIPH_AES (PowerCC27XX_PERIPH_GROUP_CLKCTL0 | CLKCTL_DESCEX0_LAES_S) 158 #define PowerLPF3_PERIPH_DMA (PowerCC27XX_PERIPH_GROUP_CLKCTL0 | CLKCTL_DESCEX0_DMA_S) 161 #define PowerLPF3_PERIPH_I2S (PowerCC27XX_PERIPH_GROUP_CLKCTL0 | CLKCTL_DESCEX0_I2S_S) 164 #define PowerLPF3_PERIPH_LGPT0 (PowerCC27XX_PERIPH_GROUP_CLKCTL0 | CLKCTL_DESCEX0_LGPT0_S) 167 #define PowerLPF3_PERIPH_LGPT1 (PowerCC27XX_PERIPH_GROUP_CLKCTL0 | CLKCTL_DESCEX0_LGPT1_S) 170 #define PowerLPF3_PERIPH_LGPT2 (PowerCC27XX_PERIPH_GROUP_CLKCTL0 | CLKCTL_DESCEX0_LGPT2_S) 173 #define PowerLPF3_PERIPH_LGPT3 (PowerCC27XX_PERIPH_GROUP_CLKCTL0 | CLKCTL_DESCEX0_LGPT3_S) 176 #define PowerLPF3_PERIPH_HSM (PowerCC27XX_PERIPH_GROUP_CLKCTL1 | CLKCTL_DESCEX1_HSM_S) 179 #define PowerLPF3_PERIPH_VCE (PowerCC27XX_PERIPH_GROUP_CLKCTL1 | CLKCTL_DESCEX1_VCE_S) 182 #define PowerLPF3_PERIPH_MCAN (PowerCC27XX_PERIPH_GROUP_CLKCTL1 | CLKCTL_DESCEX1_MCAN_S) 185 #define PowerLPF3_PERIPH_LFRD_TRC (PowerCC27XX_PERIPH_GROUP_LRFD | LRFDDBELL_CLKCTL_TRC_S) 188 #define PowerLPF3_PERIPH_LFRD_S2RRAM (PowerCC27XX_PERIPH_GROUP_LRFD | LRFDDBELL_CLKCTL_S2RRAM_S) 196 #define PowerCC27XX_NUMRESOURCES_CLKCTL0 31 197 #define PowerCC27XX_NUMRESOURCES_CLKCTL1 7 198 #define PowerCC27XX_NUMRESOURCES_LRFD 12 202 #define PowerLPF3_STANDBY 0x1 205 #define PowerLPF3_ENABLE 1 206 #define PowerLPF3_DISABLE 0 216 #define PowerLPF3_DISALLOW_SHUTDOWN 0 219 #define PowerLPF3_DISALLOW_STANDBY 1 222 #define PowerLPF3_DISALLOW_IDLE 2 225 #define PowerLPF3_NEED_FLASH_IN_IDLE 3 228 #define PowerCC27XX_NUMCONSTRAINTS 4 239 #define PowerLPF3_ENTERING_STANDBY (1 << 0) 242 #define PowerLPF3_ENTERING_SHUTDOWN (1 << 1) 245 #define PowerLPF3_AWAKE_STANDBY (1 << 2) 250 #define PowerLPF3_HFXT_AVAILABLE (1 << 3) 255 #define PowerLPF3_LFCLK_SWITCHED (1 << 4) 258 #define PowerCC27XX_NUMEVENTS 5 428 return (PowerLPF3_ResetReason)PMCTLGetResetReason();
447 HWREG(PMCTL_BASE + PMCTL_O_SLPCTL) = PMCTL_SLPCTL_SLPN_DIS;
static void PowerLPF3_releaseLatches(void)
Unlatch all IOs.
Definition: PowerCC27XX.h:445
Definition: PowerCC27XX.h:334
Definition: PowerCC27XX.h:338
Definition: PowerCC27XX.h:366
Definition: PowerCC27XX.h:356
Clock interface for the RTOS Porting Interface.
void(* Power_PolicyInitFxn)(void)
Power policy initialization function pointer.
Definition: Power.h:401
PowerLPF3_StartInitialHfxtAmpCompFxn startInitialHfxtAmpCompFxn
Pointer to the function to start the initial HFXT amplitude compensation.
Definition: PowerCC27XX.h:323
Definition: PowerCC27XX.h:350
uint32_t systemWakeupIntervalUsec
The expected interval in us between system wakeups.
Definition: PowerCC27XX.h:395
Definition: PowerCC27XX.h:367
void PowerLPF3_stopAFOSC(void)
Stop the AFOSC.
void PowerLPF3_selectEXTLF(void)
Select EXTLF as LFCLK source.
Definition: PowerCC27XX.h:348
void PowerCC27XX_standbyPolicy(void)
The STANDBY Power Policy.
Definition: PowerCC27XX.h:340
Definition: PowerCC27XX.h:354
Definition: PowerCC27XX.h:344
void(* Power_PolicyFxn)(void)
Power policy function pointer.
Definition: Power.h:406
PowerLPF3_ResetReason
Reasons the device has booted or rebooted.
Definition: PowerCC27XX.h:329
void PowerLPF3_startInitialHfxtAmpComp(void)
Start initial compensation of the HFXT amplitude.
Power_PolicyFxn policyFxn
The Power Policy function.
Definition: PowerCC27XX.h:307
Global configuration structure.
Definition: PowerCC27XX.h:270
PowerLPF3_LfoscCompensationPpmRequirement ppmRequirement
The PPM requirements.
Definition: PowerCC27XX.h:398
void PowerLPF3_adjustHfxtAmp(int_fast8_t adjustment)
Adjust the HFXT amplitude.
void PowerCC27XX_schedulerDisable(void)
void PowerLPF3_selectLFXT(void)
Select LFXT as LFCLK source.
PowerLPF3_AfoscFreq
The possible frequencies to configure the AFOSC to.
Definition: PowerCC27XX.h:364
Power_PolicyInitFxn policyInitFxn
The Power Policy's initialization function.
Definition: PowerCC27XX.h:278
Definition: PowerCC27XX.h:336
Definition: PowerCC27XX.h:352
Definition: PowerCC27XX.h:332
Definition: PowerCC27XX.h:368
void PowerLPF3_setLfoscCompensationProfile(const PowerLPF3_LfoscCompensationProfile *profile)
Set LFOSC Compensation Profile.
500 PPM
Definition: PowerCC27XX.h:377
void PowerLPF3_disableLfoscCompensation(void)
Disable LFOSC Compensation.
void PowerLPF3_selectLFOSC(void)
Select LFOSC as LFCLK source.
void(* PowerLPF3_StartInitialHfxtAmpCompFxn)(void)
Function pointer to PowerLPF3_startInitialHfxtAmpComp() or NULL.
Definition: PowerCC27XX.h:267
static PowerLPF3_ResetReason PowerLPF3_getResetReason(void)
Returns the reason for the most recent reset or wakeup.
Definition: PowerCC27XX.h:426
int_fast8_t PowerLPF3_getHfxtAmpAdjustment(void)
Check if HFXT amplitude needs to be adjusted.
LFOSC Compensation Profile structure.
Definition: PowerCC27XX.h:389
Definition: PowerCC27XX.h:342
Definition: PowerCC27XX.h:346
PowerLPF3_LfoscCompensationPpmRequirement
Possible LFOSC PPM requirements to be used by the LFOSC compensation.
Definition: PowerCC27XX.h:374
void PowerLPF3_initLfoscCompensation(void)
Initialize LFOSC Compensation.
uint16_t temperatureGradientMilliCelsiusPerSec
The absolute value of the worst case expected temperature gradient in mC/s.
Definition: PowerCC27XX.h:403
Hardware Interrupt module for the RTOS Porting Interface.
void PowerCC27XX_doWFI(void)
The wait for interrupt (WFI) policy.
void PowerCC27XX_schedulerRestore(void)
void PowerLPF3_enableLfoscCompensation(void)
Enable LFOSC Compensation.
int_fast16_t PowerLPF3_startAFOSC(PowerLPF3_AfoscFreq frequency)
Start the AFOSC.