CKMD

Instance: CKMD
Component: CKMD
Base address: 0x40001000


Clock Controller

TOP:CKMD Register Summary

Register Name

Type

Register Width (Bits)

Register Reset

Address Offset

Physical Address

DESC

RO

32

0x9B4B 1000

0x0000 0000

0x4000 1000

IMASK

RW

32

0x0000 0000

0x0000 0044

0x4000 1044

RIS

RO

32

0x0000 0000

0x0000 0048

0x4000 1048

MIS

RO

32

0x0000 0000

0x0000 004C

0x4000 104C

ISET

WO

32

0x0000 0000

0x0000 0050

0x4000 1050

ICLR

WO

32

0x0000 0000

0x0000 0054

0x4000 1054

IMSET

WO

32

0x0000 0000

0x0000 0058

0x4000 1058

IMCLR

WO

32

0x0000 0000

0x0000 005C

0x4000 105C

HFOSCCTL

RW

32

0x0000 0000

0x0000 0080

0x4000 1080

HFXTCTL

RW

32

0x0000 0000

0x0000 0084

0x4000 1084

LFOSCCTL

RW

32

0x0000 0000

0x0000 008C

0x4000 108C

LFXTCTL

RW

32

0x0000 0000

0x0000 0090

0x4000 1090

LFQUALCTL

RW

32

0x0000 2064

0x0000 0094

0x4000 1094

LFINCCTL

RW

32

0x9E84 8014

0x0000 0098

0x4000 1098

LFINCOVR

RW

32

0x0000 0000

0x0000 009C

0x4000 109C

AMPADCCTL

RW

32

0x0000 0000

0x0000 00A0

0x4000 10A0

HFTRACKCTL

RW

32

0x0040 0000

0x0000 00A4

0x4000 10A4

LDOCTL

RW

32

0x0000 0000

0x0000 00A8

0x4000 10A8

NABIASCTL

RW

32

0x0000 0000

0x0000 00AC

0x4000 10AC

LFMONCTL

RW

32

0x0000 0000

0x0000 00B0

0x4000 10B0

LFCLKSEL

RW

32

0x0000 0000

0x0000 00C0

0x4000 10C0

TDCCLKSEL

RW

32

0x0000 0000

0x0000 00C4

0x4000 10C4

ADCCLKSEL

RW

32

0x0000 0000

0x0000 00C8

0x4000 10C8

LFCLKSTAT

RO

32

0x0000 0000

0x0000 00E0

0x4000 10E0

HFXTSTAT

RO

32

0x0000 0000

0x0000 00E4

0x4000 10E4

AMPADCSTAT

RO

32

0x0000 0000

0x0000 00E8

0x4000 10E8

TRACKSTAT

RW

32

0x0000 0000

0x0000 00EC

0x4000 10EC

AMPSTAT

RO

32

0x0000 0000

0x0000 00F0

0x4000 10F0

ATBCTL0

RW

32

0x0000 0000

0x0000 0100

0x4000 1100

ATBCTL1

RW

32

0x0000 0000

0x0000 0104

0x4000 1104

DTBCTL

RW

32

0x0000 0000

0x0000 0108

0x4000 1108

TRIM0

RW

32

0x0000 0000

0x0000 0110

0x4000 1110

TRIM1

RW

32

0x006F 94D6

0x0000 0114

0x4000 1114

HFXTINIT

RW

32

0x147F 8000

0x0000 0118

0x4000 1118

HFXTTARG

RW

32

0x5446 4B6D

0x0000 011C

0x4000 111C

HFXTDYN

RW

32

0x1446 4B6D

0x0000 0120

0x4000 1120

AMPCFG0

RW

32

0x0034 8882

0x0000 0124

0x4000 1124

AMPCFG1

RW

32

0x260F F0FF

0x0000 0128

0x4000 1128

LOOPCFG

RW

32

0x605E 33B3

0x0000 012C

0x4000 112C

TDCCTL

RW

32

0x0000 0000

0x0000 0200

0x4000 1200

TDCSTAT

RO

32

0x0000 0006

0x0000 0204

0x4000 1204

TDCRESULT

RO

32

0x0000 0002

0x0000 0208

0x4000 1208

TDCSATCFG

RW

32

0x0000 0000

0x0000 020C

0x4000 120C

TDCTRIGSRC

RW

32

0x0000 0000

0x0000 0210

0x4000 1210

TDCTRIGCNT

RW

32

0x0000 0000

0x0000 0214

0x4000 1214

TDCTRIGCNTLOAD

RW

32

0x0000 0000

0x0000 0218

0x4000 1218

TDCTRIGCNTCFG

RW

32

0x0000 0000

0x0000 021C

0x4000 121C

TDCPRECTL

RW

32

0x0000 0000

0x0000 0220

0x4000 1220

TDCPRECNTR

RW

32

0x0000 0000

0x0000 0224

0x4000 1224

WDTCNT

RW

32

0x0000 0000

0x0000 0300

0x4000 1300

WDTTEST

RW

32

0x0000 0000

0x0000 0304

0x4000 1304

WDTLOCK

RW

32

0x0000 0001

0x0000 0308

0x4000 1308

TOP:CKMD Register Descriptions

TOP:CKMD:DESC

Address Offset 0x0000 0000
Physical Address 0x4000 1000 Instance 0x4000 1000
Description Description Register.

This register provides IP module ID, revision information, instance index and standard MMR registers offset.
Type RO
Bits Field Name Description Type Reset
31:16 MODID Module identifier used to uniquely identify this IP. RO 0x9B4B
15:12 STDIPOFF Standard IP MMR block offset. Standard IP MMRs are the set of from aggregated IRQ registers till DTB.
0: Standard IP MMRs do not exist
0x1-0xF: Standard IP MMRs begin at offset of (64*STDIPOFF from the base IP address)

NOTE: This IP does not have DTB as part of the Standard IP MMRs. It uses DTBCTL instead.
RO 0x1
11:8 RESERVED8 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x0
7:4 MAJREV Major revision of IP (0-15). RO 0x0
3:0 MINREV Minor revision of IP (0-15). RO 0x0

TOP:CKMD:IMASK

Address Offset 0x0000 0044
Physical Address 0x4000 1044 Instance 0x4000 1044
Description Interrupt mask.

This register selects interrupt sources which are allowed to pass from RIS to MIS when the corresponding bit-fields are set to 1.
Type RW
Bits Field Name Description Type Reset
31:18 RESERVED18 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b00 0000 0000 0000
17 LFTICK 32kHz TICK to RTC and WDT.

Either derived from selected LFCLK or generated from CLKULL in absence of LFCLK.
RW 0
16 LFGEARRSTRT LFINC filter gearing restart.

Indicates that the LFINC filter restarted gearing. Subsequent LFINC estimates may have higher variation.
RW 0
15 AMPSETTLED HFXT Amplitude compensation - settled

Indicates that the amplitude compensation FSM has reached the SETTLED or TCXOMODE state,
and the controls configured in HFXTTARG or HFXTDYN are reached.
RW 0
14 AMPCTRLATTARG HFXT Amplitude compensation - controls at target

Indicates that the control values configured in HFXTTARG or HFXTDYN are reached.
Applies to Q1CAP, Q2CAP and IREF.
RW 0
13 PRELFEDGE Pre-LF clock edge detect.

Indicates that a positive edge occured on the selected pre-LF clock LFCLKSEL.PRE.
Can be used by software to confirm that a LF clock source is running and within the expected frequency,
before selecting it as the main LF clock source.
RW 0
12 LFCLKLOSS LF clock is lost.

Indicates that no LF clock edge occured for ~49us (~1.6 times nominal period).
The system will automatically fall-back to generating LFTICK based on CLKULL,
to avoid timing corruption.
Note that this signal is NOT related to the analog LF clock-loss detector which can reset the device during STANDBY.
RW 0
11 LFCLKOOR LF clock period out-of-range.

Indicates that a LF clock period was measured to be out-of-range,
according to LFQUALCTL.MAXERR.
RW 0
10 LFCLKGOOD LF clock good.

Indicates that the LF clock is good, according to the configuration in LFQUALCTL.
RW 0
9 LFINCUPD LFINC updated.

Indicates that a new LFINC measurement value is available in LFCLKSTAT.LFINC.
RW 0
8 TDCDONE TDC done event.

Indicates that the TDC measurement is done.
RW 0
7 ADCPEAKUPD HFXT-ADC PEAK measurement update event.

Indicates that the HFXT-ADC PEAK measurement is done.
RW 0
6 ADCBIASUPD HFXT-ADC BIAS measurement update event.

Indicates that the HFXT-ADC BIAS measurement is done.
RW 0
5 ADCCOMPUPD HFXT-ADC comparison update event.

Indicates that the HFXT-ADC comparison is done.
RW 0
4 TRACKREFOOR Out-of-range indication from the tracking loop.

Indicates that the selected reference clock frequency of the tracking loop is out-of-range.
RW 0
3 TRACKREFLOSS Clock loss indication from the tracking loop.

Indicates that the selected reference clock of the tracking loop is lost.
RW 0
2 HFXTAMPGOOD HFXT amplitude good indication. RW 0
1 HFXTFAULT HFXT fault indication.

Indicates that HFXT did not start correctly, or its frequency is too low.
HFXT will not recover from this fault and has to be restarted.
This is only a one-time check at HFXT startup.
RW 0
0 HFXTGOOD HFXT good indication.

Indicates that HFXT started correctly. The frequency is not necessarily good enough for radio operation.
This is only a one-time check at HFXT startup.
RW 0

TOP:CKMD:RIS

Address Offset 0x0000 0048
Physical Address 0x4000 1048 Instance 0x4000 1048
Description Raw interrupt status.

This register reflects the state of all pending interrupts, regardless of masking. This register allows the user to implement a poll scheme. A flag set in this register can be cleared by writing 1 to the corresponding ICLR register bit.
Type RO
Bits Field Name Description Type Reset
31:18 RESERVED18 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b00 0000 0000 0000
17 LFTICK 32kHz TICK to RTC and WDT.

Either derived from selected LFCLK or generated from CLKULL in absence of LFCLK.
RO 0
16 LFGEARRSTRT LFINC filter gearing restart.

Indicates that the LFINC filter restarted gearing. Subsequent LFINC estimates may have higher variation.
RO 0
15 AMPSETTLED HFXT Amplitude compensation - settled

Indicates that the amplitude compensation FSM has reached the SETTLED or TCXOMODE state,
and the controls configured in HFXTTARG or HFXTDYN are reached.
RO 0
14 AMPCTRLATTARG HFXT Amplitude compensation - controls at target

Indicates that the control values configured in HFXTTARG or HFXTDYN are reached.
Applies to Q1CAP, Q2CAP and IREF.
RO 0
13 PRELFEDGE Pre-LF clock edge detect.

Indicates that a positive edge occured on the selected pre-LF clock LFCLKSEL.PRE.
Can be used by software to confirm that a LF clock source is running and within the expected frequency,
before selecting it as the main LF clock source.
RO 0
12 LFCLKLOSS LF clock is lost.

Indicates that no LF clock edge occured for ~49us (~1.6 times nominal period).
The system will automatically fall-back to generating LFTICK based on CLKULL,
to avoid timing corruption.
Note that this signal is NOT related to the analog LF clock-loss detector which can reset the device during STANDBY.
RO 0
11 LFCLKOOR LF clock period out-of-range.

Indicates that a LF clock period was measured to be out-of-range,
according to LFQUALCTL.MAXERR.
RO 0
10 LFCLKGOOD LF clock good.

Indicates that the LF clock is good, according to the configuration in LFQUALCTL.
RO 0
9 LFINCUPD LFINC updated.

Indicates that a new LFINC measurement value is available in LFCLKSTAT.LFINC.
RO 0
8 TDCDONE TDC done event.

Indicates that the TDC measurement is done.
RO 0
7 ADCPEAKUPD HFXT-ADC PEAK measurement update event.

Indicates that the HFXT-ADC PEAK measurement is done.
RO 0
6 ADCBIASUPD HFXT-ADC BIAS measurement update event.

Indicates that the HFXT-ADC BIAS measurement is done.
RO 0
5 ADCCOMPUPD HFXT-ADC comparison update event.

Indicates that the HFXT-ADC comparison is done.
RO 0
4 TRACKREFOOR Out-of-range indication from the tracking loop.

Indicates that the selected reference clock frequency of the tracking loop is out-of-range.
RO 0
3 TRACKREFLOSS Clock loss indication from the tracking loop.

Indicates that the selected reference clock of the tracking loop is lost.
RO 0
2 HFXTAMPGOOD HFXT amplitude good indication. RO 0
1 HFXTFAULT HFXT fault indication.

Indicates that HFXT did not start correctly, or its frequency is too low.
HFXT will not recover from this fault and has to be restarted.
This is only a one-time check at HFXT startup.
RO 0
0 HFXTGOOD HFXT good indication.

Indicates that HFXT started correctly. The frequency is not necessarily good enough for radio operation.
This is only a one-time check at HFXT startup.
RO 0

TOP:CKMD:MIS

Address Offset 0x0000 004C
Physical Address 0x4000 104C Instance 0x4000 104C
Description Masked interrupt status.

This register is simply a bitwise AND of the contents of IMASK and RIS.*] registers. A flag set in this register can be cleared by writing 1 to the corresponding ICLR register bit.
Type RO
Bits Field Name Description Type Reset
31:18 RESERVED18 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b00 0000 0000 0000
17 LFTICK 32kHz TICK to RTC and WDT.

Either derived from selected LFCLK or generated from CLKULL in absence of LFCLK.
RO 0
16 LFGEARRSTRT LFINC filter gearing restart.

Indicates that the LFINC filter restarted gearing. Subsequent LFINC estimates may have higher variation.
RO 0
15 AMPSETTLED HFXT Amplitude compensation - settled

Indicates that the amplitude compensation FSM has reached the SETTLED or TCXOMODE state,
and the controls configured in HFXTTARG or HFXTDYN are reached.
RO 0
14 AMPCTRLATTARG HFXT Amplitude compensation - controls at target

Indicates that the control values configured in HFXTTARG or HFXTDYN are reached.
Applies to Q1CAP, Q2CAP and IREF.
RO 0
13 PRELFEDGE Pre-LF clock edge detect.

Indicates that a positive edge occured on the selected pre-LF clock LFCLKSEL.PRE.
Can be used by software to confirm that a LF clock source is running and within the expected frequency,
before selecting it as the main LF clock source.
RO 0
12 LFCLKLOSS LF clock is lost.

Indicates that no LF clock edge occured for ~49us (~1.6 times nominal period).
The system will automatically fall-back to generating LFTICK based on CLKULL,
to avoid timing corruption.
Note that this signal is NOT related to the analog LF clock-loss detector which can reset the device during STANDBY.
RO 0
11 LFCLKOOR LF clock period out-of-range.

Indicates that a LF clock period was measured to be out-of-range,
according to LFQUALCTL.MAXERR.
RO 0
10 LFCLKGOOD LF clock good.

Indicates that the LF clock is good, according to the configuration in LFQUALCTL.
RO 0
9 LFINCUPD LFINC updated.

Indicates that a new LFINC measurement value is available in LFCLKSTAT.LFINC.
RO 0
8 TDCDONE TDC done event.

Indicates that the TDC measurement is done.
RO 0
7 ADCPEAKUPD HFXT-ADC PEAK measurement update event.

Indicates that the HFXT-ADC PEAK measurement is done.
RO 0
6 ADCBIASUPD HFXT-ADC BIAS measurement update event.

Indicates that the HFXT-ADC BIAS measurement is done.
RO 0
5 ADCCOMPUPD HFXT-ADC comparison update event.

Indicates that the HFXT-ADC comparison is done.
RO 0
4 TRACKREFOOR Out-of-range indication from the tracking loop.

Indicates that the selected reference clock frequency of the tracking loop is out-of-range.
RO 0
3 TRACKREFLOSS Clock loss indication from the tracking loop.

Indicates that the selected reference clock of the tracking loop is lost.
RO 0
2 HFXTAMPGOOD HFXT amplitude good indication. RO 0
1 HFXTFAULT HFXT fault indication.

Indicates that HFXT did not start correctly, or its frequency is too low.
HFXT will not recover from this fault and has to be restarted.
This is only a one-time check at HFXT startup.
RO 0
0 HFXTGOOD HFXT good indication.

Indicates that HFXT started correctly. The frequency is not necessarily good enough for radio operation.
This is only a one-time check at HFXT startup.
RO 0

TOP:CKMD:ISET

Address Offset 0x0000 0050
Physical Address 0x4000 1050 Instance 0x4000 1050
Description Interrupt set register.

This register can used by software for diagnostics and safety checking purposes. Writing a 1 to a bit in this register will set the event and the corresponding RIS bit also gets set. If the corresponding IMASK bit is set, then the corresponding MIS register bit also gets set.
Type WO
Bits Field Name Description Type Reset
31:18 RESERVED18 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b00 0000 0000 0000
17 LFTICK 32kHz TICK to RTC and WDT.

Either derived from selected LFCLK or generated from CLKULL in absence of LFCLK.
WO 0
16 LFGEARRSTRT LFINC filter gearing restart.

Indicates that the LFINC filter restarted gearing. Subsequent LFINC estimates may have higher variation.
WO 0
15 AMPSETTLED HFXT Amplitude compensation - settled

Indicates that the amplitude compensation FSM has reached the SETTLED or TCXOMODE state,
and the controls configured in HFXTTARG or HFXTDYN are reached.
WO 0
14 AMPCTRLATTARG HFXT Amplitude compensation - controls at target

Indicates that the control values configured in HFXTTARG.Q1CAP, HFXTTARG.Q2CAP and HFXTTARG.IREF or HFXTDYN.Q1CAP, HFXTDYN.Q2CAP and HFXTDYN.IREF are reached.
WO 0
13 PRELFEDGE Pre-LF clock edge detect.

Indicates that a positive edge occured on the selected pre-LF clock LFCLKSEL.PRE.
Can be used by software to confirm that a LF clock source is running and within the expected frequency,
before selecting it as the main LF clock source.
WO 0
12 LFCLKLOSS LF clock is lost.

Indicates that no LF clock edge occured for ~49us (~1.6 times nominal period).
The system will automatically fall-back to generating LFTICK based on CLKULL,
to avoid timing corruption.
Note that this signal is NOT related to the analog LF clock-loss detector which can reset the device during STANDBY.
WO 0
11 LFCLKOOR LF clock period out-of-range.

Indicates that a LF clock period was measured to be out-of-range,
according to LFQUALCTL.MAXERR.
WO 0
10 LFCLKGOOD LF clock good.

Indicates that the LF clock is good, according to the configuration in LFQUALCTL.
WO 0
9 LFINCUPD LFINC updated.

Indicates that a new LFINC measurement value is available in LFCLKSTAT.LFINC.
WO 0
8 TDCDONE TDC done event.

Indicates that the TDC measurement is done.
WO 0
7 ADCPEAKUPD HFXT-ADC PEAK measurement update event.

Indicates that the HFXT-ADC PEAK measurement is done.
WO 0
6 ADCBIASUPD HFXT-ADC BIAS measurement update event.

Indicates that the HFXT-ADC BIAS measurement is done.
WO 0
5 ADCCOMPUPD HFXT-ADC comparison update event.

Indicates that the HFXT-ADC comparison is done.
WO 0
4 TRACKREFOOR Out-of-range indication from the tracking loop.

Indicates that the selected reference clock frequency of the tracking loop is out-of-range.
WO 0
3 TRACKREFLOSS Clock loss indication from the tracking loop.

Indicates that the selected reference clock of the tracking loop is lost.
WO 0
2 HFXTAMPGOOD HFXT amplitude good indication. WO 0
1 HFXTFAULT HFXT fault indication.

Indicates that HFXT did not start correctly, or its frequency is too low.
HFXT will not recover from this fault and has to be restarted.
This is only a one-time check at HFXT startup.
WO 0
0 HFXTGOOD HFXT good indication.

Indicates that HFXT started correctly. The frequency is not necessarily good enough for radio operation.
This is only a one-time check at HFXT startup.
WO 0

TOP:CKMD:ICLR

Address Offset 0x0000 0054
Physical Address 0x4000 1054 Instance 0x4000 1054
Description Interrupt clear register.

This register allows software to clear interrupts. Writing a 1 to a bit in this register will clear the event and the corresponding RIS bit also gets cleared. If the corresponding IMASK bit is set, then the corresponding MIS register bit also gets cleared.
Type WO
Bits Field Name Description Type Reset
31:18 RESERVED18 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b00 0000 0000 0000
17 LFTICK 32kHz TICK to RTC and WDT.

Either derived from selected LFCLK or generated from CLKULL in absence of LFCLK.
WO 0
16 LFGEARRSTRT LFINC filter gearing restart.

Indicates that the LFINC filter restarted gearing. Subsequent LFINC estimates may have higher variation.
WO 0
15 AMPSETTLED HFXT Amplitude compensation - settled

Indicates that the amplitude compensation FSM has reached the SETTLED or TCXOMODE state,
and the controls configured in HFXTTARG or HFXTDYN are reached.
WO 0
14 AMPCTRLATTARG HFXT Amplitude compensation - controls at target

Indicates that the control values configured in HFXTTARG or HFXTDYN are reached.
Applies to Q1CAP, Q2CAP and IREF.
WO 0
13 PRELFEDGE Pre-LF clock edge detect.

Indicates that a positive edge occured on the selected pre-LF clock LFCLKSEL.PRE.
Can be used by software to confirm that a LF clock source is running and within the expected frequency,
before selecting it as the main LF clock source.
WO 0
12 LFCLKLOSS LF clock is lost.

Indicates that no LF clock edge occured for ~49us (~1.6 times nominal period).
The system will automatically fall-back to generating LFTICK based on CLKULL,
to avoid timing corruption.
Note that this signal is NOT related to the analog LF clock-loss detector which can reset the device during STANDBY.
WO 0
11 LFCLKOOR LF clock period out-of-range.

Indicates that a LF clock period was measured to be out-of-range,
according to LFQUALCTL.MAXERR.
WO 0
10 LFCLKGOOD LF clock good.

Indicates that the LF clock is good, according to the configuration in LFQUALCTL.
WO 0
9 LFINCUPD LFINC updated.

Indicates that a new LFINC measurement value is available in LFCLKSTAT.LFINC.
WO 0
8 TDCDONE TDC done event.

Indicates that the TDC measurement is done.
WO 0
7 ADCPEAKUPD HFXT-ADC PEAK measurement update event.

Indicates that the HFXT-ADC PEAK measurement is done.
WO 0
6 ADCBIASUPD HFXT-ADC BIAS measurement update event.

Indicates that the HFXT-ADC BIAS measurement is done.
WO 0
5 ADCCOMPUPD HFXT-ADC comparison update event.

Indicates that the HFXT-ADC comparison is done.
WO 0
4 TRACKREFOOR Out-of-range indication from the tracking loop.

Indicates that the selected reference clock frequency of the tracking loop is out-of-range.
WO 0
3 TRACKREFLOSS Clock loss indication from the tracking loop.

Indicates that the selected reference clock of the tracking loop is lost.
WO 0
2 HFXTAMPGOOD HFXT amplitude good indication. WO 0
1 HFXTFAULT HFXT fault indication.

Indicates that HFXT did not start correctly, or its frequency is too low.
HFXT will not recover from this fault and has to be restarted.
This is only a one-time check at HFXT startup.
WO 0
0 HFXTGOOD HFXT good indication.

Indicates that HFXT started correctly. The frequency is not necessarily good enough for radio operation.
This is only a one-time check at HFXT startup.
WO 0

TOP:CKMD:IMSET

Address Offset 0x0000 0058
Physical Address 0x4000 1058 Instance 0x4000 1058
Description Interrupt mask set register.

Writing a 1 to a bit in this register will set the corresponding IMASK bit.
Type WO
Bits Field Name Description Type Reset
31:18 RESERVED18 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b00 0000 0000 0000
17 LFTICK 32kHz TICK to RTC and WDT.

Either derived from selected LFCLK or generated from CLKULL in absence of LFCLK.
WO 0
16 LFGEARRSTRT LFINC filter gearing restart.

Indicates that the LFINC filter restarted gearing. Subsequent LFINC estimates may have higher variation.
WO 0
15 AMPSETTLED HFXT Amplitude compensation - settled

Indicates that the amplitude compensation FSM has reached the SETTLED or TCXOMODE state,
and the controls configured in HFXTTARG or HFXTDYN are reached.
WO 0
14 AMPCTRLATTARG HFXT Amplitude compensation - controls at target

Indicates that the control values configured in HFXTTARG or HFXTDYN are reached.
Applies to Q1CAP, Q2CAP and IREF.
WO 0
13 PRELFEDGE Pre-LF clock edge detect.

Indicates that a positive edge occured on the selected pre-LF clock LFCLKSEL.PRE.
Can be used by software to confirm that a LF clock source is running and within the expected frequency,
before selecting it as the main LF clock source.
WO 0
12 LFCLKLOSS LF clock is lost.

Indicates that no LF clock edge occured for ~49us (~1.6 times nominal period).
The system will automatically fall-back to generating LFTICK based on CLKULL,
to avoid timing corruption.
Note that this signal is NOT related to the analog LF clock-loss detector which can reset the device during STANDBY.
WO 0
11 LFCLKOOR LF clock period out-of-range.

Indicates that a LF clock period was measured to be out-of-range,
according to LFQUALCTL.MAXERR.
WO 0
10 LFCLKGOOD LF clock good.

Indicates that the LF clock is good, according to the configuration in LFQUALCTL.
WO 0
9 LFINCUPD LFINC updated.

Indicates that a new LFINC measurement value is available in LFCLKSTAT.LFINC.
WO 0
8 TDCDONE TDC done event.

Indicates that the TDC measurement is done.
WO 0
7 ADCPEAKUPD HFXT-ADC PEAK measurement update event.

Indicates that the HFXT-ADC PEAK measurement is done.
WO 0
6 ADCBIASUPD HFXT-ADC BIAS measurement update event.

Indicates that the HFXT-ADC BIAS measurement is done.
WO 0
5 ADCCOMPUPD HFXT-ADC comparison update event.

Indicates that the HFXT-ADC comparison is done.
WO 0
4 TRACKREFOOR Out-of-range indication from the tracking loop.

Indicates that the selected reference clock frequency of the tracking loop is out-of-range.
WO 0
3 TRACKREFLOSS Clock loss indication from the tracking loop.

Indicates that the selected reference clock of the tracking loop is lost.
WO 0
2 HFXTAMPGOOD HFXT amplitude good indication. WO 0
1 HFXTFAULT HFXT fault indication.

Indicates that HFXT did not start correctly, or its frequency is too low.
HFXT will not recover from this fault and has to be restarted.
This is only a one-time check at HFXT startup.
WO 0
0 HFXTGOOD HFXT good indication.

Indicates that HFXT started correctly. The frequency is not necessarily good enough for radio operation.
This is only a one-time check at HFXT startup.
WO 0

TOP:CKMD:IMCLR

Address Offset 0x0000 005C
Physical Address 0x4000 105C Instance 0x4000 105C
Description Interrupt mask clear register.

Writing a 1 to a bit in this register will clear the corresponding IMASK bit.
Type WO
Bits Field Name Description Type Reset
31:18 RESERVED18 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b00 0000 0000 0000
17 LFTICK 32kHz TICK to RTC and WDT.

Either derived from selected LFCLK or generated from CLKULL in absence of LFCLK.
WO 0
16 LFGEARRSTRT LFINC filter gearing restart.

Indicates that the LFINC filter restarted gearing. Subsequent LFINC estimates may have higher variation.
WO 0
15 AMPSETTLED HFXT Amplitude compensation - settled

Indicates that the amplitude compensation FSM has reached the SETTLED or TCXOMODE state,
and the controls configured in HFXTTARG or HFXTDYN are reached.
WO 0
14 AMPCTRLATTARG HFXT Amplitude compensation - controls at target

Indicates that the control values configured in HFXTTARG or HFXTDYN are reached.
Applies to Q1CAP, Q2CAP and IREF.
WO 0
13 PRELFEDGE Pre-LF clock edge detect.

Indicates that a positive edge occured on the selected pre-LF clock LFCLKSEL.PRE.
Can be used by software to confirm that a LF clock source is running and within the expected frequency,
before selecting it as the main LF clock source.
WO 0
12 LFCLKLOSS LF clock is lost.

Indicates that no LF clock edge occured for ~49us (~1.6 times nominal period).
The system will automatically fall-back to generating LFTICK based on CLKULL,
to avoid timing corruption.
Note that this signal is NOT related to the analog LF clock-loss detector which can reset the device during STANDBY.
WO 0
11 LFCLKOOR LF clock period out-of-range.

Indicates that a LF clock period was measured to be out-of-range,
according to LFQUALCTL.MAXERR.
WO 0
10 LFCLKGOOD LF clock good.

Indicates that the LF clock is good, according to the configuration in LFQUALCTL.
WO 0
9 LFINCUPD LFINC updated.

Indicates that a new LFINC measurement value is available in LFCLKSTAT.LFINC.
WO 0
8 TDCDONE TDC done event.

Indicates that the TDC measurement is done.
WO 0
7 ADCPEAKUPD HFXT-ADC PEAK measurement update event.

Indicates that the HFXT-ADC PEAK measurement is done.
WO 0
6 ADCBIASUPD HFXT-ADC BIAS measurement update event.

Indicates that the HFXT-ADC BIAS measurement is done.
WO 0
5 ADCCOMPUPD HFXT-ADC comparison update event.

Indicates that the HFXT-ADC comparison is done.
WO 0
4 TRACKREFOOR Out-of-range indication from the tracking loop.

Indicates that the selected reference clock frequency of the tracking loop is out-of-range.
WO 0
3 TRACKREFLOSS Clock loss indication from the tracking loop.

Indicates that the selected reference clock of the tracking loop is lost.
WO 0
2 HFXTAMPGOOD HFXT amplitude good indication. WO 0
1 HFXTFAULT HFXT fault indication.

Indicates that HFXT did not start correctly, or its frequency is too low.
HFXT will not recover from this fault and has to be restarted.
This is only a one-time check at HFXT startup.
WO 0
0 HFXTGOOD HFXT good indication.

Indicates that HFXT started correctly. The frequency is not necessarily good enough for radio operation.
This is only a one-time check at HFXT startup.
WO 0

TOP:CKMD:HFOSCCTL

Address Offset 0x0000 0080
Physical Address 0x4000 1080 Instance 0x4000 1080
Description Internal. Only to be used through TI provided API.
Type RW
Bits Field Name Description Type Reset
31:24 PW Internal. Only to be used through TI provided API. WO 0x00
23:9 RESERVED9 Internal. Only to be used through TI provided API. RO 0b000 0000 0000 0000
8 CLKSVTOVR Internal. Only to be used through TI provided API.
Value ENUM Name Description
0x0 HFOSC Internal. Only to be used through TI provided API.
0x1 HFXT Internal. Only to be used through TI provided API.
RW 0
7:2 RESERVED2 Internal. Only to be used through TI provided API. RO 0b00 0000
1 FORCEOFF Internal. Only to be used through TI provided API. RW 0
0 QUALBYP Internal. Only to be used through TI provided API. RW 0

TOP:CKMD:HFXTCTL

Address Offset 0x0000 0084
Physical Address 0x4000 1084 Instance 0x4000 1084
Description High frequency crystal control
Type RW
Bits Field Name Description Type Reset
31 AMPOVR Internal. Only to be used through TI provided API. RW 0
30:27 RESERVED27 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x0
26 BIASEN Internal. Only to be used through TI provided API. RW 0
25 LPBUFEN Internal. Only to be used through TI provided API. RW 0
24 INJECT Internal. Only to be used through TI provided API. RW 0
23 QUALBYP Internal. Only to be used through TI provided API. RW 0
22:20 RESERVED20 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000
19:8 QUALDLY Skip potentially unstable clock cycles after enabling HFXT.
Number of cycles skipped is 8*QUALDLY.
RW 0x000
7 TCXOMODE Temperature compensated crystal oscillator mode.

Set this bit if a TXCO is connected.
RW 0
6 TCXOTYPE Type of temperature compensated crystal used.

Only has effect if TCXOMODE is set.
Value ENUM Name Description
0x0 CLIPPEDSINE Use with clipped-sine TCXO
0x1 CMOS Use with CMOS TCXO
RW 0
5:3 RESERVED3 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000
2 AUTOEN Internal. Only to be used through TI provided API. RW 0
1 HPBUFEN High performance clock buffer enable.

This bit controls the clock output for the RF PLL.
It is required for radio operation.
RW 0
0 EN Internal. Only to be used through TI provided API. RW 0

TOP:CKMD:LFOSCCTL

Address Offset 0x0000 008C
Physical Address 0x4000 108C Instance 0x4000 108C
Description Low frequency oscillator control
Type RW
Bits Field Name Description Type Reset
31:1 RESERVED1 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000 0000 0000 0000 0000 0000 0000
0 EN LFOSC enable RW 0

TOP:CKMD:LFXTCTL

Address Offset 0x0000 0090
Physical Address 0x4000 1090 Instance 0x4000 1090
Description Low frequency crystal control
Type RW
Bits Field Name Description Type Reset
31:15 RESERVED15 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b0 0000 0000 0000 0000
14:13 LEAKCOMP Leakage compensation control
Value ENUM Name Description
0x0 FULL Full leakage compensation
0x1 HALF Half leakage compensation
0x3 OFF No leakage compensation
RW 0b00
12 BUFBIAS Control the BIAS current of the input amp in LP buffer
Value ENUM Name Description
0x0 MIN Minimum bias current: 25nA
0x1 MAX Maximum bias current: 50nA
RW 0
11:8 AMPBIAS Adjust current mirror ratio into oscillator core. This value is depending on crystal and is set by FW. This field uses a 2's complement encoding. RW 0x0
7:6 BIASBOOST Boost oscillator amplitude

This value depends on the crystal and needs to be configured by Firmware.
RW 0b00
5:4 REGBIAS Regulation loop bias resistor value

This value depends on the crystal and needs to be configured by Firmware.
RW 0b00
3 RESERVED3 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0
2 HPBUFEN Control the buffer used. In normal operation, low-power buffer is used in all device modes. The high-performance buffer is only used for test purposes. RW 0
1 AMPREGMODE Amplitude regulation mode
Value ENUM Name Description
0x0 LOOPEN Amplitude control loop enabled
0x1 LOOPDIS Amplitude control loop disabled
RW 0
0 EN LFXT enable RW 0

TOP:CKMD:LFQUALCTL

Address Offset 0x0000 0094
Physical Address 0x4000 1094 Instance 0x4000 1094
Description Low frequency clock qualification control
Type RW
Bits Field Name Description Type Reset
31:14 RESERVED14 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b00 0000 0000 0000 0000
13:8 MAXERR Maximum LFCLK period error.

Value given in microseconds, 3 integer bits + 3 fractional bits.
RW 0b10 0000
7:0 CONSEC Number of consecutive times the LFCLK period error has to be
smaller than MAXERR to be considered "good".
Setting this value to 0 will bypass clock qualification,
and the "good" indicator will always be 1.
RW 0x64

TOP:CKMD:LFINCCTL

Address Offset 0x0000 0098
Physical Address 0x4000 1098 Instance 0x4000 1098
Description Low frequency time increment control
Type RW
Bits Field Name Description Type Reset
31 PREVENTSTBY Controls if the LFINC filter prevents STANBY entry until settled.
Value ENUM Name Description
0x0 OFF Disable. Do not prevent STANDBY entry.
0x1 ON Enable. Prevent STANDBY entry.
RW 1
30 RESERVED30 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0
29:8 INT Integral part of the LFINC filter.

This value is updated by Hardware to reflect the current state of the filter.
It can also be written to change the current state.
RW 0b01 1110 1000 0100 1000 0000
7 STOPGEAR Controls the final gear of the LFINC filter.
Value ENUM Name Description
0x0 LOW Lowest final gear. Best settling, but less dynamic frequency tracking.
0x1 HIGH Highest final gear. Best dynamic frequency tracking, but higher variation in filter value.
RW 0
6:5 ERRTHR Controls the threshold for gearing restart of the LFINC filter.

Only effective if GEARRSTRT is not ONETHR or TWOTHR.
Value ENUM Name Description
0x0 LARGE Restart gearing on large error. Fewer false restarts, slower response on small frequency shifts.
0x1 MIDLARGE Middle value towards LARGE.
0x2 MIDSMALL Middle value towards SMALL.
0x3 SMALL Restart gearing on small error. Potentially more false restarts, faster response on small frequency shifts.
RW 0b00
4:3 GEARRSTRT Controls gearing restart of the LFINC filter.
Value ENUM Name Description
0x0 NEVER Never restart gearing. Very stable filter value, but very slow response on frequency changes.
0x1 ONETHR Restart gearing when the error accumulator crosses the threshold once.
0x2 TWOTHR Restart gearing when the error accumulator crosses the threshold twice in a row.
RW 0b10
2 SOFTRSTRT Use a higher gear after re-enabling / wakeup.

The filter will require 16-24 LFCLK periods to settle (depending on STOPGEAR), but may respond faster to frequency changes during STANDBY.
Value ENUM Name Description
0x0 OFF Don't use soft gearing restarts
0x1 ON Use soft gearing restarts
RW 1
1:0 RESERVED0 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b00

TOP:CKMD:LFINCOVR

Address Offset 0x0000 009C
Physical Address 0x4000 109C Instance 0x4000 109C
Description Low frequency time increment override control
Type RW
Bits Field Name Description Type Reset
31 OVERRIDE Override LF increment

Use the value provided in LFINC instead of the value calculated by Hardware.
RW 0
30:22 RESERVED22 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b0 0000 0000
21:0 LFINC LF increment value

This value is used when OVERRIDE is set to 1.
Otherwise the value is calculated automatically.
RW 0b00 0000 0000 0000 0000 0000

TOP:CKMD:AMPADCCTL

Address Offset 0x0000 00A0
Physical Address 0x4000 10A0 Instance 0x4000 10A0
Description Internal. Only to be used through TI provided API.
Type RW
Bits Field Name Description Type Reset
31 SWOVR Internal. Only to be used through TI provided API. RW 0
30:18 RESERVED18 Internal. Only to be used through TI provided API. RO 0b0 0000 0000 0000
17 PEAKDETEN Internal. Only to be used through TI provided API.
Value ENUM Name Description
0x0 DISABLE Internal. Only to be used through TI provided API.
0x1 ENABLE Internal. Only to be used through TI provided API.
RW 0
16 ADCEN Internal. Only to be used through TI provided API.
Value ENUM Name Description
0x0 DISABLE Internal. Only to be used through TI provided API.
0x1 ENABLE Internal. Only to be used through TI provided API.
RW 0
15 RESERVED15 Internal. Only to be used through TI provided API. RO 0
14:8 COMPVAL Internal. Only to be used through TI provided API. RW 0b000 0000
7:5 RESERVED5 Internal. Only to be used through TI provided API. RO 0b000
4 SRCSEL Internal. Only to be used through TI provided API.
Value ENUM Name Description
0x0 BIAS Internal. Only to be used through TI provided API.
0x1 PEAK Internal. Only to be used through TI provided API.
RW 0
3:2 RESERVED2 Internal. Only to be used through TI provided API. RO 0b00
1 COMPSTRT Internal. Only to be used through TI provided API. RW 0
0 SARSTRT Internal. Only to be used through TI provided API. RW 0

TOP:CKMD:HFTRACKCTL

Address Offset 0x0000 00A4
Physical Address 0x4000 10A4 Instance 0x4000 10A4
Description High frequency tracking loop control
Type RW
Bits Field Name Description Type Reset
31 EN Enable tracking loop. RW 0
30 DSMBYP Bypass Delta-Sigma-Modulation of fine trim. RW 0
29:28 RESERVED28 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b00
27:26 REFCLK Select the reference clock for the tracking loop.
Change only while the tracking loop is disabled.
Value ENUM Name Description
0x0 HFXT Select HFXT as reference clock.
0x1 LRF Select LRF reference clock.
0x2 GPI Select GPI as reference clock.
RW 0b00
25:0 RATIO Reference clock ratio.

RATIO = 24MHz / (2*reference-frequency) * 2^24
Commonly used reference clock frequencies are provided as enumerations.
Value ENUM Name Description
0x400000 REF48M Use for 48MHz reference clock
0x1800000 REF8M Use for 8MHz reference clock
0x3000000 REF4M Use for 4MHz reference clock
RW 0b00 0100 0000 0000 0000 0000 0000

TOP:CKMD:LDOCTL

Address Offset 0x0000 00A8
Physical Address 0x4000 10A8 Instance 0x4000 10A8
Description Internal. Only to be used through TI provided API.
Type RW
Bits Field Name Description Type Reset
31 SWOVR Internal. Only to be used through TI provided API. RW 0
30:5 RESERVED5 Internal. Only to be used through TI provided API. RO 0b00 0000 0000 0000 0000 0000 0000
4 HFXTLVLEN Internal. Only to be used through TI provided API. RW 0
3 STARTCTL Internal. Only to be used through TI provided API. RW 0
2 START Internal. Only to be used through TI provided API. RW 0
1 BYPASS Internal. Only to be used through TI provided API. RW 0
0 EN Internal. Only to be used through TI provided API. RW 0

TOP:CKMD:NABIASCTL

Address Offset 0x0000 00AC
Physical Address 0x4000 10AC Instance 0x4000 10AC
Description Nanoamp-bias control
Type RW
Bits Field Name Description Type Reset
31:1 RESERVED1 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000 0000 0000 0000 0000 0000 0000
0 EN Enable nanoamp-bias RW 0

TOP:CKMD:LFMONCTL

Address Offset 0x0000 00B0
Physical Address 0x4000 10B0 Instance 0x4000 10B0
Description Low-frequency clock-monitor control
Type RW
Bits Field Name Description Type Reset
31:1 RESERVED1 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000 0000 0000 0000 0000 0000 0000
0 EN Enable LFMONITOR.
Enable only after a LF clock source has been selected, enabled and is stable.
If LFMONITOR detects a clock loss, the system will be reset.
RW 0

TOP:CKMD:LFCLKSEL

Address Offset 0x0000 00C0
Physical Address 0x4000 10C0 Instance 0x4000 10C0
Description Low frequency clock selection
Type RW
Bits Field Name Description Type Reset
31:4 RESERVED4 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x000 0000
3:2 PRE Select low frequency clock source for the PRELFCLK interrupt.

Can be used by Software to confirm that the clock is running and it's frequency is good, before selecting it in MAIN.
Value ENUM Name Description
0x0 NONE No clock. Output will be tied low.
0x1 LFOSC Low frequency on-chip oscillator
0x2 LFXT Low frequency crystal oscillator
0x3 EXTLF External LF clock through GPI.
RW 0b00
1:0 MAIN Select the main low frequency clock source.

If running, this clock will be used to generate LFTICK and as CLKULL during STANDBY.
If not running, LFTICK will be generated from HFOSC and STANDBY entry will be prevented.
Value ENUM Name Description
0x0 FAKE No LF clock selected. LFTICK will be generated from HFOSC, STANDBY entry will be prevented.
0x1 LFOSC Low frequency on-chip oscillator
0x2 LFXT Low frequency crystal oscillator
0x3 EXTLF External LF clock through GPI.
RW 0b00

TOP:CKMD:TDCCLKSEL

Address Offset 0x0000 00C4
Physical Address 0x4000 10C4 Instance 0x4000 10C4
Description Internal. Only to be used through TI provided API.
Type RW
Bits Field Name Description Type Reset
31:2 RESERVED2 Internal. Only to be used through TI provided API. RO 0b00 0000 0000 0000 0000 0000 0000 0000
1:0 REFCLK Internal. Only to be used through TI provided API.
Value ENUM Name Description
0x0 NONE Internal. Only to be used through TI provided API.
0x1 CLKSVT Internal. Only to be used through TI provided API.
0x2 CLKULL Internal. Only to be used through TI provided API.
0x3 GPI Internal. Only to be used through TI provided API.
RW 0b00

TOP:CKMD:ADCCLKSEL

Address Offset 0x0000 00C8
Physical Address 0x4000 10C8 Instance 0x4000 10C8
Description ADC clock selection
Type RW
Bits Field Name Description Type Reset
31:2 RESERVED2 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b00 0000 0000 0000 0000 0000 0000 0000
1:0 SRC Select ADC clock source

Change only while ADC is disabled.
Value ENUM Name Description
0x0 CLKSVT 48MHz CLKSVT
0x1 HFXT 48MHz HFXT
RW 0b00

TOP:CKMD:LFCLKSTAT

Address Offset 0x0000 00E0
Physical Address 0x4000 10E0 Instance 0x4000 10E0
Description Low-frequency clock status
Type RO
Bits Field Name Description Type Reset
31 GOOD Low frequency clock good

Note: This is only a coarse frequency check based on LFQUALCTL. The clock may not be accurate enough for timing purposes.
RO 0
30:26 RESERVED26 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b0 0000
25 FLTSETTLED LFINC filter is running and settled. RO 0
24 LFTICKSRC Source of LFTICK.
Value ENUM Name Description
0x0 LFCLK LFTICK generated from the selected LFCLK
0x1 FAKE LFTICK generated from CLKULL (LFCLK not available)
RO 0
23:22 LFINCSRC Source of LFINC used by the RTC.

This value depends on LFINCOVR.OVERRIDE, LF clock availability, HF tracking loop status and the device state (ACTIVE/STANDBY).
Value ENUM Name Description
0x0 MEAS Using measured value.
This value is updated by hardware and can be read from LFINC.
0x1 AVG Using filtered / average value.
This value is updated by hardware and can be read and updated in LFINCCTL.INT.
0x2 OVERRIDE Using override value from LFINCOVR.LFINC
0x3 FAKE Using FAKE LFTICKs with corresponding LFINC value.
RO 0b00
21:0 LFINC Measured value of LFINC.

Given in microseconds with 16 fractional bits.
This value is calculated by Hardware.
It is the LFCLK period according to CLKULL cycles.
RO 0b00 0000 0000 0000 0000 0000

TOP:CKMD:HFXTSTAT

Address Offset 0x0000 00E4
Physical Address 0x4000 10E4 Instance 0x4000 10E4
Description HFXT status information
Type RO
Bits Field Name Description Type Reset
31 RESERVED31 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0
30:16 STARTUPTIME HFXT startup time

Can be used by software to plan starting HFXT ahead in time.
Measured whenever HFXT is enabled in CLKULL periods (24MHz), from HFXTCTL.EN until the clock is good for radio operation (amplitude compensation is settled).
RO 0b000 0000 0000 0000
15:2 RESERVED2 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b00 0000 0000 0000
1 FAULT HFXT clock fault

Indicates a lower than expected HFXT frequency.
HFXT will not recover from this fault, disabling and re-enabling HFXT is required.
RO 0
0 GOOD HFXT clock available.

The frequency is not necessarily good enough for radio operation.
RO 0

TOP:CKMD:AMPADCSTAT

Address Offset 0x0000 00E8
Physical Address 0x4000 10E8 Instance 0x4000 10E8
Description Internal. Only to be used through TI provided API.
Type RO
Bits Field Name Description Type Reset
31:25 RESERVED25 Internal. Only to be used through TI provided API. RO 0b000 0000
24 COMPOUT Internal. Only to be used through TI provided API. RO 0
23 RESERVED23 Internal. Only to be used through TI provided API. RO 0
22:16 PEAKRAW Internal. Only to be used through TI provided API. RO 0b000 0000
15:8 PEAK Internal. Only to be used through TI provided API. RO 0x00
7 RESERVED7 Internal. Only to be used through TI provided API. RO 0
6:0 BIAS Internal. Only to be used through TI provided API. RO 0b000 0000

TOP:CKMD:TRACKSTAT

Address Offset 0x0000 00EC
Physical Address 0x4000 10EC Instance 0x4000 10EC
Description HFOSC tracking loop status information
Type RW
Bits Field Name Description Type Reset
31 LOOPERRVLD Current HFOSC tracking error valid

This bit is one if the tracking loop is running and the error value is valid.
RO 0
30 RESERVED30 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0
29:16 LOOPERR Current HFOSC tracking error RO 0b00 0000 0000 0000
15:13 RESERVED13 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000
12:0 FINETRIM Current HFOSC Fine-trim value

This field uses the internal fractional representation (sign, 4 integer bits, 8 fractional bits).
The actual trim value applied to the oscillator is delta-sigma modulated 5 bits non-signed
(inverted sign bit + integer bits).
RO 0b0 0000 0000 0000

TOP:CKMD:AMPSTAT

Address Offset 0x0000 00F0
Physical Address 0x4000 10F0 Instance 0x4000 10F0
Description HFXT Amplitude Compensation Status
Type RO
Bits Field Name Description Type Reset
31:29 RESERVED29 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000
28:25 STATE Current AMPCOMP FSM state.
Value ENUM Name Description
0x0 IDLE FSM in idle state
0x1 LDOSTART Starting LDO
0x2 SHUTDN1 Second shutdown state
0x3 INJECT Injecting HFOSC for fast startup
0x4 RAMP1 Transition to HFXTTARG values
0x5 RAMP0 Initial amplitude ramping with HFXTINIT values
0x6 UPDATEDN Amplitude down correction
0x7 INJWAIT Post injection settle wait
0xA SHUTDN0 First shutdown state
0xC TXCOMODE TCXO settled state
0xE UPDATEUP Amplitude up correction
0xF SETTLED Settled state
RO 0x0
24:18 IDAC Current IDAC control value. RO 0b000 0000
17:14 IREF Current IREF control value. RO 0x0
13:8 Q2CAP Current Q2CAP control value. RO 0b00 0000
7:2 Q1CAP Current Q1CAP control value. RO 0b00 0000
1 CTRLATTARGET HFXT control values match target values.

This applies to IREF, Q1CAP, Q2CAP values.
RO 0
0 AMPGOOD HFXT amplitude good RO 0

TOP:CKMD:ATBCTL0

Address Offset 0x0000 0100
Physical Address 0x4000 1100 Instance 0x4000 1100
Description Internal. Only to be used through TI provided API.
Type RW
Bits Field Name Description Type Reset
31:19 RESERVED19 Internal. Only to be used through TI provided API. RO 0b0 0000 0000 0000
18:0 SEL Internal. Only to be used through TI provided API.
Value ENUM Name Description
0x0 OFF Internal. Only to be used through TI provided API.
0x1 HFXTANA Internal. Only to be used through TI provided API.
0x2 VDDCKM Internal. Only to be used through TI provided API.
0x4 LDOITEST Internal. Only to be used through TI provided API.
0x8 LFXTANA Internal. Only to be used through TI provided API.
0x10 ADCCOMPOUT Internal. Only to be used through TI provided API.
0x20 ADCCOMPIN Internal. Only to be used through TI provided API.
0x40 ADCDACOUT Internal. Only to be used through TI provided API.
0x80 NABIASITEST Internal. Only to be used through TI provided API.
0x100 HFOSCVREF Internal. Only to be used through TI provided API.
0x200 HFOSCVDDL Internal. Only to be used through TI provided API.
0x400 HFOSCIBIAS Internal. Only to be used through TI provided API.
0x800 LFOSCVDDL Internal. Only to be used through TI provided API.
0x1000 LFMONVTEST Internal. Only to be used through TI provided API.
0x10000 HFOSCTESTCLK Internal. Only to be used through TI provided API.
0x30000 HFXTTESTCLK Internal. Only to be used through TI provided API.
0x50000 LFOSCTESTCLK Internal. Only to be used through TI provided API.
0x70000 LFXTTESTCLK Internal. Only to be used through TI provided API.
RW 0b000 0000 0000 0000 0000

TOP:CKMD:ATBCTL1

Address Offset 0x0000 0104
Physical Address 0x4000 1104 Instance 0x4000 1104
Description Internal. Only to be used through TI provided API.
Type RW
Bits Field Name Description Type Reset
31:15 RESERVED15 Internal. Only to be used through TI provided API. RO 0b0 0000 0000 0000 0000
14:13 LFOSC Internal. Only to be used through TI provided API.
Value ENUM Name Description
0x0 OFF Internal. Only to be used through TI provided API.
0x1 TESTCLK Internal. Only to be used through TI provided API.
0x2 VDDLOCAL Internal. Only to be used through TI provided API.
0x3 BOTH Internal. Only to be used through TI provided API.
RW 0b00
12 NABIAS Internal. Only to be used through TI provided API. RW 0
11 RESERVED11 Internal. Only to be used through TI provided API. RO 0
10 LFXT Internal. Only to be used through TI provided API.
Value ENUM Name Description
0x0 OFF Internal. Only to be used through TI provided API.
0x1 TESTCLK Internal. Only to be used through TI provided API.
RW 0
9:8 LFMON Internal. Only to be used through TI provided API.
Value ENUM Name Description
0x0 OFF Internal. Only to be used through TI provided API.
0x1 TEST1 Internal. Only to be used through TI provided API.
0x2 TEST2 Internal. Only to be used through TI provided API.
RW 0b00
7 HFXT Internal. Only to be used through TI provided API. RW 0
6:1 RESERVED1 Internal. Only to be used through TI provided API. RO 0b00 0000
0 HFOSC Internal. Only to be used through TI provided API. RW 0

TOP:CKMD:DTBCTL

Address Offset 0x0000 0108
Physical Address 0x4000 1108 Instance 0x4000 1108
Description Digital test bus mux control
Type RW
Bits Field Name Description Type Reset
31:23 RESERVED23 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b0 0000 0000
22:18 DSEL2 Internal. Only to be used through TI provided API. RW 0b0 0000
17:13 DSEL1 Internal. Only to be used through TI provided API. RW 0b0 0000
12:8 DSEL0 Internal. Only to be used through TI provided API. RW 0b0 0000
7:4 CLKSEL Select clock to output on DTB[0]
Value ENUM Name Description
0x0 CLKULL Select CLKULL (24 MHz during ACTIVE, 32kHz during STANDBY)
0x1 CLKSVT Select CLKSVT (48 MHz)
0x2 CLKADC Select CLKADC (48 MHz)
0x4 TRACKREF Select tracking loop reference clock
0x7 LFCLK Select LFCLK (selected by LFCLKSEL.MAIN)
0xA HFOSC Select HFOSC after qualification
0xC HFXTBY8 Select HFXT divided by 8
0xD HFXT Select HFXT
0xE LFOSC Select LFOSC
0xF LFXT Select LFXT
RW 0x0
3:1 RESERVED1 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000
0 EN Enable DTB output RW 0

TOP:CKMD:TRIM0

Address Offset 0x0000 0110
Physical Address 0x4000 1110 Instance 0x4000 1110
Description Internal. Only to be used through TI provided API.
Type RW
Bits Field Name Description Type Reset
31:9 RESERVED9 Internal. Only to be used through TI provided API. RO 0b000 0000 0000 0000 0000 0000
8:5 HFOSC_CAP Internal. Only to be used through TI provided API. RW 0x0
4:0 HFOSC_COARSE Internal. Only to be used through TI provided API. RW 0b0 0000

TOP:CKMD:TRIM1

Address Offset 0x0000 0114
Physical Address 0x4000 1114 Instance 0x4000 1114
Description Internal. Only to be used through TI provided API.
Type RW
Bits Field Name Description Type Reset
31:30 HFXTSLICER Internal. Only to be used through TI provided API. RW 0b00
29:28 PEAKIBIAS Internal. Only to be used through TI provided API. RW 0b00
27 NABIAS_UDIGLDO Internal. Only to be used through TI provided API. RW 0
26:24 LDOBW Internal. Only to be used through TI provided API. RW 0b000
23:20 LDOFB Internal. Only to be used through TI provided API. RW 0x6
19:16 LFDLY Internal. Only to be used through TI provided API. RW 0xF
15 NABIAS_LFOSC Internal. Only to be used through TI provided API. RW 1
14:8 NABIAS_RES Internal. Only to be used through TI provided API. RW 0b001 0100
7:0 LFOSC_CAP Internal. Only to be used through TI provided API. RW 0xD6

TOP:CKMD:HFXTINIT

Address Offset 0x0000 0118
Physical Address 0x4000 1118 Instance 0x4000 1118
Description Initial values for HFXT ramping
Type RW
Bits Field Name Description Type Reset
31:30 RESERVED30 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b00
29:23 AMPTHR Amplitude threshold during HFXT ramping RW 0b010 1000
22:16 IDAC Initial HFXT IDAC current RW 0b111 1111
15:12 IREF Initial HFXT IREF current RW 0x8
11:6 Q2CAP Initial HFXT Q2 cap trim RW 0b00 0000
5:0 Q1CAP Initial HFXT Q1 cap trim RW 0b00 0000

TOP:CKMD:HFXTTARG

Address Offset 0x0000 011C
Physical Address 0x4000 111C Instance 0x4000 111C
Description Target values for HFXT ramping
Type RW
Bits Field Name Description Type Reset
31:30 AMPHYST ADC hysteresis used during IDAC updates.

Every AMPCFG1.INTERVAL, IDAC will be regulated
- up as long as ADC < AMPTHR
- down as long as ADC > AMPTHR+AMPHYST
RW 0b01
29:23 AMPTHR Minimum HFXT amplitude RW 0b010 1000
22:16 IDAC Minimum IDAC current RW 0b100 0110
15:12 IREF Target HFXT IREF current RW 0x4
11:6 Q2CAP Target HFXT Q2 cap trim RW 0b10 1101
5:0 Q1CAP Target HFXT Q1 cap trim RW 0b10 1101

TOP:CKMD:HFXTDYN

Address Offset 0x0000 0120
Physical Address 0x4000 1120 Instance 0x4000 1120
Description Alternative target values for HFXT configuration

Software can change these values to dynamically transition the HFXT configuration while HFXT is running.
Set SEL to select the alternative set of target values.
Type RW
Bits Field Name Description Type Reset
31 SEL Select the dynamic configuration.

Amplitude ramping will always happen using the values in HFXTINIT, and HFXTTARG.
Afterwards, this bit can be used to select between HFXTTARG and HFXTDYN.
Hardware will ensure a smooth transition of analog control signals.
Value ENUM Name Description
0x0 TARGET Select configuration in HFXTTARG.
0x1 DYNAMIC Select configuration in HFXTDYN.
RW 0
30 RESERVED30 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0
29:23 AMPTHR Minimum HFXT amplitude RW 0b010 1000
22:16 IDAC Minimum IDAC current RW 0b100 0110
15:12 IREF Target HFXT IREF current RW 0x4
11:6 Q2CAP Target HFXT Q2 cap trim RW 0b10 1101
5:0 Q1CAP Target HFXT Q1 cap trim RW 0b10 1101

TOP:CKMD:AMPCFG0

Address Offset 0x0000 0124
Physical Address 0x4000 1124 Instance 0x4000 1124
Description Amplitude Compensation Configuration 0
Type RW
Bits Field Name Description Type Reset
31:28 Q2DLY Q2CAP change delay.

Number of clock cycles to wait before changing Q2CAP by one step.
Clock frequency defined in FSMRATE.
RW 0x0
27:24 Q1DLY Q1CAP change delay.

Number of clock cycles to wait before changing Q1CAP by one step.
Clock frequency defined in FSMRATE.
RW 0x0
23:20 ADCDLY ADC and PEAKDET startup time.

Number of clock cycles to wait after enabling the PEAKDET and ADC before the first measurement.
Clock frequency defined in FSMRATE.
RW 0x3
19:15 LDOSTART LDO startup time.

Number of clock cycles to bypass the LDO resistors for faster startup.
Clock frequency defined in FSMRATE.
RW 0b0 1001
14:10 INJWAIT Inject HFOSC for faster HFXT startup.

This value specifies the number of clock cycles to wait after injection is done.
The clock speed is defined in FSMRATE.
RW 0b0 0010
9:5 INJTIME Inject HFOSC for faster HFXT startup.

This value specifies the number of clock cycles the injection is enabled.
The clock speed is defined in FSMRATE.
Set to 0 to disable injection.
RW 0b0 0100
4:0 FSMRATE Update rate for the AMPCOMP update rate.
Also affects the clock rate for the Amplitude ADC.

The update rate is 6MHz / (FSMRATE+1).
Value ENUM Name Description
0x0 _6M 6 MHz
0x1 _3M 3 MHz
0x2 _2M 2 MHz
0x5 _1M 1 MHz
0xB _500K 500 kHz
0x17 _250K 250 kHz
RW 0b0 0010

TOP:CKMD:AMPCFG1

Address Offset 0x0000 0128
Physical Address 0x4000 1128 Instance 0x4000 1128
Description Amplitude Compensation Configuration 1
Type RW
Bits Field Name Description Type Reset
31:28 IDACDLY IDAC change delay.

Time to wait before changing IDAC by one step.
This time needs to be long enough for the crystal to settle.
The number of clock cycles to wait is IDACDLY<<4 + 15.
Clock frequency defined in AMPCFG0.FSMRATE.
RW 0x2
27:24 IREFDLY IREF change delay.

Number of clock cycles to wait before changing IREF by one step.
Clock frequency defined in AMPCFG0.FSMRATE.
RW 0x6
23:12 BIASLT Lifetime of the amplitude ADC bias value.
This value specifies the number of adjustment intervals,
until the ADC bias value has to be measured again.
Set to 0 to disable automatic bias measurements.
RW 0x0FF
11:0 INTERVAL Interval for amplitude adjustments.
Set to 0 to disable periodic adjustments.

This value specifies the number of clock cycles between adjustments.
The clock speed is defined in AMPCFG0.FSMRATE.
RW 0x0FF

TOP:CKMD:LOOPCFG

Address Offset 0x0000 012C
Physical Address 0x4000 112C Instance 0x4000 112C
Description Configuration Register for the Tracking Loop
Type RW
Bits Field Name Description Type Reset
31:26 FINETRIM_INIT Initial value for the resistor fine trim RW 0b01 1000
25:21 BOOST_TARGET Number of error-updates using BOOST values, before using KI/KP RW 0b0 0010
20:18 KP_BOOST Proportional loop coefficient during BOOST RW 0b111
17:15 KI_BOOST Integral loop coefficient during BOOST RW 0b100
14:10 SETTLED_TARGET Number of updates before HFOSC is considered "settled" RW 0b0 1100
9:6 OOR_LIMIT Out-of-range threshold RW 0xE
5:3 KP Proportional loop coefficient RW 0b110
2:0 KI Integral loop coefficient RW 0b011

TOP:CKMD:TDCCTL

Address Offset 0x0000 0200
Physical Address 0x4000 1200 Instance 0x4000 1200
Description Internal. Only to be used through TI provided API.
Type RW
Bits Field Name Description Type Reset
31:2 RESERVED2 Internal. Only to be used through TI provided API. RO 0b00 0000 0000 0000 0000 0000 0000 0000
1:0 CMD Internal. Only to be used through TI provided API.
Value ENUM Name Description
0x0 CLR_RESULT Internal. Only to be used through TI provided API.
0x1 RUN_SYNC_START Internal. Only to be used through TI provided API.
0x2 RUN Internal. Only to be used through TI provided API.
0x3 ABORT Internal. Only to be used through TI provided API.
WO 0b00

TOP:CKMD:TDCSTAT

Address Offset 0x0000 0204
Physical Address 0x4000 1204 Instance 0x4000 1204
Description Internal. Only to be used through TI provided API.
Type RO
Bits Field Name Description Type Reset
31:10 RESERVED10 Internal. Only to be used through TI provided API. RO 0b00 0000 0000 0000 0000 0000
9 STOP_BF Internal. Only to be used through TI provided API. RO 0
8 START_BF Internal. Only to be used through TI provided API. RO 0
7 SAT Internal. Only to be used through TI provided API. RO 0
6 DONE Internal. Only to be used through TI provided API. RO 0
5:0 STATE Internal. Only to be used through TI provided API.
Value ENUM Name Description
0x0 WAIT_START Internal. Only to be used through TI provided API.
0x4 WAIT_START_STOP_CNT_EN Internal. Only to be used through TI provided API.
0x6 IDLE Internal. Only to be used through TI provided API.
0x7 CLR_CNT Internal. Only to be used through TI provided API.
0x8 WAIT_STOP Internal. Only to be used through TI provided API.
0xC WAIT_STOP_CNTDWN Internal. Only to be used through TI provided API.
0xE GET_RESULT Internal. Only to be used through TI provided API.
0xF POR Internal. Only to be used through TI provided API.
0x16 WAIT_CLR_CNT_DONE Internal. Only to be used through TI provided API.
0x1E START_FALL Internal. Only to be used through TI provided API.
0x2E FORCE_STOP Internal. Only to be used through TI provided API.
RO 0b00 0110

TOP:CKMD:TDCRESULT

Address Offset 0x0000 0208
Physical Address 0x4000 1208 Instance 0x4000 1208
Description Internal. Only to be used through TI provided API.
Type RO
Bits Field Name Description Type Reset
31:0 VALUE Internal. Only to be used through TI provided API. RO 0x0000 0002

TOP:CKMD:TDCSATCFG

Address Offset 0x0000 020C
Physical Address 0x4000 120C Instance 0x4000 120C
Description Internal. Only to be used through TI provided API.
Type RW
Bits Field Name Description Type Reset
31:5 RESERVED5 Internal. Only to be used through TI provided API. RO 0b000 0000 0000 0000 0000 0000 0000
4:0 LIMIT Internal. Only to be used through TI provided API.
Value ENUM Name Description
0x0 NONE Internal. Only to be used through TI provided API.
0x3 R12 Internal. Only to be used through TI provided API.
0x4 R13 Internal. Only to be used through TI provided API.
0x5 R14 Internal. Only to be used through TI provided API.
0x6 R15 Internal. Only to be used through TI provided API.
0x7 R16 Internal. Only to be used through TI provided API.
0x8 R17 Internal. Only to be used through TI provided API.
0x9 R18 Internal. Only to be used through TI provided API.
0xA R19 Internal. Only to be used through TI provided API.
0xB R20 Internal. Only to be used through TI provided API.
0xC R21 Internal. Only to be used through TI provided API.
0xD R22 Internal. Only to be used through TI provided API.
0xE R23 Internal. Only to be used through TI provided API.
0xF R24 Internal. Only to be used through TI provided API.
0x10 R25 Internal. Only to be used through TI provided API.
0x11 R26 Internal. Only to be used through TI provided API.
0x12 R27 Internal. Only to be used through TI provided API.
0x13 R28 Internal. Only to be used through TI provided API.
0x14 R29 Internal. Only to be used through TI provided API.
0x15 R30 Internal. Only to be used through TI provided API.
RW 0b0 0000

TOP:CKMD:TDCTRIGSRC

Address Offset 0x0000 0210
Physical Address 0x4000 1210 Instance 0x4000 1210
Description Internal. Only to be used through TI provided API.
Type RW
Bits Field Name Description Type Reset
31:16 RESERVED16 Internal. Only to be used through TI provided API. RO 0x0000
15 STOP_POL Internal. Only to be used through TI provided API.
Value ENUM Name Description
0x0 HIGH Internal. Only to be used through TI provided API.
0x1 LOW Internal. Only to be used through TI provided API.
RW 0
14:13 RESERVED13 Internal. Only to be used through TI provided API. RO 0b00
12:8 STOP_SRC Internal. Only to be used through TI provided API.
Value ENUM Name Description
0x0 LFTICK Internal. Only to be used through TI provided API.
0x1 LFOSC Internal. Only to be used through TI provided API.
0x2 LFXT Internal. Only to be used through TI provided API.
0x3 LFCLK_DLY Internal. Only to be used through TI provided API.
0x4 GPI Internal. Only to be used through TI provided API.
0x5 DTB0 Internal. Only to be used through TI provided API.
0x6 DTB1 Internal. Only to be used through TI provided API.
0x7 DTB2 Internal. Only to be used through TI provided API.
0x8 DTB3 Internal. Only to be used through TI provided API.
0x9 DTB4 Internal. Only to be used through TI provided API.
0xA DTB5 Internal. Only to be used through TI provided API.
0xB DTB6 Internal. Only to be used through TI provided API.
0xC DTB7 Internal. Only to be used through TI provided API.
0xD DTB8 Internal. Only to be used through TI provided API.
0xE DTB9 Internal. Only to be used through TI provided API.
0xF DTB10 Internal. Only to be used through TI provided API.
0x10 DTB11 Internal. Only to be used through TI provided API.
0x11 DTB12 Internal. Only to be used through TI provided API.
0x12 DTB13 Internal. Only to be used through TI provided API.
0x13 DTB14 Internal. Only to be used through TI provided API.
0x14 DTB15 Internal. Only to be used through TI provided API.
0x1F TDC_PRE Internal. Only to be used through TI provided API.
RW 0b0 0000
7 START_POL Internal. Only to be used through TI provided API.
Value ENUM Name Description
0x0 HIGH Internal. Only to be used through TI provided API.
0x1 LOW Internal. Only to be used through TI provided API.
RW 0
6:5 RESERVED5 Internal. Only to be used through TI provided API. RO 0b00
4:0 START_SRC Internal. Only to be used through TI provided API.
Value ENUM Name Description
0x0 LFTICK Internal. Only to be used through TI provided API.
0x1 LFOSC Internal. Only to be used through TI provided API.
0x2 LFXT Internal. Only to be used through TI provided API.
0x3 LFCLK_DLY Internal. Only to be used through TI provided API.
0x4 GPI Internal. Only to be used through TI provided API.
0x5 DTB0 Internal. Only to be used through TI provided API.
0x6 DTB1 Internal. Only to be used through TI provided API.
0x7 DTB2 Internal. Only to be used through TI provided API.
0x8 DTB3 Internal. Only to be used through TI provided API.
0x9 DTB4 Internal. Only to be used through TI provided API.
0xA DTB5 Internal. Only to be used through TI provided API.
0xB DTB6 Internal. Only to be used through TI provided API.
0xC DTB7 Internal. Only to be used through TI provided API.
0xD DTB8 Internal. Only to be used through TI provided API.
0xE DTB9 Internal. Only to be used through TI provided API.
0xF DTB10 Internal. Only to be used through TI provided API.
0x10 DTB11 Internal. Only to be used through TI provided API.
0x11 DTB12 Internal. Only to be used through TI provided API.
0x12 DTB13 Internal. Only to be used through TI provided API.
0x13 DTB14 Internal. Only to be used through TI provided API.
0x14 DTB15 Internal. Only to be used through TI provided API.
0x1F TDC_PRE Internal. Only to be used through TI provided API.
RW 0b0 0000

TOP:CKMD:TDCTRIGCNT

Address Offset 0x0000 0214
Physical Address 0x4000 1214 Instance 0x4000 1214
Description Internal. Only to be used through TI provided API.
Type RW
Bits Field Name Description Type Reset
31:16 RESERVED16 Internal. Only to be used through TI provided API. RO 0x0000
15:0 CNT Internal. Only to be used through TI provided API. RW 0x0000

TOP:CKMD:TDCTRIGCNTLOAD

Address Offset 0x0000 0218
Physical Address 0x4000 1218 Instance 0x4000 1218
Description Internal. Only to be used through TI provided API.
Type RW
Bits Field Name Description Type Reset
31:16 RESERVED16 Internal. Only to be used through TI provided API. RO 0x0000
15:0 CNT Internal. Only to be used through TI provided API. RW 0x0000

TOP:CKMD:TDCTRIGCNTCFG

Address Offset 0x0000 021C
Physical Address 0x4000 121C Instance 0x4000 121C
Description Internal. Only to be used through TI provided API.
Type RW
Bits Field Name Description Type Reset
31:1 RESERVED1 Internal. Only to be used through TI provided API. RO 0b000 0000 0000 0000 0000 0000 0000 0000
0 EN Internal. Only to be used through TI provided API. RW 0

TOP:CKMD:TDCPRECTL

Address Offset 0x0000 0220
Physical Address 0x4000 1220 Instance 0x4000 1220
Description Internal. Only to be used through TI provided API.
Type RW
Bits Field Name Description Type Reset
31:8 RESERVED8 Internal. Only to be used through TI provided API. RO 0x00 0000
7 RESET_N Internal. Only to be used through TI provided API. RW 0
6 RATIO Internal. Only to be used through TI provided API.
Value ENUM Name Description
0x0 DIV16 Internal. Only to be used through TI provided API.
0x1 DIV64 Internal. Only to be used through TI provided API.
RW 0
5 RESERVED5 Internal. Only to be used through TI provided API. RO 0
4:0 SRC Internal. Only to be used through TI provided API.
Value ENUM Name Description
0x0 LFTICK Internal. Only to be used through TI provided API.
0x1 LFOSC Internal. Only to be used through TI provided API.
0x2 LFXT Internal. Only to be used through TI provided API.
0x3 LFCLK_DLY Internal. Only to be used through TI provided API.
0x4 GPI Internal. Only to be used through TI provided API.
0x5 DTB0 Internal. Only to be used through TI provided API.
0x6 DTB1 Internal. Only to be used through TI provided API.
0x7 DTB2 Internal. Only to be used through TI provided API.
0x8 DTB3 Internal. Only to be used through TI provided API.
0x9 DTB4 Internal. Only to be used through TI provided API.
0xA DTB5 Internal. Only to be used through TI provided API.
0xB DTB6 Internal. Only to be used through TI provided API.
0xC DTB7 Internal. Only to be used through TI provided API.
0xD DTB8 Internal. Only to be used through TI provided API.
0xE DTB9 Internal. Only to be used through TI provided API.
0xF DTB10 Internal. Only to be used through TI provided API.
0x10 DTB11 Internal. Only to be used through TI provided API.
0x11 DTB12 Internal. Only to be used through TI provided API.
0x12 DTB13 Internal. Only to be used through TI provided API.
0x13 DTB14 Internal. Only to be used through TI provided API.
0x14 DTB15 Internal. Only to be used through TI provided API.
0x15 HFOSC Internal. Only to be used through TI provided API.
0x16 HFXT Internal. Only to be used through TI provided API.
RW 0b0 0000

TOP:CKMD:TDCPRECNTR

Address Offset 0x0000 0224
Physical Address 0x4000 1224 Instance 0x4000 1224
Description Internal. Only to be used through TI provided API.
Type RW
Bits Field Name Description Type Reset
31:17 RESERVED17 Internal. Only to be used through TI provided API. RO 0b000 0000 0000 0000
16 CAPT Internal. Only to be used through TI provided API. WO 0
15:0 CNT Internal. Only to be used through TI provided API. RO 0x0000

TOP:CKMD:WDTCNT

Address Offset 0x0000 0300
Physical Address 0x4000 1300 Instance 0x4000 1300
Description WDT counter value register
Type RW
Bits Field Name Description Type Reset
31:0 VAL Counter value.

A write to this field immediately starts (or restarts) the counter. It will count down from the written value.
If the counter reaches 0, a reset will be generated.
A write value of 0 immediately generates a reset.

This field is only writable if not locked. See WDTLOCK register.
Writing this field will automatically activate the lock.

A read returns the current value of the counter.
RW 0x0000 0000

TOP:CKMD:WDTTEST

Address Offset 0x0000 0304
Physical Address 0x4000 1304 Instance 0x4000 1304
Description WDT test mode register
Type RW
Bits Field Name Description Type Reset
31:1 RESERVED1 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000 0000 0000 0000 0000 0000 0000
0 STALLEN WDT stall enable

This field is only writable if not locked. See WDTLOCK register.
Value ENUM Name Description
0x0 DIS DISABLE

WDT continues counting while the CPU is stopped by a debugger.
0x1 EN ENABLE

WDT stops counting while the CPU is stopped by a debugger.
RW 0

TOP:CKMD:WDTLOCK

Address Offset 0x0000 0308
Physical Address 0x4000 1308 Instance 0x4000 1308
Description WDT lock register
Type RW
Bits Field Name Description Type Reset
31:0 STAT A write with value 0x1ACCE551 unlocks the watchdog registers for write access.
A write with any other value locks the watchdog registers for write access.
Writing the WDTCNT register will also lock the watchdog registers.

A read of this field returns the state of the lock (0=unlocked, 1=locked).
RW 0x0000 0001