Instance: LRFDTRC
Component: LRFDTRC
Base address: 0x40084000
Register Name |
Type |
Register Width (Bits) |
Register Reset |
Address Offset |
Physical Address |
RW |
32 |
0x0000 0000 |
0x0000 0000 |
0x4008 4000 |
|
RW |
32 |
0x0000 0000 |
0x0000 0004 |
0x4008 4004 |
|
RW |
32 |
0x0000 0000 |
0x0000 0008 |
0x4008 4008 |
|
RW |
32 |
0x0000 0000 |
0x0000 000C |
0x4008 400C |
|
RW |
32 |
0x0000 0000 |
0x0000 0014 |
0x4008 4014 |
|
RW |
32 |
0x0000 0000 |
0x0000 0018 |
0x4008 4018 |
|
RW |
32 |
0x0000 0000 |
0x0000 001C |
0x4008 401C |
|
RW |
32 |
0x0000 0000 |
0x0000 0024 |
0x4008 4024 |
|
RW |
32 |
0x0000 0000 |
0x0000 0028 |
0x4008 4028 |
|
RW |
32 |
0x0000 0000 |
0x0000 002C |
0x4008 402C |
Address Offset | 0x0000 0000 | ||
Physical Address | 0x4008 4000 | Instance | 0x4008 4000 |
Description | Tracer Configuration | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | |||||||||||||||||
31:9 | RESERVED9 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 0000 0000 0000 0000 | |||||||||||||||||
8:7 | PRESCAL | Data rate prescaler for bit clock of the serialized data
|
RW | 0b00 | |||||||||||||||||
6 | TSCLR | Writing 1 to this bit clears the TX timer
|
WO | 0 | |||||||||||||||||
5 | TSEN | Enables the Timestamp
|
RW | 0 | |||||||||||||||||
4:3 | CH3EN | Enables CH3 traces
|
RW | 0b00 | |||||||||||||||||
2:1 | CH2EN | Enables CH2 traces
|
RW | 0b00 | |||||||||||||||||
0 | CH1EN | Enables CH1 traces
|
RW | 0 |
Address Offset | 0x0000 0004 | ||
Physical Address | 0x4008 4004 | Instance | 0x4008 4004 |
Description | Channel 1 Command Register. Note only writeable when TRC.CFG.CH1EN = 1 | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | |||||||||||
31:16 | RESERVED16 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x0000 | |||||||||||
15:8 | PKTHDR | Header Byte. Reverts back to 0 when ready to transmit. A Write starts a transmission sequence.
|
RW | 0x00 | |||||||||||
7:3 | RESERVED3 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b0 0000 | |||||||||||
2:0 | PARCNT | Number of parameters to transmit. Reverts back to 0 when ready to transmit. A Write starts a transmission sequence.
|
RW | 0b000 |
Address Offset | 0x0000 0008 | ||
Physical Address | 0x4008 4008 | Instance | 0x4008 4008 |
Description | Channel 2 Command Register. Note only writeable when TRC.CFG.CH2EN = 1 | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | |||||||||||
31:16 | RESERVED16 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x0000 | |||||||||||
15:8 | PKTHDR | Header Byte. Reverts back to 0 when ready to transmit. A Write starts a transmission sequence.
|
RW | 0x00 | |||||||||||
7:3 | RESERVED3 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b0 0000 | |||||||||||
2:0 | PARCNT | Number of parameters to transmit. Reverts back to 0 when ready to transmit. A Write starts a transmission sequence.
|
RW | 0b000 |
Address Offset | 0x0000 000C | ||
Physical Address | 0x4008 400C | Instance | 0x4008 400C |
Description | Channel 3 Command Register. Note only writeable when TRC.CFG.CH3EN = 1 | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | |||||||||||
31:16 | RESERVED16 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x0000 | |||||||||||
15:8 | PKTHDR | Header Byte. Reverts back to 0 when ready to transmit. A Write starts a transmission sequence.
|
RW | 0x00 | |||||||||||
7:3 | RESERVED3 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b0 0000 | |||||||||||
2:0 | PARCNT | Number of parameters to transmit. Reverts back to 0 when ready to transmit. A Write starts a transmission sequence.
|
RW | 0b000 |
Address Offset | 0x0000 0014 | ||
Physical Address | 0x4008 4014 | Instance | 0x4008 4014 |
Description | Channel 1 Parameter 0/1 Register | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | |||||||||||
31:16 | PAR1 | Parameter 1 for Channel 1
|
RW | 0x0000 | |||||||||||
15:0 | PAR0 | Parameter 0 for Channel 1
|
RW | 0x0000 |
Address Offset | 0x0000 0018 | ||
Physical Address | 0x4008 4018 | Instance | 0x4008 4018 |
Description | Channel 2 Parameter 0/1 Register | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | |||||||||||
31:16 | PAR1 | Parameter 1 for Channel 2
|
RW | 0x0000 | |||||||||||
15:0 | PAR0 | Parameter 0 for Channel 2
|
RW | 0x0000 |
Address Offset | 0x0000 001C | ||
Physical Address | 0x4008 401C | Instance | 0x4008 401C |
Description | Channel 3 Parameter 0/1 Register | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | |||||||||||
31:16 | PAR1 | Parameter 1 for Channel 3
|
RW | 0x0000 | |||||||||||
15:0 | PAR0 | Parameter 0 for Channel 3
|
RW | 0x0000 |
Address Offset | 0x0000 0024 | ||
Physical Address | 0x4008 4024 | Instance | 0x4008 4024 |
Description | Channel 1 Parameter 2/3 Register | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | |||||||||||
31:16 | PAR3 | Parameter 3 for Channel 1
|
RW | 0x0000 | |||||||||||
15:0 | PAR2 | Parameter 2 for Channel 1
|
RW | 0x0000 |
Address Offset | 0x0000 0028 | ||
Physical Address | 0x4008 4028 | Instance | 0x4008 4028 |
Description | Channel 2 Parameter 2/3 Register | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | |||||||||||
31:16 | PAR3 | Parameter 3 for Channel 2
|
RW | 0x0000 | |||||||||||
15:0 | PAR2 | Parameter 2 for Channel 2
|
RW | 0x0000 |
Address Offset | 0x0000 002C | ||
Physical Address | 0x4008 402C | Instance | 0x4008 402C |
Description | Channel 3 Parameter 2/3 Register | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | |||||||||||
31:16 | PAR3 | Parameter 3 for Channel 3
|
RW | 0x0000 | |||||||||||
15:0 | PAR2 | Parameter 2 for Channel 3
|
RW | 0x0000 |
© 2015 - 2016. Texas Instruments | All Rights Reserved |