FLASH

Instance: FLASH
Component: FLASH
Base address: 0x40021000


This is the MMR space for the flash wrapper. The flash wrapper is targeting
multiple microcontroller platforms. The flash wrapper is a module
that manages complex flash read, program and erase memory operations.
The system is also given direct access to read flash memory contents directly for
each instantiated flash bank through FBAP ports.

TOP:FLASH Register Summary

Register Name

Type

Register Width (Bits)

Register Reset

Address Offset

Physical Address

IMASK

RW

32

0x0000 0000

0x0000 0028

0x4002 1028

RIS

RO

32

0x0000 0000

0x0000 0030

0x4002 1030

MIS

RO

32

0x0000 0000

0x0000 0038

0x4002 1038

ISET

WO

32

0x0000 0000

0x0000 0040

0x4002 1040

ICLR

WO

32

0x0000 0000

0x0000 0048

0x4002 1048

DESC

RO

32

0x0B40 1010

0x0000 00FC

0x4002 10FC

CMDEXEC

RW

32

0x0000 0000

0x0000 0100

0x4002 1100

CMDTYPE

RW

32

0x0000 0000

0x0000 0104

0x4002 1104

CMDCTL

RW

32

0x0000 0000

0x0000 0108

0x4002 1108

CMDADDR

RW

32

0x0000 0000

0x0000 0120

0x4002 1120

CMDBYTEN

RW

32

0x0000 0000

0x0000 0124

0x4002 1124

CMDDATA0

RW

32

0xFFFF FFFF

0x0000 0130

0x4002 1130

CMDDATA1

RW

32

0xFFFF FFFF

0x0000 0134

0x4002 1134

CMDDATA2

RW

32

0xFFFF FFFF

0x0000 0138

0x4002 1138

CMDDATA3

RW

32

0xFFFF FFFF

0x0000 013C

0x4002 113C

CMDWEPROTA

RW

32

0xFFFF FFFF

0x0000 01D0

0x4002 11D0

CMDWEPROTB

RW

32

0x0FFF FFFF

0x0000 01D4

0x4002 11D4

CMDWEPROTNM

RW

32

0x0000 0001

0x0000 0210

0x4002 1210

CMDWEPROTTR

RW

32

0x0000 0001

0x0000 0214

0x4002 1214

CMDWEPROTEN

RW

32

0x0000 0001

0x0000 0218

0x4002 1218

CFGCMD

RW

32

0x0000 0002

0x0000 03B0

0x4002 13B0

CFGPCNT

RW

32

0x0000 0000

0x0000 03B4

0x4002 13B4

STATCMD

RO

32

0x0000 0000

0x0000 03D0

0x4002 13D0

STATADDR

RO

32

0x0021 0000

0x0000 03D4

0x4002 13D4

STATPCNT

RO

32

0x0000 0000

0x0000 03D8

0x4002 13D8

STATMODE

RO

32

0x0000 0000

0x0000 03DC

0x4002 13DC

GBLINFO0

RO

32

0x0001 0800

0x0000 03F0

0x4002 13F0

GBLINFO1

RO

32

0x0004 0080

0x0000 03F4

0x4002 13F4

GBLINFO2

RO

32

0x0000 0001

0x0000 03F8

0x4002 13F8

BANK0INFO0

RO

32

0x0000 0100

0x0000 0400

0x4002 1400

BANK0INFO1

RO

32

0x0001 0101

0x0000 0404

0x4002 1404

TOP:FLASH Register Descriptions

TOP:FLASH:IMASK

Address Offset 0x0000 0028
Physical Address 0x4002 1028 Instance 0x4002 1028
Description Interrupt Mask Register:
The IMASK register holds the current interrupt mask settings. Masked interrupts
are read in the MIS register. PSD compliant register.
Type RW
Bits Field Name Description Type Reset
31:1 RESERVED_31_1 Reserved RW 0b000 0000 0000 0000 0000 0000 0000 0000
0 DONE Interrupt mask for DONE:
0: Interrupt is disabled in MIS register
1: Interrupt is enabled in MIS register
Value ENUM Name Description
0x0 DISABLED Interrupt is masked out
0x1 ENABLED Interrupt will request an interrupt service routine and corresponding bit in IPSTANDARD.MIS will be set
RW 0

TOP:FLASH:RIS

Address Offset 0x0000 0030
Physical Address 0x4002 1030 Instance 0x4002 1030
Description Raw Interrupt Status Register:
The RIS register reflects all pending interrupts, regardless of masking.
The RIS register allows the user to implement a poll scheme. A flag set in this
register can be cleared by writing a 1 to the ICLR register bit even if the
corresponding IMASK bit is not enabled. A flag can be set by software by writing
a 1 to the ISET register. Reading the IIDX register will also clear the
corresponding bit in RIS. PSD compliant register.
Type RO
Bits Field Name Description Type Reset
31:1 RESERVED_31_1 Reserved RO 0b000 0000 0000 0000 0000 0000 0000 0000
0 DONE Flash wrapper operation completed.
This interrupt bit is set by firmware or the corresponding bit in the ISET register.
It is cleared by the corresponding bit in in the ICLR register or reading the IIDX register when this interrupt is the highest priority.
Value ENUM Name Description
0x0 CLR Interrupt did not occur
0x1 SET Interrupt occurred
RO 0

TOP:FLASH:MIS

Address Offset 0x0000 0038
Physical Address 0x4002 1038 Instance 0x4002 1038
Description Masked Interrupt Status Register:
The MIS register is a bit-wise AND of the contents of the IMASK and RIS
registers. This is kept mainly for ARM compatibility, and has limited use since
the highest priority interrupt index is returned through the IIDX register.
PSD
compliant register.
Type RO
Bits Field Name Description Type Reset
31:1 RESERVED_31_1 Reserved RO 0b000 0000 0000 0000 0000 0000 0000 0000
0 DONE Flash wrapper operation completed.
This masked interrupt bit reflects the bitwise AND of the corresponding RIS and IMASK bits.
Value ENUM Name Description
0x0 CLR Masked interrupt did not occur
0x1 SET Masked interrupt occurred
RO 0

TOP:FLASH:ISET

Address Offset 0x0000 0040
Physical Address 0x4002 1040 Instance 0x4002 1040
Description Interrupt Set Register:
The ISET register allows software to write a 1 to set corresponding interrupt.

Safety:
This meets a safety requirement to allow software diagnostics to trigger
interrupts.
PSD compliant register.
Type WO
Bits Field Name Description Type Reset
31:1 RESERVED_31_1 Reserved WO 0b000 0000 0000 0000 0000 0000 0000 0000
0 DONE 0: No effect
1: Set the DONE interrupt in the RIS register
Value ENUM Name Description
0x0 NO_EFFECT Writing a 0 has no effect
0x1 SET Set IPSTANDARD.RIS bit
WO 0

TOP:FLASH:ICLR

Address Offset 0x0000 0048
Physical Address 0x4002 1048 Instance 0x4002 1048
Description Interrupt Clear Register.
The ICLR register allows allows software to write a 1 to clear corresponding
interrupt.
PSD compliant register.
Type WO
Bits Field Name Description Type Reset
31:1 RESERVED_31_1 Reserved WO 0b000 0000 0000 0000 0000 0000 0000 0000
0 DONE 0: No effect
1: Clear the DONE interrupt in the RIS register
Value ENUM Name Description
0x0 NO_EFFECT Writing a 0 has no effect
0x1 CLR Clear IPSTANDARD.RIS bit
WO 0

TOP:FLASH:DESC

Address Offset 0x0000 00FC
Physical Address 0x4002 10FC Instance 0x4002 10FC
Description Hardware Version Description Register:
This register identifies the flash wrapper hardware version and feature set used.
Type RO
Bits Field Name Description Type Reset
31:16 MODULEID Module ID
Value ENUM Name Description
0x0 MINIMUM Smallest value
0xFFFF MAXIMUM Highest possible value
RO 0x0B40
15:12 FEATUREVER Feature set
Value ENUM Name Description
0x0 MINIMUM Minimum Value
0xF MAXIMUM Maximum Value
RO 0x1
11:8 INSTNUM Instance number
Value ENUM Name Description
0x0 MINIMUM Smallest value
0xF MAXIMUM Highest possible value
RO 0x0
7:4 MAJREV Major Revision
Value ENUM Name Description
0x0 MINIMUM Smallest value
0xF MAXIMUM Highest possible value
RO 0x1
3:0 MINREV Minor Revision
Value ENUM Name Description
0x0 MINIMUM Smallest value
0xF MAXIMUM Highest possible value
RO 0x0

TOP:FLASH:CMDEXEC

Address Offset 0x0000 0100
Physical Address 0x4002 1100 Instance 0x4002 1100
Description Command Execute Register:
Initiates execution of the command specified in the CMDTYPE register.
This register is blocked for writes after being written to 1 and prior to
STATCMD.DONE being set by the flash wrapper hardware.
flash wrapper hardware clears this register after the processing of the command
has completed.
Type RW
Bits Field Name Description Type Reset
31:1 RESERVED_31_1 Reserved RW 0b000 0000 0000 0000 0000 0000 0000 0000
0 VAL Command Execute value
Initiates execution of the command specified in the CMDTYPE register.
Value ENUM Name Description
0x0 NOEXECUTE Command will not execute or is not executing in flash wrapper
0x1 EXECUTE Command will execute or is executing in flash wrapper
RW 0

TOP:FLASH:CMDTYPE

Address Offset 0x0000 0104
Physical Address 0x4002 1104 Instance 0x4002 1104
Description Command Type Register
This register specifies the type of command to be executed by the flash wrapper
hardware.
This register is blocked for writes after CMDEXEC is written to a 1 and
prior to STATCMD.DONE being set by the hardware to indicate that
command execution has completed.
Type RW
Bits Field Name Description Type Reset
31:7 RESERVED_31_7 Reserved RW 0b0 0000 0000 0000 0000 0000 0000
6:4 SIZE Command size
Value ENUM Name Description
0x0 ONEWORD Operate on 1 flash word
0x1 TWOWORD Operate on 2 flash words
0x2 FOURWORD Operate on 4 flash words
0x3 EIGHTWORD Operate on 8 flash words
0x4 SECTOR Operate on a flash sector
0x5 BANK Operate on an entire flash bank
RW 0b000
3 RESERVED_3 Reserved RW 0
2:0 COMMAND Command type
Value ENUM Name Description
0x0 NOOP No Operation
0x1 PROGRAM Program
0x2 ERASE Erase
0x3 READVERIFY Read Verify - Perform a standalone read verify operation.
0x4 MODECHANGE Mode Change - Perform a mode change only, no other operation.
0x5 CLEARSTATUS Clear Status - Clear status bits in FW_SMSTAT only.
0x6 BLANKVERIFY Blank Verify - Check whether a flash word is in the erased state.
This command may only be used with CMDTYPE.SIZE = ONEWORD
RW 0b000

TOP:FLASH:CMDCTL

Address Offset 0x0000 0108
Physical Address 0x4002 1108 Instance 0x4002 1108
Description Command Control Register
This register configures specific capabilities of the state machine for related to
the execution of a command.
This register is blocked for writes after CMDEXEC is written to a 1 and
prior to STATCMD.DONE being set by the hardware to indicate that
command execution has completed.
Type RW
Bits Field Name Description Type Reset
31:22 RESERVED_31_22 Reserved RW 0b00 0000 0000
21 DATAVEREN Enable invalid data verify.
This checks for 0->1 transitions in the memory when
a program operation is initiated. If such a transition is found, the program will
fail with an error without executing the program.
Value ENUM Name Description
0x0 DISABLE Disable
0x1 ENABLE Enable
RW 0
20 SSERASEDIS Disable Stair-Step Erase. If set, the default VHV trim voltage setting will be used
for all erase pulses.
By default, this bit is reset, meaning that the VHV voltage will be stepped during
successive erase pulses. The step count, step voltage, begin and end voltages
are all hard-wired.
Value ENUM Name Description
0x0 ENABLE Enable
0x1 DISABLE Disable
RW 0
19:17 RESERVED17 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000
16 ADDRXLATEOVR Override hardware address translation of address in CMDADDR from a
system address to a bank address and bank ID. Use data written to
CMDADDR directly as the bank address. Use the value written to
CMDCTL.BANKSEL directly as the bank ID. Use the value written to
CMDCTL.REGIONSEL directly as the region ID.
Value ENUM Name Description
0x0 NOOVERRIDE Do not override
0x1 OVERRIDE Override
RW 0
15:14 RESERVED14 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b00
13 RESERVED_13 Reserved RW 0
12:9 REGIONSEL Bank Region
A specific region ID can be written to this field to indicate to which region an
operation is to be applied if CMDCTL.ADDRXLATEOVR is set.
Value ENUM Name Description
0x1 MAIN Main Region
0x2 NONMAIN Non-Main Region
0x4 TRIM Trim Region
0x8 ENGR Engr Region
RW 0x0
8:4 RESERVED4 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b0 0000
3:0 MODESEL Mode
This field is only used for the Mode Change command type. Otherwise, bank
and pump modes are set automaticlly through the NW hardware.
Value ENUM Name Description
0x0 READ Read Mode
0x2 RDMARG0 Read Margin 0 Mode
0x4 RDMARG1 Read Margin 1 Mode
0x6 RDMARG0B Read Margin 0B Mode
0x7 RDMARG1B Read Margin 1B Mode
0x9 PGMVER Program Verify Mode
0xA PGMSW Program Single Word
0xB ERASEVER Erase Verify Mode
0xC ERASESECT Erase Sector
0xE PGMMW Program Multiple Word
0xF ERASEBNK Erase Bank
RW 0x0

TOP:FLASH:CMDADDR

Address Offset 0x0000 0120
Physical Address 0x4002 1120 Instance 0x4002 1120
Description Command Address Register:
This register forms the target address of a command. The use cases are as
follows:
1) For single-word program, this address indicates the flash bank word to be
programmed.
2) For multi-word program, this address indicates the first flash bank address
for the program. The address will be incremented for further words.
3) For sector erase, this address indicates the sector to be erased.
4) For bank erase, the address indicates the bank to be erased.
5) For read verify, the address indications follow program/erase listed above.
Note the address written to this register will be submitted for translation to the
flash wrapper address translation interface, and the translated address
will be used to access the bank. However, if the
CMDCTL.ADDRXLATEOVR bit is set, then the address written to this register will
be used directly as the bank address.
This register is blocked for writes after a 1 is written to the CMDEXEC
register and prior to STATCMD.DONE being set by the flash wrapper
hardware.
Type RW
Bits Field Name Description Type Reset
31:0 VAL Address value
Value ENUM Name Description
0x0 MINIMUM Minimum value of VAL
0xFFFFFFFF MAXIMUM Maximum value of VAL
RW 0x0000 0000

TOP:FLASH:CMDBYTEN

Address Offset 0x0000 0124
Physical Address 0x4002 1124 Instance 0x4002 1124
Description Command Program Byte Enable Register:
This register forms a per-byte enable for programming data. For data bytes to
be programmed, a 1 must be written to the corresponding bit in this register.
Normally, all bits are written to 1, allowing program of full flash words.
However, leaving some bits 0 allows programming of 8-bit, 16-bit, 32-bit
or 64-bit portions of a flash word.
In addtion, the read verify command will ignore data bytes read from the flash
in its comparison if the corresponding CMDBYTEN bit is 0.
ECC data bytes are protected by the 1-2 MSB bits in this register, depending on
the presence of ECC and the flash word data width.
This register is blocked for writes after a 1 is written to the CMDEXEC
register and prior to STATCMD.DONE being set by the flash wrapper
hardware.
This register is written to all 0 after the completion of all flash wrapper commands.
Type RW
Bits Field Name Description Type Reset
31:18 RESERVED_31_18 Reserved RW 0b00 0000 0000 0000
17:16 RESERVED16 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b00
15:0 VAL Command Byte Enable value.
A 1-bit per flash word byte value is placed in this register.
Value ENUM Name Description
0x0 MINIMUM Minimum value of VAL
0x3FFFF MAXIMUM Maximum value of VAL
RW 0x0000

TOP:FLASH:CMDDATA0

Address Offset 0x0000 0130
Physical Address 0x4002 1130 Instance 0x4002 1130
Description Command Data Register 0
This register forms the data for a command.
For DATAWIDTH == 128: This register represents bits 31:0 of flash word data register 0.
For DATAWIDTH == 64: This register represents bits 31:0 of flash word data register 0.
This register is blocked for writes after a 1 is written to the CMDEXEC
register and prior to STATCMD.DONE being set by the flash wrapper
hardware.
This register is used to aggregate masking for bits that do not
require additional program pulses during program operations, and will be
written to all 1 after the completion of all flash wrapper commands.

Use cases for the CMDDATA* registers are as follows:
1) Program - These registers contain the data to be programmed.
2) Erase - These registers are not used.
3) Read Verify - These registers contain data to be verified.
Type RW
Bits Field Name Description Type Reset
31:0 VAL A 32-bit data value is placed in this field.
Value ENUM Name Description
0x0 MINIMUM Minimum value of VAL
0xFFFFFFFF MAXIMUM Maximum value of VAL
RW 0xFFFF FFFF

TOP:FLASH:CMDDATA1

Address Offset 0x0000 0134
Physical Address 0x4002 1134 Instance 0x4002 1134
Description Command Data Register 1
This register forms the data for a command.
For DATAWIDTH == 128: This register represents bits 63:32 of flash word data register 0.
For DATAWIDTH == 64: This register represents bits 63:32 of flash word data register 0.
This register is blocked for writes after a 1 is written to the CMDEXEC
register and prior to CMDSTAT.DONE being set by the flash wrapper
hardware.
This register is used to aggregate masking for bits that do not
require additional program pulses during program operations, and will be
written to all 1 after the completion of all flash wrapper commands.

Use cases for the CMDDATA* registers are as follows:
1) Program - These registers contain the data to be programmed.
2) Erase - These registers are not used.
3) Read Verify - These registers contain data to be verified.
Type RW
Bits Field Name Description Type Reset
31:0 VAL A 32-bit data value is placed in this field.
Value ENUM Name Description
0x0 MINIMUM Minimum value of VAL
0xFFFFFFFF MAXIMUM Maximum value of VAL
RW 0xFFFF FFFF

TOP:FLASH:CMDDATA2

Address Offset 0x0000 0138
Physical Address 0x4002 1138 Instance 0x4002 1138
Description Command Data Register 2
This register forms the data for a command.
For DATAWIDTH == 128: This register represents bits 95:64 of flash word data register 0.
For DATAWIDTH == 64: This register represents bits 31:0 of flash word data register 1.
This register is blocked for writes after a 1 is written to the CMDEXEC
register and prior to STATCMD.DONE being set by the flash wrapper
hardware.
This register is used to aggregate masking for bits that do not
require additional program pulses during program operations, and will be
written to all 1 after the completion of all flash wrapper commands.

Use cases for the CMDDATA* registers are as follows:
1) Program - These registers contain the data to be programmed.
2) Erase - These registers are not used.
3) Read Verify - These registers contain data to be verified.
Type RW
Bits Field Name Description Type Reset
31:0 VAL A 32-bit data value is placed in this field.
Value ENUM Name Description
0x0 MINIMUM Minimum value of VAL
0xFFFFFFFF MAXIMUM Maximum value of VAL
RW 0xFFFF FFFF

TOP:FLASH:CMDDATA3

Address Offset 0x0000 013C
Physical Address 0x4002 113C Instance 0x4002 113C
Description Command Data Register 3
This register forms the data for a command.
For DATAWIDTH == 128: This register represents bits 127:96 of flash word data register 0.
For DATAWIDTH == 64: This register represents bits 63:32 of flash word data register 1.
This register is blocked for writes after a 1 is written to the CMDEXEC
register and prior to STATCMD.DONE being set by the flash wrapper
hardware.
This register is used to aggregate masking for bits that do not
require additional program pulses during program operations, and will be
written to all 1 after the completion of all flash wrapper commands.

Use cases for the CMDDATA* registers are as follows:
1) Program - These registers contain the data to be programmed.
2) Erase - These registers are not used.
3) Read Verify - These registers contain data to be verified.
Type RW
Bits Field Name Description Type Reset
31:0 VAL A 32-bit data value is placed in this field.
Value ENUM Name Description
0x0 MINIMUM Minimum value of VAL
0xFFFFFFFF MAXIMUM Maximum value of VAL
RW 0xFFFF FFFF

TOP:FLASH:CMDWEPROTA

Address Offset 0x0000 01D0
Physical Address 0x4002 11D0 Instance 0x4002 11D0
Description Command WriteErase Protect A Register
This register allows the first 32 sectors of the main region to be protected from
program or erase, with 1 bit protecting each sector. If the main region size is smaller than 32
sectors, then this register provides protection for the whole region.
This register is blocked for writes after a 1 is written to the CMDEXEC
register and prior to STATCMD.DONE being set by the flash wrapper
hardware.
In addition, this register is used to aggregate masking for sectors that do not
require additional erase pulses during bank erase operations, and will be
written to all 1 after the completion of all flash wrapper commands.
Type RW
Bits Field Name Description Type Reset
31:0 VAL Each bit protects 1 sector.

bit [0]: When 1, sector 0 of the flash memory will be protected from program
and erase.
bit [1]: When 1, sector 1 of the flash memory will be protected from program
and erase.
:
:
bit [31]: When 1, sector 31 of the flash memory will be protected from program
and erase.
Value ENUM Name Description
0x0 MINIMUM Minimum value of VAL
0xFFFFFFFF MAXIMUM Maximum value of VAL
RW 0xFFFF FFFF

TOP:FLASH:CMDWEPROTB

Address Offset 0x0000 01D4
Physical Address 0x4002 11D4 Instance 0x4002 11D4
Description Command WriteErase Protect B Register
This register allows main region sectors to be protected from program and
erase. Each bit corresponds to a group of 8 sectors.
There are 3 cases for how these protect bits are applied:
1. Single-bank system:
In the case where only a single flash bank is present,
the first 32 sectors are protected via the CMDWEPROTA register. Thus, the
protection give by the bits in CMDWEPROTB begin with sector 32.
2. Multi-bank system, Bank 0:
When multiple flash banks are present, the first
32 sectors of bank 0 are protected via the CMDWEPROTA register. Thus, only
bits 4 and above of CMDWEPROTB would be applicable to bank 0. The protection of
bit 4 and above would begin at sector 32. Bits 3:0
of WEPROTB are ignored for bank 0.
3. Multi-bank system, Banks 1-N:
For banks other than bank 0 in a multi-bank system, CMDWEPROTA has
no effect, so the bits in CMDWEPROTB will protect these banks starting
from sector 0.
This register is blocked for writes after a 1 is written to the CMDEXEC
register and prior to STATCMD.DONE being set by the flash wrapper
hardware.
In addition, this register is used to aggregate masking for sectors that do not
require additional erase pulses during bank erase operations, and will be
written to all 1 after the completion of all flash wrapper commands.
Type RW
Bits Field Name Description Type Reset
31:28 RESERVED28 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x0
27:0 VAL Each bit protects a group of 8 sectors. When a bit is 1, the associated 8 sectors
in the flash will be protected from program and erase. A maximum of 256
sectors can be protected with this register.
Value ENUM Name Description
0x0 MINIMUM Minimum value of VAL
0xFFFFFFFF MAXIMUM Maximum value of VAL
RW 0xFFF FFFF

TOP:FLASH:CMDWEPROTNM

Address Offset 0x0000 0210
Physical Address 0x4002 1210 Instance 0x4002 1210
Description Command WriteErase Protect Non-Main
Register
This register allows non-main region region sectors to be protected
from program and erase. Each bit corresponds to 1 sector.
This register is blocked for writes after a 1 is written to the CMDEXEC
register and prior to STATCMD.DONE being set by the flash wrapper
hardware.
In addition, this register is used to aggregate masking for sectors that do not
require additional erase pulses during bank erase operations, and will be
written to all 1 after the completion of all flash wrapper commands.
Type RW
Bits Field Name Description Type Reset
31:1 RESERVED1 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000 0000 0000 0000 0000 0000 0000
0 VAL Each bit protects 1 sector.

bit [0]: When 1, sector 0 of the non-main region will be protected from program
and erase.
bit [1]: When 1, sector 1 of the non-main region will be protected from program
and erase.
:
:
bit [31]: When 1, sector 31 of the non-main will be protected from program
and erase.
Value ENUM Name Description
0x0 MINIMUM Minimum value of VAL
0xFFFFFFFF MAXIMUM Maximum value of VAL
RW 1

TOP:FLASH:CMDWEPROTTR

Address Offset 0x0000 0214
Physical Address 0x4002 1214 Instance 0x4002 1214
Description Command WriteErase Protect Trim
Register
This register allows trim region sectors to be protected
from program and erase. Each bit corresponds to 1 sector.
This register is blocked for writes after a 1 is written to the CMDEXEC
register and prior to STATCMD.DONE being set by the flash wrapper
hardware.
In addition, this register is used to aggregate masking for sectors that do not
require additional erase pulses during bank erase operations, and will be
written to all 1 after the completion of all flash wrapper commands.
Type RW
Bits Field Name Description Type Reset
31:1 RESERVED1 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000 0000 0000 0000 0000 0000 0000
0 VAL Each bit protects 1 sector.

bit [0]: When 1, sector 0 of the engr region will be protected from program
and erase.
bit [1]: When 1, sector 1 of the engr region will be protected from program
and erase.
:
:
bit [31]: When 1, sector 31 of the engr region will be protected from program
and erase.
Value ENUM Name Description
0x0 MINIMUM Minimum value of VAL
0xFFFFFFFF MAXIMUM Maximum value of VAL
RW 1

TOP:FLASH:CMDWEPROTEN

Address Offset 0x0000 0218
Physical Address 0x4002 1218 Instance 0x4002 1218
Description Command WriteErase Protect Engr
Register
This register allows engr region sectors to be protected
from program and erase. Each bit corresponds to 1 sector.
This register is blocked for writes after a 1 is written to the CMDEXEC
register and prior to STATCMD.DONE being set by the flash wrapper
hardware.
In addition, this register is used to aggregate masking for sectors that do not
require additional erase pulses during bank erase operations, and will be
written to all 1 after the completion of all flash wrapper commands.
Type RW
Bits Field Name Description Type Reset
31:1 RESERVED1 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000 0000 0000 0000 0000 0000 0000
0 VAL Each bit protects 1 sector.

bit [0]: When 1, sector 0 of the engr region will be protected from program
and erase.
bit [1]: When 1, sector 1 of the engr region will be protected from program
and erase.
:
:
bit [31]: When 1, sector 31 of the engr region will be protected from program
and erase.
Value ENUM Name Description
0x0 MINIMUM Minimum value of VAL
0xFFFFFFFF MAXIMUM Maximum value of VAL
RW 1

TOP:FLASH:CFGCMD

Address Offset 0x0000 03B0
Physical Address 0x4002 13B0 Instance 0x4002 13B0
Description Command Configuration Register
This register configures specific capabilities of the state machine for related to
the execution of a command.
This register is blocked for writes after CMDEXEC is written to a 1 and
prior to STATCMD.DONE being set by the hardware to indicate that
command execution has completed.
Type RW
Bits Field Name Description Type Reset
31:7 RESERVED_31_7 Reserved RW 0b0 0000 0000 0000 0000 0000 0000
6:4 RESERVED4 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000
3:0 WAITSTATE Wait State setting for program verify, erase verify and read verify
Value ENUM Name Description
0x0 MINIMUM Minimum value
0xF MAXIMUM Maximum value
RW 0x2

TOP:FLASH:CFGPCNT

Address Offset 0x0000 03B4
Physical Address 0x4002 13B4 Instance 0x4002 13B4
Description Pulse Counter Configuration Register
This register allows further configuration of maximum pulse counts for
program and erase operations.
This register is blocked for writes after a 1 is written to the CMDEXEC
register and prior to STATCMD.DONE being set by the flash wrapper
hardware.
Type RW
Bits Field Name Description Type Reset
31:20 RESERVED20 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x000
19:17 RESERVED_17_19 Reserved RW 0b000
16 RESERVED16 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0
15:12 RESERVED_15_12 Reserved RW 0x0
11:4 MAXPCNTVAL Override maximum pulse counter with this value.
If MAXPCNTOVR = 0, then this field is ignored.
If MAXPCNTOVR = 1 and MAXERSPCNTOVR = 0, then this value will be used
to override the max pulse count for both program and erase. Full max value
will be {4'h0, MAXPCNTVAL} .
If MAXPCNTOVR = 1 and MAXERSPCNTOVR = 1, then this value will be used
to override the max pulse count for program only. Full max value will be
{4'h0, MAXPCNTVAL}.
Value ENUM Name Description
0x0 MINIMUM Minimum value
0xFF MAXIMUM Maximum value
RW 0x00
3:1 RESERVED_3_1 Reserved RW 0b000
0 MAXPCNTOVR Override hard-wired maximum pulse count. If MAXERSPCNTOVR
is not set, then setting this value alone will override the max pulse count for
both program and erase. If MAXERSPCNTOVR is set, then this bit will only
control the max pulse count setting for program.
By default, this bit is 0, and a hard-wired max pulse count is used.
Value ENUM Name Description
0x0 DEFAULT Use hard-wired (default) value for maximum pulse count
0x1 OVERRIDE Use value from MAXPCNTVAL field as maximum puse count
RW 0

TOP:FLASH:STATCMD

Address Offset 0x0000 03D0
Physical Address 0x4002 13D0 Instance 0x4002 13D0
Description Command Status Register
This register contains status regarding completion and errors of command
execution.
Type RO
Bits Field Name Description Type Reset
31:13 RESERVED_31_13 Reserved RO 0b000 0000 0000 0000 0000
12 FAILMISC Command failed due to error other than write/erase protect violation or verify
error. This is an extra bit in case a new failure mechanism is added which
requires a status bit.
Value ENUM Name Description
0x0 STATNOFAIL No Fail
0x1 STATFAIL Fail
RO 0
11:9 RESERVED_11_9 Reserved RO 0b000
8 FAILINVDATA Program command failed because an attempt was made to program a stored
0 value to a 1.
Value ENUM Name Description
0x0 STATNOFAIL No Fail
0x1 STATFAIL Fail
RO 0
7 FAILMODE Command failed because a bank has been set to a mode other than READ.
Program and Erase commands cannot be initiated unless all banks are in READ
mode.
Value ENUM Name Description
0x0 STATNOFAIL No Fail
0x1 STATFAIL Fail
RO 0
6 FAILILLADDR Command failed due to the use of an illegal address
Value ENUM Name Description
0x0 STATNOFAIL No Fail
0x1 STATFAIL Fail
RO 0
5 FAILVERIFY Command failed due to verify error
Value ENUM Name Description
0x0 STATNOFAIL No Fail
0x1 STATFAIL Fail
RO 0
4 FAILWEPROT Command failed due to Write/Erase Protect Sector Violation
Value ENUM Name Description
0x0 STATNOFAIL No Fail
0x1 STATFAIL Fail
RO 0
3 RESERVED_3 Reserved RO 0
2 CMDINPROGRESS Command In Progress
Value ENUM Name Description
0x0 STATCOMPLETE Complete
0x1 STATINPROGRESS In Progress
RO 0
1 CMDPASS Command Pass - valid when CMD_DONE field is 1
Value ENUM Name Description
0x0 STATFAIL Fail
0x1 STATPASS Pass
RO 0
0 CMDDONE Command Done
Value ENUM Name Description
0x0 STATNOTDONE Not Done
0x1 STATDONE Done
RO 0

TOP:FLASH:STATADDR

Address Offset 0x0000 03D4
Physical Address 0x4002 13D4 Instance 0x4002 13D4
Description Current Address Counter Value
Read only register giving read access to the state machine current address.
A bank id, region id and address are stored in this register and are incremented as
necessary during execution of a command.
Type RO
Bits Field Name Description Type Reset
31:26 RESERVED_31_26 Reserved RO 0b00 0000
25:21 BANKID Current Bank ID
A bank indicator is stored in this register which represents the current bank on
which the state machine is operating. There is 1 bit per bank.
Value ENUM Name Description
0x1 BANK0 Bank 0
0x2 BANK1 Bank 1
0x4 BANK2 Bank 2
0x8 BANK3 Bank 3
0x10 BANK4 Bank 4
RO 0b0 0001
20:16 REGIONID Current Region ID
A region indicator is stored in this register which represents the current flash
region on which the state machine is operating.
Value ENUM Name Description
0x1 MAIN Main Region
0x2 NONMAIN Non-Main Region
0x4 TRIM Trim Region
0x8 ENGR Engr Region
RO 0b0 0001
15:0 BANKADDR Current Bank Address
A bank offset address is stored in this register.
Value ENUM Name Description
0x0 MINIMUM Minimum value
0xFFFF MAXIMUM Maximum value
RO 0x0000

TOP:FLASH:STATPCNT

Address Offset 0x0000 03D8
Physical Address 0x4002 13D8 Instance 0x4002 13D8
Description Current Pulse Count Register:
Read only register giving read access to the state machine current pulse count
value for program/erase operations.
Type RO
Bits Field Name Description Type Reset
31:12 RESERVED_31_12 Reserved RO 0x0 0000
11:0 PULSECNT Current Pulse Counter Value
Value ENUM Name Description
0x0 MINIMUM Minimum value
0xFFF MAXIMUM Maximum value
RO 0x000

TOP:FLASH:STATMODE

Address Offset 0x0000 03DC
Physical Address 0x4002 13DC Instance 0x4002 13DC
Description Mode Status Register
Indicates one or more banks which not in READ mode, and it indicates the mode
which the bank(s) are in.
Type RO
Bits Field Name Description Type Reset
31:18 RESERVED_31_18 Reserved RO 0b00 0000 0000 0000
17 BANK1TRDY Bank 1T Ready.
Bank(s) are ready for 1T access. This is accomplished when the bank and pump
have been trimmed.
Value ENUM Name Description
0x0 FALSE Not ready
0x1 TRUE Ready
RO 0
16 BANK2TRDY Bank 2T Ready.
Bank(s) are ready for 2T access. This is accomplished when the pump has
fully driven power rails to the bank(s).
Value ENUM Name Description
0x0 FALSE Not ready
0x1 TRUE Ready
RO 0
15:12 RESERVED_15_12 Reserved RO 0x0
11:8 BANKMODE Indicates mode of bank(s) that are not in READ mode
Value ENUM Name Description
0x0 READ Read Mode
0x2 RDMARG0 Read Margin 0 Mode
0x4 RDMARG1 Read Margin 1 Mode
0x6 RDMARG0B Read Margin 0B Mode
0x7 RDMARG1B Read Margin 1B Mode
0x9 PGMVER Program Verify Mode
0xA PGMSW Program Single Word
0xB ERASEVER Erase Verify Mode
0xC ERASESECT Erase Sector
0xE PGMMW Program Multiple Word
0xF ERASEBNK Erase Bank
RO 0x0
7:5 RESERVED_7_5 Reserved RO 0b000
4:1 RESERVED1 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x0
0 BANKNOTINRD Bank not in read mode.
Indicates which banks are not in READ mode. There is 1 bit per bank.
Value ENUM Name Description
0x1 BANK0 Bank 0
0x2 BANK1 Bank 1
0x4 BANK2 Bank 2
0x8 BANK3 Bank 3
0x10 BANK4 Bank 4
RO 0

TOP:FLASH:GBLINFO0

Address Offset 0x0000 03F0
Physical Address 0x4002 13F0 Instance 0x4002 13F0
Description Global Info 0 Register
Read only register detailing information about sector size and number of banks
present.
Type RO
Bits Field Name Description Type Reset
31:19 RESERVED_31_19 Reserved RO 0b0 0000 0000 0000
18:16 NUMBANKS Number of banks instantiated
Minimum: 1
Maximum: 5
Value ENUM Name Description
0x1 MINIMUM Minimum value
0x5 MAXIMUM Maximum value
RO 0b001
15:0 SECTORSIZE Sector size in bytes
Value ENUM Name Description
0x400 ONEKB Sector size is ONEKB
0x800 TWOKB Sector size is TWOKB
RO 0x0800

TOP:FLASH:GBLINFO1

Address Offset 0x0000 03F4
Physical Address 0x4002 13F4 Instance 0x4002 13F4
Description Global Info 1 Register
Read only register detailing information about data, ecc and redundant data
widths in bits.
Type RO
Bits Field Name Description Type Reset
31:19 RESERVED_31_19 Reserved RO 0b0 0000 0000 0000
18:16 REDWIDTH Redundant data width in bits
Value ENUM Name Description
0x0 W0BIT Redundant data width is 0. Redundancy/Repair not present.
0x2 W2BIT Redundant data width is 2 bits
0x4 W4BIT Redundant data width is 4 bits
RO 0b100
15:13 RESERVED_15_13 Reserved RO 0b000
12:8 ECCWIDTH ECC data width in bits
Value ENUM Name Description
0x0 W0BIT ECC data width is 0. ECC not used.
0x8 W8BIT ECC data width is 8 bits
0x10 W16BIT ECC data width is 16 bits
RO 0b0 0000
7:0 DATAWIDTH Data width in bits
Value ENUM Name Description
0x40 W64BIT Data width is 64 bits
0x80 W128BIT Data width is 128 bits
RO 0x80

TOP:FLASH:GBLINFO2

Address Offset 0x0000 03F8
Physical Address 0x4002 13F8 Instance 0x4002 13F8
Description Global Info 2 Register
Read only register detailing information about the number of data registers
present.
Type RO
Bits Field Name Description Type Reset
31:4 RESERVED_31_4 Reserved RO 0x000 0000
3:0 DATAREGISTERS Number of data registers present.
Value ENUM Name Description
0x1 MINIMUM Minimum value of DATAREGISTERS
0x8 MAXIMUM Maximum value of DATAREGISTERS
RO 0x1

TOP:FLASH:BANK0INFO0

Address Offset 0x0000 0400
Physical Address 0x4002 1400 Instance 0x4002 1400
Description Bank Info 0 Register for bank 0.
Read only register detailing information about Main region size in the bank.
Type RO
Bits Field Name Description Type Reset
31:12 RESERVED_31_12 Reserved RO 0x0 0000
11:0 MAINSIZE Main region size in sectors
Minimum: 0x8 (8)
Maximum: 0x200 (512)
Value ENUM Name Description
0x8 MINSECTORS Minimum value of MAINSIZE
0x200 MAXSECTORS Maximum value of MAINSIZE
RO 0x100

TOP:FLASH:BANK0INFO1

Address Offset 0x0000 0404
Physical Address 0x4002 1404 Instance 0x4002 1404
Description Bank Info1 Register for bank 0.
Read only register detailing information about Non-Main, Trim, and Engr
region sizes in the bank.
Type RO
Bits Field Name Description Type Reset
31:24 RESERVED_31_24 Reserved RO 0x00
23:16 ENGRSIZE Engr region size in sectors
Minimum: 0x0 (0)
Maximum: 0x10 (16)
Value ENUM Name Description
0x0 MINSECTORS Minimum value of ENGRSIZE
0x20 MAXSECTORS Maximum value of ENGRSIZE
RO 0x01
15:8 TRIMSIZE Trim region size in sectors
Minimum: 0x0 (0)
Maximum: 0x10 (16)
Value ENUM Name Description
0x0 MINSECTORS Minimum value of TRIMSIZE
0x20 MAXSECTORS Maximum value of TRIMSIZE
RO 0x01
7:0 NONMAINSIZE Non-main region size in sectors
Minimum: 0x0 (0)
Maximum: 0x10 (16)
Value ENUM Name Description
0x0 MINSECTORS Minimum value of NONMAINSIZE
0x20 MAXSECTORS Maximum value of NONMAINSIZE
RO 0x01