DCB

Instance: DCB
Component: DCB
Base address: 0xE000ED30


TOP:DCB Register Summary

Register Name

Type

Register Width (Bits)

Register Reset

Address Offset

Physical Address

DFSR

32

0x0000 0000

0x0000 0000

0xE000 ED30

DHCSR

32

0x0000 0000

0x0000 00C0

0xE000 EDF0

DCRSR

32

0x0000 0000

0x0000 00C4

0xE000 EDF4

DCRDR

32

0x0000 0000

0x0000 00C8

0xE000 EDF8

DEMCR

32

0x0000 0000

0x0000 00CC

0xE000 EDFC

TOP:DCB Register Descriptions

TOP:DCB:DFSR

Address Offset 0x0000 0000
Physical Address 0xE000 ED30 Instance 0xE000 ED30
Description Debug Fault Status Register

Use the Debug Fault Status Register to monitor external debug requests, vector catches, data watchpoint match, BKPT instruction execution and BPU comparator matches, halt requests. Write one to clear. C_DEBUGEN must be set before any bits in DFSR are updated.
Type
Bits Field Name Description Type Reset
31:5 RESERVED5 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000 0000 0000 0000 0000 0000
4 EXTERNAL External debug request flag
0x0:No edbgrq external debug request occurred
0x1:Edbgrq has halted the core
RW 0
3 VCATCH Vector catch flag. When the VCATCH flag is set, a flag in the Debug Exception and Monitor Control Register is also set to indicate the type of vector catch.
0x0:No vector catch occurred
0x1:Vector catch occurred
RW 0
2 DWTRAP Data Watchpoint (DW) flag.
0x0:No dw match
0x1:Dw match
RW 0
1 BKPT The BKPT flag is set by the execution of the BKPT instruction or on an instruction whose address triggered the breakpoint comparator match. When the processor has halted, the return PC points to the address of the breakpointed instruction.
0x0:No bkpt instruction or hardware breakpoint match
0x1:Bkpt instruction or hardware breakpoint match
RW 0
0 HALTED Halt request flag
0x0:No halt request
0x1:Halt requested by dap access to c_halt or halted with c_step asserted
RW 0

TOP:DCB:DHCSR

Address Offset 0x0000 00C0
Physical Address 0xE000 EDF0 Instance 0xE000 EDF0
Description Debug Halting Control and Status Register

The purpose of the Debug Halting Control and Status Register (DHCSR) is to provide status information about the state of the processor, enable core debug, halt and step the processor. For writes, 0xA05F must be written to bits [31:16], otherwise the write operation is ignored and no bits are written into the register.
Type
Bits Field Name Description Type Reset
31:26 RESERVED26 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b00 0000
25 S_RESET_ST Indicates that the core has been reset, or is now being reset, since the last time this bit was read. This a sticky bit that clears on read. So, reading twice and getting 1 then 0 means it was reset in the past. Reading twice and getting 1 both times means that it is currently reset and held in reset. RO 0
24 S_RETIRE_ST Core has retired at least part of an instruction since last read. This is a sticky bit that clears on read. RO 0
23:18 RESERVED18 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b00 0000
17 S_HALT The core is halted in debug state only if S_HALT is set. RO 0
16 S_REGRDY Register Read/Write to the Debug Core Register Selector Register is available. Set in response to a successful register access. RO 0
15:4 RESERVED4 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0x000
3 C_MASKINTS When this bit is set and debug is enabled, external interrupts, SysTick, and PendSV are masked. Does not affect NMI, Hard Fault or SVCall. When C_DEBUGEN = 0, this bit has no effect. RW 0
2 C_STEP Causes a debug event on any instruction or exception being executed, resulting in the core single stepping. RW 0
1 C_HALT Halts the core. This bit is set automatically when the core triggers a debug event, for example, on a breakpoint. This bit clears on core reset. When C_DEBUGEN = 0, this bit has no effect. RW 0
0 C_DEBUGEN Enables or disable debug
Value ENUM Name Description
0x0 DBG_DIS Debug disabled
0x1 DBG_EN Debug enabled
RW 0

TOP:DCB:DCRSR

Address Offset 0x0000 00C4
Physical Address 0xE000 EDF4 Instance 0xE000 EDF4
Description Debug Core Register Selector Register

The purpose of the Debug Core Register Selector Register (DCRSR) is to select the processor register to transfer data to or from.
Type
Bits Field Name Description Type Reset
31:17 RESERVED17 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000 0000 0000
16 REGWnR Register Write-not-Read
0x0:Read
0x1:Write
WO 0
15:5 RESERVED5 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000 0000
4:0 REGSEL Select processor register
0x00:R0
0x01:R1
0x02:R2
0x03:R3
0x04:R4
0x05:R5
0x06:R6
0x07:R7
0x08:R8
0x09:R9
0x0a:R10
0x0b:R11
0x0c:R12
0x0d:Current sp
0x0e:Lr
0x0f:Debug Return Address
0x10:Xpsr flags, execution number, and state information
0x11:Msp (main sp)
0x12:Psp (process sp)
0x14:Control (dcrdr[25:24]), primask (dcrdr[0])
WO 0b0 0000

TOP:DCB:DCRDR

Address Offset 0x0000 00C8
Physical Address 0xE000 EDF8 Instance 0xE000 EDF8
Description Debug Core Register Data Register

The purpose of the Debug Core Register Data Register (DCRDR) is to hold data read from or written to core registers.
Type
Bits Field Name Description Type Reset
31:0 DBGTMP Data temporary cache, for reading and writing registers. RW 0x0000 0000

TOP:DCB:DEMCR

Address Offset 0x0000 00CC
Physical Address 0xE000 EDFC Instance 0xE000 EDFC
Description Debug Exception and Monitor Control Register

The purpose of the Debug Exception and Monitor Control Register (DEMCR) is: Global enable for the DW unit, Vector catching (that is, causes debug entry on execution of a specified vector.)
Type
Bits Field Name Description Type Reset
31:25 RESERVED25 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b000 0000
24 DWTENA Global enable or disable for the DW unit
0x0:Dw unit disabled. watchpoint cannot halt the core. the dw pcsr reads as oxffffffff.
0x1:Dw unit enabled
RW 0
23:11 RESERVED11 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b0 0000 0000 0000
10 VC_HARDERR Debug trap on a Hard Fault RW 0
9:1 RESERVED1 Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. RO 0b0 0000 0000
0 VC_CORERESET Reset Vector Catch. Halt running system if HRESETn is asserted RW 0