SimpleLink Low Power F3 Core SDK Change Log
Table of Contents
- Core SDK 7.40.02 (Dec, 2023)
- Core SDK 7.20.01 (Sep, 2023)
- Core SDK 7.20.00 (Jun, 2023)
- Core SDK 7.11.01 (Apr, 2023)
- Core SDK 7.11.00 (Apr, 2023)
- Core SDK 7.10.02 (Apr, 2023)
- Core SDK 7.10.01 (Apr, 2023)
- Core SDK 7.10.00 (Feb, 2023)
- Core SDK 6.30.00 (Sep, 2022)
- Core SDK 6.20.00 (Feb, 2021)
- Core SDK 6.10.00 (Feb, 2021)
Core SDK 7.40.02 (Dec, 2023)
New Features
ID | Summary |
---|---|
TIDRIVERS-6270 | CCFG SysConfig module should explicitly set the CRC32 checksums to 0 |
TIDRIVERS-6134 | Include FreeRTOS kernel source files in Core SDK |
TIDRIVERS-6112 | Enable gpioshutdown example |
TIDRIVERS-6110 | Add API for modular reduction for non-curve length input length |
TIDRIVERS-6103 | Do not dynamically set IPEAK in active vs standby |
TIDRIVERS-6099 | Add MessageQueueP DPL module |
TIDRIVERS-6086 | Add support for FreeRTOS tick rates != 1ms |
TIDRIVERS-6075 | Remove unused Power function prototypes |
TIDRIVERS-6072 | Improve temperature measurement accuracy of Temperature driver |
TIDRIVERS-6070 | Improve RF temperature compensation capacitor array model |
TIDRIVERS-6029 | Add UART -> SysTimer timestamp example |
TIDRIVERS-6017 | Remove SHA2 driver interrupt priority in SysConfig |
TIDRIVERS-5998 | Update Power driver APIs to use uint32_t for resource IDs instead of uint_fast16_t |
TIDRIVERS-5919 | RNG instance pool alignment should be 4-bytes instead of 32-bytes |
TIDRIVERS-5913 | Add Power_getConstraintCount |
TIDRIVERS-5889 | Update Random_seedAutomatic() to use a seed from RNG. |
TIDRIVERS-5495 | Add LogSinkUART |
TIDRIVERS-126 | Add I2CTarget driver |
LPRFXXWARE-861 | Update tempsense diode voltage-to-temp function |
FREERTOS-12 | Allow configuration of FreeRTOS source location |
FREERTOS-10 | Add support for custom tickrate in FreeRTOS Sysconfig Module |
FREERTOS-6 | FreeRTOS GCC standard library re-entrancy support causes task control block size of 340 bytes |
Bugs Resolved
ID | Summary |
---|---|
TIDRIVERS-6336 | Increase RNG's minimum entropy raw noise words from 80 to 152 to add margin for CC23x0 |
TIDRIVERS-6267 | LP_EM_CC2340R5 spicontroller and spiperipheral examples halt in boot / enter bootloader |
TIDRIVERS-6209 | FreeRTOS uses 3 priority bits instead of the supported 2 on CC23X0 devices |
TIDRIVERS-6080 | systimtimestamp example uses undefined macro |
TIDRIVERS-6067 | SysTimer (ClockP) reading after async wakeup from standby may incorrectly be 0 |
TIDRIVERS-6065 | Some PWM files not exported into SDK |
TIDRIVERS-6054 | Stopping a ClockP clock does not result in recomputation of the next timeout |
TIDRIVERS-6046 | Starting HFXT when it is already running causes TRACKREFLOSS |
TIDRIVERS-6041 | Unaligned input to AESGCM GHASH function causes memory corruption |
TIDRIVERS-5969 | GPIO_resetConfig permanently clears IO callbacks set through SysConfig |
LPRFXXWARE-864 | IntSetPriority does not re-enable interrupt if it was previously enabled |
Core SDK 7.20.01 (Sep, 2023)
New Features
ID | Summary |
---|---|
TIDRIVERS-6110 | Add API for modular reduction for non-curve length input length |
TIDRIVERS-6025 | Add Elliptic Curve Integrated Encryption Scheme (ECIES) driver for CC23x0 |
Bugs Resolved
ID | Summary |
---|---|
TIDRIVERS-6065 | Some PWM files not exported into SDK |
Core SDK 7.20.00 (Jun, 2023)
New Features
ID | Summary |
---|---|
TIDRIVERS-6038 | Change default value of LGPTimerLPF3 driver param.intPhaseLate element |
TIDRIVERS-6037 | Add support for any AES-GCM IV length on CC23x0 (only supported 12 bytes previously) |
TIDRIVERS-6025 | Add Elliptic Curve Integrated Encryption Scheme (ECIES) driver for CC23x0 |
TIDRIVERS-6010 | Clarify documented functionality of LGPT counter target value |
TIDRIVERS-6007 | Add ANSI x9.63 KDF |
TIDRIVERS-6003 | Add ECDSA public key and signature validation for CC23x0 and CC13x1/26x1 |
TIDRIVERS-6002 | Add NIST P-224 curve support for ECDSA on CC23x0 |
TIDRIVERS-5995 | Add PWM driver implementation |
TIDRIVERS-5953 | Add optional temperature compensation for CLKSVT |
TIDRIVERS-5911 | Dynamically set IPEAK in active vs standby |
TIDRIVERS-5907 | Add PWM and capture functionality to LGPT driver |
TIDRIVERS-5788 | Export driverlib library with GenLibs and DeviceFamily with GenOpts |
TIDRIVERS-5421 | ECC library has compiler warning when building drivers. |
Bugs Resolved
ID | Summary |
---|---|
TIDRIVERS-6042 | SysConfig generates code with a typo for Debug Configuration “Require debug authentication” |
TIDRIVERS-6040 | HFOSC tracking loop stops when exiting standby with debugger connected |
TIDRIVERS-5843 | Remove LegacyTerminology.h backwards compatibility header |
TIDRIVERS-5610 | SemaphoreP_pend returns prematurely on FreeRTOS |
TIDRIVERS-5306 | Include DPL in doxygen documentation |
SYSBIOS-1602 | Assert_isTrue macro expands incorrectly |
LPRFXXWARE-853 | TempDiodeGetTemp inverts current interrupt-enable state |
FREERTOS-16 | Disabling FreeRTOS SW timers causes a build error |
FREERTOS-9 | FreeRTOS ROV does not show system stack usage on CC23X0 devices |
Core SDK 7.11.01 (Apr, 2023)
New Features
ID | Summary |
---|---|
None | None |
Bugs Resolved
ID | Summary |
---|---|
None | None |
Core SDK 7.11.00 (Apr, 2023)
New Features
ID | Summary |
---|---|
None | None |
Bugs Resolved
ID | Summary |
---|---|
SYSBIOS-1602 | Assert_isTrue macro expands incorrectly |
Core SDK 7.10.02 (Apr, 2023)
New Features
ID | Summary |
---|---|
None | None |
Bugs Resolved
ID | Summary |
---|---|
None | None |
Core SDK 7.10.01 (Apr, 2023)
New Features
ID | Summary |
---|---|
None | None |
Bugs Resolved
ID | Summary |
---|---|
None | None |
Core SDK 7.10.00 (Feb, 2023)
New Features
ID | Summary |
---|---|
None | None |
Bugs Resolved
ID | Summary |
---|---|
None | None |
Core SDK 6.30.00 (Sep, 2022)
New Features
ID | Summary |
---|---|
None | None |
Bugs Resolved
ID | Summary |
---|---|
None | None |
Core SDK 6.20.00 (Feb, 2021)
New Features
ID | Summary |
---|---|
None | None |
Bugs Resolved
ID | Summary |
---|---|
None | None |
Core SDK 6.10.00 (Feb, 2021)
New Features
ID | Summary |
---|---|
None | None |
Bugs Resolved
ID | Summary |
---|---|
None | None |