Data Structures
ANSIX936KDFXX.h File Reference

Detailed Description

ANSI-X9.63 Key Derivation Function driver implementation for the CC13X1/CC26X1, CC13X2/CC26X2, CC13X4/CC26X4, and CC23X0 families.

============================================================================

This file should only be included in the board file to fill the ANSIX936KDF_config struct.

Supported Hash Type

SHA-256 is in the only hash type supported.

Limitations

#include <stdbool.h>
#include <ti/drivers/SHA2.h>
#include <ti/devices/DeviceFamily.h>
#include <ti/drivers/sha2/SHA2CC26X1.h>
Include dependency graph for ANSIX936KDFXX.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  ANSIX936KDFXX_HWAttrs
 Hardware-specific configuration attributes. More...
 
struct  ANSIX936KDFXX_Object
 ANSIX936KDFXX Object. More...
 
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale