Instance: UART1
Component: UART
Base address: 0x40035000
Universal Asynchronous Receiver/Transmitter (UART) interface
Register Name |
Type |
Register Width (Bits) |
Register Reset |
Address Offset |
Physical Address |
RW |
32 |
0x0000 0000 |
0x0000 0000 |
0x4003 5000 |
|
RW |
32 |
0x0000 0000 |
0x0000 0004 |
0x4003 5004 |
|
RO |
32 |
0x0000 0091 |
0x0000 0018 |
0x4003 5018 |
|
RW |
32 |
0x0000 0000 |
0x0000 0020 |
0x4003 5020 |
|
RW |
32 |
0x0000 0000 |
0x0000 0024 |
0x4003 5024 |
|
RW |
32 |
0x0000 0000 |
0x0000 0028 |
0x4003 5028 |
|
RW |
32 |
0x0000 0000 |
0x0000 002C |
0x4003 502C |
|
RW |
32 |
0x0000 0300 |
0x0000 0030 |
0x4003 5030 |
|
RW |
32 |
0x0000 0012 |
0x0000 0034 |
0x4003 5034 |
|
RW |
32 |
0x0000 0000 |
0x0000 0038 |
0x4003 5038 |
|
RO |
32 |
0x0000 000D |
0x0000 003C |
0x4003 503C |
|
RO |
32 |
0x0000 0000 |
0x0000 0040 |
0x4003 5040 |
|
WO |
32 |
0x0000 0000 |
0x0000 0044 |
0x4003 5044 |
|
RW |
32 |
0x0000 0000 |
0x0000 0048 |
0x4003 5048 |
|
32 |
0x0000 0000 |
0x0000 004C |
0x4003 504C |
Address Offset | 0x0000 0000 | ||
Physical Address | 0x4003 5000 | Instance | 0x4003 5000 |
Description | Data For words to be transmitted: - if the FIFOs are enabled (LCRH.FEN = 1), data written to this location is pushed onto the transmit FIFO - if the FIFOs are not enabled (LCRH.FEN = 0), data is stored in the transmitter holding register (the bottom word of the transmit FIFO). The write operation initiates transmission from the UART. The data is prefixed with a start bit, appended with the appropriate parity bit (if parity is enabled), and a stop bit. The resultant word is then transmitted. For received words: - if the FIFOs are enabled (LCRH.FEN = 1), the data byte and the 4-bit status (break, frame, parity, and overrun) is pushed onto the 12-bit wide receive FIFO - if the FIFOs are not enabled (LCRH.FEN = 0), the data byte and status are stored in the receiving holding register (the bottom word of the receive FIFO). The received data byte is read by performing reads from this register along with the corresponding status information. The status information can also be read by a read of the RSR register. |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:12 | RESERVED | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x0 0000 | ||
11 | OE | UART Overrun Error: This bit is set to 1 if data is received and the receive FIFO is already full. The FIFO contents remain valid because no more data is written when the FIFO is full, , only the contents of the shift register are overwritten. This is cleared to 0 once there is an empty space in the FIFO and a new character can be written to it. |
RO | 0 | ||
10 | BE | UART Break Error: This bit is set to 1 if a break condition was detected, indicating that the received data input (UARTRXD input pin) was held LOW for longer than a full-word transmission time (defined as start, data, parity and stop bits). In FIFO mode, this error is associated with the character at the top of the FIFO (i.e., the oldest received data character since last read). When a break occurs, a 0 character is loaded into the FIFO. The next character is enabled after the receive data input (UARTRXD input pin) goes to a 1 (marking state), and the next valid start bit is received. |
RO | 0 | ||
9 | PE | UART Parity Error: When set to 1, it indicates that the parity of the received data character does not match the parity that the LCRH.EPS and LCRH.SPS select. In FIFO mode, this error is associated with the character at the top of the FIFO (i.e., the oldest received data character since last read). |
RO | 0 | ||
8 | FE | UART Framing Error: When set to 1, it indicates that the received character did not have a valid stop bit (a valid stop bit is 1). In FIFO mode, this error is associated with the character at the top of the FIFO (i.e., the oldest received data character since last read). |
RO | 0 | ||
7:0 | DATA | Data transmitted or received: On writes, the transmit data character is pushed into the FIFO. On reads, the oldest received data character since the last read is returned. |
RW | 0x00 |
Address Offset | 0x0000 0004 | ||
Physical Address | 0x4003 5004 | Instance | 0x4003 5004 |
Description | Status This register is mapped to the same address as ECR register. Reads from this address are associated with RSR_ECR register and return the receive status. Writes to this address are associated with ECR register and clear the receive status flags (framing, parity, break, and overrun errors). If the status is read from this register, then the status information for break, framing and parity corresponds to the data character read from the Data Register, DR prior to reading the RSR_ECR. The status information for overrun is set immediately when an overrun condition occurs. |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | |||||||||||
31:4 | RESERVED | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x000 0000 | |||||||||||
3 | OE | UART Overrun Error: This bit is set to 1 if data is received and the receive FIFO is already full. The FIFO contents remain valid because no more data is written when the FIFO is full, , only the contents of the shift register are overwritten. This is cleared to 0 once there is an empty space in the FIFO and a new character can be written to it.
|
RW | 0 | |||||||||||
2 | BE | UART Break Error: This bit is set to 1 if a break condition was detected, indicating that the received data input (UARTRXD input pin) was held LOW for longer than a full-word transmission time (defined as start, data, parity and stop bits). When a break occurs, a 0 character is loaded into the FIFO. The next character is enabled after the receive data input (UARTRXD input pin) goes to a 1 (marking state), and the next valid start bit is received.
|
RW | 0 | |||||||||||
1 | PE | UART Parity Error: When set to 1, it indicates that the parity of the received data character does not match the parity that the LCRH.EPS and LCRH.SPS select.
|
RW | 0 | |||||||||||
0 | FE | UART Framing Error: When set to 1, it indicates that the received character did not have a valid stop bit (a valid stop bit is 1).
|
RW | 0 |
Address Offset | 0x0000 0018 | ||
Physical Address | 0x4003 5018 | Instance | 0x4003 5018 |
Description | Flag Reads from this register return the UART flags. |
||
Type | RO |
Bits | Field Name | Description | Type | Reset | ||
31:8 | RESERVED1 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x00 0000 | ||
7 | TXFE | UART Transmit FIFO Empty: The meaning of this bit depends on the state of LCRH.FEN . - If the FIFO is disabled, this bit is set when the transmit holding register is empty. - If the FIFO is enabled, this bit is set when the transmit FIFO is empty. This bit does not indicate if there is data in the transmit shift register. |
RO | 1 | ||
6 | RXFF | UART Receive FIFO Full: The meaning of this bit depends on the state of LCRH.FEN. - If the FIFO is disabled, this bit is set when the receive holding register is full. - If the FIFO is enabled, this bit is set when the receive FIFO is full. |
RO | 0 | ||
5 | TXFF | UART Transmit FIFO Full: Transmit FIFO full. The meaning of this bit depends on the state of LCRH.FEN. - If the FIFO is disabled, this bit is set when the transmit holding register is full. - If the FIFO is enabled, this bit is set when the transmit FIFO is full. |
RO | 0 | ||
4 | RXFE | UART Receive FIFO Empty: Receive FIFO empty. The meaning of this bit depends on the state of LCRH.FEN. - If the FIFO is disabled, this bit is set when the receive holding register is empty. - If the FIFO is enabled, this bit is set when the receive FIFO is empty. |
RO | 1 | ||
3 | BUSY | UART Busy: If this bit is set to 1, the UART is busy transmitting data. This bit remains set until the complete byte, including all the stop bits, has been sent from the shift register. This bit is set as soon as the transmit FIFO becomes non-empty, regardless of whether the UART is enabled or not. |
RO | 0 | ||
2:1 | RESERVED0 | Reserved | RO | 0b00 | ||
0 | CTS | Clear To Send: This bit is the complement of the active-low UART CTS input pin. That is, the bit is 1 when CTS input pin is LOW. |
RO | 1 |
Address Offset | 0x0000 0020 | ||
Physical Address | 0x4003 5020 | Instance | 0x4003 5020 |
Description | IrDA | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:8 | RESERVED | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0x00 0000 | ||
7:0 | ILPDVSR | 8 bit low-power divisor value | RW | 0x00 |
Address Offset | 0x0000 0024 | ||
Physical Address | 0x4003 5024 | Instance | 0x4003 5024 |
Description | Integer Baud-Rate Divisor If this register is modified while trasmission or reception is on-going, the baudrate will not be updated until transmission or reception of the current character is complete. |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:16 | RESERVED | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0x0000 | ||
15:0 | DIVINT | The integer baud rate divisor: The baud rate divisor is calculated using the formula below: Baud rate divisor = (UART reference clock frequency) / (16 * Baud rate) Baud rate divisor must be minimum 1 and maximum 65535. That is, DIVINT=0 does not give a valid baud rate. Similarly, if DIVINT=0xFFFF, any non-zero values in FBRD.DIVFRAC will be illegal. A valid value must be written to this field before the UART can be used for RX or TX operations. |
RW | 0x0000 |
Address Offset | 0x0000 0028 | ||
Physical Address | 0x4003 5028 | Instance | 0x4003 5028 |
Description | Fractional Baud-Rate Divisor If this register is modified while trasmission or reception is on-going, the baudrate will not be updated until transmission or reception of the current character is complete. |
||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:6 | RESERVED | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b00 0000 0000 0000 0000 0000 0000 | ||
5:0 | DIVFRAC | Fractional Baud-Rate Divisor: The baud rate divisor is calculated using the formula below: Baud rate divisor = (UART reference clock frequency) / (16 * Baud rate) Baud rate divisor must be minimum 1 and maximum 65535. That is, IBRD.DIVINT=0 does not give a valid baud rate. Similarly, if IBRD.DIVINT=0xFFFF, any non-zero values in DIVFRAC will be illegal. A valid value must be written to this field before the UART can be used for RX or TX operations. |
RW | 0b00 0000 |
Address Offset | 0x0000 002C | ||
Physical Address | 0x4003 502C | Instance | 0x4003 502C |
Description | Line Control | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | |||||||||||||||||
31:11 | RESERVED | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b0 0000 0000 0000 0000 0000 | |||||||||||||||||
10:9 | DELIM | In UART LIN defines the length of DELIM field that has to be sent
|
RW | 0b00 | |||||||||||||||||
8 | TXBRKSYNC | UART LIN mode TXBRKSYNC: 0: In LIN mode TXBRKSYNC will not be sent. 1: In LIN mode send TXBRKSYNC field and reset the LCRH.TXBRKSYNC bit. This bit has no effect when PEN disables parity checking and generation. |
RW | 0 | |||||||||||||||||
7 | SPS | UART Stick Parity Select: 0: Stick parity is disabled 1: The parity bit is transmitted and checked as invert of EPS field (i.e. the parity bit is transmitted and checked as 1 when EPS = 0). This bit has no effect when PEN disables parity checking and generation. |
RW | 0 | |||||||||||||||||
6:5 | WLEN | UART Word Length: These bits indicate the number of data bits transmitted or received in a frame.
|
RW | 0b00 | |||||||||||||||||
4 | FEN | UART Enable FIFOs
|
RW | 0 | |||||||||||||||||
3 | STP2 | UART Two Stop Bits Select: If this bit is set to 1, two stop bits are transmitted at the end of the frame. The receive logic does not check for two stop bits being received. |
RW | 0 | |||||||||||||||||
2 | EPS | UART Even Parity Select
|
RW | 0 | |||||||||||||||||
1 | PEN | UART Parity Enable This bit controls generation and checking of parity bit.
|
RW | 0 | |||||||||||||||||
0 | BRK | UART Send Break If this bit is set to 1, a low-level is continually output on the UARTTXD output pin, after completing transmission of the current character. For the proper execution of the break command, the software must set this bit for at least two complete frames. For normal use, this bit must be cleared to 0. |
RW | 0 |
Address Offset | 0x0000 0030 | ||
Physical Address | 0x4003 5030 | Instance | 0x4003 5030 |
Description | Control | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | |||||||||||
31:16 | RESERVED16 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x0000 | |||||||||||
15 | CTSEN | CTS hardware flow control enable
|
RW | 0 | |||||||||||
14 | RTSEN | RTS hardware flow control enable
|
RW | 0 | |||||||||||
13:12 | RESERVED12 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b00 | |||||||||||
11 | RTS | Request to Send This bit is the complement of the active-low UART RTS output. That is, when the bit is programmed to a 1 then RTS output on the pins is LOW. |
RW | 0 | |||||||||||
10 | RESERVED10 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0 | |||||||||||
9 | RXE | UART Receive Enable If the UART is disabled in the middle of reception, it completes the current character before stopping.
|
RW | 1 | |||||||||||
8 | TXE | UART Transmit Enable If the UART is disabled in the middle of transmission, it completes the current character before stopping.
|
RW | 1 | |||||||||||
7 | LBE | UART Loop Back Enable Enabling the loop-back mode connects the UARTTXD output from the UART to UARTRXD input of the UART.
|
RW | 0 | |||||||||||
6 | FCEN | UART FIFO Concatenation Enable Enabling the lFIFO concatenetion in TX moderesulting in 16 TX buffers.
|
RW | 0 | |||||||||||
5 | DORMEN | DORMEN bit is only functionally makes sense for LIN mode of operation. When dormant mode is disabled, break and synch data shall be loaded to RX FIFO and associated interrupt flags shall be set as in normal UART operation. When dormant mode is enabled, break and synch data shall not be loaded to RX FIFO and RX FIFO shall be updated with actual data (PID) only after successful reception of break/synch fields.
|
RW | 0 | |||||||||||
4 | ABDEN | This configuration bit defines whether we want automatic baud rate detection enabled or not in the LIN mode of operation.
|
RW | 0 | |||||||||||
3 | LINEN | This is the LIN Mode of operation configuration bit.
|
RW | 0 | |||||||||||
2 | SIRLP | SIR low power IrDA mode This bit selects the IrDA encoding mode
|
RW | 0 | |||||||||||
1 | SIREN | SIR Enable This bit has no effect if UARTEN bit disables the UART.
|
RW | 0 | |||||||||||
0 | UARTEN | UART Enable
|
RW | 0 |
Address Offset | 0x0000 0034 | ||
Physical Address | 0x4003 5034 | Instance | 0x4003 5034 |
Description | Interrupt FIFO Level Select | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||||||||||||||
31:6 | RESERVED | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b00 0000 0000 0000 0000 0000 0000 | ||||||||||||||
5:3 | RXSEL | Receive interrupt FIFO level select: This field sets the trigger points for the receive interrupt. Values 0b101-0b111 are reserved.
|
RW | 0b010 | ||||||||||||||
2:0 | TXSEL | Transmit interrupt FIFO level select: This field sets the trigger points for the transmit interrupt. Values 0b101-0b111 are reserved.
|
RW | 0b010 |
Address Offset | 0x0000 0038 | ||
Physical Address | 0x4003 5038 | Instance | 0x4003 5038 |
Description | Interrupt Mask Set/Clear | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:17 | RESERVED11 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b000 0000 0000 0000 | ||
16 | LINSYNCTOEIM | LIN Sync Time out error interrupt mask. A read returns the current mask for UART's LINSYNCTOE interrupt. On a write of 1, the mask of the LINSYNCTOE interrupt is set which means the interrupt state will be reflected in MIS.LINSYNCTOE. A write of 0 clears the mask which means MIS.LINSYNCTOE will not reflect the interrupt. | RW | 0 | ||
15 | LINBRKTOEIM | LIN Break field Time out error interrupt mask. A read returns the current mask for UART's LINBRKTOE interrupt. On a write of 1, the mask of the LINBRKTOE interrupt is set which means the interrupt state will be reflected in MIS.LINBRKTOE. A write of 0 clears the mask which means MIS.LINBRKTOE will not reflect the interrupt. | RW | 0 | ||
14 | LINBRKIM | LIN Break field recieved/detected interrupt mask. A read returns the current mask for UART's LINBRK interrupt. On a write of 1, the mask of the LINBRK interrupt is set which means the interrupt state will be reflected in MIS.LINBRK. A write of 0 clears the mask which means MIS.LINBRK will not reflect the interrupt. | RW | 0 | ||
13 | RXDMADONEIM | Rx DMA done interrupt mask. A read returns the current mask for UART's RXDMADONE interrupt. On a write of 1, the mask of the RXDMADONE interrupt is set which means the interrupt state will be reflected in MIS.RXDMADONEMIS. A write of 0 clears the mask which means MIS.RXDMADONEMIS will not reflect the interrupt. | RW | 0 | ||
12 | TXDMADONEIM | Tx DMA done interrupt mask. A read returns the current mask for UART's TXDMADONE interrupt. On a write of 1, the mask of the TXDMADONE interrupt is set which means the interrupt state will be reflected in MIS.TXDMADONEMIS. A write of 0 clears the mask which means MIS.TXDMADONEMIS will not reflect the interrupt. | RW | 0 | ||
11 | EOTIM | End of Transmission interrupt mask. A read returns the current mask for UART's EoT interrupt. On a write of 1, the mask of the EoT interrupt is set which means the interrupt state will be reflected in MIS.EOTMIS. A write of 0 clears the mask which means MIS.EOTMIS will not reflect the interrupt. | RW | 0 | ||
10 | OEIM | Overrun error interrupt mask. A read returns the current mask for UART's overrun error interrupt. On a write of 1, the mask of the overrun error interrupt is set which means the interrupt state will be reflected in MIS.OEMIS. A write of 0 clears the mask which means MIS.OEMIS will not reflect the interrupt. | RW | 0 | ||
9 | BEIM | Break error interrupt mask. A read returns the current mask for UART's break error interrupt. On a write of 1, the mask of the overrun error interrupt is set which means the interrupt state will be reflected in MIS.BEMIS. A write of 0 clears the mask which means MIS.BEMIS will not reflect the interrupt. | RW | 0 | ||
8 | PEIM | Parity error interrupt mask. A read returns the current mask for UART's parity error interrupt. On a write of 1, the mask of the overrun error interrupt is set which means the interrupt state will be reflected in MIS.PEMIS. A write of 0 clears the mask which means MIS.PEMIS will not reflect the interrupt. | RW | 0 | ||
7 | FEIM | Framing error interrupt mask. A read returns the current mask for UART's framing error interrupt. On a write of 1, the mask of the overrun error interrupt is set which means the interrupt state will be reflected in MIS.FEMIS. A write of 0 clears the mask which means MIS.FEMIS will not reflect the interrupt. | RW | 0 | ||
6 | RTIM | Receive timeout interrupt mask. A read returns the current mask for UART's receive timeout interrupt. On a write of 1, the mask of the overrun error interrupt is set which means the interrupt state will be reflected in MIS.RTMIS. A write of 0 clears the mask which means this bitfield will not reflect the interrupt. The raw interrupt for receive timeout RIS.RTRIS cannot be set unless the mask is set (RTIM = 1). This is because the mask acts as an enable for power saving. That is, the same status can be read from MIS.RTMIS and RIS.RTRIS. |
RW | 0 | ||
5 | TXIM | Transmit interrupt mask. A read returns the current mask for UART's transmit interrupt. On a write of 1, the mask of the overrun error interrupt is set which means the interrupt state will be reflected in MIS.TXMIS. A write of 0 clears the mask which means MIS.TXMIS will not reflect the interrupt. | RW | 0 | ||
4 | RXIM | Receive interrupt mask. A read returns the current mask for UART's receive interrupt. On a write of 1, the mask of the overrun error interrupt is set which means the interrupt state will be reflected in MIS.RXMIS. A write of 0 clears the mask which means MIS.RXMIS will not reflect the interrupt. | RW | 0 | ||
3:2 | RESERVED2 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0b00 | ||
1 | CTSMIM | Clear to Send (CTS) modem interrupt mask. A read returns the current mask for UART's clear to send interrupt. On a write of 1, the mask of the overrun error interrupt is set which means the interrupt state will be reflected in MIS.CTSMMIS. A write of 0 clears the mask which means MIS.CTSMMIS will not reflect the interrupt. | RW | 0 | ||
0 | RESERVED0 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RW | 0 |
Address Offset | 0x0000 003C | ||
Physical Address | 0x4003 503C | Instance | 0x4003 503C |
Description | Raw Interrupt Status | ||
Type | RO |
Bits | Field Name | Description | Type | Reset | ||
31:17 | RESERVED11 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 0000 0000 | ||
16 | LINSYNCTOERIS | LIN SYNC field time out interrupt status: This field returns the raw interrupt state of whether sync field is measurable in UART's LIN mode of operation. This is set when the timer measuring the SYNC field overflows. |
RO | 0 | ||
15 | LINBRKTOERIS | LIN BRK field time out interrupt status: This field returns the raw interrupt state of whether break field is measurable in UART's LIN mode of operation. This is set when the timer measuring the Break field overflows. |
RO | 0 | ||
14 | LINBRKRIS | LIN BRK detected interrupt status: This field returns the raw interrupt state of whether break field is recieved/detected in UART's LIN mode of operation. |
RO | 0 | ||
13 | RXDMADONERIS | Rx DMA done interrupt status: This field returns the raw interrupt state of UART's rx dma done interrupt. RX DMA done flag is set when you recieve rx dma done status from dma module. |
RO | 0 | ||
12 | TXDMADONERIS | Tx DMA done interrupt status: This field returns the raw interrupt state of UART's tx dma done interrupt. TX DMA done flag is set when you recieve tx dma done status from dma module. |
RO | 0 | ||
11 | EOTRIS | End of Transmission interrupt status: This field returns the raw interrupt state of UART's end of transmission interrupt. End of transmission flag is set when all the Transmit data in the FIFO and on the TX Line is tranmitted. |
RO | 0 | ||
10 | OERIS | Overrun error interrupt status: This field returns the raw interrupt state of UART's overrun error interrupt. Overrun error occurs if data is received and the receive FIFO is full. |
RO | 0 | ||
9 | BERIS | Break error interrupt status: This field returns the raw interrupt state of UART's break error interrupt. Break error is set when a break condition is detected, indicating that the received data input (UARTRXD input pin) was held LOW for longer than a full-word transmission time (defined as start, data, parity and stop bits). |
RO | 0 | ||
8 | PERIS | Parity error interrupt status: This field returns the raw interrupt state of UART's parity error interrupt. Parity error is set if the parity of the received data character does not match the parity that the LCRH.EPS and LCRH.SPS select. |
RO | 0 | ||
7 | FERIS | Framing error interrupt status: This field returns the raw interrupt state of UART's framing error interrupt. Framing error is set if the received character does not have a valid stop bit (a valid stop bit is 1). |
RO | 0 | ||
6 | RTRIS | Receive timeout interrupt status: This field returns the raw interrupt state of UART's receive timeout interrupt. The receive timeout interrupt is asserted when the receive FIFO is not empty, and no more data is received during a 32-bit period. The receive timeout interrupt is cleared either when the FIFO becomes empty through reading all the data, or when a 1 is written to ICR.RTIC. The raw interrupt for receive timeout cannot be set unless the mask is set (IMSC.RTIM = 1). This is because the mask acts as an enable for power saving. That is, the same status can be read from MIS.RTMIS and RTRIS. |
RO | 0 | ||
5 | TXRIS | Transmit interrupt status: This field returns the raw interrupt state of UART's transmit interrupt. When FIFOs are enabled (LCRH.FEN = 1), the transmit interrupt is asserted if the number of bytes in transmit FIFO is equal to or lower than the programmed trigger level (IFLS.TXSEL). The transmit interrupt is cleared by writing data to the transmit FIFO until it becomes greater than the trigger level, or by clearing the interrupt through ICR.TXIC. When FIFOs are disabled (LCRH.FEN = 0), that is they have a depth of one location, the transmit interrupt is asserted if there is no data present in the transmitters single location. It is cleared by performing a single write to the transmit FIFO, or by clearing the interrupt through ICR.TXIC. |
RO | 0 | ||
4 | RXRIS | Receive interrupt status: This field returns the raw interrupt state of UART's receive interrupt. When FIFOs are enabled (LCRH.FEN = 1), the receive interrupt is asserted if the receive FIFO reaches the programmed trigger level (IFLS.RXSEL). The receive interrupt is cleared by reading data from the receive FIFO until it becomes less than the trigger level, or by clearing the interrupt through ICR.RXIC. When FIFOs are disabled (LCRH.FEN = 0), that is they have a depth of one location, the receive interrupt is asserted if data is received thereby filling the location. The receive interrupt is cleared by performing a single read of the receive FIFO, or by clearing the interrupt through ICR.RXIC. |
RO | 0 | ||
3:2 | RESERVED2 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b11 | ||
1 | CTSRMIS | Clear to Send (CTS) modem interrupt status: This field returns the raw interrupt state of UART's clear to send interrupt. |
RO | 0 | ||
0 | RESERVED0 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 1 |
Address Offset | 0x0000 0040 | ||
Physical Address | 0x4003 5040 | Instance | 0x4003 5040 |
Description | Masked Interrupt Status | ||
Type | RO |
Bits | Field Name | Description | Type | Reset | ||
31:17 | RESERVED11 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. Read as zero, do not modify | RO | 0b000 0000 0000 0000 | ||
16 | LINSYNCTOEMIS | LIN sync field time out error interrupt status: This field returns the masked interrupt state of the LIN sync timeout error interrupt which is the AND product of raw interrupt state RIS.LINSYNCTOERIS and the mask setting IMSC.LINSYNCTOEIM. |
RO | 0 | ||
15 | LINBRKTOEMIS | LIN BRK field time out error interrupt status: This field returns the masked interrupt state of the LIN BRK timeout error interrupt which is the AND product of raw interrupt state RIS.LINBRKTOERIS and the mask setting IMSC.LINBRKTOEIM. |
RO | 0 | ||
14 | LINBRKMIS | LIN BRK field detected interrupt status: This field returns the masked interrupt state of the LIN BRK detected interrupt which is the AND product of raw interrupt state RIS.LINBRKRIS and the mask setting IMSC.LINBRKIM. |
RO | 0 | ||
13 | RXDMADONEMIS | Rx DMA done interrupt status: This field returns the masked interrupt state of the rx dma done interrupt which is the AND product of raw interrupt state RIS.RXDMADONERIS and the mask setting IMSC.RXDMADONEIM. |
RO | 0 | ||
12 | TXDMADONEMIS | Tx DMA done interrupt status: This field returns the masked interrupt state of the tx dma done interrupt which is the AND product of raw interrupt state RIS.TXDMADONERIS and the mask setting IMSC.TXDMADONEIM. |
RO | 0 | ||
11 | EOTMIS | End of Transmission interrupt status: This field returns the masked interrupt state of the End of transmission interrupt which is the AND product of raw interrupt state RIS.EOTRIS and the mask setting IMSC.EOTIM. |
RO | 0 | ||
10 | OEMIS | Overrun error masked interrupt status: This field returns the masked interrupt state of the overrun interrupt which is the AND product of raw interrupt state RIS.OERIS and the mask setting IMSC.OEIM. |
RO | 0 | ||
9 | BEMIS | Break error masked interrupt status: This field returns the masked interrupt state of the break error interrupt which is the AND product of raw interrupt state RIS.BERIS and the mask setting IMSC.BEIM. |
RO | 0 | ||
8 | PEMIS | Parity error masked interrupt status: This field returns the masked interrupt state of the parity error interrupt which is the AND product of raw interrupt state RIS.PERIS and the mask setting IMSC.PEIM. |
RO | 0 | ||
7 | FEMIS | Framing error masked interrupt status: Returns the masked interrupt state of the framing error interrupt which is the AND product of raw interrupt state RIS.FERIS and the mask setting IMSC.FEIM. | RO | 0 | ||
6 | RTMIS | Receive timeout masked interrupt status: Returns the masked interrupt state of the receive timeout interrupt. The raw interrupt for receive timeout cannot be set unless the mask is set (IMSC.RTIM = 1). This is because the mask acts as an enable for power saving. That is, the same status can be read from RTMIS and RIS.RTRIS. |
RO | 0 | ||
5 | TXMIS | Transmit masked interrupt status: This field returns the masked interrupt state of the transmit interrupt which is the AND product of raw interrupt state RIS.TXRIS and the mask setting IMSC.TXIM. |
RO | 0 | ||
4 | RXMIS | Receive masked interrupt status: This field returns the masked interrupt state of the receive interrupt which is the AND product of raw interrupt state RIS.RXRIS and the mask setting IMSC.RXIM. |
RO | 0 | ||
3:2 | RESERVED2 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 | ||
1 | CTSMMIS | Clear to Send (CTS) modem masked interrupt status: This field returns the masked interrupt state of the clear to send interrupt which is the AND product of raw interrupt state RIS.CTSRMIS and the mask setting IMSC.CTSMIM. |
RO | 0 | ||
0 | RESERVED0 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. Write 0. | RO | 0 |
Address Offset | 0x0000 0044 | ||
Physical Address | 0x4003 5044 | Instance | 0x4003 5044 |
Description | Interrupt Clear On a write of 1, the corresponding interrupt is cleared. A write of 0 has no effect. |
||
Type | WO |
Bits | Field Name | Description | Type | Reset | ||
31:17 | RESERVED11 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. Read as zero, do not modify | WO | 0b000 0000 0000 0000 | ||
16 | LINSYNCTOEIC | LIN SYNC timeout interrupt clear: Writing 1 to this field clears the rxdma done interrupt (RIS.LINSYNCTOERIS). Writing 0 has no effect. |
WO | 0 | ||
15 | LINBRKTOEIC | LIN BRK field timeout interrupt clear: Writing 1 to this field clears the rxdma done interrupt (RIS.LINBRKTOERIS). Writing 0 has no effect. |
WO | 0 | ||
14 | LINBRKIC | LIN BRK field detected interrupt clear: Writing 1 to this field clears the rxdma done interrupt (RIS.LINBRKRIS). Writing 0 has no effect. |
WO | 0 | ||
13 | RXDMADONEIC | Rx DMA Done interrupt clear: Writing 1 to this field clears the rxdma done interrupt (RIS.RXDMADONERIS). Writing 0 has no effect. |
WO | 0 | ||
12 | TXDMADONEIC | Tx DMA Done interrupt clear: Writing 1 to this field clears the txdma done interrupt (RIS.TXDMADONERIS). Writing 0 has no effect. |
WO | 0 | ||
11 | EOTIC | End of Transmission interrupt clear: Writing 1 to this field clears the End of Transmission interrupt (RIS.EOTRIS). Writing 0 has no effect. |
WO | 0 | ||
10 | OEIC | Overrun error interrupt clear: Writing 1 to this field clears the overrun error interrupt (RIS.OERIS). Writing 0 has no effect. |
WO | 0 | ||
9 | BEIC | Break error interrupt clear: Writing 1 to this field clears the break error interrupt (RIS.BERIS). Writing 0 has no effect. |
WO | 0 | ||
8 | PEIC | Parity error interrupt clear: Writing 1 to this field clears the parity error interrupt (RIS.PERIS). Writing 0 has no effect. |
WO | 0 | ||
7 | FEIC | Framing error interrupt clear: Writing 1 to this field clears the framing error interrupt (RIS.FERIS). Writing 0 has no effect. |
WO | 0 | ||
6 | RTIC | Receive timeout interrupt clear: Writing 1 to this field clears the receive timeout interrupt (RIS.RTRIS). Writing 0 has no effect. |
WO | 0 | ||
5 | TXIC | Transmit interrupt clear: Writing 1 to this field clears the transmit interrupt (RIS.TXRIS). Writing 0 has no effect. |
WO | 0 | ||
4 | RXIC | Receive interrupt clear: Writing 1 to this field clears the receive interrupt (RIS.RXRIS). Writing 0 has no effect. |
WO | 0 | ||
3:2 | RESERVED2 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. Write 0 | WO | 0b00 | ||
1 | CTSMIC | Clear to Send (CTS) modem interrupt clear: Writing 1 to this field clears the clear to send interrupt (RIS.CTSRMIS). Writing 0 has no effect. |
WO | 0 | ||
0 | RESERVED0 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. Write 0. | WO | 0 |
Address Offset | 0x0000 0048 | ||
Physical Address | 0x4003 5048 | Instance | 0x4003 5048 |
Description | DMA Control | ||
Type | RW |
Bits | Field Name | Description | Type | Reset | ||
31:3 | RESERVED | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. Read as zero, do not modify. | RW | 0b0 0000 0000 0000 0000 0000 0000 0000 | ||
2 | DMAONERR | DMA on error. If this bit is set to 1, the DMA receive request outputs (for single and burst requests) are disabled when the UART error interrupt is asserted (more specifically if any of the error interrupts RIS.PERIS, RIS.BERIS, RIS.FERIS or RIS.OERIS are asserted). | RW | 0 | ||
1 | TXDMAE | Transmit DMA enable. If this bit is set to 1, DMA for the transmit FIFO is enabled. | RW | 0 | ||
0 | RXDMAE | Receive DMA enable. If this bit is set to 1, DMA for the receive FIFO is enabled. | RW | 0 |
Address Offset | 0x0000 004C | ||
Physical Address | 0x4003 504C | Instance | 0x4003 504C |
Description | Digital Test Bus. This register is used to bring out some internal signals of the peripheral on digital test bus (DTB). | ||
Type |
Bits | Field Name | Description | Type | Reset | |||||||||||||||||||||||||||||
31:3 | RESERVED3 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b0 0000 0000 0000 0000 0000 0000 0000 | |||||||||||||||||||||||||||||
2:0 | SEL | This bit field is used to select DTB mux digital output signals.
|
RW | 0b000 |
© 2015 - 2016. Texas Instruments | All Rights Reserved |