Instance: SYS0
Component: SYS0
Base address: 0x40004000
This is top module of SYS0 for LOKI
|
Register Name |
Type |
Register Width (Bits) |
Register Reset |
Address Offset |
Physical Address |
|
RO |
32 |
0x6B4E 0010 |
0x0000 0000 |
0x4000 4000 |
|
|
RO |
32 |
0x0000 0129 |
0x0000 0004 |
0x4000 4004 |
|
|
WO |
32 |
0x0000 0000 |
0x0000 0008 |
0x4000 4008 |
|
|
WO |
32 |
0x0000 0000 |
0x0000 000C |
0x4000 400C |
|
|
RO |
32 |
0xC000 0000 |
0x0000 0010 |
0x4000 4010 |
|
|
RW |
32 |
0x0000 000F |
0x0000 0100 |
0x4000 4100 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0104 |
0x4000 4104 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0108 |
0x4000 4108 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 010C |
0x4000 410C |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0110 |
0x4000 4110 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0114 |
0x4000 4114 |
|
|
WO |
32 |
0x0000 0000 |
0x0000 0120 |
0x4000 4120 |
|
|
RO |
32 |
0x0BB9 802F |
0x0000 03FC |
0x4000 43FC |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0400 |
0x4000 4400 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0404 |
0x4000 4404 |
|
|
RW |
32 |
0x7FF8 0000 |
0x0000 0408 |
0x4000 4408 |
|
|
WO |
32 |
0x0000 0000 |
0x0000 040C |
0x4000 440C |
|
|
RW |
32 |
0x0000 0000 |
0x0000 07F8 |
0x4000 47F8 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 07FC |
0x4000 47FC |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0800 |
0x4000 4800 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0804 |
0x4000 4804 |
|
|
RW |
32 |
0x0080 0000 |
0x0000 0808 |
0x4000 4808 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 080C |
0x4000 480C |
|
|
RW |
32 |
0xB02E 603F |
0x0000 0810 |
0x4000 4810 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0814 |
0x4000 4814 |
| Address Offset | 0x0000 0000 | ||
| Physical Address | 0x4000 4000 | Instance | 0x4000 4000 |
| Description | This register identifies the peripheral | ||
| Type | RO | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:16 | MODID | Module identification contains a unique peripheral identification number. | RO | 0x6B4E | ||
| 15:12 | STDIPOFF | Standard IP registers offset. Value 0 indicates Standard IP registers are not present. Any other value between 1 to 15 indicates standard IP registers start from address offset 64 * STDIPOFF from base address. | RO | 0x0 | ||
| 11:8 | INSTIDX | Instance Index within the device. This will be a parameter to the RTL for modules that can have multiple instances. | RO | 0x0 | ||
| 7:4 | MAJREV | Major revision of the IP | RO | 0x1 | ||
| 3:0 | MINREV | Minor revision of the IP | RO | 0x0 | ||
| Address Offset | 0x0000 0004 | ||
| Physical Address | 0x4000 4004 | Instance | 0x4000 4004 |
| Description | This register identifies the configuration of the peripheral | ||
| Type | RO | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:16 | RESERVED20 | Reserved | RO | 0x0000 | ||
| 15:0 | TBITS | Total number of trim bits | RO | 0x0129 | ||
| Address Offset | 0x0000 0008 | ||
| Physical Address | 0x4000 4008 | Instance | 0x4000 4008 |
| Description | Global Lock Register. Locks both registers in both mutable and immutable sections | ||
| Type | WO | ||
| Bits | Field Name | Description | Type | Reset | |||||||||||
| 31:1 | RESERVED1 | RESERVED | RO | 0b000 0000 0000 0000 0000 0000 0000 0000 | |||||||||||
| 0 | LOCK | When LOCK is set, write access to registers in mutable and immutable section are not allowed. Registers in mutable section can be temporarily unlocked by writing the KEY to UNLOCK.KEY
|
WO | 0 | |||||||||||
| Address Offset | 0x0000 000C | ||
| Physical Address | 0x4000 400C | Instance | 0x4000 400C |
| Description | Unlocks registers in mutable section | ||
| Type | WO | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | KEY | Write the unlock key 0xC5AF_6927 to temporarily unlock registers in mutable section. The lock is set automatically if no write accesses, to the mutable section, is detected for consecutive 32 CLKULL (24MHz) clock cycles. Writing any value other that the unlock key will immediately lock the mutable register space for write access. | WO | 0x0000 0000 | ||
| Address Offset | 0x0000 0010 | ||
| Physical Address | 0x4000 4010 | Instance | 0x4000 4010 |
| Description | Lock Status Register | ||
| Type | RO | ||
| Bits | Field Name | Description | Type | Reset | |||||||||||
| 31 | VGMTIE | Internal VGM Enable Signal | RO | 1 | |||||||||||
| 30 | EMTIE | Internal EM Sensor Enable Signal | RO | 1 | |||||||||||
| 29:2 | RESERVED2 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x000 0000 | |||||||||||
| 1 | MLOCK | Lock status of registers in mutable section.
|
RO | 0 | |||||||||||
| 0 | GLOCK | Status of Global lock
|
RO | 0 | |||||||||||
| Address Offset | 0x0000 0100 | ||
| Physical Address | 0x4000 4100 | Instance | 0x4000 4100 |
| Description | This register is used to configure analog switches in ATEST module | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | |||||||||||
| 31:24 | KEY | Key must be written with value 0x5A for successful write to ATESTCFG and to unlock register state. Write with any value other than 0x5A to KEY will be ignored and register content is not updated. It is recommended to write this register with incorrect KEY to lock back register state after necessary ATESTCFG updates are done. Read value of KEY is 0x0. |
WO | 0x00 | |||||||||||
| 23:9 | RESERVED9 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 0000 0000 0000 | |||||||||||
| 8 | VSEL | Selects supply for ATEST switches.
|
RW | 0 | |||||||||||
| 7 | VA2VA1 | Enables isolation switch between VA_ATEST_A1 and VA_PAD_A1.
|
RW | 0 | |||||||||||
| 6 | VA2VA0 | Enables isolation switch between VA_ATEST_A0 and VA_PAD_A0.
|
RW | 0 | |||||||||||
| 5 | VR2VA1 | Enables isolation switch between VR_ATEST_A1 and VA_ATEST_A1.
|
RW | 0 | |||||||||||
| 4 | VR2VA0 | Enables isolation switch between VR_ATEST_A0 and VA_ATEST_A0.
|
RW | 0 | |||||||||||
| 3 | SHTVA1 | Shorts VA_ATEST_A1 to ground.
|
RW | 1 | |||||||||||
| 2 | SHTVA0 | Shorts VA_ATEST_A0 to ground.
|
RW | 1 | |||||||||||
| 1 | SHTVR1 | Shorts VR_ATEST_A1 to ground.
|
RW | 1 | |||||||||||
| 0 | SHTVR0 | Shorts VR_ATEST_A0 to ground.
|
RW | 1 | |||||||||||
| Address Offset | 0x0000 0104 | ||
| Physical Address | 0x4000 4104 | Instance | 0x4000 4104 |
| Description | This register is used to configure I2V (current to voltage converter) module. | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | |||||||||||||||||||||||||||||
| 31:4 | RESERVED4 | RESERVED | RO | 0x000 0000 | |||||||||||||||||||||||||||||
| 3:1 | RESVAL | Enables I2V module and selects resistor value.
|
RW | 0b000 | |||||||||||||||||||||||||||||
| 0 | SEL | Selects ATEST_A0 between VR and VA domains and forwards to ATEST.
|
RW | 0 | |||||||||||||||||||||||||||||
| Address Offset | 0x0000 0108 | ||
| Physical Address | 0x4000 4108 | Instance | 0x4000 4108 |
| Description | This register is used to configure temperature sensor module. | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||||||||||||||
| 31:26 | SPARE1 | Spare bits
|
RW | 0b00 0000 | ||||||||||||||
| 25:12 | RESERVED12 | RESERVED | RO | 0b00 0000 0000 0000 | ||||||||||||||
| 11 | TSENS2EN | This is the enable bit for the second temperature sensor in AUX.
|
RW | 0 | ||||||||||||||
| 10:8 | SPARE | Spare bits
|
RW | 0b000 | ||||||||||||||
| 7:2 | RESERVED2 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 0000 | ||||||||||||||
| 1:0 | SEL | Used to enable and configure temperature sensor module. Setting the value to 0x3 will disable the temperature sensor.
|
RW | 0b00 | ||||||||||||||
| Address Offset | 0x0000 010C | ||
| Physical Address | 0x4000 410C | Instance | 0x4000 410C |
| Description | This register is used to configure and check the status of low-power comparator (LPCOMP) module. | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||||||||||||||||||||||||||||||||
| 31 | RESERVED31 | RESERVED | RO | 0 | ||||||||||||||||||||||||||||||||
| 30 | HYSPOL | Spare bit for LPCOMP | RW | 0 | ||||||||||||||||||||||||||||||||
| 29:28 | ATESTMUX | Used to configure ATEST mux in comparator module and provides chosen output on VA_ATEST_A0. Note: This bit field is write-protected using global lock indicator on production device.
|
RW | 0b00 | ||||||||||||||||||||||||||||||||
| 27:25 | RESERVED25 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b000 | ||||||||||||||||||||||||||||||||
| 24 | EVTIFG | Event flag. The event flag is set when the comparator output transition is qualified based on the edge polarity configuration in EDGCFG.
|
RW | 0 | ||||||||||||||||||||||||||||||||
| 23:22 | RESERVED22 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 | ||||||||||||||||||||||||||||||||
| 21 | COUTEN | Enables LPCOMP output on device pin.
|
RW | 0 | ||||||||||||||||||||||||||||||||
| 20 | COUT | LPCOMP output status. This bit captures the value LPCOMP raw output.
|
RO | 0 | ||||||||||||||||||||||||||||||||
| 19 | RESERVED19 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0 | ||||||||||||||||||||||||||||||||
| 18 | WUENSB | Enables lpcmpcfg output to wake device from standby.
|
RW | 0 | ||||||||||||||||||||||||||||||||
| 17 | EVTEN | Enables event generation. Comparator module will produce event on ULL event fabric when EVTIFG is set.
|
RW | 0 | ||||||||||||||||||||||||||||||||
| 16 | EDGCFG | Selects positive edge or negative edge detection on comparator output to set the event flag
|
RW | 0 | ||||||||||||||||||||||||||||||||
| 15 | RESERVED15 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0 | ||||||||||||||||||||||||||||||||
| 14:12 | NSEL | Negative input selection. Setting values 0x5-0x7 will open all the switches.
|
RW | 0b000 | ||||||||||||||||||||||||||||||||
| 11:8 | PSEL | Positive input selection. Setting values 0x9-0xF will open all the switches.
|
RW | 0x0 | ||||||||||||||||||||||||||||||||
| 7:5 | HYSSEL | Used to enable and select hysteresis level.
|
RW | 0b000 | ||||||||||||||||||||||||||||||||
| 4 | DIVPATH | Used to select the path on which voltage divider is applied
|
RW | 0 | ||||||||||||||||||||||||||||||||
| 3:1 | DIV | Used to configure reference divider. Setting values 0x5-0x7 will set the divide value to 1.
|
RW | 0b000 | ||||||||||||||||||||||||||||||||
| 0 | EN | Used to enable comparator module.
|
RW | 0 | ||||||||||||||||||||||||||||||||
| Address Offset | 0x0000 0110 | ||
| Physical Address | 0x4000 4110 | Instance | 0x4000 4110 |
| Description | This register is used to configure the VGM module. | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | |||||||||||
| 31:24 | KEY | Key must be written with value 0x5A for successful write to VGMCFG and to unlock register state. Write with any value other than 0x5A to KEY will be ignored and the register content is not updated. Read value of KEY is 0x0. |
WO | 0x00 | |||||||||||
| 23:20 | RESERVED20 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x0 | |||||||||||
| 19:16 | SPARE | Spare bits | RW | 0x0 | |||||||||||
| 15:12 | RESERVED12 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x0 | |||||||||||
| 11:8 | ATBMUXSEL | These bits are used to generate VGM ATB mux selection control. | RW | 0x0 | |||||||||||
| 7:2 | RESERVED2 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 0000 | |||||||||||
| 1 | OSHDETDIS | Disables overshoot detector in VGM.
|
RW | 0 | |||||||||||
| 0 | USHTDETDIS | Disables undershoot detector in VGM.
|
RW | 0 | |||||||||||
| Address Offset | 0x0000 0114 | ||
| Physical Address | 0x4000 4114 | Instance | 0x4000 4114 |
| Description | This register is used to trim and debug VGM module. | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31 | RESERVED31 | RESERVED | RO | 0 | ||
| 30 | TMODE5 | Test mode bit for glitchy supply mux selection. | RW | 0 | ||
| 29:27 | TMODE4 | Test mode bits for VREF mux selection for overshoot detector. | RW | 0b000 | ||
| 26:24 | TMODE3 | Test mode bits for VREF mux selection for undershoot detector. | RW | 0b000 | ||
| 23:22 | RESERVED22 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b00 | ||
| 21:20 | TMODE2 | Test mode for level shifter isolation. | RW | 0b00 | ||
| 19:18 | TMODE1 | Test mode bits for low voltage SR latch reset. | RW | 0b00 | ||
| 17:16 | TMODE0 | Test mode bits for 3V SR latch reset. | RW | 0b00 | ||
| 15:12 | RESERVED12 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0x0 | ||
| 11:8 | IBPROG | These bits are used to program VGM bias current generator. | RW | 0x0 | ||
| 7:4 | OSHDETTRIM | These bits are used to trim VGM overshoot detector. | RW | 0x0 | ||
| 3:0 | USHTDETTRIM | These bits are used to trim VGM undershoot detector. | RW | 0x0 | ||
| Address Offset | 0x0000 0120 | ||
| Physical Address | 0x4000 4120 | Instance | 0x4000 4120 |
| Description | This register is used to set or clear the bits in 3V register bank for TSD comparator test control. Internal note: DFT static gating to be applied on set[2:0] and clear[2:0] outputs. |
||
| Type | WO | ||
| Bits | Field Name | Description | Type | Reset | |||||||||||||||||||||||||||||
| 31:6 | RESERVED6 | RESERVED | RO | 0b00 0000 0000 0000 0000 0000 0000 | |||||||||||||||||||||||||||||
| 5:3 | ATBCLR | Clears ATB mux select in TSD comparator. | WO | 0b000 | |||||||||||||||||||||||||||||
| 2:0 | ATBSET | Sets ATB mux select in TSD comparator.
|
WO | 0b000 | |||||||||||||||||||||||||||||
| Address Offset | 0x0000 03FC | ||
| Physical Address | 0x4000 43FC | Instance | 0x4000 43FC |
| Description | This register provides Device ID information. Note: This 32-bit register value is provided as output to DEBUGSS. |
||
| Type | RO | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:28 | VERSION | Monotonic increasing value indicating new hardware revision. A newer hardware revision shall never have a lower version than an older revision of hardware. | RO | 0x0 | ||
| 27:12 | DEVICE | Value generated by RAMP for the SOC. This value uniquely identifies the die from any other TI device. | RO | 0xBB98 | ||
| 11:1 | MANFACTURER | JEP 106 assigned manufacturer ID. This field identifies the device as a Texas Instruments device. | RO | 0b000 0001 0111 | ||
| 0 | ALWAYSONE | Value 1 in this bit field means that a 32-bit scan register exists. | RO | 1 | ||
| Address Offset | 0x0000 0400 | ||
| Physical Address | 0x4000 4400 | Instance | 0x4000 4400 |
| Description | TIMMUTE0 trim Register | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:28 | RESERVED28 | RESERVED | RO | 0x0 | ||
| 27 | GLDODISANA | PMUREG: GLDO disable control selection between digital and analog schemes. 0: digital control, 1: analog control. | RW | 0 | ||
| 26 | GLDOCOMPDIS | PMUREG: Disables DCDC load meter based comparison and GLDO turn off scheme. | RW | 0 | ||
| 25 | DISSAHYST | PMUREG: Disable hysteresis in the supply awareness circuit. | RW | 0 | ||
| 24 | VDDROKHYST | PMUREG: Increase the hysteresis for when VDDR is considered ok. | RW | 0 | ||
| 23 | SPARE | REFSYS: Spare | RW | 0 | ||
| 22:21 | TSENSE | REFSYS: Temperature sensor trim | RW | 0b00 | ||
| 20:16 | IREF | REFSYS: IREF trim | RW | 0b0 0000 | ||
| 15 | BGTRIMEN | REFSYS: BOD BG trim enable | RW | 0 | ||
| 14:10 | VDDSBOD | REFSYS: VDDS BOD trim | RW | 0b0 0000 | ||
| 9:4 | VBG | REFSYS: VBG trim | RW | 0b00 0000 | ||
| 3:0 | VREF | REFSYS: VREF trim | RW | 0x0 | ||
| Address Offset | 0x0000 0404 | ||
| Physical Address | 0x4000 4404 | Instance | 0x4000 4404 |
| Description | TIMMUTE1 trim Register | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | |||||||||||
| 31 | RESERVED31 | RESERVED | RO | 0 | |||||||||||
| 30:28 | DELTA | PMUREG: Delta trim | RW | 0b000 | |||||||||||
| 27:24 | COARSE | PMUREG: Coarse trim | RW | 0x0 | |||||||||||
| 23:20 | DIG | PMUREG: DIG LDO trim | RW | 0x0 | |||||||||||
| 19:16 | UDIG | PMUREG: UDIG LDO trim | RW | 0x0 | |||||||||||
| 15:12 | BOD | PMUREG: BOD trim | RW | 0x0 | |||||||||||
| 11 | EN_LOW_IQQ_GLDO | This bit is used to enable low IQQ mode for GLDO.
|
RW | 0 | |||||||||||
| 10 | DIS_HS_DCDC_COMP | This bit is used to disable high speed DCDC comparator.
|
RW | 0 | |||||||||||
| 9:5 | VDDRSL | PMUREG: VDDR sleep trim | RW | 0b0 0000 | |||||||||||
| 4:0 | VDDR | PMUREG: VDDR trim | RW | 0b0 0000 | |||||||||||
| Address Offset | 0x0000 0408 | ||
| Physical Address | 0x4000 4408 | Instance | 0x4000 4408 |
| Description | TIMMUTE2 trim Register | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31 | CKMDIGLOCKSEL | CKMKDIG: Selects between soft lock and global lock protection for HFOSCCTL register. 0: Soft lock, 1: Global lock. | RW | 0 | ||
| 30:25 | WTOSSEP | PMCTL: Separation between last stage with weak switch and first strong switch | RW | 0b11 1111 | ||
| 24:19 | WSTGSEP | PMCTL: Separation between weak switch stages | RW | 0b11 1111 | ||
| 18:17 | SPARE | PMUREG: Spare | RW | 0b00 | ||
| 16 | GLDOEACDIS | PMUREG: GLDO error amplifier clamp disable | RW | 0 | ||
| 15 | GLDOISINKEN | PMUREG: GLDO current sink enable | RW | 0 | ||
| 14:13 | VDDRBCMP | PMUREG: VDDR boost mode compensation | RW | 0b00 | ||
| 12:8 | RECOMPOS | PMUREG: Recharge comparator offset trim | RW | 0b0 0000 | ||
| 7:5 | ITUDIG | PMUREG: ITRIM UDIG LDO | RW | 0b000 | ||
| 4:2 | ITDIG | PMUREG: ITRIM DIG LDO | RW | 0b000 | ||
| 1:0 | ITDUMMY | PMUREG: ITRIM dummy | RW | 0b00 | ||
| Address Offset | 0x0000 040C | ||
| Physical Address | 0x4000 440C | Instance | 0x4000 440C |
| Description | TIMMUTE3 trim Register | ||
| Type | WO | ||
| Bits | Field Name | Description | Type | Reset | |||||||||||
| 31:28 | RESERVED28 | RESERVED | RO | 0x0 | |||||||||||
| 27 | ATBRESBYPCLK | TSD ATB series resistance bypass clear value. | WO | 0 | |||||||||||
| 26 | HYDISCLR | TSD hysteresis disable clear value. | WO | 0 | |||||||||||
| 25:20 | TSENSCLR | TSD comparator temperature sensor trim clear value | WO | 0b00 0000 | |||||||||||
| 19 | TMODECLR | TSD comparator bandgap reference trim clear value | WO | 0 | |||||||||||
| 18:14 | BGRCLR | TSD comparator bandgap reference trim clear value | WO | 0b0 0000 | |||||||||||
| 13 | ATBRESBYPSET | TSD ATB series resistance bypass set value.
|
WO | 0 | |||||||||||
| 12 | HYSDISSET | TSD hysteresis disable set value.
|
WO | 0 | |||||||||||
| 11:6 | TSENSSET | TSD comparator temperature sensor trim set value | WO | 0b00 0000 | |||||||||||
| 5 | TMODESET | TSD test mode select set value for trim and test.
|
WO | 0 | |||||||||||
| 4:0 | BGRSET | TSD comparator bandgap reference trim set value | WO | 0b0 0000 | |||||||||||
| Address Offset | 0x0000 07F8 | ||
| Physical Address | 0x4000 47F8 | Instance | 0x4000 47F8 |
| Description | This register is programmed by boot code with Part ID information.Note: This 32-bit register value is provided as output to DEBUGSS | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | |||||||||||
| 31 | START | Start bit
|
RW | 0 | |||||||||||
| 30:28 | MAJORREV | Monotonic increasing value indicating a new revision of the SKU significant enough that users of the device may have to revise PCB or or software design | RW | 0b000 | |||||||||||
| 27:24 | MINORREV | Monotonic increasing value indicating a new revision of the SKU that preserves compatibility with lesser MINORREV values | RW | 0x0 | |||||||||||
| 23:16 | VARIANT | Bit pattern uniquely identifying a part | RW | 0x00 | |||||||||||
| 15:0 | PART | Bit pattern uniquely identifying a part | RW | 0x0000 | |||||||||||
| Address Offset | 0x0000 07FC | ||
| Physical Address | 0x4000 47FC | Instance | 0x4000 47FC |
| Description | This register is programmed by boot code with device life cycle information | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | |||||||||||||||||||||||||||||
| 31:8 | RESERVED8 | RESERVED | RO | 0x00 0000 | |||||||||||||||||||||||||||||
| 7:0 | VAL | Device life cycle value
|
RW | 0x00 | |||||||||||||||||||||||||||||
| Address Offset | 0x0000 0800 | ||
| Physical Address | 0x4000 4800 | Instance | 0x4000 4800 |
| Description | TMUTE0 trim Register | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | CDACL | SOCADC: Lower 32 bits of CDAC trim. These bits are used in DTC. | RW | 0x0000 0000 | ||
| Address Offset | 0x0000 0804 | ||
| Physical Address | 0x4000 4804 | Instance | 0x4000 4804 |
| Description | TMUTE1 trim Register | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:0 | CDACM | SOCADC: Middle 32 bits of CDAC trim. These bits are used in DTC. | RW | 0x0000 0000 | ||
| Address Offset | 0x0000 0808 | ||
| Physical Address | 0x4000 4808 | Instance | 0x4000 4808 |
| Description | TMUTE2 trim Register | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31 | RESERVED31 | RESERVED | RO | 0 | ||
| 30:26 | IBTRIM | LPCOMP: Bias current trim, 250nA to be terminated across I2V, 1M ohm setting. Resulting target trim voltage 250mV. | RW | 0b0 0000 | ||
| 25:23 | TRIM | ADC REFBUF trim bits. | RW | 0b001 | ||
| 22:16 | LATCH | SOC ADC: Latch trim bits. These bits are used in the analog IP. | RW | 0b000 0000 | ||
| 15:4 | OFFSET | SOCADC: Offset trim bits. These bits are used in DTC. | RW | 0x000 | ||
| 3:2 | RES | SOCADC: Resistor trim bits. These bits are used in the analog IP. | RW | 0b00 | ||
| 1:0 | CDACU | SOCADC: Upper 2 bits of CDAC trim. These bits are used in DTC. | RW | 0b00 | ||
| Address Offset | 0x0000 080C | ||
| Physical Address | 0x4000 480C | Instance | 0x4000 480C |
| Description | TMUTE3 trim Register | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:26 | BATC1 | BATMON: Battery calculation coefficient 1 | RW | 0b00 0000 | ||
| 25:19 | BATC0 | BATMON: Battery calculation coefficient 0 | RW | 0b000 0000 | ||
| 18:14 | TEMPC2 | BATMON: Temperature calculation coefficient 2 | RW | 0b0 0000 | ||
| 13:8 | TEMPC1 | BATMON: Temperature calculation coefficient 1 | RW | 0b00 0000 | ||
| 7:0 | TEMPC0 | BATMON: Temperature calculation coefficient 0 | RW | 0x00 | ||
| Address Offset | 0x0000 0810 | ||
| Physical Address | 0x4000 4810 | Instance | 0x4000 4810 |
| Description | TMUTE4 trim Register | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:28 | RECHCOMPREFLVL | PMUREG: Recharge comparator reference level. Valid values are 0x2 to 0xA. Recommended default value is 0x9. Setting 0x2 corresponds to VDDR = 1.35V and 0xA corresponds to VDDR = 1.47V with 15mV linear increase for every step. | RW | 0xB | ||
| 27:26 | IOSTRCFG2 | BATMON: IO drive strength conversion parameter for the second stage | RW | 0b00 | ||
| 25:22 | IOSTRCFG1 | BATMON: IO drive strength conversion parameter for the first stage | RW | 0x0 | ||
| 21:19 | MAX | IOC: Maximum IO drive strength | RW | 0b101 | ||
| 18:16 | MED | IOC: Medium IO drive strength | RW | 0b110 | ||
| 15:13 | MIN | IOC: Minimum IO drive strength | RW | 0b011 | ||
| 12:11 | DCDCLOAD | DCDC: Set DCDC load current threshold | RW | 0b00 | ||
| 10:8 | IPEAK | DCDC: Set inductor peak current | RW | 0b000 | ||
| 7:6 | DTIME | DCDC: Dead time trim | RW | 0b00 | ||
| 5:3 | LENSEL | DCDC: Control NMOS switch strength | RW | 0b111 | ||
| 2:0 | HENSEL | DCDC: Control PMOS switch strength | RW | 0b111 | ||
| Address Offset | 0x0000 0814 | ||
| Physical Address | 0x4000 4814 | Instance | 0x4000 4814 |
| Description | TMUTE5 trim Register | ||
| Type | RW | ||
| Bits | Field Name | Description | Type | Reset | ||
| 31:13 | RESERVED13 | RESERVED | RO | 0b000 0000 0000 0000 0000 | ||
| 12:10 | DCDCDRVDS | DCDC: Driver drive strength configuration | RW | 0b000 | ||
| 9:5 | GLDOISCLR | GLDO current source trim clear value | WO | 0b0 0000 | ||
| 4:0 | GLDOISSET | GLDO current source trim set value | WO | 0b0 0000 | ||
| 4:0 | RESERVED0 | Software should not rely on the value of a reserved. Writing any other value than the reset value may result in undefined behavior. | RO | 0b0 0000 | ||
| © 2015 - 2016. Texas Instruments | All Rights Reserved |