TI BLE5-Stack API Documentation  3.02.04.00
Macros | Functions
util.h File Reference

Detailed Description

Util layer interface.

Go to the source code of this file.

Macros

#define UTIL_QUEUE_EVENT_ID   Event_Id_30
 Util Queue Event ID. More...
 

Functions

Clock_Handle Util_constructClock (Clock_Struct *pClock, Clock_FuncPtr clockCB, uint32_t clockDuration, uint32_t clockPeriod, uint8_t startFlag, UArg arg)
 Initialize a TIRTOS Clock instance. More...
 
Queue_Handle Util_constructQueue (Queue_Struct *pQueue)
 Initialize an RTOS queue to hold messages from profile to be processed. More...
 
char * Util_convertBdAddr2Str (uint8_t *pAddr)
 Convert Bluetooth address to string. Only needed when LCD display is used. More...
 
uint8_t * Util_dequeueMsg (Queue_Handle msgQueue)
 Dequeues the message from the RTOS queue. More...
 
uint8_t Util_enqueueMsg (Queue_Handle msgQueue, Event_Handle event, uint8_t *pMsg)
 Creates a queue node and puts the node in RTOS queue. More...
 
bool Util_isActive (Clock_Struct *pClock)
 Determine if a clock is currently active. More...
 
uint8_t Util_isBufSet (uint8_t *pBuf, uint8_t pattern, uint16_t len)
 Check if contents of buffer matches byte pattern. More...
 
void Util_rescheduleClock (Clock_Struct *pClock, uint32_t clockPeriod)
 Reschedule a clock by changing the timeout and period values. More...
 
void Util_restartClock (Clock_Struct *pClock, uint32_t clockTimeout)
 Restart a clock by changing the timeout. More...
 
void Util_startClock (Clock_Struct *pClock)
 Start a clock. More...
 
void Util_stopClock (Clock_Struct *pClock)
 Stop a clock. More...
 
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale