Comprehensive List of Fixed Issues¶
This section will provide a comrehensive list of the issues that have been fixed with each release of the SimpleLink Low Power F3 SDK.
Note
For more information regarding new features, fixed issues, or known issues
for a specific SDK, please reference the respective Core SDK release notes.
These can be found online through the links provided in each section, or
within the SDK at:
{SDK_INSTALL_DIR}/docs/simplelink_mcu_sdk/release_notes_coresdk_lpf3_x_xx_xx_xx.html
v7x SDKs¶
7.10.00.35 (05 May 2023)¶
ID |
Summary |
---|---|
Central failed to establish connectionWL to peer with RPA from white list |
|
Basic BLE project with multirole BLE role advertises intermittently |
|
[macOS Build] imgtool command not found - build post process step for OAD examples fails |
|
TERMINATION_IND sometimes missed when using ADV Interval < 100ms |
|
CC2340R5 current consumption increased by ~1uA due to longer duration of ‘IDLE’ state |
|
GAP_ADV_EVT_MASK_SCAN_REQ_NOTI is not processed in the controller |
|
CC23X0 hangs after calling scan_enable |
|
[PSIRT-145] Accepts PairConfirmSend with wrong values |
|
[PSIRT-144] Accepts PairRandomSend before exchanging public key |
|
[PSIRT-143] BLE secure pairing: Accepts DHKeyCheckSend with all fields zero |