|
|
Go to the documentation of this file. 38 #ifndef third_party_mcan_tcan455x_reg__include 39 #define third_party_mcan_tcan455x_reg__include 44 #define TCAN455X_DEVICE_ID0 0x0000 45 #define TCAN455X_DEVICE_ID1 0x0004 46 #define TCAN455X_REVISION 0x0008 47 #define TCAN455X_STATUS 0x000C 52 #define TCAN455X_MODE 0x0800 53 #define TCAN455X_TS_PRESCALER 0x0804 54 #define TCAN455X_TEST 0x0808 55 #define TCAN455X_IR 0x0820 56 #define TCAN455X_IE 0x0830 61 #define TCAN455X_MCAN 0x1000U 62 #define TCAN455X_MRAM 0x8000U 71 #define TCAN455X_MODE_FORCED_SET_BITS 0x00000020 74 #define TCAN455X_MODE_WAKE_PIN_MASK 0xC0000000 75 #define TCAN455X_MODE_WAKE_PIN_DIS 0x00000000 76 #define TCAN455X_MODE_WAKE_PIN_RISING 0x40000000 77 #define TCAN455X_MODE_WAKE_PIN_FALLING 0x80000000 78 #define TCAN455X_MODE_WAKE_PIN_BOTHEDGES 0xC0000000 81 #define TCAN455X_MODE_GPO2_MASK 0x00C00000 82 #define TCAN455X_MODE_GPO2_CAN_FAULT 0x00000000 83 #define TCAN455X_MODE_GPO2_MCAN_INT0 0x00400000 84 #define TCAN455X_MODE_GPO2_WDT 0x00800000 85 #define TCAN455X_MODE_GPO2_NINT 0x00C00000 88 #define TCAN455X_MODE_TESTMODE_ENMASK 0x00200000 89 #define TCAN455X_MODE_TESTMODE_EN 0x00200000 90 #define TCAN455X_MODE_TESTMODE_DIS 0x00000000 93 #define TCAN455X_MODE_NWKRQ_VOLT_MASK 0x00080000 94 #define TCAN455X_MODE_NWKRQ_VOLT_INTERNAL 0x00000000 95 #define TCAN455X_MODE_NWKRQ_VOLT_VIO 0x00080000 98 #define TCAN455X_MODE_WDT_RESET_BIT 0x00040000 101 #define TCAN455X_MODE_WDT_ACTION_MASK 0x00020000 102 #define TCAN455X_MODE_WDT_ACTION_INT 0x00000000 103 #define TCAN455X_MODE_WDT_ACTION_INH_PULSE 0x00010000 104 #define TCAN455X_MODE_WDT_ACTION_WDT_PULSE 0x00020000 107 #define TCAN455X_MODE_GPO1_MODE_MASK 0x0000C000 108 #define TCAN455X_MODE_GPO1_MODE_GPO 0x00000000 109 #define TCAN455X_MODE_GPO1_MODE_CLKOUT 0x00004000 110 #define TCAN455X_MODE_GPO1_MODE_GPI 0x00008000 113 #define TCAN455X_MODE_FAIL_SAFE_MASK 0x00002000 114 #define TCAN455X_MODE_FAIL_SAFE_EN 0x00002000 115 #define TCAN455X_MODE_FAIL_SAFE_DIS 0x00000000 118 #define TCAN455X_MODE_CLKOUT_MASK 0x00001000 119 #define TCAN455X_MODE_CLKOUT_DIV1 0x00000000 120 #define TCAN455X_MODE_CLKOUT_DIV2 0x00001000 123 #define TCAN455X_MODE_GPO1_FUNC_MASK 0x00000C00 124 #define TCAN455X_MODE_GPO1_FUNC_SPI_INT 0x00000000 125 #define TCAN455X_MODE_GPO1_FUNC_MCAN_INT1 0x00000400 126 #define TCAN455X_MODE_GPO1_FUNC_UVLO_THERM 0x00000800 129 #define TCAN455X_MODE_INH_MASK 0x00000200 130 #define TCAN455X_MODE_INH_DIS 0x00000200 131 #define TCAN455X_MODE_INH_EN 0x00000000 134 #define TCAN455X_MODE_NWKRQ_CONFIG_MASK 0x00000100 135 #define TCAN455X_MODE_NWKRQ_CONFIG_INH 0x00000000 136 #define TCAN455X_MODE_NWKRQ_CONFIG_WKRQ 0x00000100 139 #define TCAN455X_MODE_OPMODE_MASK 0x000000C0 140 #define TCAN455X_MODE_OPMODE_SLEEP 0x00000000 141 #define TCAN455X_MODE_OPMODE_STANDBY 0x00000040 142 #define TCAN455X_MODE_OPMODE_NORMAL 0x00000080 145 #define TCAN455X_MODE_WDT_MASK 0x00000008 146 #define TCAN455X_MODE_WDT_EN 0x00000008 147 #define TCAN455X_MODE_WDT_DIS 0x00000000 150 #define TCAN455X_MODE_RESET 0x00000004 153 #define TCAN455X_MODE_SWE_MASK 0x00000002 154 #define TCAN455X_MODE_SWE_DIS 0x00000002 155 #define TCAN455X_MODE_SWE_EN 0x00000000 158 #define TCAN455X_MODE_TESTMODE_MASK 0x00000001 159 #define TCAN455X_MODE_TESTMODE_PHY 0x00000000 160 #define TCAN455X_MODE_TESTMODE_CONTROLLER 0x00000001 163 #define TCAN455X_IR_CANLGND 0x08000000 164 #define TCAN455X_IR_CANBUSOPEN 0x04000000 165 #define TCAN455X_IR_CANBUSGND 0x02000000 166 #define TCAN455X_IR_CANBUSBAT 0x01000000 167 #define TCAN455X_IR_RSVD3 0x00800000 168 #define TCAN455X_IR_UVSUP 0x00400000 169 #define TCAN455X_IR_UVIO 0x00200000 170 #define TCAN455X_IR_PWRON 0x00100000 171 #define TCAN455X_IR_TSD 0x00080000 172 #define TCAN455X_IR_WDTO 0x00040000 173 #define TCAN455X_IR_RSVD2 0x00020000 174 #define TCAN455X_IR_ECCERR 0x00010000 175 #define TCAN455X_IR_CANINT 0x00008000 176 #define TCAN455X_IR_LWU 0x00004000 177 #define TCAN455X_IR_WKERR 0x00002000 178 #define TCAN455X_IR_FRAME_OVF 0x00001000 179 #define TCAN455X_IR_RSVD1 0x00000800 180 #define TCAN455X_IR_CANSLNT 0x00000400 181 #define TCAN455X_IR_RSVD0 0x00000200 182 #define TCAN455X_IR_CANDOM 0x00000100 183 #define TCAN455X_IR_GLOBALERR 0x00000080 184 #define TCAN455X_IR_nWKRQ 0x00000040 185 #define TCAN455X_IR_CANERR 0x00000020 186 #define TCAN455X_IR_CANBUSFAULT 0x00000010 187 #define TCAN455X_IR_SPIERR 0x00000008 188 #define TCAN455X_IR_SWERR 0x00000004 189 #define TCAN455X_IR_M_CAN_INT 0x00000002 190 #define TCAN455X_IR_VTWD 0x00000001 193 #define TCAN455X_IE_UVCCOUT 0x00800000 194 #define TCAN455X_IE_UVSUP 0x00400000 195 #define TCAN455X_IE_UVIO 0x00200000 196 #define TCAN455X_IE_PWRON 0x00100000 197 #define TCAN455X_IE_TSD 0x00080000 198 #define TCAN455X_IE_WDTO 0x00040000 199 #define TCAN455X_IE_RSVD2 0x00020000 200 #define TCAN455X_IE_ECCERR 0x00010000 201 #define TCAN455X_IE_CANINT 0x00008000 202 #define TCAN455X_IE_LWU 0x00004000 203 #define TCAN455X_IE_WKERR 0x00002000 204 #define TCAN455X_IE_FRAME_OVF 0x00001000 205 #define TCAN455X_IE_RSVD1 0x00000800 206 #define TCAN455X_IE_CANSLNT 0x00000400 207 #define TCAN455X_IE_RSVD0 0x00000200 208 #define TCAN455X_IE_CANDOM 0x00000100 209 #define TCAN455X_IE_MASK 0xFF69D700
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale