Application Layer

Since the Micro BLE Stack can support multiple functionalities (broadcaster, observer, or connection monitor), it is up to the application layer to define the behavior of the system. The following sections will discuss the TI provided implementations of the monitor role.

  • micro_ble_cm.c : connection monitor application

Connection Monitor (CM) Application

The connection monitor application is built on top of the uGAP layer, operating in the monitor role, and is responsible for implementing the high-level connection tracking feature. This includes:

  1. Initializing connection parameters for a connection to monitor

  2. Performing the initial scan to find a connection event

  3. Scheduling subsequent scans to continue following the connection

The following sections will describe the above list in detail.

Initializing CM Session

In order to follow a connection, the CM needs to know the connection parameters that were exchanged during the connection process between the central and peripheral devices. These include:

  • Access address

  • Connection interval

  • Hop value

  • Next channel

  • Channel map

  • CRC initialization value

These parameters can be obtained from a BLE5-Stack application by calling the HCI_EXT_GetActiveConnInfoCmd command. Once they are obtained, they should be shared (via an out of band mechanism such as UART, LIN, CAN etc) with the CM device. The CM device then can use ubCM_startNewSession() to start the initial scan.

Starting a Monitor Session

In order to start tracking a connection, the connection monitor needs to perform an initial scan with a long enough scan duration to catch a connection event. This scan should be, at worst case, the connection interval times the number of active channels in order to ensure the connection can be detected.

The logic trace below shows the initial scan of a connection monitor and it was generated by enabling the RF observable pins on the central and peripheral devices in the connection (RX/TX) as well as the connection monitor (RX). For more information regarding the RF observable pins, please refer to the Debugging RF Output section.

../_images/cm-initial-scan.png

Note

For example, if the active channel map is channel 0, 1, 2, 3, 4, 5 and the hop number is 1. The next channel sent from peripheral is 2 and connection interval is 7.5 ms. Then CM will stay at channel 2 for maximum 45 ms(6 * 7.5).

Monitoring a Connection

Once a packet is received during the initial scan, the CM will set up smaller scans based on the next expected event. Since it is now monitoring the connection, it can calculate the channel and instant (adjusted for central and peripheral sleep clock accuracy (SCA)) to listen for the next event.

The core of connection monitoring is based on

  • monitor_indicationCB : Invoked when a packet is received.

  • monitor_completeCB : Invoked when a scan window has completed.

The logic trace below shows a CM actively tracking a connection:

../_images/cm-conn.png

The sequence diagram below illustrates the whole process of how CM starts monitoring the connection and reporting RSSI to the application.

@startuml

participant CM as "Connection Monitor"
participant Basic as "Basic BLE"
participant Phone as "Phone"

Basic <-- Phone: Connection Request
== After connection has established ==
CM <- Basic: Pass needed information to Connection Monitor

rnote left
  Basic BLE device needs to pass access address,
  connection interval, channel map,
  hop increment, CRC init, and next channel
  to Connection Monitor device.
end note

activate CM
  CM --> CM: Start scanning for packet at next channel
  Phone --> Basic: Send packet
  Basic --> Phone: Send packet
...
... Connection Monitor will stay at next channel for maximum\nCI * (Number of Active Channel) amount of time...
...
  Phone --> Basic: Send packet
  Basic --> Phone: Send packet
deactivate CM

Group If Connection Monitor Initial Scan Timeout\nScan Timeout = (CI * Number of Active Channels)
  CM --> CM: Back to Idle state
  CM -> Basic: Notify Basic BLE that sync failed
  Basic -> CM: Send over needed information to restart \nConnection Monitor
end

Group After Connection Monitor syncs up

Phone --> Basic: Send packet

activate CM

CM --> CM: Scan packet sent from Phone and\nextract RSSI
[<-CM : The RSSI value from Phone will be \nsent to monitor_indicationCB

Basic --> Phone: Send packet
CM --> CM: Scan packet sent from Basic BLE device \nand extract RSSI
[<-CM : The RSSI value from Basic BLE device will \nbe sent to monitor_indicationCB
CM --> CM: Finish one monitor event
[<-CM : Send notification to monitor_completeCB \nto indicate one monitor event has finished
CM -> Basic: One monitor event success. \nSend RSSI, timeStamp and monitored channel to Basic BLE device
Deactivate CM

...
... Change to next channel and Connection Monitor continues monitoring the connection...
...
end
@enduml

Figure 103. Connection Monitor initialization and connection tracking

Lose Sync

The application layer can decide how many consecutive connection events the CM is allowed to miss by setting BLE_CONSECUTIVE_MISSED_CONN_EVT_THRES.

The CM keeps track of consecutive missed events (consecutiveTimesMissed) and total missed events (timesMissed). Those variables can be found under the ubCM_ConnInfo_t struct.

Listing 127. Connection Monitor Information
 1  typedef struct
 2  {
 3    uint8_t   sessionId;                             //! Number 1-255 assigned as they are created identifying each connection monitor session
 4    uint8_t   timesScanned;                          //! track count of recent events monitored to determine next priority CM session to avoid starvation
 5    uint8_t   timesMissed;                           //! missed count of recent events monitored
 6    uint8_t   consecutiveTimesMissed;                //! consecutive missed count of recent events monitored
 7    uint8_t   missedEvents;                          //! missed count of events since last monitoring session
 8    uint8_t   numEvents;                             //! how many connection events have passed since the last anchor point.
 9    uint32_t  accessAddr;                            //! return error code if failed to get conn info
10    uint8_t   connRole;                              //! RTLS Coordinator BLE role (4 - Peripheral, 8- Central)
11    uint16_t  connInterval;                          //! connection interval time, range 12 to 6400 in  625us increments (7.5ms to 4s)
12    uint16_t  scanDuration;                          //! Required scan window to capture minimum of 1 packet from Central and Peripheral up to max possible packet size
13    uint8_t   hopValue;                              //! Hop value for conn alg 1, integer range (5,16)
14    uint16_t  combSCA;                               //! mSCA + cmSCA
15    uint8_t   currentChan;                           //! current unmapped data channel
16    uint8_t   lastUnmappedChannel;                   //! last used unmapped channel when received data packet from the central
17    uint8_t   nextChan;                              //! next data channel
18    uint8_t   numUsedChans;                          //! count of the number of usable data channels
19    uint8_t   chanMap[CM_MAX_NUM_DATA_CHAN];         //! current channel map table that is in use for this connection
20    uint8_t   rssiCentral;                           //! last Rssi value Central
21    uint8_t   rssiPeripheral;                        //! last Rssi value Peripheral
22    uint32_t  timeStampCentral;                      //! last timeStamp Central
23    uint32_t  timeStampCentral2;                     //! last timeStamp Central
24    uint32_t  timeStampPeripheral;                   //! last timeStamp Peripheral
25    uint32_t  currentStartTime;                      //! Current anchor point
26    uint32_t  nextStartTime;                         //! Record next planned scan anchor point to compare with competing CM sessions
27    uint32_t  lastStartTime;                         //! Record last planned scan anchor point to compare with competing CM sessions
28    uint32_t  timerDrift;                            //! Clock timer drift
29    uint32_t  crcInit;                               //! crcInit value for this connection
30    uint16_t  hostConnHandle;                        //! keep connHandle from host requests
31    uint8_t   outOfSyncFlag;                         //! flag indicating that the CM session is trying to get in sync
32    uint32_t  outOfSyncTimeStamp;                    //! timeStamp for trying to get in sync
33  } ubCM_ConnInfo_t;

Once consecutiveTimesMissed is larger than BLE_CONSECUTIVE_MISSED_CONN_EVT_THRES, the CM will terminate the monitor session and notify the host. The host can then restart the monitor session by going through Initializing CM Session, Starting a Monitor Session and Monitoring a Connection.

The sequence diagram below illustrates the whole process of how a CM deals with losing sync.

@startuml

participant CM as "Connection Monitor"
participant Basic as "Basic BLE"
participant Phone as "Phone"

== BLE_CONSECUTIVE_MISSED_CONN_EVT_THRES = 30 ==
== Connection Monitor syncs up ==
Phone --> Basic: Send packet
activate CM
...
... Assume Connection Monitor has been scanning \nbut missed 30 consecutive connection events.\n connInfo->consecutiveTimesMissed is now at 30...
...

Basic --> Phone: Send packet

Group If CM successfully monitors 31st connection event

Phone --> Basic: Send packet
Basic --> Phone: Send packet

CM --> CM: connInfo->consecutiveTimesMissed = 0

CM --> CM: Finish one monitor event
[<-CM : Send notification to monitor_completeCB \nto indicate one monitor event has finished
CM -> Basic: One monitor event success. \nSend RSSI, timeStamp and monitored channel \nto Basic BLE device

end

Group If CM misses 31st connection event

Phone --> Basic: Send packet
Basic --> Phone: Send packet
CM --> CM: connInfo->consecutiveTimesMissed ++
deactivate CM

CM --> CM: Change status to CM_FAILED_NOT_ACTIVE

[<-CM: Send notification to monitor_completeCB \nto indicate the monitor session \nis no longer active
CM --> CM: Terminate the monitor session by calling \nubCM_stop
CM-> Basic: Notify Basic BLE device that the monitor session is terminated

CM --> CM: Back to Idle.
Basic -> CM: Send over needed information to \nrestart monitoring session

end

@enduml

Figure 104. Connection Monitor loses sync

Connection Information Update

A CM does not extract the payload information, it only measures the RSSI from the payload. Therefore, if there are control packets such as a channel map update or other connection parameter updates exchanged between the central and peripheral devices, the device that has a wired connection to the CM needs to pass on the information so that the CM can continue monitoring the connection.

Once the CM receives the new information, the application needs to call MicroCmApp_cmStartReq or RTLSPassive_cmStartReq which eventually calls ubCM_updateExt if the session already exists.

@startuml

participant CM as "Connection Monitor"
participant Basic as "Basic BLE"
participant Phone as "Phone"

activate CM

== Connection Monitor syncs up ==
Phone --> Basic: Send packet

Basic --> Phone: Send packet

group Channel Map Update

Phone --> Basic: Send channel map update packet
Basic --> Phone: Send packet
Basic -> CM: Send the updated channel map

CM --> CM: Update the current monitor session \nwith new information by calling \nubCM_updateExt

end

Group Connection Parameters Update

Phone --> Basic: Connection parameters update packet
Basic --> Phone: Response to the connection \nparameters update packet
Basic -> CM: Send the new connection parameters

CM --> CM: Update the current monitor session \nwith new information by calling \nubCM_updateExt

end

CM --> CM: Stop monitoring current session and \ncontinue scanning until sync found/timeout

@enduml

Figure 105. Connection Monitor control packets update

Monitor Multiple Connections

A CM can monitor multiple connections even when all of the monitored connections have different connection intervals.

To determine which connection to monitor, after ending each monitor session, the CM scheduler will sort all of the connections based on future start time. Then the CM will do a timing conflict check on selected and sec connections. If (conn1 start time + monitor/scan duration) > conn2 start time, then the CM will consider that there is conflict between connection 1 and connection 2.

The monitor/scan duration for each monitor session is determined by the following parameters:

  • Sleep Clock Accuracy (SCA) for both central and peripheral devices.

  • The processing time for the radio core and the CM software.

  • Time needed to receive only one packet per central and periperal device using 1M Phy. No MD in the same connection event.

    Note

    A CM is designed to extract RSSI information for both the central and peripheral devices when they are in a connection. It does not extract payload information; therefore, there is no need to monitor more packets.

When there is a timing conflict among monitored connections, the CM will decide which connection to monitor based on the following factors, in order of priorities from high to low:

  1. If one of the connections has larger connection interval, then the connection which the CM misses more monitored time will be scheduled.

    Note

    For example, if the next connection events for connection 1(CI = 100ms) and connection 2(CI = 40ms, cmMissedEvent = 3) are in conflict, then CM will monitor connection 2 because connection 2 missed more monitored time (100 < 40*3).

  2. The connection with the higher cmMissedEvents.

  3. The connection with the earlier start time.

The following diagram illustrates how a CM would handle a monitor session conflict:

../_images/ditaa-76eba18ba1ea6f78fd0c297945a163e33e7a8a01.png

Limitations

When requesting a new monitor session while CM has already been monitoring connection(s), the CM will process the request based on the timing of when the request comes in.

  • If the request comes in when the CM is not monitoring a connection, the request will be processed right away. This means that the CM will start scanning for a new connection immediately after receiving the request.

  • If the request comes in when the CM is monitoring a connection, the information of the new connection will be saved and processed once the current monitor session has ended.

The following diagram illustrates how the CM handles new monitor requests.

../_images/ditaa-e2dacc780740a70351163ee344a1c24ac796d180.png

Due to the nature of how Starting a Monitor Session works, the radio might still be scanning for the new connection when it is time to monitor existing connection(s). The CM will prioritize scanning for new connection over monitoring existing connection(s). Once the CM is able to track the new connection or scan timeout, it will continue monitoring the existing connections.

That being said, if there are multiple new monitor session requests coming in, then the CM will process all of the new monitor session requests before it goes back to monitor the existing connections.

In addition to the above limitations, the CM example also has the following constraints:

  • Connections must use LE Channel Selection Algorithm #1

  • Connections must use LE 1M PHY

  • Connections must exist on LE Data channels

Warning

It is not recommended to call ubCM_stop or ubCM_start in the middle of a monitor session. Calling the aforementioned APIs while the radio is active might cause unexpected behavior.