Introduction¶
This chapter serves as a guide to the Texas Instruments Over-the-Air Download (OAD) ecosystem including the custom over the air specification, application architecture, drivers, and middleware. OAD is a device firmware upgrade method that allows the firmware image running on a device to be updated over the air while providing power loss protection.
The guide will cover the principles of the OAD process, the out of the box examples included in the SimpleLink Low Power F3 SDK, and the process for adding OAD to an existing project.
The OAD guide chapter will cover:
MCUBoot and the device startup procedure (see MCUboot Overview)
OAD image header and how it is populated (see MCUBoot OAD Image Header)
OAD theory of operation and architecture
Flash layout for OAD applications
Protocol stack specific examples of OAD
How to add OAD to an existing sample application.
The supported development kit for OAD is the CC23xx LaunchPad. To follow the procedures listed in this guide, two CC23xx LaunchPad development kits are required. The flow of this document will follow the boot process of the device from MCUBoot to the user application, explaining the concepts as they come up.
OAD Topology Overview¶
Two wireless devices are required to perform an OAD. The terms for the devices involved in an OAD exchange are listed below:
The OAD target is the device that receives the incoming image over the air. The OAD target is responsible for implementing the protocol stack specific transport layer that is used for sending and receiving OAD image data.
The OAD distributor is responsible for fragmenting the new firmware image into protocol stack specific packets and sending them over the air.
Note
The OAD distributor may take any form. Below it is illustrated as a TI development kit connected to an associated PC tool, but it can also be a mobile device or another TI embedded device that implements the protocol specific transport.
Figure 123. shows a graphical relationship of the devices required for an OAD transfer.
![../_images/oad_topology.png](../_images/oad_topology.png)
Figure 123. OAD Distributor and OAD Target¶