626 #ifndef ti_drivers_spi_SPILPF3DMA__include 627 #define ti_drivers_spi_SPILPF3DMA__include 635 #include <ti/drivers/dpl/HwiP.h> 636 #include <ti/drivers/dpl/SemaphoreP.h> 637 #include <ti/drivers/dpl/SwiP.h> 675 #define SPILPF3DMA_CMD_RETURN_PARTIAL_ENABLE (SPI_CMD_RESERVED + 0) 684 #define SPILPF3DMA_CMD_RETURN_PARTIAL_DISABLE (SPI_CMD_RESERVED + 1) 692 #define SPILPF3DMA_CMD_SET_CSN_PIN (SPI_CMD_RESERVED + 2) 699 #define SPILPF3DMA_CMD_CLEAR_CSN_PIN (SPI_CMD_RESERVED + 3) 714 #define SPILPF3DMA_CMD_SET_MANUAL (SPI_CMD_RESERVED + 4) 725 #define SPILPF3DMA_CMD_CLR_MANUAL (SPI_CMD_RESERVED + 5) 737 #define SPILPF3DMA_CMD_MANUAL_START (SPI_CMD_RESERVED + 6) 758 #define SPILPF3DMA_CMD_SET_SAMPLE_DELAY (SPI_CMD_RESERVED + 7) 763 #define SPILPF3DMA_RETURN_PARTIAL_ENABLE SPILPF3DMA_CMD_RETURN_PARTIAL_ENABLE 764 #define SPILPF3DMA_RETURN_PARTIAL_DISABLE SPILPF3DMA_CMD_RETURN_PARTIAL_DISABLE 765 #define SPILPF3DMA_SET_CSN_PIN SPILPF3DMA_CMD_SET_CSN_PIN uint32_t busyBit
Definition: SPILPF3DMA.h:950
volatile uDMAControlTableEntry * dmaTxTableEntryAlt
Definition: SPILPF3DMA.h:900
uint16_t rxScratchBuf
Definition: SPILPF3DMA.h:953
volatile uDMAControlTableEntry * dmaTxTableEntryPri
Definition: SPILPF3DMA.h:896
Definition: SPILPF3DMA.h:787
volatile uDMAControlTableEntry * dmaRxTableEntryPri
Definition: SPILPF3DMA.h:898
SPI_Transaction * headPtr
Definition: SPILPF3DMA.h:937
Serial Peripheral Interface (SPI) Driver Interface.
void(* SPI_CallbackFxn)(SPI_Handle handle, SPI_Transaction *transaction)
The definition of a callback function used by the SPI driver when used in SPI_MODE_CALLBACK.
Definition: SPI.h:592
SPI_Transaction * tailPtr
Definition: SPILPF3DMA.h:938
Power_NotifyObj spiPostObj
Definition: SPILPF3DMA.h:932
size_t framesQueued
Definition: SPILPF3DMA.h:941
volatile uDMAControlTableEntry * dmaRxTableEntryAlt
Definition: SPILPF3DMA.h:902
SPI_TransferMode
SPI transfer mode determines the whether the SPI controller operates synchronously or asynchronously...
Definition: SPI.h:629
uint16_t txScratchBuf
Definition: SPILPF3DMA.h:954
SPI_Transaction * completedTransfers
Definition: SPILPF3DMA.h:939
size_t priTransferSize
Definition: SPILPF3DMA.h:943
SPI_CallbackFxn transferCallbackFxn
Definition: SPILPF3DMA.h:936
uint_least8_t picoPin
Definition: SPILPF3DMA.h:912
uint32_t baseAddr
SPI Peripheral's base address.
Definition: SPILPF3DMA.h:861
size_t altTransferSize
Definition: SPILPF3DMA.h:944
uint32_t txChannelBitMask
Definition: SPILPF3DMA.h:890
SemaphoreP_Struct transferComplete
Definition: SPILPF3DMA.h:934
Definition: SPILPF3DMA.h:799
uint32_t bitRate
Definition: SPILPF3DMA.h:947
uint32_t activeChannel
Definition: SPILPF3DMA.h:946
HwiP_Struct hwi
Definition: SPILPF3DMA.h:931
uint32_t dsample
Definition: SPILPF3DMA.h:951
uint32_t dataSize
Definition: SPILPF3DMA.h:948
const SPI_FxnTable SPILPF3DMA_fxnTable
The definition of a SPI function table that contains the required set of functions to control a speci...
Definition: SPI.h:718
uint32_t rxChannelBitMask
Definition: SPILPF3DMA.h:888
uint32_t transferTimeout
Definition: SPILPF3DMA.h:949
int32_t sclkPinMux
Definition: SPILPF3DMA.h:908
int32_t csnPinMux
Definition: SPILPF3DMA.h:910
uint8_t txChannelEvtMux
Definition: SPILPF3DMA.h:892
SPILPF3DMA_FrameSize
Definition: SPILPF3DMA.h:784
SPILPF3DMA Object.
Definition: SPILPF3DMA.h:929
SwiP_Struct swi
Definition: SPILPF3DMA.h:933
uint8_t powerID
Definition: SPILPF3DMA.h:884
Definition: SPILPF3DMA.h:786
A SPI_Transaction data structure is used with SPI_transfer(). It indicates how many SPI_FrameFormat f...
Definition: SPI.h:570
Power notify object structure.
Definition: Power.h:445
GPIO driver implementation for Low Power F3 devices.
SPI_Mode
Definitions for various SPI modes of operation.
Definition: SPI.h:597
uint8_t intNum
Definition: SPILPF3DMA.h:863
uint8_t rxChannelEvtMux
Definition: SPILPF3DMA.h:894
Definition: SPILPF3DMA.h:800
bool isOpen
Definition: SPILPF3DMA.h:961
uint_least8_t sclkPin
Definition: SPILPF3DMA.h:916
int32_t pociPinMux
Definition: SPILPF3DMA.h:904
SPI_TransferMode transferMode
Definition: SPILPF3DMA.h:956
Definition: SPILPF3DMA.h:801
uint8_t format
Definition: SPILPF3DMA.h:958
SPILPF3DMA_ReturnPartial returnPartial
Definition: SPILPF3DMA.h:960
uint_least8_t pociPin
Definition: SPILPF3DMA.h:914
SPILPF3DMA Hardware attributes.
Definition: SPILPF3DMA.h:858
uint8_t intPriority
SPILPF3DMA Peripheral's interrupt priority.
Definition: SPILPF3DMA.h:875
int32_t picoPinMux
Definition: SPILPF3DMA.h:906
size_t framesTransferred
Definition: SPILPF3DMA.h:942
UDMALPF3 driver implementation.
uint_least8_t csnPin
Definition: SPILPF3DMA.h:959
SPI_Mode mode
Definition: SPILPF3DMA.h:957
uint16_t defaultTxBufValue
Definition: SPILPF3DMA.h:886
uint_least8_t csnPin
Definition: SPILPF3DMA.h:918
uint32_t swiPriority
SPI SWI priority. The higher the number, the higher the priority. The minimum is 0 and the maximum is...
Definition: SPILPF3DMA.h:882
bool manualStart
Definition: SPILPF3DMA.h:962
SPILPF3DMA_ReturnPartial
Definition: SPILPF3DMA.h:797
uint32_t minDmaTransferSize
Definition: SPILPF3DMA.h:921