CryptoKey.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2017-2022, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
81 #ifndef ti_drivers_cryptoutils_cyptokey_CryptoKey__include
82 #define ti_drivers_cryptoutils_cyptokey_CryptoKey__include
83 
84 #include <stdint.h>
85 #include <stdbool.h>
86 
87 #ifdef __cplusplus
88 extern "C" {
89 #endif
90 
113 #define CryptoKey_STATUS_RESERVED (-32)
114 
128 #define CryptoKey_STATUS_SUCCESS (0)
129 
136 #define CryptoKey_STATUS_ERROR (-1)
137 
144 #define CryptoKey_STATUS_UNDEFINED_ENCODING (-2)
145 
154 typedef uint8_t CryptoKey_Encoding;
155 static const CryptoKey_Encoding CryptoKey_PLAINTEXT = 0x02U;
156 static const CryptoKey_Encoding CryptoKey_BLANK_PLAINTEXT = 0x04U;
157 static const CryptoKey_Encoding CryptoKey_KEYSTORE = 0x08U;
158 static const CryptoKey_Encoding CryptoKey_BLANK_KEYSTORE = 0x10U;
159 
166 typedef struct
167 {
168  uint8_t *keyMaterial;
169  uint32_t keyLength;
171 
178 typedef struct
179 {
180  uint32_t keyLength;
181  uint32_t keyID;
184 
192 typedef struct
193 {
194  CryptoKey_Encoding encoding;
195  union
196  {
199  } u;
200 } CryptoKey;
201 
212 typedef struct CryptoKey_SecurityPolicy_ CryptoKey_SecurityPolicy;
213 
222 int_fast16_t CryptoKey_getCryptoKeyType(CryptoKey *keyHandle, CryptoKey_Encoding *keyType);
223 
232 int_fast16_t CryptoKey_isBlank(CryptoKey *keyHandle, bool *isBlank);
233 
243 int_fast16_t CryptoKey_markAsBlank(CryptoKey *keyHandle);
244 
255 
269 int_fast16_t CryptoKey_verifySecureInputKey(CryptoKey *secureKey);
270 
284 int_fast16_t CryptoKey_verifySecureOutputKey(CryptoKey *secureKey);
285 
286 #ifdef __cplusplus
287 }
288 #endif
289 
290 #endif /* ti_drivers_cryptoutils_cyptokey_CryptoKey__include */
CryptoKey_Plaintext plaintext
Definition: CryptoKey.h:197
static const CryptoKey_Encoding CryptoKey_KEYSTORE
Definition: CryptoKey.h:157
uint8_t CryptoKey_Encoding
List of the different types of CryptoKey.
Definition: CryptoKey.h:154
int_fast16_t CryptoKey_verifySecureOutputKey(CryptoKey *secureKey)
Function to verify a secure output CryptoKey.
static const CryptoKey_Encoding CryptoKey_BLANK_PLAINTEXT
Definition: CryptoKey.h:156
CryptoKey datastructure.
Definition: CryptoKey.h:192
Key store CryptoKey datastructure.
Definition: CryptoKey.h:178
int_fast16_t CryptoKey_getCryptoKeyType(CryptoKey *keyHandle, CryptoKey_Encoding *keyType)
Gets the key type of the CryptoKey.
uint32_t keyID
Definition: CryptoKey.h:181
static const CryptoKey_Encoding CryptoKey_PLAINTEXT
Definition: CryptoKey.h:155
int_fast16_t CryptoKey_verifySecureInputKey(CryptoKey *secureKey)
Function to verify a secure CryptoKey.
uint32_t keyLength
Definition: CryptoKey.h:180
int_fast16_t CryptoKey_markAsBlank(CryptoKey *keyHandle)
Marks a CryptoKey as &#39;blank&#39;.
CryptoKey_Encoding encoding
Definition: CryptoKey.h:194
Plaintext CryptoKey datastructure.
Definition: CryptoKey.h:166
int_fast16_t CryptoKey_initSecurityPolicy(CryptoKey_SecurityPolicy *policy)
Function to initialize the CryptoKey_SecurityPolicy struct to its defaults.
void * keyAttributes
Definition: CryptoKey.h:182
int_fast16_t CryptoKey_isBlank(CryptoKey *keyHandle, bool *isBlank)
Wheather the CryptoKey is &#39;blank&#39; or represents valid keying material.
CryptoKey_KeyStore keyStore
Definition: CryptoKey.h:198
struct CryptoKey_SecurityPolicy_ CryptoKey_SecurityPolicy
Structure that specifies the restrictions on a CryptoKey.
Definition: CryptoKey.h:212
static const CryptoKey_Encoding CryptoKey_BLANK_KEYSTORE
Definition: CryptoKey.h:158
uint8_t * keyMaterial
Definition: CryptoKey.h:168
uint32_t keyLength
Definition: CryptoKey.h:169
© Copyright 1995-2023, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale