Disable External Flash¶
The external flash consumes energy and can be disable if not used.
By default, SysConfig generate the code to enable / disable the external
flash at the end of ti_driver_config.c
. In the current release,
this code is excluded by a #if0 endif
block.
In order to enable the code, you can follow one of the two following options
Option 1: Copy-paste the excluded code in your application
Option 2: Modify the templates used by SysConfig to generate the code. These templates are stored in
<SDK>\source\ti\drivers\.meta\templates
.In
BoardCC23XX.c.xdt
, find and remove the line#if 0
(l 64) and the line#endif
(l 151)In
BoardCC23XX.Board_init.c.xdt
, modify line 46 to uncomment the call toBoard_shutDownExtFlash()
.
Once done, restart CCS and rebuild the project (right click on the project and select “Rebuild Project”).