255 #ifndef ti_drivers_lcd_LCDDogm1286__include 256 #define ti_drivers_lcd_LCDDogm1286__include 263 #include <ti/drivers/dpl/SemaphoreP.h> 266 #define LCD_PIXELS 8192 268 #define LCD_BYTES 1024 274 #define LCD_X_MAX (LCD_COLS-1) 280 #define LCD_Y_MAX (LCD_ROWS-1) 284 #define LCD_PAGE_ROWS 8 286 #define LCD_CHAR_WIDTH 6 288 #define LCD_FONT_WIDTH 5 516 extern void LCD_close(LCD_Handle handle);
592 extern void LCD_writeLine(LCD_Handle handle,
unsigned int bufIndex,
char *str,
unsigned int uiValue,
unsigned char ucFormat,
unsigned char ucLine);
608 extern void LCD_update(LCD_Handle handle,
unsigned int bufIndex);
646 extern void LCD_updatePart(LCD_Handle handle,
unsigned int bufIndex,
unsigned char ucXFrom,
unsigned char ucXTo,
647 LCD_Page iPageFrom, LCD_Page iPageTo);
730 extern void LCD_bufferClearPart(LCD_Handle handle,
unsigned int bufIndex,
unsigned char ucXFrom,
unsigned char ucXTo,
731 LCD_Page iPageFrom, LCD_Page iPageTo);
758 extern void LCD_bufferInvert(LCD_Handle handle,
unsigned int bufIndex,
unsigned char ucXFrom,
unsigned char ucYFrom,
759 unsigned char ucXTo,
unsigned char ucYTo);
793 extern void LCD_bufferInvertPage(LCD_Handle handle,
unsigned int bufIndex,
unsigned char ucXFrom,
unsigned char ucXTo,
826 extern void LCD_bufferPrintString(LCD_Handle handle,
unsigned int bufIndex,
const char *pcStr,
unsigned char ucX,
866 LCD_Align iAlignment, LCD_Page iPage);
897 extern void LCD_bufferPrintInt(LCD_Handle handle,
unsigned int bufIndex,
int i32Number,
unsigned char ucX,
936 LCD_Align iAlignment, LCD_Page iPage);
974 extern void LCD_bufferPrintFloat(LCD_Handle handle,
unsigned int bufIndex,
float fNumber,
unsigned char ucDecimals,
975 unsigned char ucX, LCD_Page iPage);
1016 LCD_Align iAlignment, LCD_Page iPage);
1044 extern void LCD_bufferSetLine(LCD_Handle handle,
unsigned int bufIndex,
unsigned char ucXFrom,
unsigned char ucYFrom,
1045 unsigned char ucXTo,
unsigned char ucYTo);
1073 extern void LCD_bufferClearLine(LCD_Handle handle,
unsigned int bufIndex,
unsigned char ucXFrom,
unsigned char ucYFrom,
1074 unsigned char ucXTo,
unsigned char ucYTo);
1099 extern void LCD_bufferSetHLine(LCD_Handle handle,
unsigned int bufIndex,
unsigned char ucXFrom,
unsigned char ucXTo,
1125 extern void LCD_bufferClearHLine(LCD_Handle handle,
unsigned int bufIndex,
unsigned char ucXFrom,
1126 unsigned char ucXTo,
unsigned char ucY);
1151 extern void LCD_bufferSetVLine(LCD_Handle handle,
unsigned int bufIndex,
unsigned char ucX,
unsigned char ucYFrom,
1152 unsigned char ucYTo);
1177 extern void LCD_bufferClearVLine(LCD_Handle handle,
unsigned int bufIndex,
unsigned char ucX,
unsigned char ucYFrom,
1178 unsigned char ucYTo);
1205 extern void LCD_bufferHArrow(LCD_Handle handle,
unsigned int bufIndex,
unsigned char ucXFrom,
unsigned char ucXTo,
unsigned char ucY);
1232 extern void LCD_bufferVArrow(LCD_Handle handle,
unsigned int bufIndex,
unsigned char ucX,
unsigned char ucYFrom,
unsigned char ucYTo);
1254 extern void LCD_bufferSetPx(LCD_Handle handle,
unsigned int bufIndex,
unsigned char ucX,
unsigned char ucY);
1275 extern void LCD_bufferClearPx(LCD_Handle handle,
unsigned int bufIndex,
unsigned char ucX,
unsigned char ucY);
1296 extern void LCD_bufferCopy(LCD_Handle handle,
unsigned int fromBufIndex,
unsigned int toBufIndex);
1312 extern void LCD_setContrast(LCD_Handle handle,
unsigned char ucContrast);
char displayStartLine
Definition: LCDDogm1286.h:378
LCD_Command const * LCD_initCmd
Definition: LCDDogm1286.h:449
void LCD_bufferInvertPage(LCD_Handle handle, unsigned int bufIndex, unsigned char ucXFrom, unsigned char ucXTo, LCD_Page iPage)
This function inverts a range of columns in the display buffer on a specified page (for example...
void LCD_bufferClearPage(LCD_Handle handle, unsigned int bufIndex, LCD_Page iPage)
This function clears the page specified by iPage in the given buffer.
void LCD_Params_init(LCD_Params *params)
Function to initialize the LCD_Params struct to its defaults.
char setPage
Definition: LCDDogm1286.h:392
void LCD_writeLine(LCD_Handle handle, unsigned int bufIndex, char *str, unsigned int uiValue, unsigned char ucFormat, unsigned char ucLine)
Function that writes a string and value to a buffer and sends it to the LCD display. The written page is being cleared before it is written to.
void LCD_bufferPrintString(LCD_Handle handle, unsigned int bufIndex, const char *pcStr, unsigned char ucX, LCD_Page iPage)
Function that writes a string to the specified buffer.
void LCD_bufferCopy(LCD_Handle handle, unsigned int fromBufIndex, unsigned int toBufIndex)
This function copies the content of fromBufIndex to toBufIndex.
Definition: LCDDogm1286.h:307
unsigned int bufSize
Definition: LCDDogm1286.h:411
char contrastSet1
Definition: LCDDogm1286.h:387
void LCD_bufferClearVLine(LCD_Handle handle, unsigned int bufIndex, unsigned char ucX, unsigned char ucYFrom, unsigned char ucYTo)
This function clears a vertical line from (ucX,ucYFrom) to (ucX,ucYTo) from the buffer specified...
void LCD_bufferSetPx(LCD_Handle handle, unsigned int bufIndex, unsigned char ucX, unsigned char ucY)
This function sets a pixel on (ucX,ucY).
void LCD_bufferClear(LCD_Handle handle, unsigned int bufIndex)
Function that empties the specified LCD buffer.
struct LCD_Config LCD_Config
The LCD_Config structure contains a set of pointers used to characterize the LCD driver implementatio...
bool isOpen
Definition: LCDDogm1286.h:423
LCD_Align
LCD alignment enum.
Definition: LCDDogm1286.h:303
void LCD_bufferPrintFloat(LCD_Handle handle, unsigned int bufIndex, float fNumber, unsigned char ucDecimals, unsigned char ucX, LCD_Page iPage)
This function writes a number of data type float to the given buffer at a specified column and page...
uint8_t spiIndex
Definition: LCDDogm1286.h:458
char adcSet
Definition: LCDDogm1286.h:379
struct LCD_Params LCD_Params
LCD Parameters are used to with the LCD_open() call. Default values for these parameters are set usin...
LCD Object.
Definition: LCDDogm1286.h:420
unsigned int lcdWriteTimeout
Definition: LCDDogm1286.h:425
struct LCD_HWAttrs LCD_HWAttrs
LCD Hardware attributes.
char columnLo
Definition: LCDDogm1286.h:394
LCD_Buffer used to store data to be printed on the LCD display.
Definition: LCDDogm1286.h:408
char staticIndicator1
Definition: LCDDogm1286.h:390
static const LCD_Command LCD_initCmd
Definition: LCDDogm1286.h:483
Definition: LCDDogm1286.h:339
void LCD_bufferClearHLine(LCD_Handle handle, unsigned int bufIndex, unsigned char ucXFrom, unsigned char ucXTo, unsigned char ucY)
This function clears a horizontal line from (ucXFrom,ucY) to (ucXTo,ucY) from the specified buffer...
struct LCD_Object LCD_Object
LCD Object.
void LCD_bufferPrintIntAligned(LCD_Handle handle, unsigned int bufIndex, int i32Number, LCD_Align iAlignment, LCD_Page iPage)
This function writes an integer to the given buffer as specified by the iAlignment argument...
void LCD_bufferSetLine(LCD_Handle handle, unsigned int bufIndex, unsigned char ucXFrom, unsigned char ucYFrom, unsigned char ucXTo, unsigned char ucYTo)
This function draws a line in the specified buffer from (ucXFrom,ucYFrom) to (ucXTo,ucYTo). The function uses Bresenham's line algorithm.
Definition: LCDDogm1286.h:305
uint8_t lcdCsnPin
Definition: LCDDogm1286.h:455
LCD_Page
LCD page enum.
Definition: LCDDogm1286.h:317
#define LCD_ROWS
Definition: LCDDogm1286.h:276
SPI_FrameFormat spiFrameFormat
Definition: LCDDogm1286.h:369
void LCD_close(LCD_Handle handle)
Function to close the LCD instance specified by the LCD handle.
void LCD_bufferClearLine(LCD_Handle handle, unsigned int bufIndex, unsigned char ucXFrom, unsigned char ucYFrom, unsigned char ucXTo, unsigned char ucYTo)
This function clears a line in the specified buffer from (ucXFrom,ucYFrom) to (ucXTo,ucYTo). The function uses Bresenham's line algorithm.
Definition: LCDDogm1286.h:320
LCD Parameters are used to with the LCD_open() call. Default values for these parameters are set usin...
Definition: LCDDogm1286.h:363
The LCD_Config structure contains a set of pointers used to characterize the LCD driver implementatio...
Definition: LCDDogm1286.h:467
LCD_Handle LCD_open(LCD_Buffer *buffers, uint8_t nBuffers, LCD_Params *params)
Function to set up the DOGM128W-6 LCD display.
struct LCD_Buffer LCD_Buffer
LCD_Buffer used to store data to be printed on the LCD display.
void LCD_init(void)
This function initializes the LCD driver module.
void LCD_bufferPrintFloatAligned(LCD_Handle handle, unsigned int bufIndex, float fNumber, unsigned char ucDecimals, LCD_Align iAlignment, LCD_Page iPage)
This function writes a float number to the given buffer as specified by the iAlignment argument...
#define LCD_COLS
Definition: LCDDogm1286.h:270
void LCD_bufferPrintInt(LCD_Handle handle, unsigned int bufIndex, int i32Number, unsigned char ucX, LCD_Page iPage)
Function that writes an integer to the specified buffer.
LCD_X_Limit
LCD x-axis enum.
Definition: LCDDogm1286.h:337
Definition: LCDDogm1286.h:322
void LCD_bufferPrintStringAligned(LCD_Handle handle, unsigned int bufIndex, const char *pcStr, LCD_Align iAlignment, LCD_Page iPage)
This function writes a string to the given buffer specified by the iAlignment argument.
char contrastSet2
Definition: LCDDogm1286.h:388
char columnHi
Definition: LCDDogm1286.h:393
void LCD_bufferClearPx(LCD_Handle handle, unsigned int bufIndex, unsigned char ucX, unsigned char ucY)
This function clears the pixel at (ucX,ucY).
uint8_t nBuffers
Definition: LCDDogm1286.h:429
Definition: LCDDogm1286.h:325
void LCD_bufferClearPart(LCD_Handle handle, unsigned int bufIndex, unsigned char ucXFrom, unsigned char ucXTo, LCD_Page iPageFrom, LCD_Page iPageTo)
This function clears the pixels in a given piece of a page. Resolution is given in coulmns [0–127] a...
uint8_t lcdModePin
Definition: LCDDogm1286.h:451
LCD Hardware attributes.
Definition: LCDDogm1286.h:446
Definition: LCDDogm1286.h:321
char staticIndicator0
Definition: LCDDogm1286.h:389
unsigned int lcdWriteTimeout
Definition: LCDDogm1286.h:365
Definition: LCDDogm1286.h:326
struct LCD_Config * LCD_Handle
A handle that is returned from a LCD_open() call.
Definition: LCDDogm1286.h:294
char outputMode
Definition: LCDDogm1286.h:380
struct LCD_Command LCD_Command
Format of LCD commands used by the LCD controller.
char contrastSet0
Definition: LCDDogm1286.h:386
SPI Global configuration.
Definition: SPI.h:709
uint8_t lcdResetPin
Definition: LCDDogm1286.h:453
Definition: LCDDogm1286.h:306
LCD_Buffer * lcdBuffers
Definition: LCDDogm1286.h:427
enum SPI_FrameFormat_ SPI_FrameFormat
Definitions for various SPI data frame formats.
char displayType
Definition: LCDDogm1286.h:381
void LCD_bufferVArrow(LCD_Handle handle, unsigned int bufIndex, unsigned char ucX, unsigned char ucYFrom, unsigned char ucYTo)
This function draws a vertical arrow from (ucX,ucYFrom) to (ucX,ucYTo) to the buffer specified...
void LCD_update(LCD_Handle handle, unsigned int bufIndex)
Function that writes the specified buffer to the LCD display.
char lcdBias
Definition: LCDDogm1286.h:382
void LCD_bufferSetVLine(LCD_Handle handle, unsigned int bufIndex, unsigned char ucX, unsigned char ucYFrom, unsigned char ucYTo)
This function draws a vertical line from (ucX,ucYFrom) to (ucX,ucYTo) into the specified buffer...
char boosterRadio1
Definition: LCDDogm1286.h:385
void LCD_bufferInvert(LCD_Handle handle, unsigned int bufIndex, unsigned char ucXFrom, unsigned char ucYFrom, unsigned char ucXTo, unsigned char ucYTo)
This function inverts the pixels (bits) in a given region of the specified buffer.
Definition: LCDDogm1286.h:340
void LCD_updatePart(LCD_Handle handle, unsigned int bufIndex, unsigned char ucXFrom, unsigned char ucXTo, LCD_Page iPageFrom, LCD_Page iPageTo)
Function that sends the specified part of the given buffer to the corresponding part on the LCD...
Definition: LCDDogm1286.h:353
LCD_Object * object
Definition: LCDDogm1286.h:470
Definition: LCDDogm1286.h:324
char displayEn
Definition: LCDDogm1286.h:391
Definition: LCDDogm1286.h:352
char * pcBuffer
Definition: LCDDogm1286.h:410
Format of LCD commands used by the LCD controller.
Definition: LCDDogm1286.h:376
char powerControl
Definition: LCDDogm1286.h:383
void LCD_bufferSetHLine(LCD_Handle handle, unsigned int bufIndex, unsigned char ucXFrom, unsigned char ucXTo, unsigned char ucY)
This function draws a horizontal line from (ucXFrom,ucY) to (ucXTo,ucY) into the specified buffer...
void LCD_bufferHArrow(LCD_Handle handle, unsigned int bufIndex, unsigned char ucXFrom, unsigned char ucXTo, unsigned char ucY)
This function draws a horizontal arrow from (ucXFrom,ucY) to (ucXTo,ucY) to buffer specified...
Definition: LCDDogm1286.h:319
SPI_Handle spiHandle
Definition: LCDDogm1286.h:424
SemaphoreP_Struct lcdMutex
Definition: LCDDogm1286.h:426
void LCD_setContrast(LCD_Handle handle, unsigned char ucContrast)
This Function sets the LCD contrast.
char boosterRadio0
Definition: LCDDogm1286.h:384
unsigned int spiBitRate
Definition: LCDDogm1286.h:368
Definition: LCDDogm1286.h:327
Definition: LCDDogm1286.h:323
SemaphoreP_Struct bufMutex
Definition: LCDDogm1286.h:412
LCD_HWAttrs const * hwAttrs
Definition: LCDDogm1286.h:472
LCD_Y_Limit
LCD y-axis enum.
Definition: LCDDogm1286.h:350