BLE5-Stack 1.00.01 to BLE5-Stack 1.01.00

This section will describe a way to migrate a project from BLE5-Stack 1.00.01 to a BLE5-Stack 1.01.00. This approach will be modifying an existing project’s configuration to utilize BLE5-Stack 1.01.00 libraries, tools, and code.

Once the project is converted to use the updated libraries, tools, and code of BLE5-Stack 1.01.00, the application then must be engineered to account for various API changes. This guide will contain API translation tables as well as tips to aide in the transition to BLE5-Stack 1.01.00.

For this migration guide, simple_peripheral from BLE5-Stack 1.00.01 will be ported to BLE5-Stack 1.01.00. Utilize the IDE and Tools recommended by BLE5-Stack release notes.

Once project configurations are updated, follow same building procedure used prior to the port. It is assumed the latest SDK has already been installed, see SimpleLink SDKs.

When applicable, this section will use simple_peripheral from BLE5-Stack 1.00.01 as an example when porting to BLE5-Stack 1.01.00.

For API Descriptions see BLE Stack API Reference

Table of Contents:

Project Configuration Changes

Project configuration needs to be updated in order to utilize the latest tools, code, and libraries. This section describes the changes necessary in order to do so in a IDE specific way.

CCS Stack Project

  1. Updating XDC Tools to Version 3.50.3.33

    Open Project Properties of the stack project for the application being ported

    1. Select General from the Navigation Tree
    2. Select Products Tab
    3. Select XDCtools version 3.50.3.33_core (Latest)
    4. Save Changes
    ../../_images/1.0.1-to-1.1.0-porting-guide-updating-xdctools.png

    Figure 140. CCS Updating XDC Tools Visual Instructions

    This will update the XDC_CG_ROOT path variable to utilize the latest version of XDCtools.

  2. Select BLE5-Stack 1.01.00

    Open Project Properties of the stack project for the application being ported

    1. Select General from the Navigation Tree
    2. Select Products Tab
    3. Select SimpleLink CC2640R2 SDK version containing BLE5-Stack 1.01.00
    4. Save Changes
    ../../_images/1.0.1-to-1.1.0-porting-guide-updating-ble-stack.png

    Figure 141. CCS Updating BLE5-Stack Visual Instructions

    This will update the COM_TI_SIMPLELINK_CC2640R2_SDK_INSTALL_DIR path variable to utilize the SDK containing BLE5-Stack 1.01.00.

    The path variables SRC_BLE_DIR and TOOLS_BLE_DIR will automatically be updated to point to the BLE5-Stack 1.01.00 version of tools and code.

  3. Update lib_search tool to correctly pull in the proper libraries

    Open Project Properties of the stack project for the application being ported

    1. Select Build from the Navigation Tree

    2. Select Steps Tab

    3. Modify the prebuild step from

      ${TOOLS_BLE_DIR}/lib_search/lib_search         ${PROJECT_LOC}/TOOLS/build_config.opt         ${SRC_BLE_DIR}/blelib         ${PROJECT_LOC}/FlashROM_Library/lib_linker.cmd         cc2640         ${TOOLS_BLE_DIR}/lib_search/lib_search.xml         ${SRC_BLE_DIR}/symbols
      

      to the following:

      ${TOOLS_BLE_DIR}/lib_search/lib_search         --opt ${PROJECT_LOC}/TOOLS/build_config.opt         --lib-dir ${SRC_BLE_DIR}/blelib/cc26x0r2         --cmd ${PROJECT_LOC}/FlashROM_Library/lib_linker.cmd         --xml ${TOOLS_BLE_DIR}/lib_search/lib_search.xml         --sym-dir ${SRC_BLE_DIR}/symbols/cc26x0r2
      
    4. Save Changes

    ../../_images/1.0.1-to-1.1.0-porting-guide-changing-prebuild-steps.png

    Figure 142. CCS Updating Pre-Build Visual Instructions

    This change accounts for updates to the lib_search tool’s argument variables.

  4. Update include path for Controller files

    Open Project Properties of the stack project for the application being ported

    1. Select Build -> ARM Compiler -> Include Options in the Navigation Tree
    2. Select ${SRC_BLE_DIR}/controller/cc26xx_r2/inc include path
    3. Modify the path by double clicking or pressing ‘Edit’
    4. Change to ${SRC_BLE_DIR}/controller/cc26xx/inc (remove _r2)
    5. Save Changes

    See CCS Updating Include Path Visual Instructions

    Note

    The include path ${SRC_BLE_DIR}/profiles/roles can safely be removed.

    The path to controller files have changed. In order include these files, a include path needs to be updated.

  5. Update source references for Controller and GAP

    Due to path changes for several key files, the virtual links within the project need to be updated to properly find files.

    The files which have been moved are located in:

    C:\ti\simplelink_cc2640r2_sdk_1_50_00_06\source\ti\ble5stack\controller\cc26xx\inc
    
    C:\ti\simplelink_cc2640r2_sdk_1_50_00_06\source\ti\ble5stack\host
    

    Namely, controller files and GAP related files.

    Examples are ll.h located in the INCLUDE folder, and gap.c, gapbondmgr.c, and gapbondmgr.h located in the PROFILES folder.

    Open the properties of a resource file of the stack project.

    1. Select Resource in the Navigation Tree
    2. Click Edit next to the Location field
    3. Modify location to match the resource’s actual location
    4. Confirm Changes
    5. Save Changes
    ../../_images/1.0.1-to-1.1.0-porting-guide-changing-virtual-link.png

    Figure 143. CCS Updating Pre-Build Visual Instructions

    This change allows the compiler to correctly resolve locations of moved files.

CCS Application Project

  1. Updating XDC Tools to Version 3.50.3.33 and BLE5-Stack to 1.01.00

    Open Project Properties of the application project for the application being ported

    1. Select General from the Navigation Tree
    2. Select Products Tab
    3. Select XDCtools version 3.50.3.33_core (Latest)
    4. Select SimpleLink CC2640R2 SDK version containing BLE5-Stack 1.01.00
    5. Save Changes
    ../../_images/1.0.1-to-1.1.0-porting-guide-updating-xdc-and-ble5stack.png

    This will update the XDC_CG_ROOT path variable to utilize the latest version of XDCtools.

    This will update the COM_TI_SIMPLELINK_CC2640R2_SDK_INSTALL_DIR path variable to utilize the SDK containing BLE5-Stack 1.01.00.

  2. Update include path for Controller files

    Open Project Properties of the stack project for the application being ported

    1. Select Build -> ARM Compiler -> Include Options in the Navigation Tree
    2. Select ${SRC_BLE_DIR}/controller/cc26xx_r2/inc include path
    3. Modify the path by double clicking or pressing ‘Edit’
    4. Change to ${SRC_BLE_DIR}/controller/cc26xx/inc (remove _r2)
    5. Save Changes
    ../../_images/1.0.1-to-1.1.0-porting-guide-changing-include-path.png

    Figure 145. CCS Updating Include Path Visual Instructions

    Note

    The include path ${SRC_BLE_DIR}/profiles/roles can safely be removed.

    The path to controller files have changed, this change updates the include path.

  3. Add USE_CORE_SDK to Predefined Symbols

    Open Project Properties of the stack project for the application being ported

    1. Select Build -> ARM Compiler -> Predefined Symbols
    2. Click Add to enter another Symbol
    3. Add USE_CORE_SDK predefined symbol
    4. Confirm
    5. Save Changes
    ../../_images/1.0.1-to-1.1.0-porting-guide-adding-preprocessor-define.png

    Figure 146. CCS Adding Preprocessor Symbols Visual Instructions

    This will allow correct resolution of middle ware drivers by the compiler.

IAR Common Project Configuration Changes

Since both the application and stack project utilize a common custom argument variable file, only this file needs to be configured to point to the correct stack and tools.

  1. Modifying Custom Argument Variables for BLE5-Stack 1.01.00 and XDCtools 3.50.3.33_core

    1. Click Tools from the Toolbar

    2. Select Configure Custom Argument Variable item

      ../../_images/1.0.1-to-1.1.0-porting-guide-selecting-custom-args-menu.png
    3. Expand the SIMPLELINK_CC2640R2_SRC_SDK Heading

    4. Modify SIMPLELINK_CORE_SDK_INSTALL_DIR to path of SDK containing BLE5-Stack 1.01.00

    5. Modify XDCROOT to path of XDCtools 3.50.3.33_core

    6. Save Changes

      ../../_images/1.0.1-to-1.1.0-porting-guide-ble5-custom-argument-variables.png

      Figure 148. IAR Changing Argument Variables

    7. Re-launch IAR Embedded Workbench

      This will refresh all file references to use BLE5-Stack 1.01.00 and XDCtools 3.50.3.33_core.

IAR Stack Project

  1. Modifying Include Path and Preprocessor Defines

    Open Project Properties of the stack project for the application being ported

    1. Select C/C++ Compiler from the navigation tree

    2. Select Preprocessor Tab

    3. Modify include paths to point to correct directory

      Change $SRC_BLE_DIR$\controller\cc26xx_r2\inc to $SRC_BLE_DIR$\controller\cc26xx\inc

    4. Add USE_CORE_SDK to Defined Symbols

    5. Save changes

      ../../_images/1.0.1-to-1.1.0-porting-guide-iar-changing-preprocessor-include-paths.png

      Figure 149. IAR Changing Include Paths

    Note

    The include path $SRC_BLE_DIR$\profiles\roles can be safely removed

  2. Remove old referenced files

    Remove Profiles/gap.c, Profiles/gapbondmgr.h, Profiles/gapbondmgr.c

    These files have been moved, and these old project links will be using the old location.

  3. Add new files from proper locations

    Add gap.c and gapbondmgr.c from <SDK>\source\ti\ble5stack\host to the Profiles folder.

    Add gapbondmgr.h from <SDK>\source\ti\ble5stack\inc to the Profiles Folder.

IAR Application Project

  1. Modifying Include Path and Preprocessor Defines

    Open Project Properties of the stack project for the application being ported

    1. Select C/C++ Compiler from the navigation tree

    2. Select Preprocessor Tab

    3. Modify include paths to point to correct directory

      Change $SRC_BLE_DIR$\controller\cc26xx_r2\inc to $SRC_BLE_DIR$\controller\cc26xx\inc

    4. Add USE_CORE_SDK to Defined Symbols

    5. Save changes

    See IAR Changing Include Paths

    Note

    The include path $SRC_BLE_DIR$\profiles\roles can be safely removed

  2. Remove old referenced files

    Remove Profiles/gap.c, Profiles/gapbondmgr.h, Profiles/gapbondmgr.c

    These files have been moved, and these old project links will be using the old location.

  3. Add new files from proper locations

    Add gap.c and gapbondmgr.c from <SDK>\source\ti\ble5stack\host to the Profiles folder.

    Add gapbondmgr.h from <SDK>\source\ti\ble5stack\inc to the Profiles Folder.

Project Application Changes

There are a number of different changes to the API in order to improve usability and ensure support with future BLE 5 features.

Among these changes are core fundamental changes of how GAP Roles are done in BLE5-Stack. Namely, the removal of source files particular to GAP Roles, rather focusing on device behavior.

Functionality has also been relocated to other modules where necessary to further facilitate this change. Additionally, Bluetooth 5.0 features are now always enabled with no option to disable.

For more information regarding the GAP changes and how to utilize them, see Generic Access Profile (GAP)

Stack Build Configuration File

The build_config.opt specifies which stack components will be utilized, and thus which library files should be used during the Stack Project build process. This file is located in the Tools folder of the Stack Project.

BLE5-Stack 1.01.00 now comes with BLE 5.0 features always enabled. BLE 5.0 features can not be removed from the stack.

Remove any references to BLE 5.0 features in the build_config.opt

For example, if -DV50_FEATURES=PHY_LR_CFG is in the build_config.opt comment out or remove the line altogether.

GAP Role Changes

All GAP Roles source files have been removed. These files such as peripheral.c, central.c, will produce build errors and must be removed.

In general functionality of the roles has been broken into distinct GAP functions: Scanner, Advertiser, and Initiator.

These functions of GAP can be independently controlled to allow the device to function as a desired GAP Role such as peripheral or central.

Utilize GAP Changes to port application functionality.

Examples may need to be used to assist in re-architecture of the application, such as simple_peripheral or simple_central. For example, initialization of GAP Advertiser can be found in simple_central.

GATT Profile Changes

Due to changes in LinkDB defines (linkdb.h), custom GATT profiles may need to modified in order to account for the new definitions.

For example, when calling GATTServApp_InitCharCfg with an invalid handle use the following:

// Initialize Client Characteristic Configuration attributes
GATTServApp_InitCharCfg( CONNHANDLE_INVALID, simpleProfileChar4Config );

The previous define for invalid handle as defined in linkdb.h was INVALID_CONNHANDLE.

See GAP GATT Server Changes and Link Database Changes for additional changes as required.

GAP Bond Manager Changes

During the removal of GAP Roles source files, functionality relating to specific roles was moved into GAP Bond Manager. One particular change is the handling of passcodes. These are now handled via call back - see simple_peripheral or simple_central for implementation details (search for passcodeCb).

See GAP Bond Manager Changes for additional changes.

Appendix - Translation Tables

Table 17. GAP Changes
Previous Implementation New/Current implementation
Type Name Description / API / Parameter
GAP EVENT GAP_AdvertDataUpdateDone
Based on GapScan_Events:
GAP_EVT_ADV_REPORT
GAP EVENT GAP_DeviceDiscovery
Based on GapScan_Events:
GAP_EVT_SCAN_DISABLED GAP_EVT_SCAN_PRD_ENDED GAP_EVT_SCAN_DUR_ENDED
GAP EVENT GAP_AdvertDataUpdateDone Check Return Status on GapAdv_loadData
GAP EVENT GAP_MakeDiscoverableDone Check Return Status on GapAdv_enable
GAP EVENT GAP_EndDiscoverableDone Check Return Status on GapAdv_disable
GAP EVENT GAP_RandomAddrChanged Obsolete - Address Resolution is done controller
GAP EVENT GAP_LinkParamUpdate Event is same - now supports both LLCP and L2CAP
GAP PARAM TGAP_GEN_DISC_ADV_MIN Configured by durationOrMaxEvents parameter of GapAdv_enable
GAP PARAM TGAP_LIM_ADV_TIMEOUT Configured by durationOrMaxEvents parameter of GapAdv_enable
GAP PARAM TGAP_GEN_DISC_SCAN Configured by parameters of GapScan_enable
GAP PARAM TGAP_LIM_DISC_SCAN Configured by parameters of GapScan_enable
GAP PARAM TGAP_GEN_DISC_SCAN_INT Configured by interval parameter of GapScan_setPhyParams
GAP PARAM TGAP_GEN_DISC_SCAN_WIND Configured by window parameter of GapScan_setPhyParams
GAP PARAM TGAP_LIM_DISC_SCAN_INT Configured by interval parameter of GapScan_setPhyParams
GAP PARAM TGAP_LIM_DISC_SCAN_WIND Configured by window parameter of GapScan_setPhyParams
GAP PARAM TGAP_CONN_EST_ADV_TIMEOUT Configured by durationOrMaxEvents parameter of GapAdv_enable
GAP PARAM TGAP_CONN_PARAM_TIMEOUT GAP_SetParamValue with GAP_PARAM_CONN_PARAM_TIMEOUT
GAP PARAM TGAP_LIM_DISC_ADV_INT_MIN GAP_SetParamValue with GAP_ADV_PARAM_PRIMARY_INTERVAL_MIN
GAP PARAM TGAP_LIM_DISC_ADV_INT_MAX GAP_SetParamValue with GAP_ADV_PARAM_PRIMARY_INTERVAL_MAX
GAP PARAM TGAP_GEN_DISC_ADV_INT_MIN GAP_SetParamValue with GAP_ADV_PARAM_PRIMARY_INTERVAL_MIN
GAP PARAM TGAP_GEN_DISC_ADV_INT_MAX GAP_SetParamValue with GAP_ADV_PARAM_PRIMARY_INTERVAL_MAX
GAP PARAM TGAP_CONN_ADV_INT_MIN GAP_SetParamValue with GAP_ADV_PARAM_PRIMARY_INTERVAL_MIN
GAP PARAM TGAP_CONN_ADV_INT_MAX GAP_SetParamValue with GAP_ADV_PARAM_PRIMARY_INTERVAL_MAX
GAP PARAM TGAP_CONN_SCAN_INT Configured by interval parameter of GapScan_setPhyParams
GAP PARAM TGAP_CONN_SCAN_WIND Configured by window parameter of GapScan_setPhyParams
GAP PARAM TGAP_CONN_HIGH_SCAN_INT Configured by interval parameter of GapScan_setPhyParams
GAP PARAM TGAP_CONN_HIGH_SCAN_WIND Configured by window parameter of GapScan_setPhyParams
GAP PARAM TGAP_GEN_DISC_SCAN_INT Configured by interval parameter of GapScan_setPhyParams
GAP PARAM TGAP_GEN_DISC_SCAN_WIND Configured by window parameter of GapScan_setPhyParams
GAP PARAM TGAP_LIM_DISC_SCAN_INT Configured by interval parameter of GapScan_setPhyParams
GAP PARAM TGAP_LIM_DISC_SCAN_WIND Configured by window parameter of GapScan_setPhyParams
GAP PARAM TGAP_CONN_EST_INT_MIN GapInit_setPhyParam with INIT_PHYPARAM_CONN_INT_MIN
GAP PARAM TGAP_CONN_EST_INT_MAX GapInit_setPhyParam with INIT_PHYPARAM_CONN_INT_MAX
GAP PARAM TGAP_CONN_EST_SCAN_INT GapInit_setPhyParam with INIT_PHYPARAM_SCAN_INTERVAL
GAP PARAM TGAP_CONN_EST_SCAN_WIND GapInit_setPhyParam with INIT_PHYPARAM_SCAN_WINDOW
GAP PARAM TGAP_CONN_EST_SUPERV_TIMEOUT GapInit_setPhyParam with INIT_PHYPARAM_SUP_TIMEOUT
GAP PARAM TGAP_CONN_EST_LATENCY GapInit_setPhyParam with INIT_PHYPARAM_CONN_LATENCY
GAP PARAM TGAP_CONN_EST_MIN_CE_LEN Obsolete - Not Used by Controller
GAP PARAM TGAP_CONN_EST_MAX_CE_LEN Obsolete - Not Used by Controller
GAP PARAM TGAP_PRIVATE_ADDR_INT GAP_SetParamValue with GAP_PARAM_PRIVATE_ADDR_INT
GAP PARAM TGAP_CONN_PAUSE_CENTRAL Obsolete - Not Used by Controller
GAP PARAM TGAP_CONN_PAUSE_PERIPHERAL Calling GAP_UpdateLinkParamReq as desired
GAP PARAM TGAP_SM_TIMEOUT GAP_SetParamValue with GAP_PARAM_SM_TIMEOUT
GAP PARAM TGAP_SM_MIN_KEY_LEN GAP_SetParamValue with GAP_PARAM_SM_MIN_KEY_LEN
GAP PARAM TGAP_SM_MAX_KEY_LEN GAP_SetParamValue with GAP_PARAM_SM_MAX_KEY_LEN
GAP PARAM TGAP_FILTER_ADV_REPORTS Obsolete - Duplicate Filtering done in Controller
GAP PARAM TGAP_SCAN_RSP_RSSI_MIN GapScan_setParam with SCAN_PARAM_FLT_MIN_RSSI
GAP PARAM TGAP_REJECT_CONN_PARAMS GAP_SetParamValue with GAP_PARAM_LINK_UPDATE_DECISION
GAP PARAM TGAP_AUTH_TASK_ID GAP_SetParamValue with GAP_PARAM_AUTH_TASK_ID
GAP PARAM TGAP_VERIFY_CAR GAP_SetParamValue with GAP_PARAM_VERIFY_CAR
GAP PARAM TGAP_GGS_PARAMS GAP_SetParamValue with GAP_PARAM_GGS_PARAMS
GAP PARAM GAPROLE_IRK, GAPCENTRALROLE_IRK GapConfig_SetParameter with GAP_CONFIG_PARAM_IRK
GAP PARAM GAPROLE_SRK, GAPCENTRALROLE_SRK GapConfig_SetParameter with GAP_CONFIG_PARAM_SRK
GAP PARAM GAPROLE_BD_ADDR, GAPCENTRALROLE_BD_ADDR HCI_ReadBDADDRCmd
GAP PARAM GAPROLE_ADVERT_ENABLED, GAPROLE_ADV_NONCONN_ENABLED GapAdv_enable and GapAdv_disable
GAP PARAM GAPROLE_ADVERT_OFF_TIME Configured by durationOrMaxEvents parameter of GapAdv_enable
GAP PARAM GAPROLE_ADVERT_DATA
Various API:
GapAdv_loadByBuffer GapAdv_loadHandle GapAdv_prepareLoadByBuffer GapAdv_prepareLoadByHandle GapAdv_getBuffer
GAP PARAM GAPROLE_SCAN_RSP_DATA
Various API:
GapAdv_loadByBuffer GapAdv_loadHandle GapAdv_prepareLoadByBuffer GapAdv_prepareLoadByHandle GapAdv_getBuffer
GAP PARAM GAPROLE_ADV_EVENT_TYPE GapAdv_setParam or GapAdv_getParam with GAP_ADV_PARAM_PROPS
GAP PARAM GAPROLE_ADV_DIRECT_TYPE GapAdv_setParam or GapAdv_getParam with GAP_ADV_PARAM_PEER_ADDRESS_TYPE
GAP PARAM GAPROLE_ADV_DIRECT_ADDR GapAdv_setParam or GapAdv_getParam with GAP_ADV_PARAM_PEER_ADDRESS
GAP PARAM GAPROLE_ADV_CHANNEL_MAP GapAdv_setParam or GapAdv_getParam with GAP_ADV_PARAM_PRIMARY_CHANNEL_MAP
GAP PARAM GAPROLE_ADV_FILTER_POLICY GapAdv_setParam or GapAdv_getParam with GAP_ADV_PARAM_FILTER_POLICY
GAP PARAM GAPROLE_CONNHANDLE Returned for each GAP event, alternatively HCI_EXT_GetConnInfoCmd
GAP PARAM GAPROLE_RSSI_READ_RATE RSSI can be received by HCI_ReadRssiCmd
GAP PARAM GAPROLE_PARAM_UPDATE_ENABLE GAP_UpdateLinkParamReq can be called as desired
GAP PARAM GAPROLE_MIN_CONN_INTERVAL pParams.connIntervalMin parameter of GAP_EstablishLinkReq
GAP PARAM GAPROLE_MAX_CONN_INTERVAL pParams.connIntervalMax parameter of GAP_EstablishLinkReq
GAP PARAM GAPROLE_SLAVE_LATENCY pParams.connLatency parameter of GAP_EstablishLinkReq
GAP PARAM GAPROLE_TIMEOUT_MULTIPLIER pParams.connTimeout parameter of GAP_EstablishLinkReq
GAP PARAM GAPROLE_STATE Obsolete - Architecture removes need for this
GAP PARAM GAPROLE_CONN_BD_ADDR, GAPROLE_BD_ADDR_TYPE Returned in GAP_LINK_ESTABLISHED_EVENT, contained in stack message, gapEstLinkReqEvent_t
GAP PARAM GAPROLE_CONN_INTERVAL Returned from linkDB_GetInfo, as linkDBInfo_t.connInterval
GAP PARAM GAPROLE_CONN_LATENCY Returned from linkDB_GetInfo, as linkDBInfo_t.connLatency
GAP PARAM GAPROLE_CONN_TIMEOUT Returned from linkDB_GetInfo, as linkDBInfo_t.connTimeout
GAP PARAM GAPCENTRALROLE_MAX_SCAN_RES Configured by maxNumReport parameter of GapScan_enable
GAP PARAM GAPCENTRALROLE_LINK_PARAM_UPDATE_REQ_REPLY GAP_SetParamValue with GAP_PARAM_LINK_UPDATE_DECISION
GAP API GAP_DeviceInit, GAPRole_StartDevice, GAPCentralRole_StartDevice
Declaration Change - Use GAP_DeviceInit with parameter for roles desired
See GAP_Profile_Roles
GAP API GAPRole_RegisterAppCBs Obsolete - Functionality moved to GAPBondMgr_Register
GAP API GAP_SetAdvToken Obsolete - Advertisement Sets are Used
GAP API GAP_GetAdvToken Obsolete - Advertisement Sets are Used
GAP API GAP_RemoveAdvToken Obsolete - Advertisement Sets are Used
GAP API GAP_UpdateAdvTokens Obsolete - Advertisement Sets are Used
GAP API GAPRole_SendUpdateParam, GAPCentralRole_UpdateLink GAP_UpdateLinkParamReq
GAP API GAP_MakeDiscoverable GapAdv_enable
GAP API GAP_UpdateAdvertisingData GapAdv_loadData
GAP API GAP_EndDiscoverable GapAdv_disable
GAP API GAP_DeviceDiscoveryRequest, GAPCentralRole_StartDiscovery GapScan_enable
GAP API GAP_DeviceDiscoveryCancel, GAPCentralRole_CancelDiscovery GapScan_disable
GAP API GAP_ResolvePrivateAddr Obsolete - Address Resolution is done controller
GAP API GAP_EstablishLinkReq, GAPCentralRole_EstablishLink GapInit_connect, or GapInit_connectWl to use Filter Accept List
GAP API GAP_TerminateLinkReq, GAPRole_TerminateConnection, GAPCentralRole_TerminateLink GapInit_cancelConnect for connection request, GAP_TerminateLinkReq otherwise
GAP API GAP_ConfigDeviceAddr No Changes; now the only way to set address and address type across modules
GAP CB gapRolesParamUpdateCB_t, paramUpdateAppDecision_t, passThroughToApp_t These are handled through GAP_UPDATE_LINK_PARAM_REQ_EVENT, applies to the L2CAP Parameter Update Procedure as well.
GAP CB gapRolesStateNotify_t, pfnGapCentralRoleEventCB_t Moved into GAP Bond Manager callbacks, gapBondCBs_t->gapEventCB
Table 18. GAP Bond Manager Changes
Previous Implementation New/Current implementation
Type Name Description / API / Parameter
GAPBOND PARAM GAPBOND_DEFAULT_PASSCODE Use pfnPasscodeCB_t, shared default passcode defined in bcomdef.h (BAPP_DEFAULT_PASSCODE)
GAPBOND PARAM GAPBOND_REMOTE_OOB_SC_ENABLED Obsolete
GAPBOND PARAM GAPBOND_REMOTE_OOB_SC_DATA Obsolete
GAPBOND PARAM GAPBOND_LOCAL_OOB_SC_ENABLED Obsolete
GAPBOND PARAM GAPBOND_LOCAL_OOB_SC_DATA Obsolete
GAPBOND STATE GAPBOND_PAIRING_STATE_BONDED GAPBOND_PAIRING_STATE_ENCRYPTED
GAPBOND DEF GBM_QUEUE_PAIRINGS Removed, is now default behavior
GAPBOND DEF GBM_GATT_NO_CLIENT Configured by GATT_NO_CLIENT
GAPBOND DEF SNP_SECURITY Configured by GAPBONDMGR_NO_SIGNING
GAPBOND API GAPBondMgr_LinkEst Removed Application Access to API Handled Internally
GAPBOND API GAPBondMgr_LinkTerm Removed Application Access to API Handled Internally
GAPBOND API GAPBondMgr_SlaveReqSecurity GAPBondMgr_Pair, allowing both Centrals and Peripherals to request pairing
GAPBOND API GAPBondMgr_UpdateCharCfg Removed Application Access to API Handled Internally
GAPBOND API GAPBondMgr_ReadGattChar Removed Application Access to API Handled Internally
GAPBOND API GAPBondMgr_SupportsEnhancedPriv Removed Application Access to API Handled Internally
GAPBOND API GAPBondMgr_CheckNVLen Removed Application Access to API Handled Internally
GAPBOND API GAPBondMgr_syncResolvingList Removed Application Access to API Handled Internally
Table 19. GAP GATT Server Changes
Previous Implementation New/Current implementation
Type Name Description / API / Parameter
GGS PARAM GGS_PERI_PRIVACY_FLAG_ATT Obsolete
GGS PARAM GGS_RECONNCT_ADDR_ATT Obsolete
GGS PARAM GGS_PERI_PRIVACY_FLAG_PROPS Obsolete
GGS PARAM GGS_W_PERMIT_PRIVACY_FLAG_ATT Obsolete
GGS PARAM GGS_TESTMODE_W_PERMIT_PRIVACY_FLAG Obsolete
Table 20. Link Database Changes
Previous Implementation New/Current implementation
Type Name Description / API / Parameter
LinkDB API linkDB_Remove API now accepts linkDBItem_t* in addition to connection handle