EasyLink API Reference¶
EasyLink RF API for CC13xx/CC26xx family.
Overview
The EasyLink API should be used in application code. The EasyLink API is intended to abstract the RF Driver in order to give a simple API for customers to use as is or extend to suit their application use cases.
General Behavior
Before using the EasyLink API:
- The EasyLink Layer is initialized by calling EasyLink_init(). This initializes and opens the RF driver and configuring a modulation scheme passed to EasyLink_init().
- The RX and TX can operate independently of each other.
The following is true for receive operation:
- RX is enabled by calling EasyLink_receive() or EasyLink_receiveAsync().
- Entering RX can be immediate or scheduled.
- EasyLink_receive() is blocking and EasyLink_receiveAsync() is nonblocking.
- the EasyLink API does not queue messages so calling another API function while in EasyLink_receiveAsync() will return EasyLink_Status_Busy_Error
- an Async operation can be cancelled with EasyLink_abort()
The following apply for transmit operation:
- TX is enabled by calling EasyLink_transmit() or EasyLink_transmitAsync().
- TX can be immediate or scheduled.
- EasyLink_transmit() is blocking and EasyLink_transmitAsync() is nonblocking
- EasyLink_transmit() for a scheduled command, or if TX can not start
- the EasyLink API does not queue messages so calling another API function while in EasyLink_transmitAsync() will return EasyLink_Status_Busy_Error
- an Async operation can be cancelled with EasyLink_abort()
Error handling
The EasyLink API will return EasyLink_Status containing success or error code. The EasyLink_Status code are:
- EasyLink_Status_Success
- EasyLink_Status_Config_Error
- EasyLink_Status_Param_Error
- EasyLink_Status_Mem_Error
- EasyLink_Status_Cmd_Error
- EasyLink_Status_Tx_Error
- EasyLink_Status_Rx_Error
- EasyLink_Status_Rx_Timeout
- EasyLink_Status_Busy_Error
- EasyLink_Status_Aborted
Power Management
The TI-RTOS power management framework will try to put the device into the most power efficient mode whenever possible. Please see the technical reference manual for further details on each power mode.
The EasyLink Layer uses the power management offered by the RF driver Refer to the RF drive documentation for more details.
Frame Structure
The EasyLink implements a basic header for transmitting and receiving data. This header supports addressing for a star or point-to-point network with acknowledgments.
Packet structure:
_________________________________________________________
| | | |
| 1B Length | 1-64b Dst Address | Payload |
|___________|___________________|_________________________|
Defines
-
EASYLINK_API_VERSION¶ EasyLink API Version.
-
EASYLINK_MAX_ADDR_SIZE¶ defines the Tx/Rx Max Address Size
-
EASYLINK_MAX_ADDR_FILTERS¶ defines the Max number of Rx Address filters
-
EASYLINK_WHITENING_MODE¶ defines the whitening mode
-
EasyLink_RadioTime_To_ms(radioTime)¶ macro to convert from Radio Time Ticks to ms
-
EasyLink_ms_To_RadioTime(ms)¶ macro to convert from ms to Radio Time Ticks
-
EasyLink_us_To_RadioTime(us)¶ macro to convert from us to Radio Time Ticks
-
EasyLink_PHY_CUSTOM¶ Phy Type defines so we can use them in checks.
-
EasyLink_PHY_50KBPS2GFSK¶
-
EasyLink_PHY_625BPSLRM¶
-
EasyLink_PHY_2_4_200KBPS2GFSK¶
-
EasyLink_PHY_5KBPSSLLR¶
-
EasyLink_PHY_2_4_100KBPS2GFSK¶
-
EasyLink_PHY_2_4_250KBPS2GFSK¶
-
EasyLink_PHY_200KBPS2GFSK¶
Typedefs
-
typedef uint32_t
(* EasyLink_GetRandomNumber)(void)¶ EasyLink 32-bit Random number generator function type used in the clear channel assessment algorithm.
-
typedef void
(* EasyLink_ReceiveCb)(EasyLink_RxPacket *rxPacket, EasyLink_Status status)¶ EasyLink Callback function type for Received packet, registered with EasyLink_ReceiveAsync()
-
typedef void
(* EasyLink_TxDoneCb)(EasyLink_Status status)¶ EasyLink Callback function type for Tx Done registered with EasyLink_TransmitAsync()
Enums
-
EasyLink_Status¶ EasyLink Status and error codes.
Values:
-
0¶ Success.
-
1¶ Configuration error.
-
2¶ Param error.
-
3¶ Memory Error.
-
4¶ Memory Error.
-
5¶ Tx Error.
-
6¶ Rx Error.
-
7¶ Rx Error.
-
8¶ Rx Buffer Error.
-
9¶ Busy Error.
-
10¶ Command stopped or aborted.
-
-
EasyLink_PhyType¶ Phy Type passed to EasyLink_init()
Values:
-
0 Customer Phy specific settings exported from SmartRF Studio.
-
1 Phy settings for Sub1G 50kbps data rate, IEEE 802.15.4g GFSK.
-
2 Phy settings for Sub1G 625bps data rate, Long Range Mode.
-
3 Phy settings for 2.4Ghz 200kbps data rate, IEEE 802.15.4g GFSK.
-
4 SimpleLink Long Range (5 kbps)
-
5 Phy settings for 2.4Ghz 100kbps data rate, IEEE 802.15.4g GFSK.
-
6 Phy settings for 2.4Ghz 250kbps data rate, IEEE 802.15.4g GFSK.
-
7 Phy settings for 200kbps data rate, IEEE 802.15.4g GFSK.
-
EasyLink_Num_Phy_Settings¶
-
-
EasyLink_CtrlOption¶ Advance configuration options.
Values:
-
0 Set the number of bytes in Addr for both Addr Filter and Tx/Rx operations
-
1 Set a timeout value for inactivity on the radio, i.e. if the radio stays idle for this amount of time it is automatically powered down
-
2 Set Multiclient mode for application that will use multiple RF clients. Must be set before calling EasyLink_init().
-
3 Relative time in ticks from Async Rx start to TimeOut. A value of 0 means no timeout
-
4 Enable/Disable Test mode for Tone.
-
5 Enable/Disable Test mode for Signal.
-
6 Enable/Disable Rx Test mode for Tone.
-
Functions
-
void
EasyLink_Params_init(EasyLink_Params * params)¶ Initializes the radio with specified Phy settings and RF client events.
This function configures the radio phy settings. If the ui32ModType is EasyLink_Phy_Custom then the configuration is taken from srf_settings.h. If a specific phy configuration is required (and not supported by any of the defined Phy types in EasyLink_PhyType then you can cut and past the RF setting from the SmartRF Studio code export tool. This will copy and use the RF_prop, RF_cmdPropRadioDivSetup and RF_cmdFs commands, as well as the Sync word from the RF_cmdPropTx and RF_cmdPropRx commands. The function configures the callback for client events. The client events that trigger the callback are set using the nClientEventMask type in EasyLink_Params. A pointer to the desired callback should be provided to the pClientEventCb type of the EasyLink_Params structure.
Default values are: ui32ModType = EasyLink_Phy_50kbps2gfsk RF_ClientCallback = NULL RF_ClientEventMask = 0 pGrnFxn = (EasyLink_GetRandomNumber)rand
- Parameters
params: The descriptor for the Phy mode and event callback settings
- Return
- EasyLink_Status
-
EasyLink_Status
EasyLink_init(EasyLink_Params * params)¶ Initializes the radio with specified Phy settings, CCA random number generator, and RF client events.
This function configures the radio phy settings. If the ui32ModType is EasyLink_Phy_Custom then the configuration is taken from srf_settings.h. If a specific phy configuration is required (and not supported by any of the defined Phy types in EasyLink_PhyType then you can cut and past the RF setting from the SmartRF Studio code export tool. This will copy and use the RF_prop, RF_cmdPropRadioDivSetup and RF_cmdFs commands, as well as the Sync word from the RF_cmdPropTx and RF_cmdPropRx commands. The function configures the callback for client events. The client events that trigger the callback are set using the nClientEventMask type in EasyLink_Params. A pointer to the desired callback should be provided to the pClientEventCb type of the EasyLink_Params structure.
- Return
- EasyLink_Status
- Parameters
params: The descriptor for the Phy mode, random number generator, and event callback settings
-
EasyLink_Status
EasyLink_getAbsTime(uint32_t * pui32AbsTime)¶ Gets the absolute radio time.
This function returns the absolute radio time and can be used for monitoring or Tx/Rx events using the EasyLink_TxPacket and EasyLink_RxPacket::absTime field.
- Return
- EasyLink_Status
- Parameters
pui32AbsTime: Pointer to return the signed RSSI value (dBm)
-
EasyLink_Status
EasyLink_getRssi(int8_t * pi8Rssi)¶ Gets the RSSI value of an ongoing Radio Operation.
This function returns the RSSI from an ongoing receiver radio operation. It is useful in receiver test modes to detect the presence of both modulated and unmodulated carrier waves
- Return
- EasyLink_Status
- Note
- if no RSSI is available the function writes -128 to the value argument
- Parameters
pi8Rssi: Pointer to return the signed RSSI value (dBm)
-
EasyLink_Status
EasyLink_transmit(EasyLink_TxPacket * txPacket)¶ Sends a Packet with blocking call.
This function is a blocking call to send a packet. If the Tx is successfully scheduled then the function will block until the Tx is complete.
- Return
- EasyLink_Status
- Parameters
txPacket: The descriptor for the packet to be Tx’ed.
-
EasyLink_Status
EasyLink_transmitAsync(EasyLink_TxPacket * txPacket, EasyLink_TxDoneCb cb)¶ Sends a Packet with non blocking call.
This function is a non blocking call to send a packet. If the Tx is successfully scheduled then the callback will be call once the Tx is complete.
- Return
- EasyLink_Status
- Parameters
txPacket: The descriptor for the packet to be Tx’ed.cb: The tx done function pointer.
-
EasyLink_Status
EasyLink_transmitCcaAsync(EasyLink_TxPacket * txPacket, EasyLink_TxDoneCb cb)¶ Sends a Packet with non blocking call if the channel is idle.
This function is a non blocking call to send a packet. It will check for a clear channel prior to transmission. If the channel is busy it will backoff for a random period, in time units of EASYLINK_CCA_BACKOFF_TIMEUNITS, before reassessing. It does this a certain number (EASYLINK_MAX_CCA_BACKOFF_WINDOW - EASYLINK_MIN_CCA_BACKOFF_WINDOW) of times before quitting unsuccessfully and running to the callback. If the Tx is successfully scheduled then the callback will be called once the Tx is complete.
- Return
- EasyLink_Status
- Parameters
txPacket: The descriptor for the packet to be Tx’ed.cb: The tx done function pointer.
-
EasyLink_Status
EasyLink_receive(EasyLink_RxPacket * rxPacket)¶ Blocking call that waits for an Rx Packet.
This function is a blocking call to wait for an Rx packet.
- Return
- EasyLink_Status
- Parameters
rxPacket: The descriptor for the packet to be Rx’ed.
-
EasyLink_Status
EasyLink_receiveAsync(EasyLink_ReceiveCb cb, uint32_t absTime)¶ Enables Asynchronous Packet Rx with non blocking call.
This function is a non blocking call to Rx a packet. The Rx is turned on and the Callback is called once a packet is received. The Rx will timeout if EasyLink_Ctrl_AsyncRx_TimeOut ctrl message is used to set the timeout to something other than 0.
- Return
- EasyLink_Status
- Parameters
cb: The rx function pointer.absTime: Start time of Rx (0: now !0: absolute radio time to start Rx)
-
EasyLink_Status
EasyLink_abort(void)¶ Abort a previously call Async Tx/Rx.
This function is a blocking call to abort a previous Async Tx/Rx
- Return
- EasyLink_Status
-
EasyLink_Status
EasyLink_setFrequency(uint32_t ui32Frequency)¶ Sets the Frequency.
This function set the radio to the specified frequency. Note that this will be rounded to the nearest frequency supported by the Frequency Synthesizer.
- Return
- EasyLink_Status
- Parameters
ui32Frequency: Frequency in units of kHz
-
uint32_t
EasyLink_getFrequency(void)¶ Gets the Frequency.
This function gets Frequency in units of kHz. This function will return the value set in the Frequency Synthesizer, and may not be the same as set using EasyLink_setFrequency(). Note that this value does not include any offsets for deviations due to factors such as temperature and hence this API should not be used to get an accurate measure of frequency.
- Return
- Frequency in units of kHz
-
EasyLink_Status
EasyLink_enableRxAddrFilter(uint8_t * pui8AddrFilterTable, uint8_t ui8AddrSize, uint8_t ui8NumAddrs)¶ Enables the address filter.
This function enables the address filter to filter out address that are not in the address table provided.
- Return
- EasyLink_Status
- Parameters
pui8AddrFilterTable: A uint8 pointer to a variable size 2d array containing the addresses to filter on.ui8AddrSize: The size of the address elementsui8NumAddrs: The number of address elements
-
EasyLink_Status
EasyLink_getIeeeAddr(uint8_t * ieeeAddr)¶ Gets the IEEE address.
This function gets the IEEE address
- Return
- EasyLink_Status
- Parameters
ieeeAddr: pointer to an 8 element byte array to write the IEEE address to.
-
EasyLink_Status
EasyLink_setRfPower(int8_t i8TxPowerDbm)¶ Sets the TX Power.
This function sets the Tx Power
- Note
- The PA mode is chosen at build time, run-time switching from high PA to default PA (or vice versa) is not supported.
- Return
- EasyLink_Status
- Parameters
i8TxPowerDbm: The Tx power in dBm’s to be set.- All platforms other than the CC1352P: Value of -10 dBm or values in the range of 0-14 dBm are accepted. Values above 14 are set to 14 dBm while those below 0 are set to -10 dBm
- CC1352P Default PA: -20 to 14 dBm. Values above 14 dBm will be set to 14 dBm, while values below -20 dBm will cause a configuration error
- CC1352P High PA: 14 to 20 dBm. Values above 20 dBm will be set to 20 dBm, while values below 14 dBm will cause a configuration error
-
EasyLink_Status
EasyLink_getRfPower(int8_t * pi8TxPowerDbm)¶ Gets the TX Power.
This function gets the Tx Power in dBm, values ranging from -10 to 14 dBm should be expect
- Return
- EasyLink_Status
- Parameters
pi8TxPowerDbm: Pointer to return the transmission power value (dBm)
-
EasyLink_Status
EasyLink_setCtrl(EasyLink_CtrlOption Ctrl, uint32_t ui32Value)¶ Sets advanced configuration options.
This function allows setting some of the advanced configuration options
- Return
- EasyLink_Status
- Parameters
Ctrl: The control option to be setui32Value: The value to set the control option to
-
EasyLink_Status
EasyLink_getCtrl(EasyLink_CtrlOption Ctrl, uint32_t * pui32Value)¶ Gets advanced configuration options.
This function allows getting some of the advanced configuration options
- Return
- EasyLink_Status
- Parameters
Ctrl: The control option to getpui32Value: Pointer to return the control option value
Variables
-
EasyLink_RfSetting EasyLink_supportedPhys[] Array containing all the supported EasyLink_rfSettings.
-
const uint8_t
EasyLink_numSupportedPhys¶ Size of the EasyLink_supportedPhys array.
-
struct
EasyLink_Params¶ - #include <EasyLink.h>
Structure for EasyLink_init() and EasyLink_Params_init()
Public Members
-
EasyLink_PhyType
ui32ModType¶ PHY type.
-
RF_ClientCallback
pClientEventCb¶ Client event callback function.
-
RF_ClientEventMask
nClientEventMask¶ Client event mask.
-
EasyLink_GetRandomNumber
pGrnFxn¶ Pointer to function that returns a 32-bit unsigned random number.
-
EasyLink_PhyType
-
struct
EasyLink_RfSetting¶ - #include <EasyLink.h>
Structure for EasyLink_init() containing pointers to all the commands necessary to define an RF setting.
Public Members
-
EasyLink_PhyType
EasyLink_phyType¶ The PHY type that this RF setting defines
-
RF_Mode*
RF_pProp¶ Pointer to RF Mode Command.
-
rfc_CMD_PROP_RADIO_DIV_SETUP_t*
RF_pCmdPropRadioDivSetup¶
-
rfc_CMD_PROP_RADIO_SETUP_t*
RF_pCmdPropRadioSetup¶
-
union EasyLink_RfSetting::@0
RF_uCmdPropRadio¶ Union containing either a pointer to a divided radio setup command or a pointer to a radio setup command
-
rfc_CMD_FS_t*
RF_pCmdFs¶ Pointer to a frequency setup command.
-
rfc_CMD_PROP_TX_t*
RF_pCmdPropTx¶ Pointer to a RF TX command.
-
rfc_CMD_PROP_TX_ADV_t*
RF_pCmdPropTxAdv¶ Pointer to an advanced RF TX command
-
rfc_CMD_PROP_RX_ADV_t*
RF_pCmdPropRxAdv¶ Pointer to an advanced RF RX command
-
RF_TxPowerTable_Entry*
RF_pTxPowerTable¶ Pointer to a Tx power table.
-
uint8_t
RF_txPowerTableSize¶ Tx power table size.
-
EasyLink_PhyType
-
struct
EasyLink_TxPacket¶ - #include <EasyLink.h>
Structure for the TX Packet.
-
struct
EasyLink_RxPacket¶ - #include <EasyLink.h>
Structure for the RX’ed Packet.
Public Members
-
uint8_t EasyLink_RxPacket::dstAddr[8] Dst Address of RX’ed packet.
-
int8_t
rssi¶ rssi of RX’ed packet
-
uint32_t
absTime¶ Absolute time to turn on Rx when passed (0 for immediate), Or Absolute time that packet was Rx when returned.
-
uint32_t
rxTimeout¶ Relative time in ticks from Rx start to Rx TimeOut a value of 0 means no timeout
-
uint8_t
len¶ length of RX’ed packet
-
uint8_t EasyLink_RxPacket::payload[128] payload of RX’ed packet
-
Defines
-
EASYLINK_DEFAULT_ADDR¶ Defines the address that will accompany each packet sent from this device when EASYLINK_USE_DEFAULT_ADDR is true. It can also be thought of as this device’s own address. Organized in little endian format (e.g.an address of 0xABCD should be defined as {0xCD,0xAB})
-
EASYLINK_USE_DEFAULT_ADDR¶ When false, the Easylink stack expects the application to provide an accompanying address for each EasyLink_TxPacket passed to the EasyLink_transmit(), EasyLink_transmitAsync(), and EasyLink_transmitCcaAsync() APIs. Otherwise, these APIs will use the address defined in EASYLINK_DEFAULT_ADDR.
-
EASYLINK_MAX_DATA_LENGTH¶ Defines the largest Tx/Rx payload that the interface can support.
-
EASYLINK_ADDR_SIZE¶ Defines the default address size for rx and tx operations.
-
EASYLINK_ENABLE_ADDR_FILTERING¶ Enables of disables address filtering by default.
-
EASYLINK_NUM_ADDR_FILTER¶ The table for setting the Rx Address Filters.
-
EASYLINK_ADDR_FILTER_TABLE¶ The table for setting the Rx Address Filters.
-
EASYLINK_IDLE_TIMEOUT¶ Defines the time for the radio to return to idle after inactivity.
-
EASYLINK_ENABLE_MULTI_CLIENT¶ Enables or disables the application to use multiple RF clients.
-
EASYLINK_ASYNC_RX_TIMEOUT¶ Defines the relative time from async RX start to timeout. A value of 0 means no timeout.
-
EASYLINK_MIN_CCA_BACKOFF_WINDOW¶ Minimum CCA back-off window in units of EASYLINK_CCA_BACKOFF_TIMEUNITS, as a power of 2.
-
EASYLINK_MAX_CCA_BACKOFF_WINDOW¶ Maximum CCA back-off window in units of EASYLINK_CCA_BACKOFF_TIMEUNITS, as a power of 2.
-
EASYLINK_CCA_BACKOFF_TIMEUNITS¶ The back-off time units in microseconds.
-
EASYLINK_CS_RSSI_THRESHOLD_DBM¶ RSSI threshold for Clear Channel Assessment (CCA)
-
EASYLINK_CHANNEL_IDLE_TIME_US¶ Time for which the channel RSSI must remain below the specified threshold for the channel to be considered idle.
-
EASYLINK_PARAM_CONFIG¶ EasyLink default parameter configuration.