Clocks

Clock instances are functions that can be scheduled to run after a certain number of system ticks. Clock instances are either one-shot or periodic. These instances start immediately upon creation, are configured to start after a delay, and can be stopped at any time. All clock instances are executed when they expire in the context of a Swi. The following example shows the minimum resolution is the TI-RTOS clock tick period set in the TI-RTOS configuration file (.cfg).

Note

The default TI-RTOS kernel tick period is 1 millisecond. For CC2640R2 devices, this is reconfigured in the TI-RTOS configuration file (.cfg):

Clock.tickPeriod = 10;

Each system tick, which is derived from the real-time clock RTC, launches a Clock object that compares the running tick count with the period of each clock to determine if the associated function should run. For higher-resolution timers, TI recommends using a 16-bit hardware timer channel or the sensor controller. See the Clock module in the package ti.sysbios.knl section of the TI-RTOS Kernel User Guide for more information on these functions.

Note

The Sensor Controller is not available on the CC2640R2L.

You can use the Kernel’s Clock APIs directly in your application and in addition the Util module also contains a set of abstracted TI-RTOS Clock functions as shown here:

Functional Example

The following example was taken from the simple_peripheral project in BLE5-Stack.

@startuml
hide footbox

participant simple_perpherial.c as A
box "Swi context"
    participant "Clock Object" as B
end box

activate A
group Initialize Clock object
    autonumber
    A -> B : Util_clockConstruct()
    autonumber stop
    A <-- B
end

...

group Start Clock object
    A -> B : Util_clockStart()

    B --> A
    note left: Event_pend(event,...)

    deactivate A
end

...

group Clock function triggers after expiration
    autonumber resume
    rnote over B
        The Clock object invokes supplied function pointer
        (e.g. SimplePeripheral_performPeriodicTask())
        This function only posts a signal such as an Event
    end note
    B -> B : SimplePeripheral_clockHandler();
    activate B
    autonumber stop
    B -> : Event_post(event, SP_PERIODIC_EVT);
    B <--
    deactivate B
end

group Process period function and restart Clock object
    -> A : Unblocked due to posted SP_PERIODIC_EVT.
    activate A
    rnote over A
        Given that an event was posted, we can process the
        periodic function from a Task context
        (e.g. SimplePeripheral_performPeriodicTask())
    end note
    autonumber resume
    A -> A : SimplePeripheral_performPeriodicTask()
    activate A

    rnote over A
        Restart the clock after the periodic process
    end note
    deactivate A
    autonumber stop
    A -> B : Util_startClock();
    B --> A

    deactivate A
    note left: Event_pend(event,...)
end

rnote over A, B
    The Clock object will trigger after
    expiration and the cycle will repeat itself.
end note

...

@enduml

Figure 46. Triggering Clock objects

Step 1 in Triggering Clock objects constructs the Clock object via Util_constructClock(). After the example entered a connected state, it will then start the Clock object via a Util_startClock().

Listing 14. Constructing periodicClock Clock object in simple_peripheral
// Clock instances for internal periodic events.
static Clock_Struct periodicClock;

// Create one-shot clocks for internal periodic events.
Util_constructClock(&periodicClock, SimplePeripheral_clockHandler,
    SP_PERIODIC_EVT_PERIOD, 0, false, SP_PERIODIC_EVT);

Step 2 in Triggering Clock objects, after the Clock object’s timer expired, it will execute SimplePeripheral_clockHandler() within a Swi context. As this call cannot be blocked and blocks all Tasks, it is kept short by invoking an Event_post(SP_PERIODIC_EVT) for post processing in simple_peripheral.

Listing 15. Defining SimplePeripheral_clockHandler()
static void SimplePeripheral_clockHandler(UArg arg)
{
    /* arg is passed in from Clock_construct() */
    Event_post(events, arg);
}

Attention

Clock functions must not call blocking kernel APIs or TI-RTOS driver APIs! Executing long routines will impact real-time constraints placed in high priority tasks allocated for wireless protocol stacks!

Step 3 in Triggering Clock objects, the simple_peripheral task is unblocked due the Event_post(SP_PERIODIC_EVT), where it proceeds to invoke the SimplePeripheral_performPeriodicTask() function. Afterwards, to restart the periodic execution of this function, it will restart the periodicClock Clock object.

Listing 16. Servicing the SP_PERIODIC_EVT event
if (events & SP_PERIODIC_EVT)
{
  // Perform periodic application task
  SimplePeripheral_performPeriodicTask();

  Util_startClock(&periodicClock);
}