SDSPI.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2017-2019, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 /*!***************************************************************************
33  * @file SDSPI.h
34  *
35  * @brief SD driver implementation built on the TI SPI driver.
36  *
37  * The SDSPI header file should be included in an application as follows:
38  * @code
39  * #include <ti/drivers/SD.h>
40  * #include <ti/drivers/sd/SDSPI.h>
41  * @endcode
42  *
43  * Refer to @ref SD.h for a complete description of APIs & example of use.
44  *
45  * This SD driver implementation can be used to communicate with SD cards
46  * via a SPI peripheral. This driver leverages the TI SPI driver to transfer
47  * data to/from the host processor to the SD card. The SD card chip select
48  * is also handled by this driver via the TI GPIO driver. Both the SPI
49  * driver instance & the GPIO pin (used as chip select) must be specified
50  * in the SDSPI hardware attributes.
51  *
52  * Note: This driver requires that the 'defaultTxBufValue' field in the SPI
53  * driver hardware attributes be set to '0xFF'.
54  *
55  * ## Data location & alignment #
56  *
57  * This driver relies on the TI SPI driver to configure the SPI peripheral &
58  * perform data transfers. This means that data to be transferred must comply
59  * with rules & restrictions set SPI driver (memory alignment & DMA
60  * accessibility requirements). Refer to @ref SPI.h & the device specific
61  * SPI implementation header files for details.
62  *
63  * <hr>
64  */
65 
66 #ifndef ti_drivers_sd_SDSPI__include
67 #define ti_drivers_sd_SDSPI__include
68 
69 #ifdef __cplusplus
70 extern "C" {
71 #endif
72 
73 #include <stdint.h>
74 #include <ti/drivers/dpl/SemaphoreP.h>
75 #include <ti/drivers/SD.h>
76 #include <ti/drivers/SPI.h>
77 
78 /* SDSPI function table */
79 extern const SD_FxnTable SDSPI_fxnTable;
80 
104 typedef struct SDSPI_HWAttrs_ {
105  uint_least8_t spiIndex;
106  uint16_t spiCsGpioIndex;
107 } SDSPI_HWAttrs;
108 
114 typedef struct SDSPI_Object_ {
115  SemaphoreP_Handle lockSem;
118  bool isOpen;
119 } SDSPI_Object;
120 
121 #ifdef __cplusplus
122 }
123 #endif
124 
125 #endif /* ti_drivers_sd_SDSPI__include */
uint_least8_t spiIndex
Definition: SDSPI.h:105
Serial Peripheral Interface (SPI) Driver Interface.
uint16_t spiCsGpioIndex
Definition: SDSPI.h:106
SPI_Handle spiHandle
Definition: SDSPI.h:116
SDSPI Object.
Definition: SDSPI.h:114
struct SDSPI_HWAttrs_ SDSPI_HWAttrs
Secure Digital (SD) Driver.
SPI Global configuration.
Definition: SPI.h:742
The definition of a SD function table that contains the required set of functions to control a specif...
Definition: SD.h:285
enum SD_CardType_ SD_CardType
SD Card type inserted.
const SD_FxnTable SDSPI_fxnTable
SemaphoreP_Handle lockSem
Definition: SDSPI.h:115
SD_CardType cardType
Definition: SDSPI.h:117
Definition: SDSPI.h:104
struct SDSPI_Object_ SDSPI_Object
SDSPI Object.
bool isOpen
Definition: SDSPI.h:118
© Copyright 1995-2021, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale