BLE-Stack 3.03.04 to BLE-Stack 3.03.05¶
This section will describe a way to migrate a project from BLE-Stack 3.03.04 to a BLE-Stack 3.03.05.
There are little or no changes in the examples, but the method provided below is a general safe approach to adopt.
For this migration guide, simple_peripheral from BLE-Stack 3.03.04 will be ported over to BLE-Stack 3.03.05. Because the directory structure is identical between the two releases, the recommended approach is to start with a BLE-Stack 3.03.05 project that contains the same base functionality as the porting target project and merge in any custom functionality.
Choose a BLE-Stack 3.03.05 example project that contains your target project’s base functionality.
For reference, see available sample projects that start with simple_.
In this example, we’re going to use simple_peripheral as the starting BLE-Stack 3.03.04 sample project.
Transfer all modified application files from BLE-Stack 3.03.04 into the BLE-Stack 3.03.05 example project.
In this example, the following files from BLE-Stack 3.03.04 were moved into simple_peripheral BLE-Stack 3.03.05 example:
simple_peripheral.c
simple_peripheral.h
If necessary, update the project to use the newer TI-RTOS drivers that are supplied with the SimpleLink CC2640R2 SDK.
Refer to the Core SDK release notes for additional information and the TI-RTOS examples included with SimpleLink CC2640R2 SDK.
For additional information on how BLE-Stack 3.03.04 uses TI-RTOS see TI-RTOS (RTOS Kernel) Overview
For any utilized TI Drivers, review TI-RTOS Kernel Users Guide and Driver APIs.