331 #include "hal_assert.h" 351 #define HCI_SUCCESS 0x00 352 #define HCI_ERROR_CODE_UNKNOWN_HCI_CMD 0x01 353 #define HCI_ERROR_CODE_UNKNOWN_CONN_ID 0x02 354 #define HCI_ERROR_CODE_HW_FAILURE 0x03 355 #define HCI_ERROR_CODE_PAGE_TIMEOUT 0x04 356 #define HCI_ERROR_CODE_AUTH_FAILURE 0x05 357 #define HCI_ERROR_CODE_PIN_KEY_MISSING 0x06 358 #define HCI_ERROR_CODE_MEM_CAP_EXCEEDED 0x07 359 #define HCI_ERROR_CODE_CONN_TIMEOUT 0x08 360 #define HCI_ERROR_CODE_CONN_LIMIT_EXCEEDED 0x09 361 #define HCI_ERROR_CODE_SYNCH_CONN_LIMIT_EXCEEDED 0x0A 362 #define HCI_ERROR_CODE_ACL_CONN_ALREADY_EXISTS 0x0B 363 #define HCI_ERROR_CODE_CMD_DISALLOWED 0x0C 364 #define HCI_ERROR_CODE_CONN_REJ_LIMITED_RESOURCES 0x0D 365 #define HCI_ERROR_CODE_CONN_REJECTED_SECURITY_REASONS 0x0E 366 #define HCI_ERROR_CODE_CONN_REJECTED_UNACCEPTABLE_BDADDR 0x0F 367 #define HCI_ERROR_CODE_CONN_ACCEPT_TIMEOUT_EXCEEDED 0x10 368 #define HCI_ERROR_CODE_UNSUPPORTED_FEATURE_PARAM_VALUE 0x11 369 #define HCI_ERROR_CODE_INVALID_HCI_CMD_PARAMS 0x12 370 #define HCI_ERROR_CODE_REMOTE_USER_TERM_CONN 0x13 371 #define HCI_ERROR_CODE_REMOTE_DEVICE_TERM_CONN_LOW_RESOURCES 0x14 372 #define HCI_ERROR_CODE_REMOTE_DEVICE_TERM_CONN_POWER_OFF 0x15 373 #define HCI_ERROR_CODE_CONN_TERM_BY_LOCAL_HOST 0x16 374 #define HCI_ERROR_CODE_REPEATED_ATTEMPTS 0x17 375 #define HCI_ERROR_CODE_PAIRING_NOT_ALLOWED 0x18 376 #define HCI_ERROR_CODE_UNKNOWN_LMP_PDU 0x19 377 #define HCI_ERROR_CODE_UNSUPPORTED_REMOTE_FEATURE 0x1A 378 #define HCI_ERROR_CODE_SCO_OFFSET_REJ 0x1B 379 #define HCI_ERROR_CODE_SCO_INTERVAL_REJ 0x1C 380 #define HCI_ERROR_CODE_SCO_AIR_MODE_REJ 0x1D 381 #define HCI_ERROR_CODE_INVALID_LMP_PARAMS 0x1E 382 #define HCI_ERROR_CODE_UNSPECIFIED_ERROR 0x1F 383 #define HCI_ERROR_CODE_UNSUPPORTED_LMP_PARAM_VAL 0x20 384 #define HCI_ERROR_CODE_ROLE_CHANGE_NOT_ALLOWED 0x21 385 #define HCI_ERROR_CODE_LMP_LL_RESP_TIMEOUT 0x22 386 #define HCI_ERROR_CODE_LMP_ERR_TRANSACTION_COLLISION 0x23 387 #define HCI_ERROR_CODE_LMP_PDU_NOT_ALLOWED 0x24 388 #define HCI_ERROR_CODE_ENCRYPT_MODE_NOT_ACCEPTABLE 0x25 389 #define HCI_ERROR_CODE_LINK_KEY_CAN_NOT_BE_CHANGED 0x26 390 #define HCI_ERROR_CODE_REQ_QOS_NOT_SUPPORTED 0x27 391 #define HCI_ERROR_CODE_INSTANT_PASSED 0x28 392 #define HCI_ERROR_CODE_PAIRING_WITH_UNIT_KEY_NOT_SUPPORTED 0x29 393 #define HCI_ERROR_CODE_DIFFERENT_TRANSACTION_COLLISION 0x2A 394 #define HCI_ERROR_CODE_RESERVED1 0x2B 395 #define HCI_ERROR_CODE_QOS_UNACCEPTABLE_PARAM 0x2C 396 #define HCI_ERROR_CODE_QOS_REJ 0x2D 397 #define HCI_ERROR_CODE_CHAN_ASSESSMENT_NOT_SUPPORTED 0x2E 398 #define HCI_ERROR_CODE_INSUFFICIENT_SECURITY 0x2F 399 #define HCI_ERROR_CODE_PARAM_OUT_OF_MANDATORY_RANGE 0x30 400 #define HCI_ERROR_CODE_RESERVED2 0x31 401 #define HCI_ERROR_CODE_ROLE_SWITCH_PENDING 0x32 402 #define HCI_ERROR_CODE_RESERVED3 0x33 403 #define HCI_ERROR_CODE_RESERVED_SLOT_VIOLATION 0x34 404 #define HCI_ERROR_CODE_ROLE_SWITCH_FAILED 0x35 405 #define HCI_ERROR_CODE_EXTENDED_INQUIRY_RESP_TOO_LARGE 0x36 406 #define HCI_ERROR_CODE_SIMPLE_PAIRING_NOT_SUPPORTED_BY_HOST 0x37 407 #define HCI_ERROR_CODE_HOST_BUSY_PAIRING 0x38 408 #define HCI_ERROR_CODE_CONN_REJ_NO_SUITABLE_CHAN_FOUND 0x39 409 #define HCI_ERROR_CODE_CONTROLLER_BUSY 0x3A 410 #define HCI_ERROR_CODE_UNACCEPTABLE_CONN_PARAMETERS 0x3B 411 #define HCI_ERROR_CODE_DIRECTED_ADV_TIMEOUT 0x3C 412 #define HCI_ERROR_CODE_CONN_TERM_MIC_FAILURE 0x3D 413 #define HCI_ERROR_CODE_CONN_FAILED_TO_ESTABLISH 0x3E 414 #define HCI_ERROR_CODE_MAC_CONN_FAILED 0x3F 415 #define HCI_ERROR_CODE_COARSE_CLOCK_ADJUST_REJECTED 0x40 416 #define HCI_ERROR_CODE_TYPE0_SUBMAP_NOT_DEFINED 0x41 417 #define HCI_ERROR_CODE_UNKNOWN_ADVERTISING_IDENTIFIER 0x42 418 #define HCI_ERROR_CODE_LIMIT_REACHED 0x43 419 #define HCI_ERROR_CODE_OPERATION_CANCELLED_BY_HOST 0x44 426 #define HCI_MAX_NUM_CMD_BUFFERS LL_MAX_NUM_CMD_BUFFERS 427 #if defined(CC2540) || defined(CC2541) || defined(CC2541S) 428 #define HCI_MAX_NUM_DATA_BUFFERS LL_MAX_NUM_DATA_BUFFERS //<! Max Num Data Buffers 429 #endif // CC2540 | CC2541 | CC2541S 432 #define FIRST_PKT_HOST_TO_CTRL LL_DATA_FIRST_PKT_HOST_TO_CTRL 433 #define CONTINUING_PKT LL_DATA_CONTINUATION_PKT 434 #define FIRST_PKT_CTRL_TO_HOST LL_DATA_FIRST_PKT_CTRL_TO_HOST 438 #define HCI_RSSI_NOT_AVAILABLE LL_RSSI_NOT_AVAILABLE 444 #define HCI_DISCONNECT_AUTH_FAILURE HCI_ERROR_CODE_AUTH_FAILURE 445 #define HCI_DISCONNECT_REMOTE_USER_TERM HCI_ERROR_CODE_REMOTE_USER_TERM_CONN 446 #define HCI_DISCONNECT_REMOTE_DEV_LOW_RESOURCES HCI_ERROR_CODE_REMOTE_DEVICE_TERM_CONN_LOW_RESOURCES 447 #define HCI_DISCONNECT_REMOTE_DEV_POWER_OFF HCI_ERROR_CODE_REMOTE_DEVICE_TERM_CONN_POWER_OFF 448 #define HCI_DISCONNECT_UNSUPPORTED_REMOTE_FEATURE HCI_ERROR_CODE_UNSUPPORTED_REMOTE_FEATURE 449 #define HCI_DISCONNECT_KEY_PAIRING_NOT_SUPPORTED HCI_ERROR_CODE_PAIRING_WITH_UNIT_KEY_NOT_SUPPORTED 450 #define HCI_DISCONNECT_UNACCEPTABLE_CONN_INTERVAL HCI_ERROR_CODE_UNACCEPTABLE_CONN_INTERVAL 458 #define HCI_READ_CURRENT_TX_POWER_LEVEL LL_READ_CURRENT_TX_POWER_LEVEL 459 #define HCI_READ_MAX_TX_POWER_LEVEL LL_READ_MAX_TX_POWER_LEVEL 466 #define HCI_CTRL_TO_HOST_FLOW_CTRL_OFF 0 467 #define HCI_CTRL_TO_HOST_FLOW_CTRL_ACL_ON_SYNCH_OFF 1 468 #define HCI_CTRL_TO_HOST_FLOW_CTRL_ACL_OFF_SYNCH_ON 2 469 #define HCI_CTRL_TO_HOST_FLOW_CTRL_ACL_ON_SYNCH_ON 3 476 #define HCI_PUBLIC_DEVICE_ADDRESS LL_DEV_ADDR_TYPE_PUBLIC 477 #define HCI_RANDOM_DEVICE_ADDRESS LL_DEV_ADDR_TYPE_RANDOM 484 #define HCI_CONNECTABLE_UNDIRECTED_ADV LL_ADV_CONNECTABLE_UNDIRECTED_EVT 485 #define HCI_CONNECTABLE_DIRECTED_HDC_ADV LL_ADV_CONNECTABLE_DIRECTED_HDC_EVT 486 #define HCI_SCANNABLE_UNDIRECTED LL_ADV_SCANNABLE_UNDIRECTED_EVT 487 #define HCI_NONCONNECTABLE_UNDIRECTED_ADV LL_ADV_NONCONNECTABLE_UNDIRECTED_EVT 488 #define HCI_CONNECTABLE_DIRECTED_LDC_ADV LL_ADV_CONNECTABLE_DIRECTED_LDC_EVT 495 #define HCI_ADV_CHAN_37 LL_ADV_CHAN_37 496 #define HCI_ADV_CHAN_38 LL_ADV_CHAN_38 497 #define HCI_ADV_CHAN_39 LL_ADV_CHAN_39 498 #define HCI_ADV_CHAN_ALL (LL_ADV_CHAN_37 | LL_ADV_CHAN_38 | LL_ADV_CHAN_39) 505 #define HCI_ADV_WL_POLICY_ANY_REQ LL_ADV_WL_POLICY_ANY_REQ 506 #define HCI_ADV_WL_POLICY_WL_SCAN_REQ LL_ADV_WL_POLICY_WL_SCAN_REQ 507 #define HCI_ADV_WL_POLICY_WL_CONNECT_IND LL_ADV_WL_POLICY_WL_CONNECT_IND 508 #define HCI_ADV_WL_POLICY_WL_ALL_REQ LL_ADV_WL_POLICY_WL_ALL_REQ 515 #define HCI_ENABLE_ADV LL_ADV_MODE_ON 516 #define HCI_DISABLE_ADV LL_ADV_MODE_OFF 523 #define HCI_SCAN_PASSIVE LL_SCAN_PASSIVE 524 #define HCI_SCAN_ACTIVE LL_SCAN_ACTIVE 531 // Scan White List Policy 532 #define HCI_SCAN_WL_POLICY_ANY_ADV_PKTS LL_SCAN_WL_POLICY_ANY_ADV_PKTS 533 #define HCI_SCAN_WL_POLICY_USE_WHITE_LIST LL_SCAN_WL_POLICY_USE_WHITE_LIST 541 #define HCI_FILTER_REPORTS_DISABLE LL_FILTER_REPORTS_DISABLE 542 #define HCI_FILTER_REPORTS_ENABLE LL_FILTER_REPORTS_ENABLE 550 #define HCI_SCAN_STOP LL_SCAN_STOP 551 #define HCI_SCAN_START LL_SCAN_START 558 #define HCI_INIT_WL_POLICY_USE_PEER_ADDR LL_INIT_WL_POLICY_USE_PEER_ADDR 559 #define HCI_INIT_WL_POLICY_USE_WHITE_LIST LL_INIT_WL_POLICY_USE_WHITE_LIST 566 #define HCI_ENCRYPTION_OFF LL_ENCRYPTION_OFF 567 #define HCI_ENCRYPTION_ON LL_ENCRYPTION_ON 574 #define HCI_DIRECT_TEST_PAYLOAD_PRBS9 LL_DIRECT_TEST_PAYLOAD_PRBS9 575 #define HCI_DIRECT_TEST_PAYLOAD_0x0F LL_DIRECT_TEST_PAYLOAD_0x0F 576 #define HCI_DIRECT_TEST_PAYLOAD_0x55 LL_DIRECT_TEST_PAYLOAD_0x55 577 #define HCI_DIRECT_TEST_PAYLOAD_PRBS15 LL_DIRECT_TEST_PAYLOAD_PRBS15 578 #define HCI_DIRECT_TEST_PAYLOAD_0xFF LL_DIRECT_TEST_PAYLOAD_0xFF 579 #define HCI_DIRECT_TEST_PAYLOAD_0x00 LL_DIRECT_TEST_PAYLOAD_0x00 580 #define HCI_DIRECT_TEST_PAYLOAD_0xF0 LL_DIRECT_TEST_PAYLOAD_0xF0 581 #define HCI_DIRECT_TEST_PAYLOAD_0xAA LL_DIRECT_TEST_PAYLOAD_0xAA 588 #define HCI_DTM_STANDARD_MODULATION_INDEX LL_DTM_STANDARD_MODULATION_INDEX 589 #define HCI_DTM_STABLE_MODULATION_INDEX LL_DTM_STABLE_MODULATION_INDEX 596 #define HCI_EXT_DTM_TX_CONTINUOUS LL_EXT_DTM_TX_CONTINUOUS 603 #define HCI_DISABLE_ADDR_RESOLUTION LL_DISABLE_ADDR_RESOLUTION 604 #define HCI_ENABLE_ADDR_RESOLUTION LL_ENABLE_ADDR_RESOLUTION 605 #define HCI_NETWORK_PRIVACY_MODE LL_NETWORK_PRIVACY_MODE 606 #define HCI_DEVICE_PRIVACY_MODE LL_DEVICE_PRIVACY_MODE 613 #define HCI_PHY_USE_PHY_PARAM LL_PHY_USE_PHY_PARAM 614 #define HCI_PHY_USE_ANY_PHY LL_PHY_USE_ANY_PHY 615 #define HCI_PHY_1_MBPS LL_PHY_1_MBPS 616 #define HCI_PHY_2_MBPS LL_PHY_2_MBPS 617 #define HCI_PHY_CODED LL_PHY_CODED 624 #define PHY_UPDATE_COMPLETE_EVENT_1M 1 625 #define PHY_UPDATE_COMPLETE_EVENT_2M 2 626 #define PHY_UPDATE_COMPLETE_EVENT_CODED 3 633 #define HCI_EXT_RX_GAIN_STD LL_EXT_RX_GAIN_STD 634 #define HCI_EXT_RX_GAIN_HIGH LL_EXT_RX_GAIN_HIGH 641 #if defined( CC26XX ) || defined( CC13XX ) 642 #define HCI_EXT_TX_POWER_MINUS_21_DBM LL_EXT_TX_POWER_MINUS_21_DBM 643 #define HCI_EXT_TX_POWER_MINUS_18_DBM LL_EXT_TX_POWER_MINUS_18_DBM 644 #define HCI_EXT_TX_POWER_MINUS_15_DBM LL_EXT_TX_POWER_MINUS_15_DBM 645 #define HCI_EXT_TX_POWER_MINUS_12_DBM LL_EXT_TX_POWER_MINUS_12_DBM 646 #define HCI_EXT_TX_POWER_MINUS_9_DBM LL_EXT_TX_POWER_MINUS_9_DBM 647 #define HCI_EXT_TX_POWER_MINUS_6_DBM LL_EXT_TX_POWER_MINUS_6_DBM 648 #define HCI_EXT_TX_POWER_MINUS_3_DBM LL_EXT_TX_POWER_MINUS_3_DBM 649 #define HCI_EXT_TX_POWER_0_DBM LL_EXT_TX_POWER_0_DBM 650 #define HCI_EXT_TX_POWER_1_DBM LL_EXT_TX_POWER_1_DBM 651 #define HCI_EXT_TX_POWER_2_DBM LL_EXT_TX_POWER_2_DBM 652 #define HCI_EXT_TX_POWER_3_DBM LL_EXT_TX_POWER_3_DBM 653 #define HCI_EXT_TX_POWER_4_DBM LL_EXT_TX_POWER_4_DBM 654 #define HCI_EXT_TX_POWER_5_DBM LL_EXT_TX_POWER_5_DBM 656 #define HCI_EXT_TX_POWER_MINUS_23_DBM LL_EXT_TX_POWER_MINUS_23_DBM 657 #define HCI_EXT_TX_POWER_MINUS_6_DBM LL_EXT_TX_POWER_MINUS_6_DBM 658 #define HCI_EXT_TX_POWER_0_DBM LL_EXT_TX_POWER_0_DBM 659 #define HCI_EXT_TX_POWER_4_DBM LL_EXT_TX_POWER_4_DBM 660 #endif // CC26XX/CC13XX 667 #define HCI_EXT_ENABLE_ONE_PKT_PER_EVT LL_EXT_ENABLE_ONE_PKT_PER_EVT 668 #define HCI_EXT_DISABLE_ONE_PKT_PER_EVT LL_EXT_DISABLE_ONE_PKT_PER_EVT 677 #define HCI_EXT_ENABLE_CLK_DIVIDE_ON_HALT LL_EXT_ENABLE_CLK_DIVIDE_ON_HALT 678 #define HCI_EXT_DISABLE_CLK_DIVIDE_ON_HALT LL_EXT_DISABLE_CLK_DIVIDE_ON_HALT 687 #define HCI_EXT_NV_IN_USE LL_EXT_NV_IN_USE 688 #define HCI_EXT_NV_NOT_IN_USE LL_EXT_NV_NOT_IN_USE 695 #define HCI_EXT_ENABLE_FAST_TX_RESP_TIME LL_EXT_ENABLE_FAST_TX_RESP_TIME 696 #define HCI_EXT_DISABLE_FAST_TX_RESP_TIME LL_EXT_DISABLE_FAST_TX_RESP_TIME 703 #define HCI_EXT_ENABLE_SL_OVERRIDE LL_EXT_ENABLE_SL_OVERRIDE 704 #define HCI_EXT_DISABLE_SL_OVERRIDE LL_EXT_DISABLE_SL_OVERRIDE 711 #define HCI_EXT_TX_MODULATED_CARRIER LL_EXT_TX_MODULATED_CARRIER 712 #define HCI_EXT_TX_UNMODULATED_CARRIER LL_EXT_TX_UNMODULATED_CARRIER 719 #define HCI_PTM_SET_FREQ_TUNE_DOWN LL_EXT_SET_FREQ_TUNE_DOWN 720 #define HCI_PTM_SET_FREQ_TUNE_UP LL_EXT_SET_FREQ_TUNE_UP 729 #define HCI_EXT_PM_IO_PORT_P0 LL_EXT_PM_IO_PORT_P0 730 #define HCI_EXT_PM_IO_PORT_P1 LL_EXT_PM_IO_PORT_P1 731 #define HCI_EXT_PM_IO_PORT_P2 LL_EXT_PM_IO_PORT_P2 732 #define HCI_EXT_PM_IO_PORT_NONE LL_EXT_PM_IO_PORT_NONE 734 #define HCI_EXT_PM_IO_PORT_PIN0 LL_EXT_PM_IO_PORT_PIN0 735 #define HCI_EXT_PM_IO_PORT_PIN1 LL_EXT_PM_IO_PORT_PIN1 736 #define HCI_EXT_PM_IO_PORT_PIN2 LL_EXT_PM_IO_PORT_PIN2 737 #define HCI_EXT_PM_IO_PORT_PIN3 LL_EXT_PM_IO_PORT_PIN3 738 #define HCI_EXT_PM_IO_PORT_PIN4 LL_EXT_PM_IO_PORT_PIN4 739 #define HCI_EXT_PM_IO_PORT_PIN5 LL_EXT_PM_IO_PORT_PIN5 740 #define HCI_EXT_PM_IO_PORT_PIN6 LL_EXT_PM_IO_PORT_PIN6 741 #define HCI_EXT_PM_IO_PORT_PIN7 LL_EXT_PM_IO_PORT_PIN7 750 #define HCI_EXT_PER_RESET LL_EXT_PER_RESET 751 #define HCI_EXT_PER_READ LL_EXT_PER_READ 760 #define HCI_EXT_HALT_DURING_RF_DISABLE LL_EXT_HALT_DURING_RF_DISABLE 761 #define HCI_EXT_HALT_DURING_RF_ENABLE LL_EXT_HALT_DURING_RF_ENABLE 770 #define HCI_EXT_SET_USER_REVISION LL_EXT_SET_USER_REVISION 771 #define HCI_EXT_READ_BUILD_REVISION LL_EXT_READ_BUILD_REVISION 778 #define HCI_EXT_RESET_SYSTEM_HARD LL_EXT_RESET_SYSTEM_HARD 779 #define HCI_EXT_RESET_SYSTEM_SOFT LL_EXT_RESET_SYSTEM_SOFT 788 #define HCI_EXT_DISABLE_OVERLAPPED_PROCESSING LL_EXT_DISABLE_OVERLAPPED_PROCESSING 789 #define HCI_EXT_ENABLE_OVERLAPPED_PROCESSING LL_EXT_ENABLE_OVERLAPPED_PROCESSING 798 #define HCI_EXT_DISABLE_NUM_COMPL_PKTS_ON_EVENT LL_EXT_DISABLE_NUM_COMPL_PKTS_ON_EVENT 799 #define HCI_EXT_ENABLE_NUM_COMPL_PKTS_ON_EVENT LL_EXT_ENABLE_NUM_COMPL_PKTS_ON_EVENT 806 #define HCI_EXT_DISABLE_SCAN_REQUEST_REPORT LL_EXT_DISABLE_SCAN_REQUEST_REPORT 807 #define HCI_EXT_ENABLE_SCAN_REQUEST_REPORT LL_EXT_ENABLE_SCAN_REQUEST_REPORT 818 #define HCI_LINK_TYPE_SCO_BUFFER_OVERFLOW 0 819 #define HCI_LINK_TYPE_ACL_BUFFER_OVERFLOW 1 828 #define HCI_EXT_RF_SETUP_1M_PHY LL_EXT_RF_SETUP_1M_PHY 829 #define HCI_EXT_RF_SETUP_2M_PHY LL_EXT_RF_SETUP_2M_PHY 830 #define HCI_EXT_RF_SETUP_CODED_S8_PHY LL_EXT_RF_SETUP_CODED_S8_PHY 831 #define HCI_EXT_RF_SETUP_CODED_S2_PHY LL_EXT_RF_SETUP_CODED_S2_PHY 841 typedef uint8 hciStatus_t;
1073 uint8 p256Key[LL_SC_P256_KEY_LEN];
1082 uint8 dhKey[LL_SC_DHKEY_LEN];
1135 #if defined( CC26XX ) || defined( CC13XX ) 1136 PACKED_TYPEDEF_STRUCT
1139 #endif // CC26XX/CC13XX 1143 uint8 addr[LL_DEVICE_ADDR_LEN];
1147 #if defined( CC26XX ) || defined( CC13XX ) 1148 PACKED_TYPEDEF_STRUCT
1151 #endif // CC26XX/CC13XX 1156 uint16 numMMissedEvents;
1181 extern void *HCI_bm_alloc( uint16 size );
1196 extern uint8 HCI_ValidConnTimeParams( uint16 connIntervalMin,
1197 uint16 connIntervalMax,
1199 uint16 connTimeout );
1206 extern void HCI_TestAppTaskRegister( uint8 taskID );
1213 extern void HCI_GAPTaskRegister( uint8 taskID );
1220 extern void HCI_L2CAPTaskRegister( uint8 taskID );
1227 extern void HCI_SMPTaskRegister( uint8 taskID );
1234 extern void HCI_ExtTaskRegister( uint8 taskID );
1260 extern hciStatus_t HCI_SendDataPkt( uint16 connHandle,
1280 extern hciStatus_t HCI_DisconnectCmd( uint16 connHandle,
1375 extern hciStatus_t HCI_SetControllerToHostFlowCtrlCmd( uint8 flowControlEnable );
1396 extern hciStatus_t HCI_HostBufferSizeCmd( uint16 hostAclPktLen,
1397 uint8 hostSyncPktLen,
1398 uint16 hostTotalNumAclPkts,
1399 uint16 hostTotalNumSyncPkts );
1432 uint16 *connHandles,
1433 uint16 *numCompletedPkts );
1447 uint16 *aptoValue );
1570 extern hciStatus_t HCI_LE_SetRandomAddressCmd( uint8 *pRandAddr );
1589 extern hciStatus_t HCI_LE_SetAdvParamCmd( uint16 advIntervalMin,
1590 uint16 advIntervalMax,
1593 uint8 directAddrType,
1595 uint8 advChannelMap,
1596 uint8 advFilterPolicy );
1609 extern hciStatus_t HCI_LE_SetAdvDataCmd( uint8 dataLen,
1623 extern hciStatus_t HCI_LE_SetScanRspDataCmd( uint8 dataLen,
1636 extern hciStatus_t HCI_LE_SetAdvEnableCmd( uint8 advEnable );
1646 extern hciStatus_t HCI_LE_ReadAdvChanTxPowerCmd(
void );
1664 extern hciStatus_t HCI_LE_SetScanParamCmd( uint8 scanType,
1665 uint16 scanInterval,
1668 uint8 filterPolicy );
1682 extern hciStatus_t HCI_LE_SetScanEnableCmd( uint8 scanEnable,
1683 uint8 filterDuplicates );
1709 extern hciStatus_t HCI_LE_CreateConnCmd( uint16 scanInterval,
1711 uint8 initFilterPolicy,
1715 uint16 connIntervalMin,
1716 uint16 connIntervalMax,
1730 extern hciStatus_t HCI_LE_CreateConnCancelCmd(
void );
1804 extern hciStatus_t HCI_LE_ConnUpdateCmd( uint16 connHandle,
1805 uint16 connIntervalMin,
1806 uint16 connIntervalMax,
1918 extern hciStatus_t HCI_LE_StartEncyptCmd( uint16 connHandle,
1934 extern hciStatus_t HCI_LE_LtkReqReplyCmd( uint16 connHandle,
1948 extern hciStatus_t HCI_LE_LtkReqNegReplyCmd( uint16 connHandle );
2033 extern hciStatus_t HCI_LE_RemoteConnParamReqReplyCmd( uint16 connHandle,
2034 uint16 connIntervalMin,
2035 uint16 connIntervalMax,
2057 extern hciStatus_t HCI_LE_RemoteConnParamReqNegReplyCmd( uint16 connHandle,
2165 uint8 *peerIdAddr );
2211 uint8 *peerIdAddr );
2232 uint8 *localIdAddr );
2250 extern hciStatus_t HCI_LE_SetAddressResolutionEnableCmd( uint8 addrResolutionEnable );
2289 uint8 privacyMode );
2310 extern hciStatus_t HCI_LE_ReadLocalP256PublicKeyCmd(
void );
2331 extern hciStatus_t HCI_LE_GenerateDHKeyCmd( uint8 *publicKey );
2463 int16 rxPathParam );
2536 extern hciStatus_t HCI_EXT_ClkDivOnHaltCmd( uint8 control );
2559 extern hciStatus_t HCI_EXT_DeclareNvUsageCmd( uint8 mode );
2846 extern hciStatus_t HCI_EXT_SetBDADDRCmd( uint8 *bdAddr );
2994 extern hciStatus_t HCI_EXT_MapPmIoPortCmd( uint8 ioPort, uint8 ioPin );
3088 extern hciStatus_t HCI_EXT_ExtendRfRangeCmd(
void );
3102 extern hciStatus_t HCI_EXT_HaltDuringRfCmd( uint8 mode );
3161 extern hciStatus_t HCI_EXT_AdvEventNoticeCmd( uint8 taskID, uint16 taskEvent );
3277 extern hciStatus_t HCI_EXT_DelaySleepCmd( uint16 delay );
3313 extern hciStatus_t HCI_EXT_LLTestModeCmd( uint8 testCase );
3326 extern hciStatus_t HCI_EXT_OverlappedProcessingCmd( uint8 mode );
3387 extern hciStatus_t HCI_EXT_GetConnInfoCmd( uint8 *numAllocConns,
3388 uint8 *numActiveConns,
3389 hciConnInfo_t *activeConnInfo );
3438 extern hciStatus_t HCI_EXT_ReadRandAddrCmd(
void );
hciStatus_t HCI_EXT_PacketErrorRateCmd(uint16 connHandle, uint8 command)
osal_event_hdr_t hdr
osal event header
Definition: hci.h:1004
uint8 BLEEventCode
BLE Event Code.
Definition: hci.h:927
uint8 status
status of event
Definition: hci.h:940
This API allows the software components in the Z-Stack to be written independently of the specifics o...
uint8 eventType
scan request event type
Definition: hci.h:916
uint16 * pNumCompletedPackets
pointer to the number of completed packets array
Definition: hci.h:971
hciStatus_t HCI_EXT_SetMaxDataLenCmd(uint16 txOctets, uint16 txTime, uint16 rxOctets, uint16 rxTime)
uint16 connHandle
connection handle
Definition: hci.h:1060
uint8 status
status of event
Definition: hci.h:928
uint8 status
status of event
Definition: hci.h:1049
uint8 addrType
public or random address type
Definition: hci.h:895
uint8 pktType
packet type
Definition: hci.h:1113
uint8 BLEEventCode
BLE Event Code.
Definition: hci.h:949
uint8 clockAccuracy
connection clock accuracy
Definition: hci.h:878
osal_event_hdr_t hdr
osal event header
Definition: hci.h:1096
uint16 Interval_Min
minimum connection interval
Definition: hci.h:1038
hciStatus_t HCI_LE_SetDefaultPhyCmd(uint8 allPhys, uint8 txPhy, uint8 rxPhy)
HCI Packet event.
Definition: hci.h:1103
osal_event_hdr_t hdr
osal event header
Definition: hci.h:958
#define B_RANDOM_NUM_SIZE
BLE Random Number Size.
Definition: bcomdef.h:140
uint8 numHandles
number of handles
Definition: hci.h:969
uint8 * pReturnParam
pointer to the return parameter
Definition: hci.h:980
hciStatus_t HCI_LE_ReadRemoteUsedFeaturesCmd(uint16 connHandle)
osal_event_hdr_t hdr
osal event header
Definition: hci.h:948
uint16 dataPktLen
data packet length
Definition: hci.h:1089
Command Status Event.
Definition: hci.h:993
uint16 connHandle
connection handle
Definition: hci.h:1050
osal_event_hdr_t hdr
osal event header
Definition: hci.h:1058
osal_event_hdr_t hdr
osal event header
Definition: hci.h:914
hciStatus_t HCI_LE_TestEndCmd(void)
hciStatus_t HCI_LE_SetResolvablePrivateAddressTimeoutCmd(uint16 rpaTimeout)
hciStatus_t HCI_EXT_SetMaxDtmTxPowerCmd(uint8 txPower)
Hardware Error Event.
Definition: hci.h:1002
hciStatus_t HCI_EXT_ModemTestTxCmd(uint8 cwMode, uint8 txChan)
hciStatus_t HCI_LE_TransmitterTestCmd(uint8 txChan, uint8 dataLen, uint8 pktPayload)
uint8 peerAddrType
peer address type
Definition: hci.h:873
uint8 status
status of event
Definition: hci.h:1012
hciStatus_t HCI_LE_RandCmd(void)
LE Advertising Report Event.
Definition: hci.h:892
hciStatus_t HCI_LE_ReadRfPathCompCmd(void)
#define B_MAX_ADV_LEN
BLE Maximum Advertising Packet Length.
Definition: bcomdef.h:137
hciStatus_t HCI_LE_ReadResolvingListSizeCmd(void)
LE Data Length Change Event.
Definition: hci.h:1056
hciStatus_t HCI_SetEventMaskPage2Cmd(uint8 *pMask)
hciStatus_t HCI_LE_ReadLocalSupportedFeaturesCmd(void)
uint8 numDevices
number of discovered devices
Definition: hci.h:907
uint16 connectionHandle
connection handle
Definition: hci.h:855
uint16 connHandle
connection handle
Definition: hci.h:1114
uint8 BLEEventCode
BLE Event Code.
Definition: hci.h:1059
hciStatus_t HCI_EXT_EnablePTMCmd(void)
hciStatus_t HCI_LE_SetDataLenCmd(uint16 connHandle, uint16 txOctets, uint16 txTime)
osal_event_hdr_t hdr
osal event header
Definition: hci.h:938
LE Phy Update Complete Event.
Definition: hci.h:1045
osal_event_hdr_t hdr
osal event header
Definition: hci.h:1027
osal_event_hdr_t hdr
osal event header
Definition: hci.h:968
uint8 BLEEventCode
BLE Event Code.
Definition: hci.h:1035
hciStatus_t HCI_LE_EnhancedRxTestCmd(uint8 rxChan, uint8 rxPhy, uint8 modIndex)
uint8 BLEEventCode
BLE Event code.
Definition: hci.h:1071
osal_event_hdr_t hdr
osal event header
Definition: hci.h:986
hciStatus_t HCI_WriteAuthPayloadTimeoutCmd(uint16 connHandle, uint16 aptoValue)
osal_event_hdr_t hdr
osal event header
Definition: hci.h:1011
hciStatus_t HCI_LE_SetHostChanClassificationCmd(uint8 *chanMap)
uint8 BLEEventCode
BLE Event Code.
Definition: hci.h:1080
union _hciEvt_BLEConnComplete_u_ hciEvt_BLEConnComplete_u
LE Connection Complete Event.
uint16 connInterval
connection interval
Definition: hci.h:859
uint16 Interval_Max
maximum connection interval
Definition: hci.h:1039
uint8 length
length of parametric data, in bytes
Definition: hci.h:987
hciStatus_t HCI_EXT_NumComplPktsLimitCmd(uint8 limit, uint8 flushOnEvt)
uint16 connectionHandle
connection handle
Definition: hci.h:941
uint8 BLEEventCode
BLE Event Code.
Definition: hci.h:1048
uint16 maxRxTime
maximum receive time
Definition: hci.h:1064
hciStatus_t HCI_ReadRssiCmd(uint16 connHandle)
uint8 status
status
Definition: hci.h:1072
uint16 connectionHandle
connection handle
Definition: hci.h:871
uint16 connTimeout
connection supervision timeout
Definition: hci.h:932
uint8 encEnable
encryption enabled or not
Definition: hci.h:952
uint16 Latency
slave latency
Definition: hci.h:1040
hciStatus_t HCI_LE_ReadSupportedStatesCmd(void)
uint16 connLatency
connection latency
Definition: hci.h:876
uint8 linkType
synchronous or asynchronous buffer overflow
Definition: hci.h:1021
Vendor Specific Command Complete Event.
Definition: hci.h:984
osal_event_hdr_t hdr
osal event header
Definition: hci.h:926
hciStatus_t HCI_EXT_DecryptCmd(uint8 *key, uint8 *encText)
hciStatus_t HCI_EXT_SetFreqTuneCmd(uint8 step)
hciStatus_t HCI_EXT_SetDtmTxPktCntCmd(uint16 txPktCnt)
Data structure for HCI Command Complete Event Return Parameter.
Definition: hci.h:1086
hciStatus_t HCI_LE_EnhancedTxTestCmd(uint8 txChan, uint8 payloadLen, uint8 payloadType, uint8 txPhy)
hciStatus_t HCI_SetEventMaskCmd(uint8 *pMask)
hciStatus_t HCI_LE_AddWhiteListCmd(uint8 addrType, uint8 *devAddr)
uint8 clockAccuracy
connection clock accuracy
Definition: hci.h:862
Disconnection Complete Event.
Definition: hci.h:1009
hciStatus_t HCI_EXT_SaveFreqTuneCmd(void)
hciStatus_t HCI_LE_ReadSuggestedDefaultDataLenCmd(void)
hciStatus_t HCI_EXT_ResetSystemCmd(uint8 mode)
osal_event_hdr_t hdr
OSAL Event header.
Definition: hci.h:1112
Authenticated Payload Timeout Expired Event.
Definition: hci.h:1025
hciStatus_t HCI_EXT_EnhancedModemTestTxCmd(uint8 cwMode, uint8 rfPhy, uint8 rfChan)
hciStatus_t HCI_LE_ReadWhiteListSizeCmd(void)
uint16 connHandle
connection handle
Definition: hci.h:1037
uint16 maxTxTime
maximum transmission time
Definition: hci.h:1062
hciStatus_t HCI_LE_SetEventMaskCmd(uint8 *pEventMask)
int8 rssi
report RSSI
Definition: hci.h:899
uint16 connLatency
connection latency
Definition: hci.h:931
uint8 BLEEventCode
BLE Event Code.
Definition: hci.h:906
uint8 * pData
data
Definition: hci.h:1117
hciStatus_t HCI_EXT_SetRxGainCmd(uint8 rxGain)
uint8 reason
reason
Definition: hci.h:951
int8 rssi
report RSSI
Definition: hci.h:920
uint8 BLEEventCode
BLE Event Code.
Definition: hci.h:959
uint16 cmdOpcode
command opcode
Definition: hci.h:998
uint8 chSelAlgo
channel selection algorithm
Definition: hci.h:1099
hciStatus_t HCI_ReadRemoteVersionInfoCmd(uint16 connHandle)
osal_event_hdr_t hdr
OSAL event header.
Definition: hci.h:1105
hciStatus_t HCI_EXT_EndModemTestCmd(void)
hciStatus_t HCI_LE_ReadTxPowerCmd(void)
hciStatus_t HCI_LE_EncryptCmd(uint8 *key, uint8 *plainText)
hciStatus_t HCI_ReadLocalVersionInfoCmd(void)
hciStatus_t HCI_LE_ReadBufSizeCmd(void)
hciStatus_t HCI_LE_ReadLocalResolvableAddressCmd(uint8 localIdAddrType, uint8 *localIdAddr)
osal_event_hdr_t hdr
osal event header
Definition: hci.h:1070
hciStatus_t HCI_EXT_ModemHopTestTxCmd(void)
Command Complete Event.
Definition: hci.h:975
uint8 rxPhy
RX PHY.
Definition: hci.h:1052
hciEvt_DevInfo_t * devInfo
pointer to the array of devInfo
Definition: hci.h:908
LE Channel Selection Algorithm Event.
Definition: hci.h:1094
uint16 connHandle
connection handle
Definition: hci.h:950
HCI Data Packet.
Definition: hci.h:1110
uint8 status
status
Definition: hci.h:1081
uint8 status
status of event
Definition: hci.h:854
uint16 connTimeout
connection supervision timeout
Definition: hci.h:877
uint16 Timeout
supervision timeout
Definition: hci.h:1041
LE Generate DHKey Complete Event.
Definition: hci.h:1077
hciStatus_t HCI_EXT_EnhancedModemHopTestTxCmd(uint8 payloadLen, uint8 payloadType, uint8 rfPhy)
uint16 * pConnectionHandle
pointer to the connection handle array
Definition: hci.h:970
LE Remote Connection Parameter Request Event.
Definition: hci.h:1032
hciStatus_t HCI_EXT_PERbyChanCmd(uint16 connHandle, perByChan_t *perByChan)
uint16 connLatency
connection latency
Definition: hci.h:860
uint8 status
status of event
Definition: hci.h:1036
hciStatus_t HCI_ReadLocalSupportedCommandsCmd(void)
uint8 BLEEventCode
BLE Event Code.
Definition: hci.h:915
hciStatus_t HCI_EXT_ModemTestRxCmd(uint8 rxChan)
uint16 connInterval
connection interval
Definition: hci.h:875
uint8 bleChan
BLE channel.
Definition: hci.h:919
uint8 eventType
advertisement or scan response event type
Definition: hci.h:894
osal_event_hdr_t hdr
osal event header
Definition: hci.h:852
hciEvt_BLEEnhConnComplete_t enhEvt
enhanced connection complete event
Definition: hci.h:888
osal_event_hdr_t hdr
osal event header
Definition: hci.h:868
hciStatus_t HCI_LE_ClearResolvingListCmd(void)
hciStatus_t HCI_EXT_SetSlaveLatencyOverrideCmd(uint8 control)
hciStatus_t HCI_EXT_OnePktPerEvtCmd(uint8 control)
uint16 connTimeout
connection supervision timeout
Definition: hci.h:861
Type definitions and macros for BLE stack.
VS LE Scan Request Report Event.
Definition: hci.h:912
hciStatus_t HCI_EXT_SetFastTxResponseTimeCmd(uint8 control)
LE Encryption Change Event.
Definition: hci.h:946
hciStatus_t HCI_EXT_BuildRevisionCmd(uint8 mode, uint16 userRevNum)
hciStatus_t HCI_LE_ReadPhyCmd(uint16 connHandle)
uint16 connInterval
connection interval
Definition: hci.h:930
uint8 * pEventParam
event parameters
Definition: hci.h:989
hciEvt_BLEConnComplete_t legEvt
connection complete event
Definition: hci.h:887
hciStatus_t HCI_ReadTransmitPowerLevelCmd(uint16 connHandle, uint8 txPwrType)
uint8 cmdStatus
command status
Definition: hci.h:996
LE Enhanced Connection Complete Event.
Definition: hci.h:866
hciStatus_t HCI_LE_SetPhyCmd(uint16 connHandle, uint8 allPhys, uint8 txPhy, uint8 rxPhy, uint16 phyOpts)
uint16 connHandle
connection handle
Definition: hci.h:1028
uint16 cmdOpcode
command opcode
Definition: hci.h:979
uint8 BLEEventCode
BLE Event Code.
Definition: hci.h:853
uint32_t len
Image length in bytes.
Definition: oad_image_header.h:529
Number of Completed Packets Event.
Definition: hci.h:966
hciStatus_t HCI_LE_ReadPeerResolvableAddressCmd(uint8 peerIdAddrType, uint8 *peerIdAddr)
OSAL Event Header.
Definition: osal.h:92
hciStatus_t HCI_EXT_SetLocalSupportedFeaturesCmd(uint8 *localFeatures)
hciStatus_t HCI_LE_ReceiverTestCmd(uint8 rxChan)
uint8 BLEEventCode
BLE Event Code.
Definition: hci.h:869
uint8 txPhy
TX PHY.
Definition: hci.h:1051
hciStatus_t HCI_LE_RemoveDeviceFromResolvingListCmd(uint8 peerIdAddrType, uint8 *peerIdAddr)
hciStatus_t HCI_LE_RemoveWhiteListCmd(uint8 addrType, uint8 *devAddr)
uint8 numDataPkts
number of data packets
Definition: hci.h:1090
hciStatus_t HCI_EXT_EnhancedModemTestRxCmd(uint8 rfPhy, uint8 rfChan)
uint16 pktLen
packet length
Definition: hci.h:1116
osal_event_hdr_t hdr
osal event header
Definition: hci.h:1079
uint8 peerAddrType
peer address type
Definition: hci.h:857
osal_event_hdr_t hdr
osal event header
Definition: hci.h:995
hciStatus_t HCI_EXT_ConnEventNoticeCmd(uint16 connHandle, uint8 taskID, uint16 taskEvent)
uint16 cmdOpcode
command opcode
Definition: hci.h:988
uint8 reason
reason
Definition: hci.h:1014
uint8 numHciCmdPkt
number of HCI Command Packet
Definition: hci.h:978
osal_event_hdr_t hdr
osal event header
Definition: hci.h:1034
uint8 hardwareCode
hardware error code
Definition: hci.h:1005
#define B_ADDR_LEN
Default Public and Random Address Length.
Definition: bcomdef.h:115
Data Buffer Overflow Event.
Definition: hci.h:1018
uint8 role
role of connection
Definition: hci.h:872
LE Connection Complete Event.
Definition: hci.h:850
uint8 numHciCmdPkt
number of HCI command packets
Definition: hci.h:997
uint16 encryptedDiversifier
encrypted diversifier
Definition: hci.h:962
hciStatus_t HCI_LE_AddDeviceToResolvingListCmd(uint8 peerIdAddrType, uint8 *peerIdAddr, uint8 *peerIRK, uint8 *localIRK)
LE Read Remote Used Features Complete Event.
Definition: hci.h:936
uint8 peerAddrType
peer address type
Definition: hci.h:917
hciStatus_t HCI_ReadLocalSupportedFeaturesCmd(void)
hciStatus_t HCI_LE_ReadChannelMapCmd(uint16 connHandle)
uint16 connHandle
connection handle
Definition: hci.h:1098
uint8 status
status of event
Definition: hci.h:1088
hciStatus_t HCI_LE_ClearWhiteListCmd(void)
osal_event_hdr_t hdr
osal event header
Definition: hci.h:977
hciStatus_t HCI_LE_ReadMaxDataLenCmd(void)
hciStatus_t HCI_EXT_SetSCACmd(uint16 scaInPPM)
uint16 maxTxOctets
maximum transmission bytes
Definition: hci.h:1061
hciStatus_t HCI_ReadBDADDRCmd(void)
osal_event_hdr_t hdr
osal event header
Definition: hci.h:1047
hciStatus_t HCI_HostNumCompletedPktCmd(uint8 numHandles, uint16 *connHandles, uint16 *numCompletedPkts)
hciStatus_t HCI_ReadAuthPayloadTimeoutCmd(uint16 connHandle, uint16 *aptoValue)
LE Connection Complete Event.
Definition: hci.h:885
LE Connection Update Complete Event.
Definition: hci.h:924
uint8 BLEEventCode
BLE Event Code.
Definition: hci.h:1097
hciStatus_t HCI_EXT_SetTxPowerCmd(uint8 txPower)
uint8 status
status of event
Definition: hci.h:870
hciStatus_t HCI_LE_WriteSuggestedDefaultDataLenCmd(uint16 txOctets, uint16 txTime)
LE Read P256 Public Key Complete Event.
Definition: hci.h:1068
uint8 dataLen
length of report data
Definition: hci.h:897
uint8 * pData
data
Definition: hci.h:1106
LE Advertising Packet Report Event.
Definition: hci.h:903
hciStatus_t HCI_EXT_DisconnectImmedCmd(uint16 connHandle)
uint16 connHandle
connection handle
Definition: hci.h:1013
uint8 BLEEventCode
BLE Event Code.
Definition: hci.h:939
hciStatus_t HCI_LE_WriteRfPathCompCmd(int16 txPathParam, int16 rxPathParam)
uint8 pbFlag
flag
Definition: hci.h:1115
uint16 maxRxOctets
maximum receive bytes
Definition: hci.h:1063
uint8 role
role of connection
Definition: hci.h:856
hciStatus_t HCI_ResetCmd(void)
osal_event_hdr_t hdr
osal event header
Definition: hci.h:1020
hciStatus_t HCI_LE_SetPrivacyModeCmd(uint8 peerIdAddrType, uint8 *peerIdAddr, uint8 privacyMode)
uint16 connectionHandle
connection handle
Definition: hci.h:929
LE Long Term Key Requested Event.
Definition: hci.h:956
osal_event_hdr_t hdr
osal event header
Definition: hci.h:905
uint16 connHandle
connection handle
Definition: hci.h:960