BLE-Stack 3.00.00 to BLE-Stack 3.00.01

This section will describe a way to migrate a project from BLE-Stack 3.00.00 to a BLE-Stack 3.00.01 project.

For this migration guide, simple_peripheral from BLE-Stack 3.00.00 will be ported over to BLE-Stack 3.00.01. Because the directory structure is nearly identical between the two releases, the recommended approach is to start with a BLE-Stack 3.00.01 project that contains the same base functionality as the porting target project and merge in any custom functionality.

  1. Choose a BLE-Stack 3.00.01 example project that contains your target project’s base functionality.

    For reference, see available sample projects that start with simple_

    In this example, we’re going to use simple_peripheral as the starting BLE-Stack 3.00.01 sample project.

  2. Transfer all modified application files from BLE-Stack 3.00.00 into the BLE-Stack 3.00.01 example project.

    In this example, the following files from BLE-Stack 3.00.00 were moved into simple_peripheral BLE-Stack 3.00.01 example:

    • simple_peripheral.c
    • simple_peripheral.h
    • simple_gatt_profile.c
    • simple_gatt_profile.h

    Modify main.c in the BLE-Stack 3.00.01 example if additional tasks were added in the BLE-Stack 3.00.00 project.

    Attention

    For applications using Directed Advertisements comment out #define GBM_GATT_NO_CLIENT in gapbondmgr.c of BLE-Stack 3.00.00 project to remain compliant with the Bluetooth Core Specification Version 5.1.

    1
    2
    3
    4
    5
    #ifdef GATT_NO_CLIENT
    #ifndef GBM_GATT_NO_CLIENT
    //#define GBM_GATT_NO_CLIENT // <-- Comment this out
    #endif // !GBM_GATT_NO_CLIENT
    #endif // GATT_NO_CLIENT
    

    See Directed Advertisements as GATT Server for more information.

  3. If necessary, update the project to use the newer TI-RTOS drivers that are supplied with the SimpleLink CC2640R2 SDK.

    The following drivers have changed from BLE-Stack 3.00.00. Please see the changes to these drivers by comparing the supplied headers between those in simplelink_cc2640r2_sdk_1_00_00_2 and those in the SimpleLink CC2640R2 SDK.

    • ADCCC26XX.h
    • RF.h

    Also, refer to the Upgrade and Compatibility Information for additional information and the TI-RTOS examples included with SimpleLink CC2640R2 SDK.

    For additional information on how BLE-Stack 3.00.01 uses TI-RTOS see TI-RTOS (RTOS Kernel) Overview

    For any utilized TI Drivers, review TI-RTOS Kernel Users Guide and Driver APIs.