![]() |
![]() |
|
TI BLE-Stack for Bluetooth API Documentation
3.03.01.00
|
GAPBondMgr layer interface.
Go to the source code of this file.
Data Structures | |
| struct | gapBondEccKeys_t |
| Public and Private ECC Keys. More... | |
| struct | gapBondOobSC_t |
| Secure Connections Out of Band. More... | |
Macros | |
| #define | ECC_KEYLEN 32 |
| 256 bit keys | |
| #define | GAP_BONDINGS_MAX 10 |
| Maximum number of bonds that can be saved in NV. | |
| #define | GAP_CHAR_CFG_MAX 4 |
| Maximum number of characteristic configuration that can be saved in NV. | |
| #define | GAPBOND_AUTO_SYNC_WL 0x40D |
| Synchronize the whitelist with bonded devices (Read/Write) More... | |
| #define | GAPBOND_BOND_COUNT 0x40E |
| Gets the total number of bonds stored in NV (Read-only) More... | |
| #define | GAPBOND_BOND_FAIL_ACTION 0x40F |
| The action that the device takes after an unsuccessful bonding attempt (Write-only) More... | |
| #define | GAPBOND_BONDING_ENABLED 0x406 |
| Whether to request bonding during pairing (Read/Write) More... | |
| #define | GAPBOND_DEFAULT_PASSCODE 0x408 |
| This parameter is only used by the Host Test app Application (network processor) The Id of this parameter is used to store the password locally. the GAP Bond manager is not storing any default password anymore, everytime a password is needed, pfnPasscodeCB_t will be call. More... | |
| #define | GAPBOND_ECC_KEYS 0x413 |
| The private and public keys to use for Secure Connections pairing (Read/Write) More... | |
| #define | GAPBOND_ECCKEY_REGEN_POLICY 0x412 |
| ECC Key Regeneration Policy (Read/Write) More... | |
| #define | GAPBOND_ERASE_ALLBONDS 0x409 |
| Erase all bonds from SNV and remove all bonded devices (Write) More... | |
| #define | GAPBOND_ERASE_SINGLEBOND 0x410 |
| Erase a single bonded device (Write-only) More... | |
| #define | GAPBOND_FAIL_INITIATE_PAIRING 0x01 |
| Initiate pairing upon unsuccessful bonding. | |
| #define | GAPBOND_FAIL_NO_ACTION 0x00 |
| Take no action upon unsuccessful bonding. | |
| #define | GAPBOND_FAIL_TERMINATE_ERASE_BONDS 0x03 |
| Terminate link and erase all existing bonds on device upon unsuccessful bonding. | |
| #define | GAPBOND_FAIL_TERMINATE_LINK 0x02 |
| Terminate link upon unsuccessful bonding. | |
| #define | GAPBOND_INITIATE_WAIT 0x401 |
| The amount of time (in ms) to wait for a pairing request before sending the slave initiate request (Read/Write) More... | |
| #define | GAPBOND_IO_CAP_DISPLAY_ONLY 0x00 |
| Display Only Device. | |
| #define | GAPBOND_IO_CAP_DISPLAY_YES_NO 0x01 |
| Display and Yes and No Capable. | |
| #define | GAPBOND_IO_CAP_KEYBOARD_DISPLAY 0x04 |
| Both Keyboard and Display Capable. | |
| #define | GAPBOND_IO_CAP_KEYBOARD_ONLY 0x02 |
| Keyboard Only. | |
| #define | GAPBOND_IO_CAP_NO_INPUT_NO_OUTPUT 0x03 |
| No Display or Input Device. | |
| #define | GAPBOND_IO_CAPABILITIES 0x403 |
| The I/O capabilities of the local device (Read/Write) More... | |
| #define | GAPBOND_KEY_DIST_LIST 0x407 |
| Key distribution list for pairing (Read/Write) More... | |
| #define | GAPBOND_KEYDIST_MENCKEY 0x10 |
| Master Encrypton Key. | |
| #define | GAPBOND_KEYDIST_MIDKEY 0x20 |
| Master IRK and ID information. | |
| #define | GAPBOND_KEYDIST_MLINK 0x80 |
| Master Link Key. | |
| #define | GAPBOND_KEYDIST_MSIGN 0x40 |
| Master CSRK. | |
| #define | GAPBOND_KEYDIST_SENCKEY 0x01 |
| Slave Encryption Key. | |
| #define | GAPBOND_KEYDIST_SIDKEY 0x02 |
| Slave IRK and ID information. | |
| #define | GAPBOND_KEYDIST_SLINK 0x08 |
| Slave Link Key. | |
| #define | GAPBOND_KEYDIST_SSIGN 0x04 |
| Slave CSRK. | |
| #define | GAPBOND_KEYSIZE 0x40C |
| Key Size used in pairing. (Read/Write) More... | |
| #define | GAPBOND_LOCAL_OOB_SC_DATA 0x417 |
| Local OOB Secure Connections Data (Read/Write) More... | |
| #define | GAPBOND_LOCAL_OOB_SC_ENABLED 0x416 |
| Validate Local OOB Secure Connections Data (Read/Write) More... | |
| #define | GAPBOND_LRU_BOND_REPLACEMENT 0x418 |
| Enable / Disable LRU Bond Replacement Scheme (Read/Write) More... | |
| #define | GAPBOND_MITM_PROTECTION 0x402 |
| Whether to use authenticated pairing (Read/Write) More... | |
| #define | GAPBOND_OOB_DATA 0x405 |
| OOB data to use for pairing (Read/Write) More... | |
| #define | GAPBOND_OOB_ENABLED 0x404 |
| Whether to use OOB for pairing (Read/Write) More... | |
| #define | GAPBOND_PAIRING_MODE 0x400 |
| Whether to allow pairing, and if so, whether to initiate pairing. (Read/Write) More... | |
| #define | GAPBOND_PAIRING_MODE_INITIATE 0x02 |
| Don't wait, initiate a pairing request or slave security request. | |
| #define | GAPBOND_PAIRING_MODE_NO_PAIRING 0x00 |
| Pairing is not allowed. | |
| #define | GAPBOND_PAIRING_MODE_WAIT_FOR_REQ 0x01 |
| Wait for a pairing request or slave security request. | |
| #define | GAPBOND_PAIRING_STATE_BOND_SAVED 0x03 |
| Bonding record saved in NV. | |
| #define | GAPBOND_PAIRING_STATE_BONDED 0x02 |
| Bonding Complete. More... | |
| #define | GAPBOND_PAIRING_STATE_CAR_READ 0x04 |
| Central Address Resolution Characteristic Read. | |
| #define | GAPBOND_PAIRING_STATE_COMPLETE 0x01 |
| Pairing Complete. More... | |
| #define | GAPBOND_PAIRING_STATE_STARTED 0x00 |
| Pairing Started. More... | |
| #define | GAPBOND_REGENERATE_ALWAYS 0x00 |
| Regenerate after each usage. | |
| #define | GAPBOND_REGENERATE_NEVER 0xFF |
| Never regenerate, always use the same pair. | |
| #define | GAPBOND_REMOTE_OOB_SC_DATA 0x415 |
| Remote OOB Secure Connections Data (Read/Write) More... | |
| #define | GAPBOND_REMOTE_OOB_SC_ENABLED 0x414 |
| Validate Remote OOB Secure Connections Data (Read/Write) More... | |
| #define | GAPBOND_SECURE_CONNECTION 0x411 |
| Define Secure Connections Usage during Pairing (Read/Write) More... | |
| #define | GAPBOND_SECURE_CONNECTION_ALLOW 0x01 |
| Secure Connections are supported. | |
| #define | GAPBOND_SECURE_CONNECTION_NONE 0x00 |
| Secure Connections not supported. | |
| #define | GAPBOND_SECURE_CONNECTION_ONLY 0x02 |
| Secure Connections Only Mode. | |
| #define | SMP_PAIRING_FAILED_AUTH_REQ 0x03 |
| The pairing procedure can't be performed as authentication requirements can't be met due to IO capabilities of one or both devices. | |
| #define | SMP_PAIRING_FAILED_CMD_NOT_SUPPORTED 0x07 |
| The SMP command received is not supported on this device. | |
| #define | SMP_PAIRING_FAILED_CONFIRM_VALUE 0x04 |
| The confirm value doesn't match the calculated compare value. | |
| #define | SMP_PAIRING_FAILED_DHKEY_CHECK_FAILED 0x0B |
| Indicates to the remote device that the DHKey Check value received does not match the one calculated by the local device. | |
| #define | SMP_PAIRING_FAILED_ENC_KEY_SIZE 0x06 |
| The resultant encryption key size is insufficient for the security requirements of this device. | |
| #define | SMP_PAIRING_FAILED_INVALID_PARAMETERS 0x0A |
| Indicates that the command length is invalid or that a parameter is outside of the specified range. | |
| #define | SMP_PAIRING_FAILED_NOT_SUPPORTED 0x05 |
| Pairing isn't supported by the device. | |
| #define | SMP_PAIRING_FAILED_NUM_COMPARISON_FAILED 0x0C |
| Indicates that the confirm value in the numeric comparison protocol do not match. | |
| #define | SMP_PAIRING_FAILED_OOB_NOT_AVAIL 0x02 |
| The OOB data is not available. | |
| #define | SMP_PAIRING_FAILED_PASSKEY_ENTRY_FAILED 0x01 |
| The user input of the passkey failed, for example, the user cancelled the operation. | |
| #define | SMP_PAIRING_FAILED_REPEATED_ATTEMPTS 0x09 |
| Pairing or authentication procedure is disallowed because too little time has elapsed since the last pairing request or security request. | |
| #define | SMP_PAIRING_FAILED_UNSPECIFIED 0x08 |
| Pairing failed due to an unspecified reason. | |
Typedefs | |
| typedef void(* | pfnPairStateCB_t) (uint16_t connectionHandle, uint8_t state, uint8_t status) |
| Pairing State Callback Function. More... | |
| typedef void(* | pfnPasscodeCB_t) (uint8_t *deviceAddr, uint16_t connectionHandle, uint8_t uiInputs, uint8_t uiOutputs, uint32_t numComparison) |
| Passcode and Numeric Comparison Callback Function. More... | |
Functions | |
| uint8_t | GAPBondMgr_CheckNVLen (uint8_t id, uint8_t len) |
| This function will check the length of a Bond Manager NV Item. More... | |
| bStatus_t | GAPBondMgr_GetParameter (uint16_t param, void *pValue) |
| Get a GAP Bond Manager parameter. More... | |
| bStatus_t | GAPBondMgr_LinkEst (uint8_t addrType, uint8_t *pDevAddr, uint16_t connHandle, uint8_t role) |
| Notify the Bond Manager that a connection has been made. More... | |
| void | GAPBondMgr_LinkTerm (uint16_t connHandle) |
| Notify the Bond Manager that a connection has been terminated. More... | |
| bStatus_t | GAPBondMgr_PasscodeRsp (uint16_t connectionHandle, uint8_t status, uint32_t passcode) |
| Respond to a passcode request. More... | |
| uint8_t | GAPBondMgr_ProcessGAPMsg (gapEventHdr_t *pMsg) |
| This is a bypass mechanism to allow the bond manager to process GAP messages. More... | |
| bStatus_t | GAPBondMgr_ReadCentAddrResChar (uint16_t connectionHandle) |
| Read Central Address Resolution Characteristic. More... | |
| void | GAPBondMgr_Register (gapBondCBs_t *pCB) |
| Register callback functions with the bond manager. More... | |
| uint8_t | GAPBondMgr_ResolveAddr (uint8_t addrType, uint8_t *pDevAddr, uint8_t *pResolvedAddr) |
| Resolve an address from bonding information. More... | |
| bStatus_t | GAPBondMgr_ServiceChangeInd (uint16_t connectionHandle, uint8_t setParam) |
| Set/clear the service change indication in a bond record. More... | |
| bStatus_t | GAPBondMgr_SetParameter (uint16_t param, uint8_t len, void *pValue) |
| Set a GAP Bond Manager parameter. More... | |
| void | GAPBondMgr_SlaveReqSecurity (uint16_t connHandle, uint8_t authReq) |
| Notify the Bond Manager that a Slave Security Request is received. More... | |
| uint8_t | GAPBondMgr_SupportsEnhancedPriv (uint8_t *pPeerIdAddr) |
| Determine if peer device supports enhanced privacy by checking the Enhanced Privacy state flag of the bond record that corresponds to the peer's identity address. More... | |
| bStatus_t | GAPBondMgr_syncResolvingList (void) |
| This function will add all device address and IRK pairs from bond records to the Controller. Used with PRIVACY_1_2_CFG. More... | |
| bStatus_t | GAPBondMgr_UpdateCharCfg (uint16_t connectionHandle, uint16_t attrHandle, uint16_t value) |
| Update the Characteristic Configuration in a bond record. More... | |