603 #ifndef ti_drivers_spi_SPICC26XXDMA__include 604 #define ti_drivers_spi_SPICC26XXDMA__include 617 #include <ti/drivers/dpl/HwiP.h> 618 #include <ti/drivers/dpl/SemaphoreP.h> 619 #include <ti/drivers/dpl/SwiP.h> 652 #define SPICC26XXDMA_CMD_RETURN_PARTIAL_ENABLE (SPI_CMD_RESERVED + 0) 661 #define SPICC26XXDMA_CMD_RETURN_PARTIAL_DISABLE (SPI_CMD_RESERVED + 1) 669 #define SPICC26XXDMA_CMD_SET_CSN_PIN (SPI_CMD_RESERVED + 2) 673 #define SPICC26XXDMA_RETURN_PARTIAL_ENABLE SPICC26XXDMA_CMD_RETURN_PARTIAL_ENABLE 674 #define SPICC26XXDMA_RETURN_PARTIAL_DISABLE SPICC26XXDMA_CMD_RETURN_PARTIAL_DISABLE 675 #define SPICC26XXDMA_SET_CSN_PIN SPICC26XXDMA_CMD_SET_CSN_PIN Definition: SPICC26XXDMA.h:695
uint8_t PIN_Id
Pin identifier data type.
Definition: PIN.h:577
PIN_Id csnPin
Definition: SPICC26XXDMA.h:832
const SPI_FxnTable SPICC26XXDMA_fxnTable
uint16_t defaultTxBufValue
Definition: SPICC26XXDMA.h:781
uint32_t baseAddr
Definition: SPICC26XXDMA.h:755
void(* SPI_CallbackFxn)(SPI_Handle handle, SPI_Transaction *transaction)
The definition of a callback function used by the SPI driver when used in SPI_MODE_CALLBACK.
Definition: SPI.h:569
enum SPI_Mode_ SPI_Mode
Definitions for various SPI modes of operation.
Power_NotifyObj spiPostObj
Definition: SPICC26XXDMA.h:851
unsigned int bitRate
SPI bit rate in Hz.
Definition: SPICC26XXDMA.h:816
A SPI_Transaction data structure is used with SPI_transfer(). It indicates how many SPI_FrameFormat f...
Definition: SPI.h:548
SPI_CallbackFxn transferCallbackFxn
Definition: SPICC26XXDMA.h:808
struct SPICC26XXDMA_Object * SPICC26XXDMA_Handle
uint32_t minDmaTransferSize
Definition: SPICC26XXDMA.h:796
uint8_t intPriority
SPI CC26XXDMA Peripheral's interrupt priority.
Definition: SPICC26XXDMA.h:771
uint32_t rxChannelBitMask
Definition: SPICC26XXDMA.h:783
void * spiPreFxn
Definition: SPICC26XXDMA.h:848
UDMACC26XX Global configuration.
Definition: UDMACC26XX.h:231
uint32_t txChannelBitMask
Definition: SPICC26XXDMA.h:785
uint16_t scratchBuf
Definition: SPICC26XXDMA.h:845
Power manager interface for CC26XX/CC13XX.
Power notify object structure.
Definition: Power.h:121
PIN_Id clkPin
Definition: SPICC26XXDMA.h:791
SPICC26XXDMA Hardware attributes.
Definition: SPICC26XXDMA.h:753
volatile bool spiPowerConstraint
Definition: SPICC26XXDMA.h:853
PIN_Id misoPin
Definition: SPICC26XXDMA.h:789
SPI_TransferMode transferMode
Definition: SPICC26XXDMA.h:806
SPICC26XXDMA Object.
Definition: SPICC26XXDMA.h:804
enum SPI_TransferMode_ SPI_TransferMode
SPI transfer mode determines the whether the SPI controller operates synchronously or asynchronously...
Device-specific pin & GPIO driver for CC26xx family [def].
The definition of a SPI function table that contains the required set of functions to control a speci...
Definition: SPI.h:683
void * spiPostFxn
Definition: SPICC26XXDMA.h:849
PIN_State pinState
Definition: SPICC26XXDMA.h:835
SPI_Mode mode
Definition: SPICC26XXDMA.h:809
SPICC26XXDMA_FrameSize
Definition: SPICC26XXDMA.h:694
SPICC26XXDMA_FrameSize frameSize
Definition: SPICC26XXDMA.h:829
UDMACC26XX driver implementation.
bool returnPartial
Definition: SPICC26XXDMA.h:842
struct SPICC26XXDMA_Object SPICC26XXDMA_Object
SPICC26XXDMA Object.
struct SPICC26XXDMA_HWAttrsV1 SPICC26XXDMA_HWAttrsV1
SPICC26XXDMA Hardware attributes.
PIN_Id csnPin
Definition: SPICC26XXDMA.h:793
UDMACC26XX_Handle udmaHandle
Definition: SPICC26XXDMA.h:839
uint8_t intNum
Definition: SPICC26XXDMA.h:757
PIN_Id mosiPin
Definition: SPICC26XXDMA.h:787
unsigned int transferTimeout
Definition: SPICC26XXDMA.h:807
underlying data structure for type PIN_State
Definition: PIN.h:707
enum SPI_FrameFormat_ SPI_FrameFormat
Definitions for various SPI data frame formats.
HwiP_Struct hwi
Definition: SPICC26XXDMA.h:821
SPI_FrameFormat frameFormat
Definition: SPICC26XXDMA.h:818
Power_NotifyObj spiPreObj
Definition: SPICC26XXDMA.h:850
SemaphoreP_Struct transferComplete
Definition: SPICC26XXDMA.h:823
SwiP_Struct swi
Definition: SPICC26XXDMA.h:822
size_t amtDataXferred
Definition: SPICC26XXDMA.h:827
bool isOpen
Definition: SPICC26XXDMA.h:855
uint32_t swiPriority
SPI SWI priority. The higher the number, the higher the priority. The minimum is 0 and the maximum is...
Definition: SPICC26XXDMA.h:777
Definition: SPICC26XXDMA.h:696
PowerCC26XX_Resource powerMngrId
Definition: SPICC26XXDMA.h:779
size_t currentXferAmt
Definition: SPICC26XXDMA.h:828
PIN_Handle pinHandle
Definition: SPICC26XXDMA.h:836
unsigned int dataSize
Definition: SPICC26XXDMA.h:817
SPI_Transaction * currentTransaction
Definition: SPICC26XXDMA.h:826