125 #ifndef ti_drivers_pwm__PWMTimerCC26XX_include 126 #define ti_drivers_pwm__PWMTimerCC26XX_include 148 #define PWMTimerCC26XX_CMD_DEBUG_STALL PWM_CMD_RESERVED + 0 153 #define CMD_ARG_DEBUG_STALL_OFF (uint32_t)GPTimerCC26XX_DEBUG_STALL_OFF 154 #define CMD_ARG_DEBUG_STALL_ON (uint32_t)GPTimerCC26XX_DEBUG_STALL_ON uint8_t PIN_Id
Pin identifier data type.
Definition: PIN.h:577
PWM_IdleLevel idleLevel
Definition: PWMTimerCC26XX.h:212
bool isOpen
Definition: PWMTimerCC26XX.h:204
GPTimer driver implementation for CC26XX/CC13XX.
PWM_Period_Units periodUnit
Definition: PWMTimerCC26XX.h:206
PWMTimer26XX Object.
Definition: PWMTimerCC26XX.h:202
bool isRunning
Definition: PWMTimerCC26XX.h:205
uint32_t periodCounts
Definition: PWMTimerCC26XX.h:208
uint32_t dutyValue
Definition: PWMTimerCC26XX.h:210
PWMTimer26XX Hardware attributes.
Definition: PWMTimerCC26XX.h:182
struct PWMTimerCC26XX_Object PWMTimerCC26XX_Object
PWMTimer26XX Object.
The definition of a PWM function table that contains the required set of functions to control a speci...
Definition: PWM.h:442
uint32_t periodValue
Definition: PWMTimerCC26XX.h:207
enum PWM_Period_Units_ PWM_Period_Units
PWM period unit definitions. Refer to device specific implementation if using PWM_PERIOD_COUNTS (raw ...
struct PWMTimerCC26XX_HwAttrs PWMTimerCC26XX_HwAttrs
PWMTimer26XX Hardware attributes.
uint8_t gpTimerUnit
Definition: PWMTimerCC26XX.h:185
GPTimerCC26XX_Handle hTimer
Definition: PWMTimerCC26XX.h:213
PWM_Duty_Units dutyUnit
Definition: PWMTimerCC26XX.h:209
GPTimer Global configuration.
Definition: GPTimerCC26XX.h:406
PIN_Id pwmPin
Definition: PWMTimerCC26XX.h:184
const PWM_FxnTable PWMTimerCC26XX_fxnTable
enum PWM_IdleLevel_ PWM_IdleLevel
Idle output level when PWM is not running (stopped / not started).
uint32_t dutyCounts
Definition: PWMTimerCC26XX.h:211
Generic PIN & GPIO driver.
enum PWM_Duty_Units_ PWM_Duty_Units
PWM duty cycle unit definitions. Refer to device specific implementation if using PWM_DUTY_COUNTS (ra...