NVSCC26XX.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2015-2018, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 /*!*****************************************************************************
33  * @file NVSCC26XX.h
34  * @brief Non-Volatile Storage driver for CC13XX/CC26XX devices.
35  *
36  * ## Interrupt Latency During Flash Operations #
37  *
38  * When writing or erasing flash, interrupts must be disabled to avoid
39  * executing code in flash while the flash is being reprogrammed. This
40  * constraint is handled by the driver. Application code does not need
41  * to safeguard against this.
42  *
43  * Additionally, to avoid extremely large interrupt latencies that would be
44  * incurred if entire blocks were written with interrupts disabled, block
45  * writes to flash are broken into multiple smaller sizes.
46  *
47  * Even with this scheme in place, latencies of roughly 64 microseconds will
48  * be incurred while flash is being written to.
49  *
50  * A similar caveat applies to flash erase operations. Erasing an entire
51  * flash sector (the minimal amount that can be erased at a time) can take
52  * roughly 8 milliseconds. This entire operation must be performed with
53  * interrupts disabled. Here again, this requirement is met internally
54  * by the driver and flash region erases are performed one sector at a
55  * time to minimize this significant latency impact.
56  *
57  * Care must be taken by the user to not perform flash write or erase
58  * operations during latency critical phases of an application. See the
59  * NVS_lock() and NVS_unlock() API descriptions for more information.
60  *
61  * ## Maximum flash writes before erase #
62  *
63  * On CC13XX & CC26XX memory rows can be 128 or 256 bytes in length; refer to
64  * the device datasheet for the exact size. A maximum of 83 write operations
65  * can be performed on a memory row. Once the limit is reached, the row must
66  * be erased before it is written to again.
67  *
68  * \note The 83 write limit persists through device reset & power cycles.
69  * If 60 write operations were performed on a memory page & the device is
70  * reset; the page can still only be written to 23 more times before it must
71  * be erased.
72  *
73  * A write "Scoreboard" can be enabled in this driver; the scoreboard keeps
74  * track of how many times a page has been written to. It is provided as a
75  * debug tool to ensure the 83 write limit is not exceeded. If a page is
76  * written to more than 83 times, the NVSCC26XX driver will spin forever.
77  * Each byte in the scoreboard corresponds to a memory page in the NVS region.
78  * The byte is incremented when the memory is written to & set to 0 when
79  * erased.
80  *
81  * To enable the "scoreboard" the "NVSCC26XX_INSTRUMENTED" symbol must be
82  * defined when the driver is compiled. Three new fields are added to the
83  * #NVSCC26XX_HWAttrs structure:
84  * * scoreboard - a buffer provided by the application where each byte
85  * represents how many times a page has been written to.
86  * * scoreboardSize - number of bytes in the scoreboard.
87  * *flashPageSize - number of bytes in a flash page (i.e. 128 or 256)
88  *
89  * When configured correctly, the scoreboard can be viewed in a memory browser.
90  *
91  * \note The scoreboard will only keep track of writes to flash within a
92  * NVS region using a NVS driver. Writes performed outside the NVS
93  * region or without the NVS driver are untracked.
94  *
95  * \note The scoreboard is in RAM & will be lost on reset or power cycle.
96  *
97  *
98  * ============================================================================
99  */
100 
101 #ifndef ti_drivers_nvs_NVSCC26XX__include
102 #define ti_drivers_nvs_NVSCC26XX__include
103 
104 #include <stdint.h>
105 #include <stdbool.h>
106 
107 #if defined (__cplusplus)
108 extern "C" {
109 #endif
110 
117 #define NVSCC26XX_STATUS_LOW_VOLTAGE (NVS_STATUS_RESERVED - 1)
118 
151 extern const NVS_FxnTable NVSCC26XX_fxnTable;
152 
293 typedef struct NVSCC26XX_HWAttrs {
294  void *regionBase;
301  size_t regionSize;
312 #if defined(NVSCC26XX_INSTRUMENTED)
313  uint8_t *scoreboard;
314  size_t scoreboardSize;
315  uint32_t flashPageSize;
316 #endif
318 
319 /*
320  * @brief NVSCC26XX Object
321  *
322  * The application must not access any member variables of this structure!
323  */
324 typedef struct NVSCC26XX_Object {
325  bool opened; /* Has this region been opened */
327 
333 extern void NVSCC26XX_close(NVS_Handle handle);
334 extern int_fast16_t NVSCC26XX_control(NVS_Handle handle, uint_fast16_t cmd,
335  uintptr_t arg);
336 extern int_fast16_t NVSCC26XX_erase(NVS_Handle handle, size_t offset,
337  size_t size);
338 extern void NVSCC26XX_getAttrs(NVS_Handle handle, NVS_Attrs *attrs);
339 extern void NVSCC26XX_init();
340 extern int_fast16_t NVSCC26XX_lock(NVS_Handle handle, uint32_t timeout);
341 extern NVS_Handle NVSCC26XX_open(uint_least8_t index, NVS_Params *params);
342 extern int_fast16_t NVSCC26XX_read(NVS_Handle handle, size_t offset,
343  void *buffer, size_t bufferSize);
344 extern void NVSCC26XX_unlock(NVS_Handle handle);
345 extern int_fast16_t NVSCC26XX_write(NVS_Handle handle, size_t offset,
346  void *buffer, size_t bufferSize, uint_fast16_t flags);
349 #if defined (__cplusplus)
350 }
351 #endif /* defined (__cplusplus) */
352 
354 #endif /* ti_drivers_nvs_NVSCC26XX__include */
NVS attributes.
Definition: NVS.h:417
const NVS_FxnTable NVSCC26XX_fxnTable
void * regionBase
Definition: NVSCC26XX.h:294
struct NVSCC26XX_HWAttrs NVSCC26XX_HWAttrs
NVSCC26XX hardware attributes.
NVS Parameters.
Definition: NVS.h:406
struct NVSCC26XX_Object NVSCC26XX_Object
bool opened
Definition: NVSCC26XX.h:325
Definition: NVSCC26XX.h:324
size_t regionSize
Definition: NVSCC26XX.h:301
NVSCC26XX hardware attributes.
Definition: NVSCC26XX.h:293
NVS Global configuration.
Definition: NVS.h:545
The definition of an NVS function table that contains the required set of functions to control a spec...
Definition: NVS.h:502
© Copyright 1995-2018, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale