269 #ifndef ti_drivers_adc_adcbufcc26xx__include 270 #define ti_drivers_adc_adcbufcc26xx__include 287 #include <ti/devices/DeviceFamily.h> 288 #include DeviceFamily_constructPath(driverlib/aux_adc.h) 290 #include <ti/drivers/dpl/HwiP.h> 291 #include <ti/drivers/dpl/ClockP.h> 292 #include <ti/drivers/dpl/SemaphoreP.h> 293 #include <ti/drivers/dpl/SwiP.h> 322 #define ADCBufCC26XX_CMD_ACQUIRE_ADC_SEMAPHORE ADCBuf_CMD_RESERVED + 1 337 #define ADCBufCC26XX_CMD_KEEP_ADC_SEMAPHORE ADCBuf_CMD_RESERVED + 2 346 #define ADCBufCC26XX_CMD_KEEP_ADC_SEMAPHORE_DISABLE ADCBuf_CMD_RESERVED + 3 353 #define ADCBufCC26XX_CMD_RELEASE_ADC_SEMAPHORE ADCBuf_CMD_RESERVED + 4 360 #define ADCBufCC26XX_RESOLUTION 12 362 #define ADCBufCC26XX_BYTES_PER_SAMPLE 2 ADCBufCC26XX_Sampling_Mode
Specifies whether the internal reference of the ADC is sourced from the battery voltage or a fixed in...
Definition: ADCBufCC26XX.h:390
Definition: ADCBufCC26XX.h:391
Definition: ADCBufCC26XX.h:442
Definition: ADCBufCC26XX.h:404
GPTimerCC26XX_Handle timerHandle
Definition: ADCBufCC26XX.h:579
GPTimer driver implementation for CC26XX/CC13XX.
enum ADCBuf_Recurrence_Mode_ ADCBuf_Recurrence_Mode
ADC trigger mode settings.
ADCBufCC26XX_Reference_Source refSource
Definition: ADCBufCC26XX.h:477
struct ADCBufCC26XX_Object * ADCBufCC26XX_Handle
bool inputScalingEnabled
Definition: ADCBufCC26XX.h:493
bool adcSemaphoreInPossession
Definition: ADCBufCC26XX.h:554
Definition: ADCBufCC26XX.h:408
bool isOpen
Definition: ADCBufCC26XX.h:550
ADCBufCC26XX Hardware Attributes.
Definition: ADCBufCC26XX.h:516
An ADCBuf_Conversion data structure is used with ADCBuf_convert(). It indicates which channel to perf...
Definition: ADCBuf.h:237
ADCBuf_Return_Mode returnMode
Definition: ADCBufCC26XX.h:561
Definition: ADCBufCC26XX.h:415
Definition: ADCBufCC26XX.h:412
enum ADCBuf_Return_Mode_ ADCBuf_Return_Mode
ADC return mode settings.
ADCBufCC26XX_Sampling_Mode samplingMode
Definition: ADCBufCC26XX.h:475
uint32_t swiPriority
ADC SWI priority. The higher the number, the higher the priority. The minimum is 0 and the maximum is...
Definition: ADCBufCC26XX.h:522
UDMACC26XX Global configuration.
Definition: UDMACC26XX.h:231
Power manager interface for CC26XX/CC13XX.
uint32_t semaphoreTimeout
Definition: ADCBufCC26XX.h:581
CC26XX specfic extension to ADCBuf_Params.
Definition: ADCBufCC26XX.h:471
PIN_Handle pinHandle
Definition: ADCBufCC26XX.h:573
Definition: ADCBufCC26XX.h:409
uint8_t intPriority
ADC peripheral's interrupt priority.
Definition: ADCBufCC26XX.h:536
ADCBufCC26XX_Reference_Source refSource
Definition: ADCBufCC26XX.h:556
Definition: ADCBufCC26XX.h:411
bool inputScalingEnabled
Definition: ADCBufCC26XX.h:552
Device-specific pin & GPIO driver for CC26xx family [def].
ADCBufCC26XX_Sampling_Duration samplingDuration
Definition: ADCBufCC26XX.h:473
Definition: ADCBufCC26XX.h:410
struct ADCBufCC26XX_Object ADCBufCC26XX_Object
ADCBufCC26XX Object.
bool keepADCSemaphore
Definition: ADCBufCC26XX.h:553
The definition of an ADCBuf function table that contains the required set of functions to control a s...
Definition: ADCBuf.h:385
ADCBufCC26XX_Sampling_Duration samplingDuration
Definition: ADCBufCC26XX.h:558
ADCBuf_Callback callbackFxn
Definition: ADCBufCC26XX.h:559
ADCBuf_Recurrence_Mode recurrenceMode
Definition: ADCBufCC26XX.h:560
Definition: ADCBufCC26XX.h:413
Definition: ADCBufCC26XX.h:416
Definition: ADCBufCC26XX.h:392
UDMACC26XX driver implementation.
Definition: ADCBufCC26XX.h:407
Definition: ADCBufCC26XX.h:441
struct ADCBufCC26XX_ParamsExtension ADCBufCC26XX_ParamsExtension
CC26XX specfic extension to ADCBuf_Params.
ADCBufCC26XX_Reference_Source
Specifies whether the internal reference of the ADC is sourced from the battery voltage or a fixed in...
Definition: ADCBufCC26XX.h:440
UDMACC26XX_Handle udmaHandle
Definition: ADCBufCC26XX.h:576
Definition: ADCBufCC26XX.h:405
bool conversionInProgress
Definition: ADCBufCC26XX.h:551
SemaphoreP_Struct conversionComplete
Definition: ADCBufCC26XX.h:567
uint8_t currentChannel
Definition: ADCBufCC26XX.h:555
struct ADCBufCC26XX_AdcChannelLutEntry ADCBufCC26XX_AdcChannelLutEntry
Table entry that maps a virtual adc channel to a dio and its corresponding internal analogue signal...
ADCBufCC26XX_AdcChannelLutEntry const * adcChannelLut
Definition: ADCBufCC26XX.h:538
GPTimer Global configuration.
Definition: GPTimerCC26XX.h:406
underlying data structure for type PIN_State
Definition: PIN.h:707
ADCBufCC26XX_Sampling_Mode samplingMode
Definition: ADCBufCC26XX.h:557
uint8_t dio
Definition: ADCBufCC26XX.h:460
PIN_State pinState
Definition: ADCBufCC26XX.h:572
ADCBuf_Conversion * currentConversion
Definition: ADCBufCC26XX.h:569
struct ADCBufCC26XX_HWAttrs ADCBufCC26XX_HWAttrs
ADCBufCC26XX Hardware Attributes.
SwiP_Struct swi
Definition: ADCBufCC26XX.h:566
uint32_t samplingFrequency
Definition: ADCBufCC26XX.h:582
void(* ADCBuf_Callback)(ADCBuf_Handle handle, ADCBuf_Conversion *conversion, void *completedADCBuffer, uint32_t completedChannel)
The definition of a callback function used by the ADC driver when used in ADCBuf_RETURN_MODE_CALLBACK...
Definition: ADCBuf.h:251
uint8_t compBInput
Definition: ADCBufCC26XX.h:461
Definition: ADCBufCC26XX.h:406
Definition: ADCBufCC26XX.h:414
ADCBufCC26XX Object.
Definition: ADCBufCC26XX.h:548
const ADCBuf_FxnTable ADCBufCC26XX_fxnTable
HwiP_Struct hwi
Definition: ADCBufCC26XX.h:565
Table entry that maps a virtual adc channel to a dio and its corresponding internal analogue signal...
Definition: ADCBufCC26XX.h:459
Generic PIN & GPIO driver.
uint16_t * activeSampleBuffer
Definition: ADCBufCC26XX.h:562
ADCBufCC26XX_Sampling_Duration
Amount of time the ADC spends sampling the analogue input.
Definition: ADCBufCC26XX.h:403