268 #ifndef ti_drivers_adc_adcbufcc26xx__include 269 #define ti_drivers_adc_adcbufcc26xx__include 286 #include <ti/devices/DeviceFamily.h> 287 #include DeviceFamily_constructPath(driverlib/aux_adc.h) 289 #include <ti/drivers/dpl/HwiP.h> 290 #include <ti/drivers/dpl/ClockP.h> 291 #include <ti/drivers/dpl/SemaphoreP.h> 292 #include <ti/drivers/dpl/SwiP.h> 321 #define ADCBufCC26X2_CMD_ACQUIRE_ADC_SEMAPHORE ADCBuf_CMD_RESERVED + 1 336 #define ADCBufCC26X2_CMD_KEEP_ADC_SEMAPHORE ADCBuf_CMD_RESERVED + 2 345 #define ADCBufCC26X2_CMD_KEEP_ADC_SEMAPHORE_DISABLE ADCBuf_CMD_RESERVED + 3 352 #define ADCBufCC26X2_CMD_RELEASE_ADC_SEMAPHORE ADCBuf_CMD_RESERVED + 4 359 #define ADCBufCC26X2_RESOLUTION 12 361 #define ADCBufCC26X2_BYTES_PER_SAMPLE 2 Power manager interface for CC26X2.
ADCBufCC26X2 Hardware Attributes.
Definition: ADCBufCC26X2.h:513
Definition: ADCBufCC26X2.h:406
SemaphoreP_Struct conversionComplete
Definition: ADCBufCC26X2.h:566
Definition: ADCBufCC26X2.h:391
struct ADCBufCC26X2_ParamsExtension ADCBufCC26X2_ParamsExtension
CC26X2 specfic extension to ADCBuf_Params.
GPTimer driver implementation for CC26XX/CC13XX.
Definition: ADCBufCC26X2.h:408
enum ADCBuf_Recurrence_Mode_ ADCBuf_Recurrence_Mode
ADC trigger mode settings.
ADCBufCC26X2_Reference_Source refSource
Definition: ADCBufCC26X2.h:476
ADCBufCC26X2_AdcChannelLutEntry const * adcChannelLut
Definition: ADCBufCC26X2.h:535
uint32_t samplingFrequency
Definition: ADCBufCC26X2.h:581
ADCBuf_Recurrence_Mode recurrenceMode
Definition: ADCBufCC26X2.h:559
ADCBuf_Return_Mode returnMode
Definition: ADCBufCC26X2.h:560
An ADCBuf_Conversion data structure is used with ADCBuf_convert(). It indicates which channel to perf...
Definition: ADCBuf.h:237
Table entry that maps a virtual adc channel to a dio and its corresponding internal analogue signal...
Definition: ADCBufCC26X2.h:458
enum ADCBuf_Return_Mode_ ADCBuf_Return_Mode
ADC return mode settings.
UDMACC26XX Global configuration.
Definition: UDMACC26XX.h:231
PIN_State pinState
Definition: ADCBufCC26X2.h:571
HwiP_Struct hwi
Definition: ADCBufCC26X2.h:564
ADCBuf_Callback callbackFxn
Definition: ADCBufCC26X2.h:558
ADCBufCC26X2_Sampling_Mode samplingMode
Definition: ADCBufCC26X2.h:556
Definition: ADCBufCC26X2.h:405
uint8_t currentChannel
Definition: ADCBufCC26X2.h:554
Definition: ADCBufCC26X2.h:404
struct ADCBufCC26X2_HWAttrs ADCBufCC26X2_HWAttrs
ADCBufCC26X2 Hardware Attributes.
Definition: ADCBufCC26X2.h:390
PIN_Handle pinHandle
Definition: ADCBufCC26X2.h:572
ADCBufCC26X2_Sampling_Duration
Amount of time the ADC spends sampling the analogue input.
Definition: ADCBufCC26X2.h:402
Definition: ADCBufCC26X2.h:412
Device-specific pin & GPIO driver for CC26xx family [def].
ADCBufCC26X2_Sampling_Duration samplingDuration
Definition: ADCBufCC26X2.h:557
bool conversionInProgress
Definition: ADCBufCC26X2.h:550
Definition: ADCBufCC26X2.h:440
bool inputScalingEnabled
Definition: ADCBufCC26X2.h:492
ADCBufCC26X2_Reference_Source refSource
Definition: ADCBufCC26X2.h:555
The definition of an ADCBuf function table that contains the required set of functions to control a s...
Definition: ADCBuf.h:385
uint8_t compBInput
Definition: ADCBufCC26X2.h:460
ADCBufCC26X2 Object.
Definition: ADCBufCC26X2.h:547
UDMACC26XX driver implementation.
Definition: ADCBufCC26X2.h:410
CC26X2 specfic extension to ADCBuf_Params.
Definition: ADCBufCC26X2.h:470
ADCBufCC26X2_Sampling_Duration samplingDuration
Definition: ADCBufCC26X2.h:472
ADCBuf_Conversion * currentConversion
Definition: ADCBufCC26X2.h:568
uint32_t semaphoreTimeout
Definition: ADCBufCC26X2.h:580
UDMACC26XX_Handle udmaHandle
Definition: ADCBufCC26X2.h:575
Definition: ADCBufCC26X2.h:409
struct ADCBufCC26X2_Object ADCBufCC26X2_Object
ADCBufCC26X2 Object.
uint8_t dio
Definition: ADCBufCC26X2.h:459
Definition: ADCBufCC26X2.h:411
GPTimer Global configuration.
Definition: GPTimerCC26XX.h:406
underlying data structure for type PIN_State
Definition: PIN.h:707
const ADCBuf_FxnTable ADCBufCC26X2_fxnTable
ADCBufCC26X2_Sampling_Mode samplingMode
Definition: ADCBufCC26X2.h:474
Definition: ADCBufCC26X2.h:407
struct ADCBufCC26X2_AdcChannelLutEntry ADCBufCC26X2_AdcChannelLutEntry
Table entry that maps a virtual adc channel to a dio and its corresponding internal analogue signal...
GPTimerCC26XX_Handle timerHandle
Definition: ADCBufCC26X2.h:578
Definition: ADCBufCC26X2.h:441
Definition: ADCBufCC26X2.h:415
void(* ADCBuf_Callback)(ADCBuf_Handle handle, ADCBuf_Conversion *conversion, void *completedADCBuffer, uint32_t completedChannel)
The definition of a callback function used by the ADC driver when used in ADCBuf_RETURN_MODE_CALLBACK...
Definition: ADCBuf.h:251
uint32_t swiPriority
ADC SWI priority. The higher the number, the higher the priority. The minimum is 0 and the maximum is...
Definition: ADCBufCC26X2.h:519
bool adcSemaphoreInPossession
Definition: ADCBufCC26X2.h:553
uint8_t intPriority
ADC peripheral's interrupt priority.
Definition: ADCBufCC26X2.h:533
Definition: ADCBufCC26X2.h:413
bool keepADCSemaphore
Definition: ADCBufCC26X2.h:552
Definition: ADCBufCC26X2.h:403
SwiP_Struct swi
Definition: ADCBufCC26X2.h:565
bool isOpen
Definition: ADCBufCC26X2.h:549
Definition: ADCBufCC26X2.h:414
bool inputScalingEnabled
Definition: ADCBufCC26X2.h:551
ADCBufCC26X2_Reference_Source
Specifies whether the internal reference of the ADC is sourced from the battery voltage or a fixed in...
Definition: ADCBufCC26X2.h:439
struct ADCBufCC26X2_Object * ADCBufCC26X2_Handle
Generic PIN & GPIO driver.
uint16_t * activeSampleBuffer
Definition: ADCBufCC26X2.h:561
ADCBufCC26X2_Sampling_Mode
Specifies whether the internal reference of the ADC is sourced from the battery voltage or a fixed in...
Definition: ADCBufCC26X2.h:389
uint8_t gpTimerUnit
Definition: ADCBufCC26X2.h:537