OAD Application¶
The application layer is responsible for plugging the OAD module. The OAD profile and communication with the BLE-Stack is encapsulated inside the OAD module.
The responsibilities of the application depend on which OAD solution is used. In on-chip OAD, the user application is only responsible for plugging the OAD reset service. The TI- provided persistent application is responsible for plugging the OAD profile module that manages the download. In the case of off-chip OAD, the user application is responsible for plugging the OAD module.
An application developer wishing to implement use the TI OAD solution will not need to worry about implementing the OAD state machine, but instead can just include the OAD module or reset service and make the proper calls as detailed in Adding BLE OAD to an Existing Project. However, the details of the OAD module layer are documented here for completeness and to aide in debugging.
OAD Module Architecture¶
The building blocks of the OAD software architecture are detailed below. In the case of off-chip OAD the green block is the user application thread. In the case of on-chip OAD the green block is the persistent application thread that is part of the persistent application image. In the figure below the following terms have been abbreviated for compactness in the image.
- CB : Callback
- SVC: BLE Service
- Func: Function
![../_images/ditaa-7382bbf87f7b2caa69a8ed798a00a953afaa88ba.png](../_images/ditaa-7382bbf87f7b2caa69a8ed798a00a953afaa88ba.png)
Internally the OAD module is responsible for the following:
- Implementing the OAD profile
- Plugging the GATT read and write callback from the BLE-Stack
- Serializing and de-serializing structures from over the messages
- Sending OAD related requests and responses to the BLE-Stack to be sent over the air
- Queuing up messages from stack callbacks to be processed later by the application
- Implementing the OAD state machine, and ensuring proper state transitions
- Implementing the OAD inactivity timers
- Implementing getter/setter functions for the application to use and configure the OAD module
External to the OAD module the application task is responsible for the following. See Adding BLE OAD to an Existing Project more more information.
- Plugging an OAD event handler
- Calling the OAD event processing function in a task context when events are posted.
- Resetting the device when the
OAD_DL_COMPLETE
event is received.
A message sequence chart is included below to show a sample of an application’s interaction with the OAD module.
![]()
Figure 85. OAD Module/ Application interaction¶
OAD State Machine¶
The following section aims to describe the OAD process at a high level.
Device Reset/Image Switching¶
If using on-chip OAD, the OAD profile/module is not implemented by the user applcation. Therefore, there must be a way for the peer device that is initiating an OAD to indicate that an on-chip OAD target is to reboot in the persistent app. This is achieved through the OAD reset service.
The reset service command contains information about whether to reboot and load the user app or to reboot and load into the persistent app. When using secure OAD, this command also contains a signature to verify that the command is sent by a known peer device. If the reset command indicates to jump to the persistent app and the security check passes then the reset service will set the BIM var to instruct the BIM to boot into the persistent app and then trigger a device reset.(See Application Execution switching using RAM for more info).
After the device has booted into the persistent app, the OAD process continues as described below. From this point it is identical to the off-chip process.
![]()
Figure 86. OAD Reset Service/User Application Interaction¶
OAD Module State Diagram¶
The OAD module implements an ‘OAD State Machine’ for performing the OAD. The following state machine depicts the OAD module state transitions and its interactions with the OAD communication profile messages for both on-chip and off-chip OAD.
![../_images/oad_state_machine.png](../_images/oad_state_machine.png)
Figure 87. OAD Types Overview
The states and state transitions are encapsulated inside the OAD module, but some of the critical states are described below to aide in understanding.
Note these sections refer to internal state handling and transitions local to the target device. For a summary of the over the air sequence see Sequence diagram for OAD process and for a breakdown of the different types of profile messages and how to interpret them over the air please see BLE-Stack OAD Profile.
Image Validation¶
After establishing a new connection, updating the connection interval for a faster OAD and enabling notifications of OAD Image Identify and OAD Image Block characteristics on the OAD target, the OAD distributor shall write to the Image Identify characteristic of the OAD target. The message data will be the header retrieved from the OAD Image available for OAD.
On receiving the Image Identify message, the OAD target will verify that the contents of the image can be supported. This is done by checking the Image Header fields, BIM & header versions, and length of the image.
The OAD target will then perform boundary checks in the case of an Application Only or Stack Only OAD. This is done to ensure no boundary violations will occur between the upgraded image and the images that remain on the device.
Additionally, if security is enabled then the OAD module will check the image identify command for a signature to ensure that the command came from a trusted peer.
Image Block Transfers¶
After the Image Validation has completed, the OAD target will switch to the configuration state. There it will get the block size and set image count. When the OAD distributor sends the Start OAD Command to the Control Characteristic (for more details see OAD Control Characteristic Supported Commands.), the OAD target will respond with a Control characteristic notification requesting the first block. The OAD distributor will then send the first block to the OAD target.
This process continues with the OAD target notifying the OAD distributor of the next block it needs and the OAD distributor sending the requested image block until all blocks have been transferred.
Completion of the OAD Process¶
After receiving the complete image, the CRC32 of the entire image will be calculated and the’CRC32 status’ bytes will be set accordingly. If the computed CRC matches with the ‘CRC’ field of received image, it switches to ‘End’ state.
After the OAD process is complete the system will wait for the newly downloaded image to be enabled. Once the image is successfully enabled the OAD module will signal to the app that it should reset. After reset the BIM will process the new image accordingly.