35 #include "hal_assert.h" 47 #define ICALL_SERVICE_CLASS_MASK 0xFFF8 55 #define ICALL_SERVICE_INSTANCE_MASK 0x0007 63 #define ICALL_SERVICE_CLASS_PRIMITIVE 0x0008 68 #define ICALL_SERVICE_CLASS_BLE 0x0010 71 #define ICALL_SERVICE_CLASS_TIMAC 0x0018 74 #define ICALL_SERVICE_CLASS_REMOTI_RTI 0x0020 77 #define ICALL_SERVICE_CLASS_REMOTI_RCN 0x0028 80 #define ICALL_SERVICE_CLASS_ZSTACK 0x0030 83 #define ICALL_SERVICE_CLASS_NPI 0x0038 86 #define ICALL_SERVICE_CLASS_BLE_MSG 0x0050 96 #define ICALL_SERVICE_CLASS_CRYPTO 0x0080 103 #define ICALL_SERVICE_CLASS_BLE_BOARD 0x0088 110 #define ICALL_SERVICE_CLASS_TIMAC_BOARD 0x0090 117 #define ICALL_SERVICE_CLASS_RADIO 0x0098 124 #define ICALL_SERVICE_CLASS_DUMMY 0x0100 132 #define ICALL_SERVICE_CLASS_DUMMY_BOARD 0x0200 137 #define ICALL_INVALID_ENTITY_ID 0xffu 142 #define ICALL_INVALID_TIMER_ID NULL 152 #define ICALL_UNDEF_DEST_ID 0xffu 156 #define ICALL_ERRNO_SUCCESS 0 159 #define ICALL_ERRNO_TIMEOUT 1 162 #define ICALL_ERRNO_NOMSG 2 169 #define ICALL_ERRNO_INVALID_SERVICE -1 175 #define ICALL_ERRNO_INVALID_FUNCTION -2 178 #define ICALL_ERRNO_INVALID_PARAMETER -3 181 #define ICALL_ERRNO_NO_RESOURCE -4 188 #define ICALL_ERRNO_UNKNOWN_THREAD -5 191 #define ICALL_ERRNO_CORRUPT_MSG -6 194 #define ICALL_ERRNO_OVERFLOW -7 197 #define ICALL_ERRNO_UNDERFLOW -8 200 #define ICALL_MSG_FORMAT_KEEP 0 206 #define ICALL_MSG_FORMAT_1ST_CHAR_TASK_ID 1 212 #define ICALL_MSG_FORMAT_3RD_CHAR_TASK_ID 2 218 #define ICALL_MSG_FORMAT_DIRECT_API_ID 3 223 #define ICALL_LITE_DIRECT_API_DONE_CMD_ID 0x42 230 #define ICALL_TIMEOUT_FOREVER 0xfffffffful 236 #ifndef ICALL_TIMEOUT_PREDEFINE 237 #define ICALL_TIMEOUT_PREDEFINE 5000 243 #define ICALL_SEMAPHORE_MODE_COUNTING 0 248 #define ICALL_SEMAPHORE_MODE_BINARY 1 254 #define ICALL_PRIMITIVE_FUNC_ENROLL 0 257 #define ICALL_PRIMITIVE_FUNC_REGISTER_APP 1 260 #define ICALL_PRIMITIVE_FUNC_MSG_ALLOC 2 263 #define ICALL_PRIMITIVE_FUNC_MSG_FREE 3 266 #define ICALL_PRIMITIVE_FUNC_MALLOC 4 269 #define ICALL_PRIMITIVE_FUNC_FREE 5 272 #define ICALL_PRIMITIVE_FUNC_SEND_MSG 6 275 #define ICALL_PRIMITIVE_FUNC_FETCH_MSG 7 278 #define ICALL_PRIMITIVE_FUNC_SEND_SERV_MSG 8 281 #define ICALL_PRIMITIVE_FUNC_FETCH_SERV_MSG 9 284 #define ICALL_PRIMITIVE_FUNC_WAIT 10 287 #define ICALL_PRIMITIVE_FUNC_SIGNAL 11 290 #define ICALL_PRIMITIVE_FUNC_ABORT 12 293 #define ICALL_PRIMITIVE_FUNC_ENABLE_INT 13 296 #define ICALL_PRIMITIVE_FUNC_DISABLE_INT 14 299 #define ICALL_PRIMITIVE_FUNC_ENABLE_MINT 15 302 #define ICALL_PRIMITIVE_FUNC_DISABLE_MINT 16 305 #define ICALL_PRIMITIVE_FUNC_REGISTER_ISR 17 308 #define ICALL_PRIMITIVE_FUNC_GET_TICKS 18 311 #define ICALL_PRIMITIVE_FUNC_SET_TIMER_MSECS 19 314 #define ICALL_PRIMITIVE_FUNC_GET_TICK_PERIOD 20 317 #define ICALL_PRIMITIVE_FUNC_GET_MAX_MILLISECONDS 21 320 #define ICALL_PRIMITIVE_FUNC_ENTITY2SERVICE 22 323 #define ICALL_PRIMITIVE_FUNC_PWR_UPD_ACTIVITY_COUNTER 23 326 #define ICALL_PRIMITIVE_FUNC_PWR_REGISTER_NOTIFY 24 329 #define ICALL_PRIMITIVE_FUNC_WAIT_MATCH 25 332 #define ICALL_PRIMITIVE_FUNC_GET_ENTITY_ID 26 335 #define ICALL_PRIMITIVE_FUNC_SET_TIMER 27 338 #define ICALL_PRIMITIVE_FUNC_STOP_TIMER 28 344 #define ICALL_PRIMITIVE_FUNC_PWR_CONFIG_AC_ACTION 29 347 #define ICALL_PRIMITIVE_FUNC_PWR_REQUIRE 30 350 #define ICALL_PRIMITIVE_FUNC_PWR_DISPENSE 31 353 #define ICALL_PRIMITIVE_FUNC_THREAD_SERVES 32 356 #define ICALL_PRIMITIVE_FUNC_PWR_IS_STABLE_XOSC_HF 33 359 #define ICALL_PRIMITIVE_FUNC_PWR_GET_TRANSITION_STATE 34 362 #define ICALL_PRIMITIVE_FUNC_CREATE_TASK 35 365 #define ICALL_PRIMITIVE_FUNC_CREATE_SEMAPHORE 36 368 #define ICALL_PRIMITIVE_FUNC_WAIT_SEMAPHORE 37 371 #define ICALL_PRIMITIVE_FUNC_SWITCH_XOSC_HF 38 374 #define ICALL_PRIMITIVE_FUNC_PWR_GET_XOSC_STARTUP_TIME 39 377 #define ICALL_PRIMITIVE_FUNC_REGISTER_ISR_EXT 40 381 #define ICALL_PRIMITIVE_FUNC_POST_SEMAPHORE 41 384 #define ICALL_PRIMITIVE_FUNC_CREATE_EVENT 42 387 #define ICALL_PRIMITIVE_FUNC_WAIT_EVENT 43 390 #define ICALL_PRIMITIVE_FUNC_POST_EVENT 44 398 #define ICALL_MSG_FUNC_GET_LOCAL_MSG_ENTITY_ID 0 407 #define ICALL_MSG_EVENT_ID Event_Id_31 416 #define ICALL_WAITMATCH_EVENT_ID Event_Id_29 457 uint32_t totalFreeSize;
458 uint32_t largestFreeSize;
580 void (*isrfunc)(void);
588 void (*isrfunc)(void);
667 void (*entryfn)(
size_t arg);
673 #ifdef ICALL_RTOS_SEMAPHORE_API 704 #ifdef ICALL_RTOS_EVENTS_API 706 typedef struct _icall_create_event_args_t
710 } ICall_CreateEventArgs;
713 typedef struct _icall_post_event_args_t
718 } ICall_PostEventArgs;
721 typedef struct _icall_wait_event_args_t
725 uint_least32_t milliseconds;
726 } ICall_WaitEventArgs;
736 typedef struct _icall_msg_hdr_t
934 PACKED_TYPEDEF_STRUCT
936 uint_least32_t *pointerStack;
937 icall_lite_id_t directAPI;
938 } icall_directAPIMsg_t;
940 PACKED_TYPEDEF_STRUCT
943 icall_directAPIMsg_t msg;
951 uint_least32_t imgTaskPriority;
952 uint_least32_t imgTaskStackSize;
953 void *ICall_imgInitParam;
954 } ICall_RemoteTask_t;
1054 ICall_EntityID dest,
1055 ICall_MSGFormat format,
1074 ICall_Errno
ICall_registerApp(ICall_EntityID *entity, ICall_SyncHandle *msgSyncHdl);
1136 ICall_ServiceEnum dest,
1137 ICall_MSGFormat format,
void *msg);
1169 ICall_EntityID *dest,
1185 ICall_Errno
ICall_wait(uint_fast32_t milliseconds);
1211 ICall_EntityID *entity,
1212 ICall_SyncHandle *msgSyncHdl);
1256 ICall_EntityID dest,
1257 ICall_MSGFormat format,
1280 ICall_EntityID *dest,
1303 ICall_ServiceEnum *servId);
1306 #ifdef HEAPMGR_METRICS 1613 uint_fast16_t stacksize,
size_t arg);
1615 #ifdef ICALL_RTOS_SEMAPHORE_API 1630 #ifdef ICALL_RTOS_SEMAPHORE_API 1642 #ifdef ICALL_RTOS_EVENTS_API 1650 ICall_createEvent(
void);
1659 ICall_postEvent(ICall_Event event, uint32_t events);
1674 ICall_waitEvent(ICall_Event event, uint_fast32_t milliseconds);
1677 #ifdef ICALL_RTOS_SEMAPHORE_API 1724 ICall_ServiceEnum *src,
1725 ICall_EntityID *dest,
1783 ICall_SyncHandle *msgSyncHdl)
1788 args.
hdr.
func = ICALL_PRIMITIVE_FUNC_REGISTER_APP;
1808 args.
hdr.
func = ICALL_PRIMITIVE_FUNC_MSG_ALLOC;
1827 args.
hdr.
func = ICALL_PRIMITIVE_FUNC_MSG_FREE;
1874 ICall_ServiceEnum dest,
1875 ICall_MSGFormat format,
void *msg)
1879 args.
hdr.
func = ICALL_PRIMITIVE_FUNC_SEND_SERV_MSG;
1917 ICall_EntityID *dest,
1923 args.
hdr.
func = ICALL_PRIMITIVE_FUNC_FETCH_SERV_MSG;
1944 static ICall_Errno
ICall_wait(uint_fast32_t milliseconds)
1948 args.
hdr.
func = ICALL_PRIMITIVE_FUNC_WAIT;
1958 static ICall_Errno
ICall_signal(ICall_SyncHandle msgSyncHdl)
1962 args.
hdr.
func = ICALL_PRIMITIVE_FUNC_SIGNAL;
1986 ICall_EntityID *entity,
1987 ICall_SyncHandle *msgSyncHdl)
1992 args.
hdr.
func = ICALL_PRIMITIVE_FUNC_ENROLL;
2014 args.
hdr.
func = ICALL_PRIMITIVE_FUNC_MALLOC;
2033 args.
hdr.
func = ICALL_PRIMITIVE_FUNC_FREE;
2052 static ICall_Errno
ICall_send(ICall_EntityID src,
2053 ICall_EntityID dest,
2054 ICall_MSGFormat format,
2059 args.
hdr.
func = ICALL_PRIMITIVE_FUNC_SEND_MSG;
2087 ICall_EntityID *dest,
2093 args.
hdr.
func = ICALL_PRIMITIVE_FUNC_FETCH_MSG;
2122 ICall_ServiceEnum *servId)
2127 args.
hdr.
func = ICALL_PRIMITIVE_FUNC_ENTITY2SERVICE;
2145 HAL_ASSERT( HAL_ASSERT_CAUSE_ICALL_ABORT );
2149 args.
func = ICALL_PRIMITIVE_FUNC_ABORT;
2163 args.
hdr.
func = ICALL_PRIMITIVE_FUNC_ENABLE_INT;
2178 args.
hdr.
func = ICALL_PRIMITIVE_FUNC_DISABLE_INT;
2192 args.
func = ICALL_PRIMITIVE_FUNC_ENABLE_MINT;
2205 args.
func = ICALL_PRIMITIVE_FUNC_DISABLE_MINT;
2222 args.
hdr.
func = ICALL_PRIMITIVE_FUNC_REGISTER_ISR;
2233 args.
hdr.
func = ICALL_PRIMITIVE_FUNC_REGISTER_ISR_EXT;
2244 static uint_fast32_t
2249 args.
hdr.
func = ICALL_PRIMITIVE_FUNC_GET_TICKS;
2258 static uint_fast32_t
2263 args.
hdr.
func = ICALL_PRIMITIVE_FUNC_GET_TICK_PERIOD;
2274 static uint_fast32_t
2279 args.
hdr.
func = ICALL_PRIMITIVE_FUNC_GET_MAX_MILLISECONDS;
2317 args.
hdr.
func = ICALL_PRIMITIVE_FUNC_SET_TIMER_MSECS;
2360 args.
hdr.
func = ICALL_PRIMITIVE_FUNC_SET_TIMER;
2381 args.
hdr.
func = ICALL_PRIMITIVE_FUNC_STOP_TIMER;
2407 args.
hdr.
func = ICALL_PRIMITIVE_FUNC_PWR_UPD_ACTIVITY_COUNTER;
2435 args.
hdr.
func = ICALL_PRIMITIVE_FUNC_PWR_CONFIG_AC_ACTION;
2456 args.
hdr.
func = ICALL_PRIMITIVE_FUNC_PWR_REQUIRE;
2477 args.
hdr.
func = ICALL_PRIMITIVE_FUNC_PWR_DISPENSE;
2495 args.
hdr.
func = ICALL_PRIMITIVE_FUNC_PWR_IS_STABLE_XOSC_HF;
2511 args.
func = ICALL_PRIMITIVE_FUNC_SWITCH_XOSC_HF;
2525 args.
hdr.
func = ICALL_PRIMITIVE_FUNC_PWR_GET_XOSC_STARTUP_TIME;
2550 args.
hdr.
func = ICALL_PRIMITIVE_FUNC_PWR_REGISTER_NOTIFY;
2569 args.
hdr.
func = ICALL_PRIMITIVE_FUNC_PWR_GET_TRANSITION_STATE;
2592 uint_fast16_t stacksize,
size_t arg)
2597 args.
hdr.
func = ICALL_PRIMITIVE_FUNC_CREATE_TASK;
2605 #ifdef ICALL_RTOS_SEMAPHORE_API 2616 static ICall_Semaphore
2623 args.
hdr.
func = ICALL_PRIMITIVE_FUNC_CREATE_SEMAPHORE;
2635 #ifdef ICALL_RTOS_SEMAPHORE_API 2649 args.
hdr.
func = ICALL_PRIMITIVE_FUNC_POST_SEMAPHORE;
2655 #ifdef ICALL_RTOS_EVENTS_API 2663 ICall_createEvent(
void)
2665 ICall_CreateEventArgs args;
2669 args.hdr.func = ICALL_PRIMITIVE_FUNC_CREATE_EVENT;
2686 ICall_postEvent(ICall_Event event, uint32_t events)
2688 ICall_PostEventArgs args;
2691 args.hdr.func = ICALL_PRIMITIVE_FUNC_POST_EVENT;
2693 args.events = events;
2710 ICall_waitEvent(ICall_Event event, uint_fast32_t milliseconds)
2712 ICall_WaitEventArgs args;
2715 args.hdr.func = ICALL_PRIMITIVE_FUNC_WAIT_EVENT;
2717 args.milliseconds = milliseconds;
2722 #ifdef ICALL_RTOS_SEMAPHORE_API 2742 args.
hdr.
func = ICALL_PRIMITIVE_FUNC_WAIT_SEMAPHORE;
2778 ICall_ServiceEnum *src,
2779 ICall_EntityID *dest,
2785 args.
hdr.
func = ICALL_PRIMITIVE_FUNC_WAIT_MATCH;
2811 static ICall_EntityID
2817 args.
hdr.
func = ICALL_PRIMITIVE_FUNC_GET_ENTITY_ID;
2841 args.
hdr.
func = ICALL_PRIMITIVE_FUNC_THREAD_SERVES;
uint_fast8_t ICall_threadServes(ICall_ServiceEnum service)
Checks whether the calling thread provides the designated service.
ICall_FuncArgsHdr hdr
common arguments field to store source of the message
Definition: icall.h:525
ICall_Errno ICall_createTask(void(*entryfn)(size_t arg), uint_fast8_t priority, uint_fast16_t stacksize, size_t arg)
Creates a new RTOS task.
ICall_RemotiCmdEvent_t
RemoTI RNP and Remote Icall Messaging Interface Enumeration.
Definition: icall.h:915
ICall_Semaphore sem
semaphore
Definition: icall.h:692
void * ICall_Event
Event data type.
Definition: icall.h:445
uint32_t ICall_pwrGetXOSCStartupTime(uint_fast32_t timeUntilWakeupInMs)
uint_least32_t timeUntilWakeupInMs
field matching timeUntilWakeupInMs argument
Definition: icall.h:651
void * ICall_TimerID
Timer id data type.
Definition: icall.h:452
ICall_Errno ICall_enrollService(ICall_ServiceEnum service, ICall_ServiceFunc fn, ICall_EntityID *entity, ICall_SyncHandle *msgSyncHdl)
Registers a service entity.
ICall_FuncArgsHdr hdr
common arguments
Definition: icall.h:807
void * ICall_SyncHandle
Synchronization object data type.
Definition: icall.h:438
uint_fast8_t ICall_PwrTransition
Power state transition type of the following values:
Definition: icall.h:756
ICall_Errno ICall_pwrDispense(ICall_PwrBitmap_t bitmap)
Releases power constraints and dependencies.
ICall_enrollService arguments
Definition: icall.h:879
bool incFlag
a boolean flag to indicate either increment or decrement
Definition: icall.h:617
ICall_MSGFormat format
Message format.
Definition: icall.h:518
uint_least8_t mode
semaphore mode. Either ICALL_SEMAPHORE_MODE_BINARY or ICALL_SEMAPHORE_MODE_COUNTING ...
Definition: icall.h:683
struct _icall_thread_serves_args_t ICall_ThreadServesArgs
ICall_threadServes argument
uint_least8_t localId
local entity ID
Definition: icall.h:911
struct _icall_send_args_t ICall_SendArgs
ICall_sendServiceMsg and ICall_send arguments
ICall_LeaveCS leavecs
leave CS
Definition: icall.h:854
ICall_CSState(* ICall_EnterCS)(void)
Critical section entry function pointer type.
Definition: icall.h:829
int intPriority
interrupt priority
Definition: icall.h:589
void(* ICall_TimerCback)(void *arg)
Prototype of a callback function for timer.
Definition: icall.h:476
int_fast16_t ICall_Errno
Error code data type.
Definition: icall.h:426
ICall_Errno ICall_wait(uint_fast32_t milliseconds)
Waits for a signal to the semaphore associated with the calling thread.
ICall_sendServiceMsg and ICall_send arguments
Definition: icall.h:509
void(* ICall_LeaveCS)(ICall_CSState key)
Critical section exit function pointer type.
Definition: icall.h:837
int ICall_getHeapMgrSanityCheck()
the function retrieve information about the osal heap.
ICall_pwrRegisterNotify arguments
Definition: icall.h:786
ICall_Errno ICall_pwrRequire(ICall_PwrBitmap_t bitmap)
Sets power constraints and dependencies.
struct _icall_post_semaphore_args_t ICall_PostSemaphoreArgs
ICall_postSemaphore argument
ICall_FuncArgsHdr hdr
common arguments
Definition: icall.h:650
uint_fast32_t ICall_getTickPeriod(void)
Gets the tick period.
uint_least16_t stacksize
task priority as understood by underlying RTOS implementation
Definition: icall.h:669
uint_least8_t priority
task priority as understood by underlying RTOS implementation
Definition: icall.h:668
ICall_Errno ICall_enableInt(int intnum)
Enables interrupt.
ICall_signal arguments
Definition: icall.h:550
uint_least32_t ICall_CSState
Critical section state data type.
Definition: icall.h:822
struct _icall_register_isr_args_t ICall_RegisterISRArgs
ICall_registerISR arguments
ICall_FuncArgsHdr hdr
common arguments
Definition: icall.h:691
struct _icall_set_timer_args_t ICall_SetTimerArgs
ICall_setTimer arguments
bool(* ICall_MsgMatchFn)(ICall_ServiceEnum src, ICall_EntityID dest, const void *msg)
Prototype of a function used to compare a received message for a match.
Definition: icall.h:469
ICall_createTask argument
Definition: icall.h:664
ICall_ServiceEnum servId
service id
Definition: icall.h:799
Event for app RTI->stack RTI module.
Definition: icall.h:919
ICall_EntityID entityId
entity id
Definition: icall.h:529
ICall_signal arguments
Definition: icall.h:543
ICall Lite Command Status.
Definition: icall.h:929
ICall_FuncArgsHdr hdr
common arguments
Definition: icall.h:632
ICall_stopTimer arguments
Definition: icall.h:899
struct _icall_getuint32_args_t ICall_GetUint32Args
ICall_getTicks , ICall_getTickPeriod and ICall_getMaxMSecs arguments
ICall_ServiceEnum servId
Service ID of destination.
Definition: icall.h:516
ICall_FuncArgsHdr hdr
common arguments
Definition: icall.h:698
uint_fast32_t ICall_getMaxMSecs(void)
Gets the maximum timeout period supported by ICall_setTimerMSecs function.
struct _icall_wait_semaphore_args_t ICall_WaitSemaphoreArgs
ICall_waitSemaphore argument
uint_least32_t value
field to store the retrieved value
Definition: icall.h:599
ICall_ServiceFunc fn
handler function which handles function calls to the service
Definition: icall.h:883
uint_fast8_t ICall_pwrGetTransitionState(void)
Retrieves power transition state.
ICall_EntityID entity
client entity id
Definition: icall.h:808
ICall_FuncID func
function id
Definition: icall.h:482
struct _ICall_LiteCmdStatus_ ICall_LiteCmdStatus
ICall Lite Command Status.
#define ICALL_ERRNO_SUCCESS
ICall function return value for successful operation.
Definition: icall.h:156
ICall_SyncHandle msgSyncHdl
field to store the synchronous object handle associated with the calling thread
Definition: icall.h:490
ICall_PwrNotifyData * obj
data object
Definition: icall.h:790
ICall_FuncArgsHdr hdr
common arguments
Definition: icall.h:563
void * msg
field to store the starting address of the message body
Definition: icall.h:801
ICall_FuncArgsHdr hdr
common arguments
Definition: icall.h:666
Power state transition notify function data object type.
Definition: icall.h:776
bool pwrRequired
the result of current activity counter
Definition: icall.h:618
uint_least8_t ICall_MSGFormat
Message conversion format data type.
Definition: icall.h:432
union _icall_send_args_t::@0 dest
union of entity and service ID's
ICall_Errno ICall_registerISR(int intnum, void(*isrfunc)(void))
Registers an interrupt service routine.
uint_least16_t ICall_FuncID
Function id data type.
Definition: icall.h:435
ICall_FuncArgsHdr hdr
Common arguments.
Definition: icall.h:908
struct _icall_pwr_get_transition_state_args_t ICall_PwrGetTransitionStateArgs
ICall_pwrGetTransitionState arguments
struct _icall_pwr_bitmap_args_t ICall_PwrBitmapArgs
ICall_pwrConfigActivityCounterAction , ICall_pwrRequire and ICall_pwrDispense arguments.
ICall_pwrGetTransitionState arguments
Definition: icall.h:639
struct _icall_intnum_args_t ICall_IntNumArgs
ICall_enableInt and ICall_disableInt arguments
ICall_EnterCS entercs
enter CS
Definition: icall.h:853
ICall_Errno ICall_setTimer(uint_fast32_t ticks, ICall_TimerCback cback, void *arg, ICall_TimerID *id)
Set up or restart a timer. Note that the timer setup initially by this function may be restarted usin...
ICall_pwrIsStableXOSCHF arguments
Definition: icall.h:605
ICall_freeMsg or ICall_free arguments
Definition: icall.h:502
ICall_postSemaphore argument
Definition: icall.h:689
ICall_Errno ICall_pwrConfigACAction(ICall_PwrBitmap_t bitmap)
Configures power constraint/dependency set/release actions upon activity counter change.
ICall_enableInt and ICall_disableInt arguments
Definition: icall.h:569
ICall_Semaphore ICall_createSemaphore(uint_fast8_t mode, int initcount)
Creates a semaphore.
void * ptr
pointer to the address of a memory block to free
Definition: icall.h:505
ICall_threadServes argument
Definition: icall.h:656
struct _icall_register_isr_args_ext_t ICall_RegisterISRArgs_Ext
ICall_registerISR_Ext arguments.
void ICall_freeMsg(void *msg)
Frees the memory block allocated for a message.
Common service function arguments.
Definition: icall.h:479
ICall_EntityID entityId
Entity ID of destination.
Definition: icall.h:515
ICall_Dispatcher dispatch
ICall dispatcher.
Definition: icall.h:852
ICall_fetchServiceMsg and ICall_fetchMsg arguments
Definition: icall.h:523
bool value
Definition: icall.h:610
ICall_EntityID entity
entity id
Definition: icall.h:910
void ICall_createRemoteTasksAtRuntime(ICall_RemoteTask_t *remoteTaskTable, uint8_t nb_elems)
Create remote tasks with parameters define at runtime.
struct _icall_register_app_args_t ICall_RegisterAppArgs
ICall_registerApp arguments
ICall_FuncArgsHdr hdr
common arguments
Definition: icall.h:901
struct _icall_remote_task_arg_t ICall_RemoteTaskArg
Data type of the first argument passed to the entry point of an image which contains a remote task...
void ICall_free(void *msg)
Frees an allocated memory block.
size_t arg
argument passed to the task entry function
Definition: icall.h:670
ICall_registerISR_Ext arguments.
Definition: icall.h:584
struct _icall_wait_match_args_t ICall_WaitMatchArgs
ICall_waitMatch arguments
void * ICall_allocMsg(size_t size)
Allocates memory block for a message.
ICall_FuncArgsHdr hdr
common arguments
Definition: icall.h:578
size_t size
size of the message body in bytes
Definition: icall.h:497
struct _icall_create_task_args_t ICall_CreateTaskArgs
ICall_createTask argument
ICall_FuncArgsHdr hdr
common arguments
Definition: icall.h:504
ICall_SyncHandle msgSyncHdl
field to store the synchronous object handle associated with the calling thread
Definition: icall.h:885
ICall_Errno ICall_waitSemaphore(ICall_Semaphore sem, uint_fast32_t milliseconds)
Waits on a semaphore.
ICall_EntityID entity
field to store the entity id assigned to the application
Definition: icall.h:489
struct _icall_enroll_service_args_t ICall_EnrollServiceArgs
ICall_enrollService arguments
#define ICALL_MSG_FUNC_GET_LOCAL_MSG_ENTITY_ID
Messaging service function id for translating ICall_entityID to locally understandable id...
Definition: icall.h:398
ICall_Errno ICall_disableInt(int intnum)
Disables interrupt.
struct _icall_alloc_args_t ICall_AllocArgs
ICall_allocMsg or ICall_malloc arguments
Data type of the first argument passed to the entry point of an image which contains a remote task...
Definition: icall.h:850
ICall_FuncArgsHdr hdr
common arguments
Definition: icall.h:641
ICall_Errno ICall_signal(ICall_SyncHandle msgSyncHdl)
Signals a semaphore.
void * msg
pointer to the message body to send
Definition: icall.h:519
ICall_FuncArgsHdr hdr
common arguments
Definition: icall.h:616
ICall_ServiceEnum servId
Service ID of destination.
Definition: icall.h:659
ICall_Errno ICall_entityId2ServiceId(ICall_EntityID entityId, ICall_ServiceEnum *servId)
Transforms and entityId into a serviceId. Note that this function is useful in case an application wa...
struct _icall_get_local_msg_entity_id_args_t ICall_GetLocalMsgEntityIdArgs
ICall_getLocalMsgEntityId arguments
void * ICall_malloc(uint_least16_t size)
Allocates a memory block.
struct _icall_func_args_hdr_t ICall_FuncArgsHdr
Common service function arguments.
ICall_Errno ICall_disableMInt(void)
Disables master interrupt and context switching.
ICall_SyncHandle syncHandle
handle of a synchronous object to signal
Definition: icall.h:546
struct _icall_pwr_get_xosc_startup_time_args_t ICall_PwrGetXOSCStartupTimeArgs
ICall_pwrGetXOSCStartupTime arguments
ICall_FuncArgsHdr hdr
common arguments
Definition: icall.h:796
void * ptr
pointer to store the start address of the newly allocated memory block
Definition: icall.h:498
ICall_LeaveCS ICall_leaveCriticalSection
Leave critical section function pointer of the current image.
ICall_Errno ICall_abort(void)
Aborts.
void(* ICall_PwrNotifyFn)(ICall_PwrTransition pwrTrans, struct _icall_pwr_notify_data_t *obj)
Definition: icall.h:770
#define ICALL_INVALID_ENTITY_ID
Entity ID used to indicate invalid entity.
Definition: icall.h:137
ICall_EntityID dest
field to store the entity id of the destination of the message
Definition: icall.h:531
ICall_getTicks , ICall_getTickPeriod and ICall_getMaxMSecs arguments
Definition: icall.h:596
ICall_Errno(* ICall_ServiceFunc)(ICall_FuncArgsHdr *args)
Call dispatcher service handler function pointer type.
Definition: icall.h:876
ICall_EntityID ICall_searchServiceEntity(ICall_ServiceEnum service)
Search for a service entity entry.
ICall_Errno ICall_sendServiceMsg(ICall_EntityID src, ICall_ServiceEnum dest, ICall_MSGFormat format, void *msg)
Sends a message to a registered server.
struct _icall_free_args_t ICall_FreeArgs
ICall_freeMsg or ICall_free arguments
ICall_SyncHandle syncHandle
handle of a synchronous object to signal
Definition: icall.h:553
ICall_FuncArgsHdr hdr
common arguments
Definition: icall.h:496
struct _icall_entity2service_args_t ICall_EntityId2ServiceIdArgs
ICall_entityId2ServiceId arguments
ICall_pwrConfigActivityCounterAction , ICall_pwrRequire and ICall_pwrDispense arguments.
Definition: icall.h:630
uint_fast32_t ICall_PwrBitmap_t
Power control bitmap type.
Definition: icall.h:624
ICall_PwrNotifyFn _private
a field for private use. Do not access the field. User data should follow this field.
Definition: icall.h:782
ICall_FuncArgsHdr hdr
common arguments
Definition: icall.h:598
uint32_t events
events
Definition: icall.h:554
ICall_ServiceEnum service
service id
Definition: icall.h:481
ICall_ServiceEnum servId
field to store the service id
Definition: icall.h:565
ICall_Errno ICall_send(ICall_EntityID src, ICall_EntityID dest, ICall_MSGFormat format, void *msg)
Sends a message to an entity.
ICall_entityId2ServiceId arguments
Definition: icall.h:561
#define ICALL_SERVICE_CLASS_PRIMITIVE
Service class enumerated value for primitive service.
Definition: icall.h:63
void * msg
field to store the starting address of the message body
Definition: icall.h:532
ICall_Errno ICall_postSemaphore(ICall_Semaphore sem)
Post on a semaphore.
uint_least32_t milliseconds
timeout period in milliseconds
Definition: icall.h:797
ICall_Errno(* ICall_Dispatcher)(ICall_FuncArgsHdr *args)
Call dispatcher function pointer type.
Definition: icall.h:817
ICall_FuncArgsHdr hdr
common arguments
Definition: icall.h:488
struct _icall_get_entity_id_args_t ICall_GetEntityIdArgs
ICall_getEntityId arguments
Event for app RTI->stack RC App.
Definition: icall.h:917
void(* isrfunc)(void)
pointer to the interrupt service function
Definition: icall.h:580
uint_fast8_t state
power transition state
Definition: icall.h:642
ICall_FuncArgsHdr hdr
common arguments
Definition: icall.h:658
uint_fast8_t ICall_getLocalMsgEntityId(ICall_ServiceEnum service, ICall_EntityID entity)
Retrieves an internal ID understood only by a service entity, corresponding to an ICall entity ID...
void ICall_stopTimer(ICall_TimerID id)
Stops a timer.
struct _icall_getbool_args_t ICall_GetBoolArgs
ICall_pwrIsStableXOSCHF arguments
int initcount
semaphore initial count value
Definition: icall.h:684
struct _icall_pwr_notify_data_t ICall_PwrNotifyData
Power state transition notify function data object type.
ICall_FuncArgsHdr hdr
common arguments
Definition: icall.h:552
struct _icall_stop_timer_args_t ICall_StopTimerArgs
ICall_stopTimer arguments
ICall_getEntityId arguments
Definition: icall.h:805
ICall_allocMsg or ICall_malloc arguments
Definition: icall.h:494
ICall_Errno ICall_registerISR_Ext(int intnum, void(*isrfunc)(void), int intPriority)
ICall Register ISR.
ICall_Errno ICall_pwrSwitchXOSCHF(void)
Switch clock source to HF XOSC. This function must be called after HF XOSC is stable.
ICall_waitMatch arguments
Definition: icall.h:794
ICall_EnterCS ICall_enterCriticalSection
Enter critical section function pointer of the current image.
bool ICall_pwrIsStableXOSCHF(void)
Checks whether HF XOSC is stable. This function must be called after HF XOSC is turned on (through po...
ICall_EntityID dest
field to store the entity id of the destination of the message
Definition: icall.h:800
int_least32_t intnum
interrupt number
Definition: icall.h:587
struct _icall_signal_args_t ICall_SignalArgs
ICall_signal arguments
ICall_Errno ICall_pwrRegisterNotify(ICall_PwrNotifyFn fn, ICall_PwrNotifyData *obj)
Registers a power state transition notify function.
ICall_Errno ICall_setTimerMSecs(uint_fast32_t msecs, ICall_TimerCback cback, void *arg, ICall_TimerID *id)
Set up or restart a timer. Note that the timer setup initially by this function may be restarted usin...
ICall_FuncArgsHdr hdr
common arguments
Definition: icall.h:881
uint_least32_t value
field to store the retrieved value
Definition: icall.h:652
ICall_wait arguments
Definition: icall.h:536
ICall_Errno ICall_sendServiceComplete(ICall_EntityID src, ICall_EntityID dest, ICall_MSGFormat format, void *msg)
function to indicate that servicing an direct API call is done
void ICall_createRemoteTasks(void)
Create remote tasks.
struct _icall_wait_args_t ICall_WaitArgs
ICall_wait arguments
ICall_TimerID timerid
timer ID
Definition: icall.h:893
void * arg
pointer to an argument to be passed to the callback function
Definition: icall.h:895
SYNC message from RNP app -> stack.
Definition: icall.h:922
ICall_ServiceEnum service
service id
Definition: icall.h:909
ICall_FuncArgsHdr hdr
common arguments
Definition: icall.h:511
ICall_waitSemaphore argument
Definition: icall.h:696
int_least32_t intnum
interrupt number
Definition: icall.h:572
struct _icall_pwr_upd_activity_counter_args_t ICall_PwrUpdActivityCounterArgs
ICall_pwrUpdActivityCounter arguments
uint_least32_t milliseconds
timeout in milliseconds
Definition: icall.h:700
Event for stack RTI->app RTI module.
Definition: icall.h:920
ICall_FuncArgsHdr hdr
common arguments
Definition: icall.h:788
uint_least8_t cmdId
command id (applicable only to User Profile subgrp)
Definition: icall.h:931
ICall_FuncArgsHdr hdr
common arguments
Definition: icall.h:677
ICall_registerISR arguments
Definition: icall.h:576
ICall_FuncArgsHdr hdr
common arguments
Definition: icall.h:571
ICall_FuncArgsHdr hdr
common arguments
Definition: icall.h:538
ICall_EntityID entityId
entity id
Definition: icall.h:564
void * ICall_Semaphore
Semaphore used for ICall.
Definition: icall.h:441
uint_least32_t icall_lite_id_t
ICall Lite ID.
Definition: icall.h:926
void(* entryfn)(size_t arg)
task entry function
Definition: icall.h:667
uint_least32_t milliseconds
timeout period in milliseconds
Definition: icall.h:539
ICall_EntityID entity
field to store the assigned entity id
Definition: icall.h:884
ICall_MsgMatchFn matchFn
match function
Definition: icall.h:798
ICall_TimerCback cback
callback function
Definition: icall.h:894
void(* isrfunc)(void)
pointer to ISR
Definition: icall.h:588
struct _icall_create_semaphore_args_t ICall_CreateSemaphoreArgs
ICall_createSemaphore argument
ICall_registerApp arguments
Definition: icall.h:486
Event for stack->app RC App.
Definition: icall.h:918
ICall_FuncArgsHdr hdr
Definition: icall.h:608
ICall_pwrUpdActivityCounter arguments
Definition: icall.h:614
ICall_Semaphore sem
semaphore
Definition: icall.h:699
uint_fast32_t ICall_getTicks(void)
Gets the current tick counter value.
void ICall_init(void)
Initializes the dispatcher implementation.
void * ICall_mallocLimited(uint_least16_t size)
ICall_getLocalMsgEntityId arguments
Definition: icall.h:906
void ICall_getHeapMgrGetMetrics(uint32_t *pBlkMax, uint32_t *pBlkCnt, uint32_t *pBlkFree, uint32_t *pMemAlo, uint32_t *pMemMax, uint32_t *pMemUB)
the function retrieve information about the osal heap. Note :ICall_getHeapMgrGetMetrics will not work...
ICall_ServiceEnum servId
service id
Definition: icall.h:528
ICall_createSemaphore argument
Definition: icall.h:675
struct _icall_pwr_register_notify_args_t ICall_PwrRegisterNotifyArgs
ICall_pwrRegisterNotify arguments
uint_least8_t ICall_resetReason
Special global variable to set the reset reason by the boot code, before ICall is initialized...
ICall_pwrGetXOSCStartupTime arguments
Definition: icall.h:648
uint_least8_t ICall_EntityID
Entity id data type.
Definition: icall.h:449
int_least32_t intnum
interrupt number
Definition: icall.h:579
ASYNC message from RNP app->stack.
Definition: icall.h:921
ICall_Dispatcher ICall_dispatcher
Call dispatcher pointer of the current image.
ICall_EntityID src
Entity id of the sender of the message Destination id.
Definition: icall.h:512
ICall_FuncArgsHdr hdr
common arguments
Definition: icall.h:586
ICall_FuncArgsHdr hdr
common arguments
Definition: icall.h:545
struct _icall_fetch_msg_args_t ICall_FetchMsgArgs
ICall_fetchServiceMsg and ICall_fetchMsg arguments
ICall_PwrNotifyFn fn
notify function to handle notification
Definition: icall.h:789
ICall_Errno ICall_fetchMsg(ICall_EntityID *src, ICall_EntityID *dest, void **msg)
Retrieves a message, queued to receive queue of the calling thread.
ICall_setTimer arguments
Definition: icall.h:889
ICall_Errno ICall_fetchServiceMsg(ICall_ServiceEnum *src, ICall_EntityID *dest, void **msg)
Retrieves a message received at the message queue associated with the calling thread.
uint_least32_t timeout
timeout period
Definition: icall.h:892
ICall_ServiceEnum service
service id of the enrolling service
Definition: icall.h:882
ICall_Errno ICall_enableMInt(void)
Enables master interrupt and context switching.
void(* ICall_RemoteTaskEntry)(const ICall_RemoteTaskArg *arg0, void *arg1)
Service entry function prototype.
Definition: icall.h:867
uint_fast8_t result
Result (true or false)
Definition: icall.h:660
ICall_TimerID timerid
timer ID
Definition: icall.h:902
uint_least16_t ICall_ServiceEnum
Service enumeration data type.
Definition: icall.h:429
ICall_Semaphore sem
created semaphore
Definition: icall.h:685
void ICall_getHeapStats(ICall_heapStats_t *stats)
Get Statistic on Heap.
ICall_Errno ICall_waitMatch(uint_least32_t milliseconds, ICall_MsgMatchFn matchFn, ICall_ServiceEnum *src, ICall_EntityID *dest, void **msg)
Waits for and retrieves a message received at the message queue associated with the calling thread...
struct _icall_signal_events_args_t ICall_SignalEventsArgs
ICall_signal arguments
uint32_t icall_directAPI(uint8_t service, icall_lite_id_t id,...)
generic variadic function to translate API id to a functional call in the stack context,
union _icall_fetch_msg_args_t::@1 src
union of service and entity id's
ICall_EntityID ICall_getEntityId(void)
Retrieves an entity ID of (arbitrary) one of the entities registered from the calling thread...
ICall_FuncArgsHdr hdr
common arguments
Definition: icall.h:891
bool ICall_pwrUpdActivityCounter(bool incFlag)
Increments or decrements power activity counter.
ICall_Errno ICall_registerApp(ICall_EntityID *entity, ICall_SyncHandle *msgSyncHdl)
Registers an application.
ICall_PwrBitmap_t bitmap
power configuration bitmap
Definition: icall.h:633