Terms and Definitions¶
Bluetooth Low Energy Terms and Acronyms¶
- Application-program interface
- API
- Refers to the function call.
- BLE
- Bluetooth Low Energy
- BR
- Basic Rate
- BR/EDR
- Basic Rate/Enhanced Data Rate
- CCCD
- Client Characteristic Configuration Descriptor
- Coding Indication
- CI
- Bit field in every BLE packet sent on LE Coded PHY that indicates the coding of the PDU (S=2 or S=8).
- Device Address
- A 48-bit value used to identify a device. A device address can be public, random static, or random private.
- Forward Error Correction
- FEC
- Error correction used to improve the sensitivity in the LE Coded PHY.
- GAP
- Generic Access Protocol
- GFSK
- Gaussian Frequency-Shift Keying
- HCI
- Host Control Interface
- Identity Address
- IA
- A Resolvable Private Address that is resolvable with an Identity Resolving Key yields an Identity Address.
- Identity Resolving Key
- IRK
- A key exchanged during Phase 3 of the bonding process. A Resolving List contains a local and a peer Identity Resolving Key as well as an Identity Address.
- ISM
- Industrial, Scientific, and Medical
- L2CAP
- Link Logical Control and Adaption Protocol
- LE
- Low Energy
- Link Budget
- The link budget is the ratio between the Tx power and the Rx sensitivity level.
- Link Layer
- LL
- A Bluetooth low energy stack layer in on the controller side.
- LTK
- Long Term Key
- A term defined by the Bluetooth Core Specification Version 5.0 referring to the key used for encypted connections.
- Physical layer
- PHY
- The physical layer is the lowest layer of the Bluetooth protocol stack. It configures the physical parameters of the radio transmission and reception. It determines how a bit (and its value) are represented over the air.
- PDU
- Protocol Data Unit
- Resolving List
- RL
- A Link Layer maintained table of one or more entries of a local and peer Identity Resolving Key associated to an Identity Address.
- Resolvable Private Address
- RPA
- A resolvable address is one that can be resolved given that the device has an Identity Resolving Key. By resolving a Resolvable Private Address one can determine its Identity Address.
- Resolvable Private Address Only
- RPAO
- A required GATT characteristic called “Resolvable Private Address Only” that is used with Network Privacy Mode.
- Simple Non-Volatile storage
- SNV
- An abstraction layer used by the BLE stack for reading and writing to non volatile memory. The GAPBondMgr layer of stack uses SNV to store keys. This region can also be used by the user.
- White List
- WL
- A filter policy in the Controller’s Link Layer that can prevent unwanted link layer events from waking up the host.
General Terms and Acronyms¶
- BIM
- Boot Image Manager, the software bootloader
- .bss
- Block started by symbol. This memory section usually contains uninitialized variables including the task stacks.
- CCA
- CCFG
- Customer Configuration
- CCFG
- Customer Configuration Area, contains lock-bits on flash page 31 and the Customer Configuration Table (.ccfg)
- CCS
- Code Composer Studio
- GPRAM
- General purpose RAM. This memory area is used for the cache per default, but can be configured to be used as RAM.
- IAR
- IAR Systems
- MCU
- Micro-controller Unit
- OAD
- Over the Air Download
- RCFG
- TI-RTOS in ROM Configuration Table
- ROM
- Read-only Memory
- SNV
- Simple Non-Volatile storage
- SNP
- Simple Network Processor, a BLE network processor implementation that supports the peripheral and broadcaster GAP Roles.
- Network Processor
- NP
- A device that contains the wireless protocol stack as well as RF hardware. Stack functionality is exposed via a serial interface.
- Application Processor
- AP
- An processor that implements the customer application as well the serial command interface to communicate with a network processor.
- UNPI
- Unified Network Processor Interface, a standardized serial transport format that is implemented by TI for the purposes of interfacing to network processor devices like the SNP. UNPI also manages the handshaking required for the serial interface.
- RTSC
- Real Time Software Components. See RTSC and RTSC-Pedia.
- VIMS
- Versatile Instruction Memory System. A system control module that handles access to the device memory areas from the CPU and system bus. You can read more in the Technical Reference Manual .
- cJTAG
- Class 4 IEEE 1149.7: Standard for Reduced-pin and Enhanced-functionality Test Access Port and Boundary-scan Architecture. This is known by acronym cJTAG (compact JTAG).
- JTAG
- IEEE standard 1149.1: Standard Test Access Port and Boundary Scan Architecture Test Access Port (TAP). This standard is known by the acronym JTAG (Joint Test Action Group).
TI-RTOS Terms and Acronyms¶
- Hwi
- A TI-RTOS Hardware interrupt.
- Idle Task
- A TI-RTOS default task that is executes when no other higher priority thread needs to run.
- ROV
- Runtime Object View
- A TI-RTOS kernel plugin for CCS and IAR to view a target’s instrumentation data.
- RTC
- Real-time Clock
- RTSC
- Real Time Software Componenets. A toolset for creating reusable code, used by TI-RTOS.
- Swi
- A TI-RTOS Software interrupt.
- TI-RTOS
- Texas Instruments Real Time Operating System
- Zero-Latency Interrupts
- An interrupt that will not be routed through the TI-RTOS kernel’s Hwi dispatcher. For more information, see this wiki article.
Sensor Controller Terms and Acronyms¶
- SC
- Sensor Controller
- SCS
- Sensor Controller Studio
Over the Air Download (OAD) Terms and Acronyms¶
- BIM
- Boot Image Manager
- A bootloader that runs after the device’s ROM startup code. The BIM is responsible for analyzing the image header of all images and determining the most suitable image to run. Once the BIM has found the proper image, it will jump to it’s program entry.
- Factory Image
- The factory image is a “golden” image that resides in external flash as a failsafe mechanism.
- OAD
- Over the Air Download
- The process of performing a device firmware update over the air.
- OAD Target
- The device whose firmware is being upgraded over the air. This is assumed to be a CC26xx device running the TI protocol specific transport for OAD.
- OAD Distributor
- The device responsible for accepting an OAD enabled image from the compiler and transferring it over the air to the OAD Target.