TI BLE5-Stack API Documentation
1.01.02.00
|
LinkDB layer interface
Go to the source code of this file.
Data Structures | |
struct | linkDBInfo_t |
Information pertaining to the linklinkDB info. More... | |
Macros | |
#define | CONNHANDLE_ALL 0xFFFD |
Terminates all links. | |
#define | CONNHANDLE_INVALID 0xFFFF |
Invalid connection handle, used for no connection handle. | |
#define | CONNHANDLE_LOOPBACK 0xFFFE |
Loopback connection handle, used to loopback a message. | |
#define | LINBDB_ERR_INSUFFICIENT_KEYSIZE 0x0c |
Link is encrypted but the key size is too small. | |
#define | LINK_AUTHENTICATED 0x02 |
Link is authenticated. | |
#define | LINK_BOUND 0x04 |
Link is bonded. | |
#define | LINK_CONNECTED 0x01 |
Link is connected. | |
#define | LINK_ENCRYPTED 0x10 |
Link is encrypted. | |
#define | LINK_IN_UPDATE 0x40 |
Link is in update procedure. | |
#define | LINK_NOT_CONNECTED 0x00 |
Link isn't connected. | |
#define | LINK_PAIR_TIMEOUT 0x80 |
Pairing attempt has been timed out. | |
#define | LINK_SECURE_CONNECTIONS 0x20 |
Link uses Secure Connections. | |
#define | linkDB_Authenticated(connectionHandle) linkDB_State( (connectionHandle), LINK_AUTHENTICATED ) |
#define | linkDB_Bonded(connectionHandle) linkDB_State( (connectionHandle), LINK_BOUND ) |
#define | linkDB_Encrypted(connectionHandle) linkDB_State( (connectionHandle), LINK_ENCRYPTED ) |
#define | LINKDB_ERR_INSUFFICIENT_AUTHEN 0x05 |
Link isn't even encrypted. | |
#define | LINKDB_ERR_INSUFFICIENT_ENCRYPTION 0x0f |
Link is encrypted but it's not authenticated. | |
#define | linkDB_Up(connectionHandle) linkDB_State( (connectionHandle), LINK_CONNECTED ) |
Functions | |
uint8 | linkDB_GetInfo (uint16 connectionHandle, linkDBInfo_t *pInfo) |
uint8 | linkDB_NumActive (void) |
uint8 | linkDB_NumConns (void) |
uint8 | linkDB_State (uint16 connectionHandle, uint8 state) |