65 #ifndef ti_drivers_nvs_NVSCC26XX__include 66 #define ti_drivers_nvs_NVSCC26XX__include 71 #if defined (__cplusplus) 81 #define NVSCC26XX_STATUS_LOW_VOLTAGE (NVS_STATUS_RESERVED - 1) 251 extern void NVSCC26XX_close(
NVS_Handle handle);
252 extern int_fast16_t NVSCC26XX_control(
NVS_Handle handle, uint_fast16_t cmd,
254 extern int_fast16_t NVSCC26XX_erase(
NVS_Handle handle,
size_t offset,
257 extern void NVSCC26XX_init();
258 extern int_fast16_t NVSCC26XX_lock(
NVS_Handle handle, uint32_t timeout);
260 extern int_fast16_t NVSCC26XX_read(
NVS_Handle handle,
size_t offset,
261 void *buffer,
size_t bufferSize);
262 extern void NVSCC26XX_unlock(
NVS_Handle handle);
263 extern int_fast16_t NVSCC26XX_write(
NVS_Handle handle,
size_t offset,
264 void *buffer,
size_t bufferSize, uint_fast16_t flags);
267 #if defined (__cplusplus) NVS attributes.
Definition: NVS.h:431
const NVS_FxnTable NVSCC26XX_fxnTable
void * regionBase
Definition: NVSCC26XX.h:233
struct NVSCC26XX_HWAttrs NVSCC26XX_HWAttrs
NVSCC26XX attributes.
NVS Parameters.
Definition: NVS.h:410
struct NVSCC26XX_Object NVSCC26XX_Object
bool opened
Definition: NVSCC26XX.h:243
Definition: NVSCC26XX.h:242
size_t regionSize
Definition: NVSCC26XX.h:234
NVSCC26XX attributes.
Definition: NVSCC26XX.h:232
NVS Global configuration.
Definition: NVS.h:555
The definition of an NVS function table that contains the required set of functions to control a spec...
Definition: NVS.h:512