49 #ifndef ti_drivers_adc_ADCCC26XX__include 50 #define ti_drivers_adc_ADCCC26XX__include 65 #include <ti/devices/DeviceFamily.h> 66 #include DeviceFamily_constructPath(driverlib/aux_adc.h) ADCCC26XX_Trigger_Source triggerSource
Definition: ADCCC26XX.h:144
Definition: ADCCC26XX.h:90
Definition: ADCCC26XX.h:83
ADCCC26XX_Reference_Source refSource
Definition: ADCCC26XX.h:142
ADCCC26XX Object.
Definition: ADCCC26XX.h:152
Definition: ADCCC26XX.h:114
bool returnAdjustedVal
Definition: ADCCC26XX.h:140
bool isProtected
Definition: ADCCC26XX.h:156
Power manager interface for CC26XX/CC13XX.
struct ADCCC26XX_Object ADCCC26XX_Object
ADCCC26XX Object.
ADCCC26XX_Sampling_Duration
Amount of time the ADC spends sampling the analogue input.
Definition: ADCCC26XX.h:77
const ADC_FxnTable ADCCC26XX_fxnTable
ADCCC26XX_Trigger_Source
List of sources the ADC can be configured to trigger off of.
Definition: ADCCC26XX.h:124
Definition: ADCCC26XX.h:89
Device-specific pin & GPIO driver for CC26xx family [def].
Definition: ADCCC26XX.h:84
Definition: ADCCC26XX.h:87
Definition: ADCCC26XX.h:88
The definition of a ADC function table that contains the required set of functions to control a speci...
Definition: ADC.h:273
uint8_t adcCompBInput
Definition: ADCCC26XX.h:139
Definition: ADCCC26XX.h:79
underlying data structure for type PIN_State
Definition: PIN.h:680
uint8_t adcDIO
Definition: ADCCC26XX.h:138
bool isOpen
Definition: ADCCC26XX.h:155
ADCCC26XX Hardware attributes These fields are used by driverlib APIs and therefore must be populated...
Definition: ADCCC26XX.h:137
Definition: ADCCC26XX.h:82
Definition: ADCCC26XX.h:78
struct ADCCC26XX_HWAttrs ADCCC26XX_HWAttrs
ADCCC26XX Hardware attributes These fields are used by driverlib APIs and therefore must be populated...
PIN_Handle pinHandle
Definition: ADCCC26XX.h:154
PIN_State pinState
Definition: ADCCC26XX.h:153
Definition: ADCCC26XX.h:85
Definition: ADCCC26XX.h:80
bool inputScalingEnabled
Definition: ADCCC26XX.h:141
ADCCC26XX_Sampling_Duration samplingDuration
Definition: ADCCC26XX.h:143
Definition: ADCCC26XX.h:125
Definition: ADCCC26XX.h:81
Generic PIN & GPIO driver.
Definition: ADCCC26XX.h:86
ADCCC26XX_Reference_Source
Specifies whether the internal reference of the ADC is sourced from the battery voltage or a fixed in...
Definition: ADCCC26XX.h:113
Definition: ADCCC26XX.h:115