Z-Stack 3.2.0 to Z-Stack 3.3.0¶
This section will describe a way to migrate a project from Z-Stack 3.2.0 to a Z-Stack 3.3.0 project.
For this guide, samplelight from Z-Stack 3.2.0 will be ported over to Z-Stack 3.3.0. The two releases have major differences mostly pertaining to:
Bug fixes listed in the Zigbee Release Notes
Merging of the CC13X2 and CC26X2 SDKs
ICall deprecation and replacement with OSALPort
Re-organization of the directory structure
The recommended approach is to start with a Z-Stack 3.3.0 project that contains the same base application as the porting target project and merge any custom functionality
Choose a Z-Stack 3.3.0 example project that contains your target project’s base functionality. For reference and use in this example, zc_light from C:\ti\simplelink_cc13xx_cc26xx_sdk_x_xx_xx_xx\examples\rtos\CC13xx or CC26xx_LAUNCHXL\zstack is chosen as a starting point.
No changes are required for the Z-Stack 3.3.0
zcl_samplelight_data.corzcl_samplelight.hfiles unless clusters, attributes, or simple descriptors were added or altered in the Z-Stack 3.2.0 project. However, please note thatZCL_CLUSTER_ID_GEN_BASICandZCL_CLUSTER_ID_GEN_SCENESattribute records have been added whereasZCL_CLUSTER_ID_HA_DIAGNOSTIChas been removed. Some global functions for attribute updates which can be accessed by the application have also been added.
The following items specifically concern zcl_samplelight.c:
All ICall local variables have been replaced with
// Semaphore used to post events to the application thread static Semaphore_Handle appSemHandle; static Semaphore_Struct appSem; /* App service ID used for messaging with stack service task */ static uint8_t appServiceTaskId; /* App service task events, set by the stack service task when sending a message */ static uint32_t appServiceTaskEvents;
The following have been redefined:
appServiceTaskIDreplaceszclSampleLight_EntityappServiceTaskEventsreplaceseventsappSemHandlereplacessem
Local functions have been added and will be discussed by the points below.
static void zclSampleLight_RemoveAppNvmData(void); static uint8 zclSampleLight_SceneStoreCB(zclSceneReq_t *pReq); static void zclSampleLight_SceneRecallCB(zclSceneReq_t *pReq); ZStatus_t zclSampleLight_ReadWriteAttrCB( uint16 clusterId, uint16 attrId, uint8 oper, uint8 *pValue, uint16 *pLen );
#. zclSampleLight_task is replaced with the generic sampleApp_task. Changes to
main.c of the Application → Startup folder must also be applied.
ICall_registerApp(&zclSampleLight_Entity, &sem);has been removed fromzclSampleLight_initialization(void)and the following OSALPort registration code is now included:Semaphore_Params semParam; Semaphore_Params_init(&semParam); semParam.mode = ti_sysbios_knl_Semaphore_Mode_BINARY; Semaphore_construct(&appSem, 0, &semParam); appSemHandle = Semaphore_handle(&appSem); appServiceTaskId = OsalPort_registerTask(Task_self(), appSemHandle, &appServiceTaskEvents);
zclSampleLight_RemoveAppNvmData();is added to theif(key == KEY_RIGHT)statement ofstatic void zclSampleLight_initialization(void)and is declared as follows:/********************************************************************* * @fn zclSampleLight_RemoveAppNvmData * * @brief Callback when Application performs reset to Factory New Reset. * Application must restore the application to default values * * @param none * * @return none */ static void zclSampleLight_RemoveAppNvmData(void) { #ifdef ZCL_GROUPS uint8 numGroups; uint16 groupList[APS_MAX_GROUPS]; uint8 i; if ( numGroups = aps_FindAllGroupsForEndpoint( SAMPLELIGHT_ENDPOINT, groupList ) ) { for ( i = 0; i < numGroups; i++ ) { #if defined ( ZCL_SCENES ) zclGeneral_RemoveAllScenes( SAMPLELIGHT_ENDPOINT, groupList[i] ); #endif } aps_RemoveAllGroup( SAMPLELIGHT_ENDPOINT ); } #endif }
zclSampleLight_process_loopnow uses OSALPort instead of ICall to receive messages.static void zclSampleLight_process_loop(void) { /* Forever loop */ for(;;) { zstackmsg_genericReq_t *pMsg = NULL; /* Wait for response message */ if(Semaphore_pend(appSemHandle, BIOS_WAIT_FOREVER )) { /* Retrieve the response message */ if((pMsg = (zstackmsg_genericReq_t*) OsalPort_msgReceive( appServiceTaskId )) != NULL) { zclSampleLight_processZStackMsgs(pMsg); #ifdef PER_TEST per_interface_processZStackMsg(pMsg); #endif if(pMsg != NULL) { OsalPort_msgDeallocate((uint8_t*)pMsg); } }
Global variables for cluster attributes, like
zclSampleLight_OnOffand `` zclSampleLight_LevelCurrentLevel`` have been replaced with attribute functions as reflected inzcl_samplelight_data.candzcl_samplelight.h.Scene and attribute callbacks have been added:
/****************************************************************************** * * Functions for processing ZCL Foundation incoming Command/Response messages * *****************************************************************************/ /********************************************************************* * @fn zclSampleLight_SceneRecallCB * * @brief Callback from the ZCL Scenes Cluster Library * to recall a set of attributes from a stored scene. * * @param none * * @return none */ static void zclSampleLight_SceneRecallCB( zclSceneReq_t *pReq ) { zclGeneral_Scene_extField_t extField; uint8 *pBuf; uint8 extLen = 0; pBuf = pReq->scene->extField; extField.AttrLen = pBuf[2]; while(extLen < ZCL_GEN_SCENE_EXT_LEN) { //Parse ExtField extField.ClusterID = BUILD_UINT16(pBuf[0],pBuf[1]); extField.AttrLen = pBuf[2]; extField.AttrBuf = &pBuf[3]; if(extField.AttrLen == 0xFF || extField.ClusterID == 0xFFFF) { break; } //If On/Off then retrieve the attribute if(extField.ClusterID == ZCL_CLUSTER_ID_GEN_ON_OFF) { uint8 tempState = *extField.AttrBuf; zclSampleLight_updateOnOffAttribute(tempState); } //If Level Control then retrieve the attribute else if(extField.ClusterID == ZCL_CLUSTER_ID_GEN_LEVEL_CONTROL) { uint8 tempState = *extField.AttrBuf; zclSampleLight_updateCurrentLevelAttribute(tempState); } //Move to the next extension field (increase pointer by clusterId, Attribute len field, and attribute) pBuf += sizeof(uint16) + sizeof(uint8) + extField.AttrLen; extLen += sizeof(uint16) + sizeof(uint8) + extField.AttrLen; //increase ExtField } //Update scene attributes zclSampleLight_ScenesValid = TRUE; zclSampleLight_ScenesCurrentGroup = pReq->scene->groupID; zclSampleLight_ScenesCurrentScene = pReq->scene->ID; zclSampleLight_UpdateLedState(); } /********************************************************************* * @fn zclSampleLight_SceneStoreCB * * @brief Callback from the ZCL Scenes Cluster Library * to store a set of attributes to a specific scene. * * @param none * * @return none */ static uint8 zclSampleLight_SceneStoreCB( zclSceneReq_t *pReq ) { zclGeneral_Scene_extField_t extField; uint8 *pBuf; uint8 extLen = 0; uint8 sceneChanged = FALSE; pBuf = pReq->scene->extField; extField.AttrLen = pBuf[2]; while(extLen < ZCL_GEN_SCENE_EXT_LEN) { //Parse ExtField extField.ClusterID = BUILD_UINT16(pBuf[0],pBuf[1]); extField.AttrLen = pBuf[2]; extField.AttrBuf = &pBuf[3]; if(extField.AttrLen == 0xFF || extField.ClusterID == 0xFFFF) { break; } //If On/Off then store attribute if(extField.ClusterID == ZCL_CLUSTER_ID_GEN_ON_OFF) { uint8 tempState = zclSampleLight_getOnOffAttribute(); if(*extField.AttrBuf != tempState ) { sceneChanged = TRUE; } *extField.AttrBuf = tempState; } //If Level Control then store attribute else if(extField.ClusterID == ZCL_CLUSTER_ID_GEN_LEVEL_CONTROL) { uint8 tempState = zclSampleLight_getCurrentLevelAttribute(); if(*extField.AttrBuf != tempState ) { sceneChanged = TRUE; } *extField.AttrBuf = tempState; } //Move to the next extension field (increase pointer by clusterId, Attribute len field, and attribute) pBuf += sizeof(uint16) + sizeof(uint8) + extField.AttrLen; extLen += sizeof(uint16) + sizeof(uint8) + extField.AttrLen; //increase ExtField } //Update scene attributes zclSampleLight_ScenesValid = TRUE; zclSampleLight_ScenesCurrentGroup = pReq->scene->groupID; zclSampleLight_ScenesCurrentScene = pReq->scene->ID; return sceneChanged; } /********************************************************************* * @fn zclSampleLight_ReadWriteAttrCB * * @brief Handle ATTRID_SCENES_COUNT, ATTRID_ON_OFF and ATTRID_LEVEL_CURRENT_LEVEL. * Only to be called if any of the attributes change. * * @param clusterId - cluster that attribute belongs to * @param attrId - attribute to be read or written * @param oper - ZCL_OPER_LEN, ZCL_OPER_READ, or ZCL_OPER_WRITE * @param pValue - pointer to attribute value, OTA endian * @param pLen - length of attribute value read, native endian * * @return status */ ZStatus_t zclSampleLight_ReadWriteAttrCB( uint16 clusterId, uint16 attrId, uint8 oper, uint8 *pValue, uint16 *pLen ) { if(clusterId == ZCL_CLUSTER_ID_GEN_SCENES) { if(attrId == ATTRID_SCENES_COUNT) { return zclGeneral_ReadSceneCountCB(clusterId,attrId,oper,pValue,pLen); } } return ZSuccess; }
zclSampleLight_SceneStoreCBandzclSampleLight_SceneRecallCBare added to thezclSampleLight_CmdCallbackstable.gp_[Get/Set]CommissioningModeis renamedgp_[Get/Set]SinkCommissioningMode, changes are only required ifENABLE_GREENPOWER_COMBO_BASICis defined.Add any other Z-Stack 3.2.0 application changes to the Z-Stack 3.3.0 file if not pertaining to the items listed above.
Note
Difference comparison software is recommended for discerning all differences between software stacks.