SimpleLink™ CC13xx CC26xx SDK 8.33.00.16 Release Notes

Table of Contents

Introduction

The SimpleLink™ Low Power F2 Software Development Kit (SDK), formerly known as the CC13xx and CC26xx SDK, delivers components that enable engineers to develop applications on the Texas Instruments SimpleLink CC13xx and CC26xx family of wireless microcontrollers (MCUs). This software toolkit provides a cohesive and consistent software experience for all SimpleLink CC13xx and CC26xx wireless MCU users by packaging essential software components, such as a Bluetooth® Low Energy (LE) protocol stack supporting Bluetooth 5.2, Zigbee 3.0 compliant protocol suite, RF-Proprietary examples, TI 15.4 Stack, TI Wi-SUN FAN Stack, Amazon Sidewalk examples, as well as the TI-RTOS7 and FreeRTOS kernels and TI Drivers in one easy-to-use software package along with example applications and documentation. In addition, the Dynamic Multi-Protocol Manager (DMM) software component enables multiprotocol development on a single SimpleLink wireless MCU.

Although not included in the SDK, SimpleLink CC13xx and CC26xx wireless MCUs are also capable of supporting the following wireless solutions: Please refer to their respective repositories for resources and more information.

The SimpleLink MCU portfolio offers a single development environment that delivers flexible hardware, software, and tool options for customers developing wired and wireless applications. With 100 percent code reuse across host MCUs, Wi-Fi™, Bluetooth Low Energy, Sub-1GHz devices and more, choose the MCU or connectivity standard that fits your design. A one-time investment with the SimpleLink software development kit allows you to reuse often, opening the door to create unlimited applications. For more information, visit www.ti.com/simplelink.

This is version 8.33.00.16 of the SimpleLink Low Power F2 SDK. This SDK is also available on GitHub at https://github.com/TexasInstruments/simplelink-lowpower-f2-sdk

Documentation

What’s New

This version only contains updates for TI Wi-SUN Stack. Other components remain the same as in SIMPLELINK-LOWPOWER-F2-SDK version 8.31.00.11.

Refer to the Document Overview for the individual release notes and details for starting development with each SDK component.

Refer to the included Change Log for a summary of new features and fixed issues since the last SDK release.

If you want to download or install a subset of the SimpleLink F2 SDK components, please use SDK composer on TI Resource Explorer. This feature lets you select only the SDK components you need and save up to 1.1 GB on the installation size.

Upcoming Features

We are thrilled to announce the release of Code Composer Studio v20, the culmination of years of dedication and hard work from our team! This release represents a significant milestone in our journey to provide best-in-class IDEs for our customers. CCS is now based on the Theia framework, which allows us to provide a ‘VS Code’ like experience for both desktop and cloud – a first in the embedded industry! CCSv20 supersedes the CCSv12.8 release stream for all supported TI Devices. No further releases of the Eclipse based product are planned, see the Transition Roadmap for more details.

CCSv20 downloads can be accessed from the ti.com tools folder: https://www.ti.com/tool/download/CCSTUDIO

Documentation and Video collateral to support the release can be found here:

We recommend customers who are starting new development programs to leverage CCS Theia from the start, and existing users of CCS Eclipse to take the time to transition to CCS Theia, see Migration Guide for help migrating from CCS Eclipse IDE to CCS Theia IDE.

Please note the following features are not yet supported in CCS Theia:

Upgrade and Compatibility Information

Operating System Support

Dependencies

SimpleLink Low Power F2 SDK 8.33.00.16 was built & tested on a Windows host platform using the following Integrated Development Environments (IDEs) and components. Using an IDE or toolchain version not listed below may result in compatibility issues with this SDK release. Refer to the individual component release notes in the Document Overview for each component’s supported code generation tools.

Device Support

This SDK supports the following SimpleLink CC13xx and CC26xx wireless MCUs:

Sub-1GHz Devices 2.4GHz Devices Dual Band Devices
CC1311P3 CC2642R CC1352P
CC1311R3 CC2642R-Q1 CC1352P7
CC1312R CC2651P3 CC1352R
CC1312R7 CC2651R3 CC1354P10
CC1312PSIP CC2652P CC1354R10
CC1314R10 CC2652P7
CC2652R
CC2652RB
CC2652R7
CC2652RSIP
CC2652PSIP
CC2651RS3IPA
CC2674R10
CC2674P10

Development Board Support

The following table lists the supported development boards for each device supported in this SDK. Note: LaunchPad™ Development kits are not available for all device variants. As such, alternative options for development are presented in this table.

A Modular LaunchPad™ must be used together with the Modular LaunchPad™ Emulator (an LP-XDS110 or LP-XDS110ET).

SimpleLink Device TI tool page Dev.ti.com
Sub-1GHz Devices
CC1311P3 LP-CC1311P3 CC1311P3 LaunchPad™ quick start guide
CC1311R3 Use LP-CC1311P3 CC1311P3 LaunchPad™ quick start guide
CC1312R CC1312R LaunchPad™ CC1312R LaunchPad™ quick start guide
CC1312R7 LP-CC1312R7 CC1312R7 LaunchPad™ quick start guide
CC1312PSIP LP-EM-CC1312PSIP CC1312PSIP Modular LaunchPad™ quick start guide
CC1314R10 LP-EM-CC1314R10 CC1314R10 Modular LaunchPad™ quick start guide
2.4GHz Devices
CC2642R CC26X2R LaunchPad™ CC26X2R LaunchPad™ quick start guide
CC2642R-Q1 CC26X2R LaunchPad™ CC26X2R LaunchPad™ quick start guide
CC2651P3 LP-CC2651P3 CC2651P3 LaunchPad™ quick start guide
CC2651R3 Use LP-CC2651P3 CC2651P3 LaunchPad™ quick start guide
CC2652P Use CC1352P LaunchPad™ CC1352P1 LaunchPad™ quick start guide or
CC1352P2 LaunchPad™ quick start guide or
CC1352P4 LaunchPad™ quick start guide
CC2652P7 Use LP-CC1352P7-1 or
LP-CC1352P7-4
CC1352P71 LaunchPad™ quick start guide or
CC1352P74 LaunchPad™ quick start guide
CC2652R CC26X2R LaunchPad™ CC26X2R LaunchPad™ quick start guide
CC2652RB CC2652RB LaunchPad™ CC2652RB LaunchPad™ quick start guide
CC2652R7 LP-CC2652R7 CC2652R7 LaunchPad™ quick start guide
CC2652RSIP LP-CC2652RSIP CC2652RSIP LaunchPad™ quick start guide
CC2652PSIP LP-CC2652PSIP CC2652PSIP LaunchPad™ quick start guide
CC2651R3SIPA LP-CC2651R3SIPA CC2651R3SIPA LaunchPad™ quick start guide
CC2674R10 Use LP-EM-CC1354P10 CC1354P10 Modular LaunchPad™ quick start guide
CC2674P10 Use LP-EM-CC1354P10 CC1354P10 Modular LaunchPad™ quick start guide
Dual Band Devices
CC1352P CC1352P LaunchPad™ CC1352P1 LaunchPad™ quick start guide or
CC1352P2 LaunchPad™ quick start guide or
CC1352P4 LaunchPad™ quick start guide
CC1352P7 LP-CC1352P7-1 or
LP-CC1352P7-4
CC1352P71 LaunchPad™ quick start guide or
CC1352P74 LaunchPad™ quick start guide
CC1352R CC1352R LaunchPad™ or
LPSTK-CC1352R
CC1352R LaunchPad™ quick start guide or
CC1352R LaunchPad™ SensorTag kit quick start guide
CC1354P10 LP-EM-CC1354P10 CC1354P10 Modular LaunchPad™ quick start guide

Known Issues

Versioning

This product follows a version format, M.mm.pp.bb, where:

Technical Support and Product Updates