Changelog
Table of Contents
New Features
BLE5-Stack
| ID | Summary |
|---|---|
| BLE_AGAMA-4952 | [SDAA] Expose Reduced Configuration Option to Sysconfig |
| BLE_AGAMA-4926 | [EXAMPLE] Add Examples Support for CC2674-P10 |
Proprietary RF
| ID | Summary |
|---|---|
| PROPRF-1310 | Add support for LP_CC2674P10 |
TI 15.4-Stack
| ID | Summary |
|---|---|
| TI154STACK-4483 | TI 15.4-Stack FH low power broadcast mode |
TI Wi-SUN FAN
| ID | Summary |
|---|---|
| WISUN-1211 | Wi-SUN CSMP agent support on CC13x2 and CC13x4 devices |
| WISUN-1210 | [SPS] Performance Benchmarking for TCP |
| WISUN-1208 | [SPS] MQTT Example - Embedded |
| WISUN-1207 | [SPS] MQTT Example - Linux Host |
| WISUN-1206 | [SPS] Button Press Demo (TCP) |
| WISUN-1205 | [SPS] TCP Socket Core Implementation |
TI Wireless Solar Management System
| ID | Summary |
|---|---|
| None | None |
TI Z-Stack
| ID | Summary |
|---|---|
| ZIGBEE-2101 | Add support for LP_CC2674P10 |
DMM
| ID | Summary |
|---|---|
| DMM-1423 | Add support for LP_EM_CC2674P10 for DMM examples |
| DMM-1416 | Add ability to close registered DMM Client |
SimpleLink Common Components Module (SCCM)
| ID | Summary |
|---|---|
| SCCM-422 | Generate MCUboot examples for CC2674x10 |
| SCCM-410 | Enable image encryption using ECIES for MCUboot |
| SCCM-409 | MCUBoot update from 1.8 to 2.0 |
| SCCM-225 | Add SysConfig Support to MCUboot Examples |
TI-RTOS and Drivers
| ID | Summary |
|---|---|
| TIPOSIX-30 | Return error when POSIX timer overflows FreeRTOS ticks |
| TIDRIVERS-6562 | Update GCC version to 12.3 |
| TIDRIVERS-6509 | Hide GPIO Configurations in SysConfig module if marked as do not configure. |
| TIDRIVERS-6464 | Add board support for LP_EM_CC2674P10 |
| TIDRIVERS-6342 | Add support for 64-bit getSystemTicks API |
Radio Software Bundle (RFLib)
| ID | Summary |
|---|---|
| RFCORE-1044 | CC1354P: PA Table Update - 10 dBm: Improved Performance |
| RFCORE-1040 | CC2674R10: PA Table Update - 5 dBm: Characterized |
| RFCORE-1039 | CC1354P: PA Table Update - 5 dBm: Improved Performance |
| RFCORE-1037 | CC1354R10: PA Table Update - 5 dBm: Improved Performance |
| RFCORE-1041 | CC2674P10: PA Table Update - 10 dBm: Characterized |
| RFCORE-1043 | CC1354P: PA Table Update - 20 dBm: Improved Performance |
| RFCORE-1042 | CC2674P10: PA Table Update - 20 dBm: Characterized |
Fixed Issues
BLE5-Stack
| ID | Summary |
|---|---|
| BLE_AGAMA-4943 | Peripheral not checking RPA in CONN_IND packet from Central |
| BLE_AGAMA-4927 | MR stop responding when connecting multiple bonded devices at once |
| BLE_AGAMA-4907 | When Scanning is set to high priority and Advertisement is off, there will be only scan operation, no connection event will be maintained. |
| BLE_AGAMA-4902 | [SWAT][BBR] Basic Broadcaster Fail To Advertise in TIRTOS |
| BLE_AGAMA-4884 | After connecting/disconnecting multiple times, CC26xx will send pin/key missing at the last step of the encryption procedure |
| BLE_AGAMA-4810 | Connection param and channel map update call backs are coming earlier than the actual instant where the change is reflected in the connection causing CM instability |
| BLE_AGAMA-3427 | System goes to halAssertHandlerExt when more than LL_MAX_NUM_CTRL_PROC_PKTS are queued |
Proprietary RF
| ID | Summary |
|---|---|
| PROPRF-1310 | Add support for LP_CC2674P10 |
TI 15.4-Stack
| ID | Summary |
|---|---|
| TI154STACK-4491 | CUI_DISABLE does not exclude all status line prints in the sensor_oad_onchip_secure example |
| TI154STACK-4490 | Joining devices crash when no nearby networks have permit join enabled |
| TI154STACK-4487 | Typo in SBL Binary File Generation section of example readme |
| TI154STACK-4485 | Sysconfig does not support migration from CC1311R3 RGZ to RKP package TI15.4 |
| TI154STACK-4484 | There is a memory leak when App sends large packet (more than limited size) or MAC is in bad state |
| TI154STACK-4482 | Zero Data Frame not sent out even though FP bit is set |
| TI154STACK-4480 | aborting RX command even when no RX command has been scheduled after a reset - race condition |
| TI154STACK-4477 | 15.4 MAC must clear source matching table entries during MAC_RESET |
| TI154STACK-4476 | Low temp causes radio to fail |
| TI154STACK-4472 | When receiving a broadcast message every 1 s the sleepy sensor is sometimes staying in RX for a full broadcast interval instead of going to sleep after receiving the broadcast message |
TI Wi-SUN FAN
| ID | Summary |
|---|---|
| WISUN-1213 | Wi-SUN Router Node running with RCP Host has Memory leaks |
TI Wireless Solar Management System
| ID | Summary |
|---|---|
| None | None |
TI Z-Stack
| ID | Summary |
|---|---|
| ZIGBEE-2089 | Fix migration path for CC1354x10RGZ device |
DMM
| ID | Summary |
|---|---|
| None | None |
SimpleLink Common Components Module (SCCM)
| ID | Summary |
|---|---|
| SCCM-403 | [nvocmp.c] Compilation warnings due to unused variables |
| SCCM-402 | [BIM] Bootloader fails when using optimization -O0 with TIClang |
TI-RTOS and Drivers
| ID | Summary |
|---|---|
| TIDRIVERS-6757 | UART2 Driver Race Condition on Blocking or Callback Mode Write |
| TIDRIVERS-6741 | CAN examples dereference NULL pointer if UART2_open fails. |
| TIDRIVERS-6735 | UART2_EVENT_TX_BEGIN called several times in one transmit |
| TIDRIVERS-6709 | CAN driver does not provide userArg to event callback |
| TIDRIVERS-6708 | Fix a race condition in SPI DMA (start a new transfer right before the end of the existing transfer) |
| SYSBIOS-1613 | Hwi_construct2 returns ‘0’ as hwi handle for GCC compiler |
| FREERTOS-37 | Lowest interrupt priority is miscalculated |
Radio Software Bundle (RFLib)
| ID | Summary |
|---|---|
| RFCORE-1036 | cc13x4_cc26x4: Non-reentrant code in Coex patch causes IEEE CSMA command to stall indefinitely |
Known Issues
BLE5-Stack
| ID | Summary |
|---|---|
| BLE_AGAMA-4995 | [Build][Debug][IAR]-Error For Persistent_app App In CC26X2PSIP Platform: Error[Lp015]: section placement failure: overcommitted content in [0x3'80d0-0x5'5fff] |
| BLE_AGAMA-4936 | When there are two ADV with different RPAs generating from the same IRK, CC2642 can hardly scan the ADVs |
| BLE_AGAMA-4855 | [Multi Connect] CC2651P3 Central fails to connect to more than 5 testers with privacy enable |
| BLE_AGAMA-4846 | [Data Stream][Display] display_printf() is fail when try to print data larger then threshold of 300-500 bytes |
| BLE_AGAMA-4837 | [IOP][Android 14][One Plus 11] With privacy enabled, reconnection fails after after Pairing & Bonding |
| BLE_AGAMA-4830 | [SWAT] Scanner failes after receiving an incorrect event type |
| BLE_AGAMA-4484 | multi_role FreeRTOS support removed from CC13XX / CC26XX |
| BLE_AGAMA-4354 | Under some conditions, CREATE_SYNC or AOA_ENABLE are not sent by RTLS Manager |
| BLE_AGAMA-4324 | [Build] -Path Too Long-Error[Ms003] In simple_peripheral_oad_offchip_src_iar |
| BLE_AGAMA-4029 | Updating BLE Scan Response Data Prevents BLE ADV from being sent when using >1 Advertisement set. |
| BLE_AGAMA-4009 | [RTLS] - RTLS tests with multiple responders stopped after several start/stop AOA commands |
| BLE_AGAMA-3896 | [RTLS] In robustness test with multiple responders, Passive sometimes does not respond to AOA start or stop commands |
| BLE_AGAMA-3774 | Under certain conditions the CC2652R1 failed to synchronize to periodic advertising |
| BLE_AGAMA-3752 | [CC2651] Host_test memory limitation using CCS+TI-CLANG |
| BLE_AGAMA-3540 | [RTLS Agent] RTLS Agent sometimes shows exception when there are huge amount of data to be processed in the PC |
| BLE_AGAMA-3486 | Device asserts upon connection when HeapMem and HeapTrack is used |
| BLE_AGAMA-3381 | Simple Peripheral example application spinlocks while pairing, when compiled with IAR in Debug configuration |
| BLE_AGAMA-3107 | [CLAOA] parsing errors when trying to parse CL_AOA_RESULT_RAW events when using periodic interval smaller than 300ms |
| BLE_AGAMA-3077 | [RTLS] CTE reception on the 2M PHY do not meet spec requirements |
| BLE_AGAMA-3076 | [RTLS] CTEs sent on the 2M PHY do not meet spec requirements |
| BLE_AGAMA-2266 | Central not able to find peer device advertising Extended ADV with aux offset bigger than 16.3ms |
| BLE_AGAMA-2033 | [RTLS] Passive Application is not functioning well in Debug configuration. WA: Change the optimization in Debug configuration to High (as in Release) |
| BLE_AGAMA-1675 | IOP: Device fails to pair with Meizu Pro 7 |
| BLE_AGAMA-139 | When using multi-role, the random address will display in the serial terminal, instead of the “Work With” selection |
| BLE_AGAMA-80 | The NVS Driver is now used for bond storage. It is not possible to retain OSAL_SNV contents when upgrading from earlier BLE5 1.1.x releases. |
Proprietary RF
| ID | Summary |
|---|---|
| None | None |
TI 15.4-Stack
| ID | Summary |
|---|---|
| None | None |
TI Wi-SUN FAN
| ID | Summary |
|---|---|
| WISUN-1222 | ns_node example IAR compilation fails for LP_EM_CC1312PSIP |
| WISUN-1196 | RCP UDP/TCP iperf throughput performance is slower than expected |
TI Wireless Solar Management System
| ID | Summary |
|---|---|
| None | None |
TI Z-Stack
| ID | Summary |
|---|---|
| None | None |
DMM
| ID | Summary |
|---|---|
| None | None |
SimpleLink Common Components Module (SCCM)
| ID | Summary |
|---|---|
| None | None |
TI-RTOS and Drivers
| ID | Summary |
|---|---|
| TIDRIVERS-7244 | Changing the muxing on an IO can cause glitches under some conditions |
| TIDRIVERS-6863 | JSON library unstable for gcc 12.3 |
| TIDRIVERS-6211 | Adding 3rd SPI instance in GCC project fails but works with TI Clang |
| TIDRIVERS-4127 | ADCBuf causes jitter when switching clock sources |
| SYSBIOS-642 | Seconds_getTime() for MSP432P always returns ‘0’ in nanoseconds field |
| SYSBIOS-446 | Reported CPU load is not 100% when a task is in “while 1 {}” loop |
| SYSBIOS-98 | Load module won't work correctly if the TI-RTOS Power module is enabled for CC3200 or MSP432 |
Radio Software Bundle (RFLib)
| ID | Summary |
|---|---|
| RFDRIVER-862 | RF_ratDispatchTime() doesn't check if RF_currClient is null before derefencing it, causing a fault |